aboutsummaryrefslogblamecommitdiffstats
blob: b05fda13a1d1581df84aeaac499e5c3ababb44c3 (plain) (tree)































                                                                           

                                      
 
                                                          




                                                                          
                                                                      






                                                                           

                                       
                                     
                              

 
                                                
                             
                                          
                                 



                                          



                                                                   
                                                                                

                          

                             








                                                                     
 
                                                                    

                                                               
                               
               








                                                    
                                                          



                                                               
                                                                  




                                       
                                                                                                  





                                                                    
                                                    







                                                                         
                                                         




                                                                                         

     

                              
 
                  
 
/*
 * Copyright (C) 2012 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include <unistd.h>
#include <dirent.h>
#include <errno.h>
#include <stdlib.h>
#include <string.h>
#include <sys/types.h>
#include <sys/wait.h>
#include <sys/stat.h>
#include <signal.h>
#include <fcntl.h>

#include "ui.h"
#include "cutils/properties.h"
#include "install.h"
#include "common.h"
#include "adb_install.h"
#include "minadbd/fuse_adb_provider.h"
#include "fuse_sideload.h"

static void set_usb_driver(RecoveryUI* ui, bool enabled) {
    int fd = open("/sys/class/android_usb/android0/enable", O_WRONLY);
    if (fd < 0) {
        ui->Print("failed to open driver control: %s\n", strerror(errno));
        return;
    }
    if (TEMP_FAILURE_RETRY(write(fd, enabled ? "1" : "0", 1)) == -1) {
        ui->Print("failed to set driver control: %s\n", strerror(errno));
    }
    if (close(fd) < 0) {
        ui->Print("failed to close driver control: %s\n", strerror(errno));
    }
}

static void stop_adbd(RecoveryUI* ui) {
    ui->Print("Stopping adbd...\n");
    property_set("ctl.stop", "adbd");
    set_usb_driver(ui, false);
}

static void maybe_restart_adbd(RecoveryUI* ui) {
    if (is_ro_debuggable()) {
        ui->Print("Restarting adbd...\n");
        set_usb_driver(ui, true);
        property_set("ctl.start", "adbd");
    }
}

// How long (in seconds) we wait for the host to start sending us a
// package, before timing out.
#define ADB_INSTALL_TIMEOUT 300

int apply_from_adb(RecoveryUI* ui, bool* wipe_cache, const char* install_file) {
    modified_flash = true;

    stop_adbd(ui);
    set_usb_driver(ui, true);

    ui->Print("\n\nNow send the package you want to apply\n"
              "to the device with \"adb sideload <filename>\"...\n");

    pid_t child;
    if ((child = fork()) == 0) {
        execl("/sbin/recovery", "recovery", "--adbd", NULL);
        _exit(-1);
    }

    // FUSE_SIDELOAD_HOST_PATHNAME will start to exist once the host
    // connects and starts serving a package.  Poll for its
    // appearance.  (Note that inotify doesn't work with FUSE.)
    int result = INSTALL_ERROR;
    int status;
    bool waited = false;
    struct stat st;
    for (int i = 0; i < ADB_INSTALL_TIMEOUT; ++i) {
        if (waitpid(child, &status, WNOHANG) != 0) {
            result = INSTALL_ERROR;
            waited = true;
            break;
        }

        if (stat(FUSE_SIDELOAD_HOST_PATHNAME, &st) != 0) {
            if (errno == ENOENT && i < ADB_INSTALL_TIMEOUT-1) {
                sleep(1);
                continue;
            } else {
                ui->Print("\nTimed out waiting for package.\n\n");
                result = INSTALL_ERROR;
                kill(child, SIGKILL);
                break;
            }
        }
        result = install_package(FUSE_SIDELOAD_HOST_PATHNAME, wipe_cache, install_file, false, 0);
        break;
    }

    if (!waited) {
        // Calling stat() on this magic filename signals the minadbd
        // subprocess to shut down.
        stat(FUSE_SIDELOAD_HOST_EXIT_PATHNAME, &st);

        // TODO(dougz): there should be a way to cancel waiting for a
        // package (by pushing some button combo on the device).  For now
        // you just have to 'adb sideload' a file that's not a valid
        // package, like "/dev/null".
        waitpid(child, &status, 0);
    }

    if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) {
        if (WEXITSTATUS(status) == 3) {
            ui->Print("\nYou need adb 1.0.32 or newer to sideload\nto this device.\n\n");
        } else if (!WIFSIGNALED(status)) {
            ui->Print("\n(adbd status %d)\n", WEXITSTATUS(status));
        }
    }

    set_usb_driver(ui, false);
    maybe_restart_adbd(ui);

    return result;
}