aboutsummaryrefslogblamecommitdiffstats
blob: fdcbfe84485148307a158709148893acf46e71e0 (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16















                                                                           

                  

                  



                      
                     

                   



                    
                                 

                                      
                                   
                    
                            
                   
 
                   
                   
 
                                     
 
                                       
 





                                                 
 






                                                                  
 






                                                                                            
 
 
                                           
                                                       

 

                                                                       








                                                             
 



                                                   
 


                                 
 




                                                                            
 














                                                                                        
 


                                                       
     

             
 

                                                                               

 
                                           

                                               

 
                                             








                                                             
 



                                                   
 




                                                                         
 
                                    

 



















                                                                                        

 
















                                                            
                                                              





























                                                                                                    
     











                                                                          
     



                                                                                         
     
   
 



















                                                                                                    
     
 











                                                 

     















                                                                                         
              

           
 
 
                                       
                                        

 
                            





                                                                 
 



                                             
 

                                                                                       
                                                           



                                                       
                                                             

                  
     

           
 
/*
 * Copyright (C) 2007 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "roots.h"

#include <ctype.h>
#include <fcntl.h>
#include <stdlib.h>
#include <sys/mount.h>
#include <sys/stat.h>
#include <sys/types.h>
#include <sys/wait.h>
#include <unistd.h>

#include <algorithm>
#include <string>
#include <vector>

#include <android-base/logging.h>
#include <android-base/properties.h>
#include <android-base/stringprintf.h>
#include <android-base/unique_fd.h>
#include <cryptfs.h>
#include <ext4_utils/wipe.h>
#include <fs_mgr.h>

#include "common.h"
#include "mounts.h"

static struct fstab* fstab = nullptr;

extern struct selabel_handle* sehandle;

void load_volume_table() {
  fstab = fs_mgr_read_fstab_default();
  if (!fstab) {
    LOG(ERROR) << "Failed to read default fstab";
    return;
  }

  int ret = fs_mgr_add_entry(fstab, "/tmp", "ramdisk", "ramdisk");
  if (ret == -1) {
    LOG(ERROR) << "Failed to add /tmp entry to fstab";
    fs_mgr_free_fstab(fstab);
    fstab = nullptr;
    return;
  }

  printf("recovery filesystem table\n");
  printf("=========================\n");
  for (int i = 0; i < fstab->num_entries; ++i) {
    const Volume* v = &fstab->recs[i];
    printf("  %d %s %s %s %lld\n", i, v->mount_point, v->fs_type, v->blk_device, v->length);
  }
  printf("\n");
}

Volume* volume_for_path(const char* path) {
  return fs_mgr_get_entry_for_mount_point(fstab, path);
}

// Mount the volume specified by path at the given mount_point.
int ensure_path_mounted_at(const char* path, const char* mount_point) {
  Volume* v = volume_for_path(path);
  if (v == nullptr) {
    LOG(ERROR) << "unknown volume for path [" << path << "]";
    return -1;
  }
  if (strcmp(v->fs_type, "ramdisk") == 0) {
    // The ramdisk is always mounted.
    return 0;
  }

  if (!scan_mounted_volumes()) {
    LOG(ERROR) << "Failed to scan mounted volumes";
    return -1;
  }

  if (!mount_point) {
    mount_point = v->mount_point;
  }

  const MountedVolume* mv = find_mounted_volume_by_mount_point(mount_point);
  if (mv != nullptr) {
    // Volume is already mounted.
    return 0;
  }

  mkdir(mount_point, 0755);  // in case it doesn't already exist

  if (strcmp(v->fs_type, "ext4") == 0 || strcmp(v->fs_type, "squashfs") == 0 ||
      strcmp(v->fs_type, "vfat") == 0) {
    int result = mount(v->blk_device, mount_point, v->fs_type, v->flags, v->fs_options);
    if (result == -1 && fs_mgr_is_formattable(v)) {
      PLOG(ERROR) << "Failed to mount " << mount_point << "; formatting";
      bool crypt_footer = fs_mgr_is_encryptable(v) && !strcmp(v->key_loc, "footer");
      if (fs_mgr_do_format(v, crypt_footer) == 0) {
        result = mount(v->blk_device, mount_point, v->fs_type, v->flags, v->fs_options);
      } else {
        PLOG(ERROR) << "Failed to format " << mount_point;
        return -1;
      }
    }

    if (result == -1) {
      PLOG(ERROR) << "Failed to mount " << mount_point;
      return -1;
    }
    return 0;
  }

  LOG(ERROR) << "unknown fs_type \"" << v->fs_type << "\" for " << mount_point;
  return -1;
}

int ensure_path_mounted(const char* path) {
  // Mount at the default mount point.
  return ensure_path_mounted_at(path, nullptr);
}

int ensure_path_unmounted(const char* path) {
  const Volume* v = volume_for_path(path);
  if (v == nullptr) {
    LOG(ERROR) << "unknown volume for path [" << path << "]";
    return -1;
  }
  if (strcmp(v->fs_type, "ramdisk") == 0) {
    // The ramdisk is always mounted; you can't unmount it.
    return -1;
  }

  if (!scan_mounted_volumes()) {
    LOG(ERROR) << "Failed to scan mounted volumes";
    return -1;
  }

  MountedVolume* mv = find_mounted_volume_by_mount_point(v->mount_point);
  if (mv == nullptr) {
    // Volume is already unmounted.
    return 0;
  }

  return unmount_mounted_volume(mv);
}

static int exec_cmd(const std::vector<std::string>& args) {
  CHECK_NE(static_cast<size_t>(0), args.size());

  std::vector<char*> argv(args.size());
  std::transform(args.cbegin(), args.cend(), argv.begin(),
                 [](const std::string& arg) { return const_cast<char*>(arg.c_str()); });
  argv.push_back(nullptr);

  pid_t child;
  if ((child = vfork()) == 0) {
    execv(argv[0], argv.data());
    _exit(EXIT_FAILURE);
  }

  int status;
  waitpid(child, &status, 0);
  if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) {
    LOG(ERROR) << args[0] << " failed with status " << WEXITSTATUS(status);
  }
  return WEXITSTATUS(status);
}

static ssize_t get_file_size(int fd, uint64_t reserve_len) {
  struct stat buf;
  int ret = fstat(fd, &buf);
  if (ret) return 0;

  ssize_t computed_size;
  if (S_ISREG(buf.st_mode)) {
    computed_size = buf.st_size - reserve_len;
  } else if (S_ISBLK(buf.st_mode)) {
    computed_size = get_block_device_size(fd) - reserve_len;
  } else {
    computed_size = 0;
  }

  return computed_size;
}

int format_volume(const char* volume, const char* directory) {
  const Volume* v = volume_for_path(volume);
  if (v == nullptr) {
    LOG(ERROR) << "unknown volume \"" << volume << "\"";
    return -1;
  }
  if (strcmp(v->fs_type, "ramdisk") == 0) {
    LOG(ERROR) << "can't format_volume \"" << volume << "\"";
    return -1;
  }
  if (strcmp(v->mount_point, volume) != 0) {
    LOG(ERROR) << "can't give path \"" << volume << "\" to format_volume";
    return -1;
  }
  if (ensure_path_unmounted(volume) != 0) {
    LOG(ERROR) << "format_volume: Failed to unmount \"" << v->mount_point << "\"";
    return -1;
  }
  if (strcmp(v->fs_type, "ext4") != 0 && strcmp(v->fs_type, "f2fs") != 0) {
    LOG(ERROR) << "format_volume: fs_type \"" << v->fs_type << "\" unsupported";
    return -1;
  }

  // If there's a key_loc that looks like a path, it should be a block device for storing encryption
  // metadata. Wipe it too.
  if (v->key_loc != nullptr && v->key_loc[0] == '/') {
    LOG(INFO) << "Wiping " << v->key_loc;
    int fd = open(v->key_loc, O_WRONLY | O_CREAT, 0644);
    if (fd == -1) {
      PLOG(ERROR) << "format_volume: Failed to open " << v->key_loc;
      return -1;
    }
    wipe_block_device(fd, get_file_size(fd));
    close(fd);
  }

  ssize_t length = 0;
  if (v->length != 0) {
    length = v->length;
  } else if (v->key_loc != nullptr && strcmp(v->key_loc, "footer") == 0) {
    android::base::unique_fd fd(open(v->blk_device, O_RDONLY));
    if (fd == -1) {
      PLOG(ERROR) << "get_file_size: failed to open " << v->blk_device;
      return -1;
    }
    length = get_file_size(fd.get(), CRYPT_FOOTER_OFFSET);
    if (length <= 0) {
      LOG(ERROR) << "get_file_size: invalid size " << length << " for " << v->blk_device;
      return -1;
    }
  }

  if (strcmp(v->fs_type, "ext4") == 0) {
    static constexpr int kBlockSize = 4096;
    std::vector<std::string> mke2fs_args = {
      "/sbin/mke2fs_static", "-F", "-t", "ext4", "-b", std::to_string(kBlockSize),
    };

    int raid_stride = v->logical_blk_size / kBlockSize;
    int raid_stripe_width = v->erase_blk_size / kBlockSize;
    // stride should be the max of 8KB and logical block size
    if (v->logical_blk_size != 0 && v->logical_blk_size < 8192) {
      raid_stride = 8192 / kBlockSize;
    }
    if (v->erase_blk_size != 0 && v->logical_blk_size != 0) {
      mke2fs_args.push_back("-E");
      mke2fs_args.push_back(
          android::base::StringPrintf("stride=%d,stripe-width=%d", raid_stride, raid_stripe_width));
    }
    mke2fs_args.push_back(v->blk_device);
    if (length != 0) {
      mke2fs_args.push_back(std::to_string(length / kBlockSize));
    }

    int result = exec_cmd(mke2fs_args);
    if (result == 0 && directory != nullptr) {
      std::vector<std::string> e2fsdroid_args = {
        "/sbin/e2fsdroid_static",
        "-e",
        "-f",
        directory,
        "-a",
        volume,
        v->blk_device,
      };
      result = exec_cmd(e2fsdroid_args);
    }

    if (result != 0) {
      PLOG(ERROR) << "format_volume: Failed to make ext4 on " << v->blk_device;
      return -1;
    }
    return 0;
  }

  // Has to be f2fs because we checked earlier.
  std::vector<std::string> f2fs_args = { "/sbin/mkfs.f2fs", "-t", "-d1", v->blk_device };
  if (length >= 512) {
    f2fs_args.push_back(std::to_string(length / 512));
  }

  int result = exec_cmd(f2fs_args);
  if (result != 0) {
    PLOG(ERROR) << "format_volume: Failed to make f2fs on " << v->blk_device;
    return -1;
  }
  return 0;
}

int format_volume(const char* volume) {
  return format_volume(volume, nullptr);
}

int setup_install_mounts() {
  if (fstab == nullptr) {
    LOG(ERROR) << "can't set up install mounts: no fstab loaded";
    return -1;
  }
  for (int i = 0; i < fstab->num_entries; ++i) {
    const Volume* v = fstab->recs + i;

    // We don't want to do anything with "/".
    if (strcmp(v->mount_point, "/") == 0) {
      continue;
    }

    if (strcmp(v->mount_point, "/tmp") == 0 || strcmp(v->mount_point, "/cache") == 0) {
      if (ensure_path_mounted(v->mount_point) != 0) {
        LOG(ERROR) << "Failed to mount " << v->mount_point;
        return -1;
      }
    } else {
      if (ensure_path_unmounted(v->mount_point) != 0) {
        LOG(ERROR) << "Failed to unmount " << v->mount_point;
        return -1;
      }
    }
  }
  return 0;
}