aboutsummaryrefslogblamecommitdiffstats
path: root/ui.cpp
blob: 78b6e4f1b95b203bdaef09ca2b43a5846fd1798c (plain) (tree)





























                                                                           
                                    


                                  
                  






                                      






                                    



                               

                                                  
                                                

 









                                                                    













                                                                           
                         
                                 
 
                                                                                                  
 
                                                                      

 
                                                         
                          
                                                
                  
     








                                                           








                                                            


             
                    

     
                                                  
                                      
     















                                                                      
                                                       
                              
                            
                        
 


                                         
                         
                                 
                               



                                            


                                                                             
            
                                        
                                        
                                
         

                           
                                   


                                           
                                                 


                                  




                                       
                                 
                                                                           
                                         
             


                                   
                                 




                  



                                                    
                   












                                                               









                                                                   
                           






                                                                    
                                    





                                                       
                                                                                     
         
                                                     









                                                                            
                                   







                                                                            
                                                                        
                                                                                 






                                                                             
                                        





                                           






                                           



                                                       





                                           





                                                                                                
                            














                                                                                     

     
                                                  
                           








                                               




                                   
                   
                                              
 
 
                                    
 





                                                
/*
 * Copyright (C) 2011 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include <errno.h>
#include <fcntl.h>
#include <linux/input.h>
#include <pthread.h>
#include <stdarg.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/stat.h>
#include <sys/time.h>
#include <sys/types.h>
#include <time.h>
#include <unistd.h>

#include <android-base/properties.h>
#include <cutils/android_reboot.h>

#include "common.h"
#include "roots.h"
#include "device.h"
#include "minui/minui.h"
#include "screen_ui.h"
#include "ui.h"

#define UI_WAIT_KEY_TIMEOUT_SEC    120

RecoveryUI::RecoveryUI()
        : key_queue_len(0),
          key_last_down(-1),
          key_long_press(false),
          key_down_count(0),
          enable_reboot(true),
          consecutive_power_keys(0),
          last_key(-1),
          has_power_key(false),
          has_up_key(false),
          has_down_key(false) {
    pthread_mutex_init(&key_queue_mutex, nullptr);
    pthread_cond_init(&key_queue_cond, nullptr);
    memset(key_pressed, 0, sizeof(key_pressed));
}

void RecoveryUI::OnKeyDetected(int key_code) {
    if (key_code == KEY_POWER) {
        has_power_key = true;
    } else if (key_code == KEY_DOWN || key_code == KEY_VOLUMEDOWN) {
        has_down_key = true;
    } else if (key_code == KEY_UP || key_code == KEY_VOLUMEUP) {
        has_up_key = true;
    }
}

int RecoveryUI::InputCallback(int fd, uint32_t epevents, void* data) {
    return reinterpret_cast<RecoveryUI*>(data)->OnInputEvent(fd, epevents);
}

// Reads input events, handles special hot keys, and adds to the key queue.
static void* InputThreadLoop(void*) {
    while (true) {
        if (!ev_wait(-1)) {
            ev_dispatch();
        }
    }
    return nullptr;
}

void RecoveryUI::Init() {
    ev_init(InputCallback, this);

    ev_iterate_available_keys(std::bind(&RecoveryUI::OnKeyDetected, this, std::placeholders::_1));

    pthread_create(&input_thread_, nullptr, InputThreadLoop, nullptr);
}

int RecoveryUI::OnInputEvent(int fd, uint32_t epevents) {
    struct input_event ev;
    if (ev_get_input(fd, epevents, &ev) == -1) {
        return -1;
    }

    if (ev.type == EV_SYN) {
        return 0;
    } else if (ev.type == EV_REL) {
        if (ev.code == REL_Y) {
            // accumulate the up or down motion reported by
            // the trackball.  When it exceeds a threshold
            // (positive or negative), fake an up/down
            // key event.
            rel_sum += ev.value;
            if (rel_sum > 3) {
                ProcessKey(KEY_DOWN, 1);   // press down key
                ProcessKey(KEY_DOWN, 0);   // and release it
                rel_sum = 0;
            } else if (rel_sum < -3) {
                ProcessKey(KEY_UP, 1);     // press up key
                ProcessKey(KEY_UP, 0);     // and release it
                rel_sum = 0;
            }
        }
    } else {
        rel_sum = 0;
    }

    if (ev.type == EV_KEY && ev.code <= KEY_MAX) {
        ProcessKey(ev.code, ev.value);
    }

    return 0;
}

// Process a key-up or -down event.  A key is "registered" when it is
// pressed and then released, with no other keypresses or releases in
// between.  Registered keys are passed to CheckKey() to see if it
// should trigger a visibility toggle, an immediate reboot, or be
// queued to be processed next time the foreground thread wants a key
// (eg, for the menu).
//
// We also keep track of which keys are currently down so that
// CheckKey can call IsKeyPressed to see what other keys are held when
// a key is registered.
//
// updown == 1 for key down events; 0 for key up events
void RecoveryUI::ProcessKey(int key_code, int updown) {
    bool register_key = false;
    bool long_press = false;
    bool reboot_enabled;

    pthread_mutex_lock(&key_queue_mutex);
    key_pressed[key_code] = updown;
    if (updown) {
        ++key_down_count;
        key_last_down = key_code;
        key_long_press = false;
        key_timer_t* info = new key_timer_t;
        info->ui = this;
        info->key_code = key_code;
        info->count = key_down_count;
        pthread_t thread;
        pthread_create(&thread, nullptr, &RecoveryUI::time_key_helper, info);
        pthread_detach(thread);
    } else {
        if (key_last_down == key_code) {
            long_press = key_long_press;
            register_key = true;
        }
        key_last_down = -1;
    }
    reboot_enabled = enable_reboot;
    pthread_mutex_unlock(&key_queue_mutex);

    if (register_key) {
        switch (CheckKey(key_code, long_press)) {
          case RecoveryUI::IGNORE:
            break;

          case RecoveryUI::TOGGLE:
            ShowText(!IsTextVisible());
            break;

          case RecoveryUI::REBOOT:
            if (reboot_enabled) {
                android::base::SetProperty(ANDROID_RB_PROPERTY, "reboot,");
                while (true) { pause(); }
            }
            break;

          case RecoveryUI::ENQUEUE:
            EnqueueKey(key_code);
            break;
        }
    }
}

void* RecoveryUI::time_key_helper(void* cookie) {
    key_timer_t* info = (key_timer_t*) cookie;
    info->ui->time_key(info->key_code, info->count);
    delete info;
    return nullptr;
}

void RecoveryUI::time_key(int key_code, int count) {
    usleep(750000);  // 750 ms == "long"
    bool long_press = false;
    pthread_mutex_lock(&key_queue_mutex);
    if (key_last_down == key_code && key_down_count == count) {
        long_press = key_long_press = true;
    }
    pthread_mutex_unlock(&key_queue_mutex);
    if (long_press) KeyLongPress(key_code);
}

void RecoveryUI::EnqueueKey(int key_code) {
    pthread_mutex_lock(&key_queue_mutex);
    const int queue_max = sizeof(key_queue) / sizeof(key_queue[0]);
    if (key_queue_len < queue_max) {
        key_queue[key_queue_len++] = key_code;
        pthread_cond_signal(&key_queue_cond);
    }
    pthread_mutex_unlock(&key_queue_mutex);
}

int RecoveryUI::WaitKey() {
    pthread_mutex_lock(&key_queue_mutex);

    // Time out after UI_WAIT_KEY_TIMEOUT_SEC, unless a USB cable is
    // plugged in.
    do {
        struct timeval now;
        struct timespec timeout;
        gettimeofday(&now, nullptr);
        timeout.tv_sec = now.tv_sec;
        timeout.tv_nsec = now.tv_usec * 1000;
        timeout.tv_sec += UI_WAIT_KEY_TIMEOUT_SEC;

        int rc = 0;
        while (key_queue_len == 0 && rc != ETIMEDOUT) {
            rc = pthread_cond_timedwait(&key_queue_cond, &key_queue_mutex, &timeout);
        }
    } while (IsUsbConnected() && key_queue_len == 0);

    int key = -1;
    if (key_queue_len > 0) {
        key = key_queue[0];
        memcpy(&key_queue[0], &key_queue[1], sizeof(int) * --key_queue_len);
    }
    pthread_mutex_unlock(&key_queue_mutex);
    return key;
}

bool RecoveryUI::IsUsbConnected() {
    int fd = open("/sys/class/android_usb/android0/state", O_RDONLY);
    if (fd < 0) {
        printf("failed to open /sys/class/android_usb/android0/state: %s\n",
               strerror(errno));
        return 0;
    }

    char buf;
    // USB is connected if android_usb state is CONNECTED or CONFIGURED.
    int connected = (TEMP_FAILURE_RETRY(read(fd, &buf, 1)) == 1) && (buf == 'C');
    if (close(fd) < 0) {
        printf("failed to close /sys/class/android_usb/android0/state: %s\n",
               strerror(errno));
    }
    return connected;
}

bool RecoveryUI::IsKeyPressed(int key) {
    pthread_mutex_lock(&key_queue_mutex);
    int pressed = key_pressed[key];
    pthread_mutex_unlock(&key_queue_mutex);
    return pressed;
}

bool RecoveryUI::IsLongPress() {
    pthread_mutex_lock(&key_queue_mutex);
    bool result = key_long_press;
    pthread_mutex_unlock(&key_queue_mutex);
    return result;
}

bool RecoveryUI::HasThreeButtons() {
    return has_power_key && has_up_key && has_down_key;
}

void RecoveryUI::FlushKeys() {
    pthread_mutex_lock(&key_queue_mutex);
    key_queue_len = 0;
    pthread_mutex_unlock(&key_queue_mutex);
}

RecoveryUI::KeyAction RecoveryUI::CheckKey(int key, bool is_long_press) {
    pthread_mutex_lock(&key_queue_mutex);
    key_long_press = false;
    pthread_mutex_unlock(&key_queue_mutex);

    // If we have power and volume up keys, that chord is the signal to toggle the text display.
    if (HasThreeButtons()) {
        if (key == KEY_VOLUMEUP && IsKeyPressed(KEY_POWER)) {
            return TOGGLE;
        }
    } else {
        // Otherwise long press of any button toggles to the text display,
        // and there's no way to toggle back (but that's pretty useless anyway).
        if (is_long_press && !IsTextVisible()) {
            return TOGGLE;
        }

        // Also, for button-limited devices, a long press is translated to KEY_ENTER.
        if (is_long_press && IsTextVisible()) {
            EnqueueKey(KEY_ENTER);
            return IGNORE;
        }
    }

    // Press power seven times in a row to reboot.
    if (key == KEY_POWER) {
        pthread_mutex_lock(&key_queue_mutex);
        bool reboot_enabled = enable_reboot;
        pthread_mutex_unlock(&key_queue_mutex);

        if (reboot_enabled) {
            ++consecutive_power_keys;
            if (consecutive_power_keys >= 7) {
                return REBOOT;
            }
        }
    } else {
        consecutive_power_keys = 0;
    }

    last_key = key;
    return IsTextVisible() ? ENQUEUE : IGNORE;
}

void RecoveryUI::KeyLongPress(int) {
}

void RecoveryUI::SetEnableReboot(bool enabled) {
    pthread_mutex_lock(&key_queue_mutex);
    enable_reboot = enabled;
    pthread_mutex_unlock(&key_queue_mutex);
}