aboutsummaryrefslogblamecommitdiffstats
path: root/ui.h
blob: 4c54d6915d129e550864dd656098d968fe07e8a5 (plain) (tree)


















                                                                           

                        
                 
 

                 

                                                                     
        




















                      
               
 
                          
 

                                                                                                   
                                               
 
                                                              
                                                  
 
                                                          

                                                             
 
                               

                                                             
                                                                     



                                                                                 

                                                                                       









                                               

                                                                                               



                                                                              
 
                         
 
                                                                
                        
 

                                     
 

                                                                                                    

                                 





                                              
                               

                           

                                                                                                    
                                                           

                                                          


                                                                                                    

                                     



                                                                                                    



                                             

                                                                                                 


                                                                              

                                                                                               

                                      
                                                                                                




                                


                                                                                                   

                                  

                                   
 


                                                                
         












                               



                                            









                                              

                         
















                                                          









                                                                                   
                                  
 

                          
                                      
 



                                                                                       
  

                        
/*
 * Copyright (C) 2011 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef RECOVERY_UI_H
#define RECOVERY_UI_H

#include <linux/input.h>
#include <pthread.h>
#include <time.h>

#include <string>

// Abstract class for controlling the user interface during recovery.
class RecoveryUI {
 public:
  enum Icon {
    NONE,
    INSTALLING_UPDATE,
    ERASING,
    NO_COMMAND,
    ERROR
  };

  enum ProgressType {
    EMPTY,
    INDETERMINATE,
    DETERMINATE
  };

  enum KeyAction {
    ENQUEUE,
    TOGGLE,
    REBOOT,
    IGNORE
  };

  RecoveryUI();

  virtual ~RecoveryUI() {}

  // Initializes the object; called before anything else. UI texts will be initialized according to
  // the given locale. Returns true on success.
  virtual bool Init(const std::string& locale);

  // Shows a stage indicator. Called immediately after Init().
  virtual void SetStage(int current, int max) = 0;

  // Sets the overall recovery state ("background image").
  virtual void SetBackground(Icon icon) = 0;
  virtual void SetSystemUpdateText(bool security_update) = 0;

  // --- progress indicator ---
  virtual void SetProgressType(ProgressType determinate) = 0;

  // Shows a progress bar and define the scope of the next operation:
  //   portion - fraction of the progress bar the next operation will use
  //   seconds - expected time interval (progress bar moves at this minimum rate)
  virtual void ShowProgress(float portion, float seconds) = 0;

  // Sets progress bar position (0.0 - 1.0 within the scope defined by the last call to
  // ShowProgress).
  virtual void SetProgress(float fraction) = 0;

  // --- text log ---

  virtual void ShowText(bool visible) = 0;

  virtual bool IsTextVisible() = 0;

  virtual bool WasTextEverVisible() = 0;

  // Writes a message to the on-screen log (shown if the user has toggled on the text display).
  // Print() will also dump the message to stdout / log file, while PrintOnScreenOnly() not.
  virtual void Print(const char* fmt, ...) __printflike(2, 3) = 0;
  virtual void PrintOnScreenOnly(const char* fmt, ...) __printflike(2, 3) = 0;

  virtual void ShowFile(const char* filename) = 0;

  // --- key handling ---

  // Waits for a key and return it. May return -1 after timeout.
  virtual int WaitKey();

  virtual bool IsKeyPressed(int key);
  virtual bool IsLongPress();

  // Returns true if you have the volume up/down and power trio typical of phones and tablets, false
  // otherwise.
  virtual bool HasThreeButtons();

  // Returns true if it has a power key.
  virtual bool HasPowerKey() const;

  // Returns true if it supports touch inputs.
  virtual bool HasTouchScreen() const;

  // Erases any queued-up keys.
  virtual void FlushKeys();

  // Called on each key press, even while operations are in progress. Return value indicates whether
  // an immediate operation should be triggered (toggling the display, rebooting the device), or if
  // the key should be enqueued for use by the main thread.
  virtual KeyAction CheckKey(int key, bool is_long_press);

  // Called when a key is held down long enough to have been a long-press (but before the key is
  // released). This means that if the key is eventually registered (released without any other keys
  // being pressed in the meantime), CheckKey will be called with 'is_long_press' true.
  virtual void KeyLongPress(int key);

  // Normally in recovery there's a key sequence that triggers immediate reboot of the device,
  // regardless of what recovery is doing (with the default CheckKey implementation, it's pressing
  // the power button 7 times in row). Call this to enable or disable that feature. It is enabled by
  // default.
  virtual void SetEnableReboot(bool enabled);

  // --- menu display ---

  // Display some header text followed by a menu of items, which appears at the top of the screen
  // (in place of any scrolling ui_print() output, if necessary).
  virtual void StartMenu(const char* const* headers, const char* const* items,
                         int initial_selection) = 0;

  // Sets the menu highlight to the given index, wrapping if necessary. Returns the actual item
  // selected.
  virtual int SelectMenu(int sel) = 0;

  // Ends menu mode, resetting the text overlay so that ui_print() statements will be displayed.
  virtual void EndMenu() = 0;

 protected:
  void EnqueueKey(int key_code);

  // The normal and dimmed brightness percentages (default: 50 and 25, which means 50% and 25% of
  // the max_brightness). Because the absolute values may vary across devices. These two values can
  // be configured via subclassing. Setting brightness_normal_ to 0 to disable screensaver.
  unsigned int brightness_normal_;
  unsigned int brightness_dimmed_;
  std::string brightness_file_;
  std::string max_brightness_file_;

  // Whether we should listen for touch inputs (default: false).
  bool touch_screen_allowed_;

 private:
  enum class ScreensaverState {
    DISABLED,
    NORMAL,
    DIMMED,
    OFF
  };

  struct key_timer_t {
    RecoveryUI* ui;
    int key_code;
    int count;
  };

  // The sensitivity when detecting a swipe.
  const int kTouchLowThreshold;
  const int kTouchHighThreshold;

  void OnKeyDetected(int key_code);
  void OnTouchDetected(int dx, int dy);
  int OnInputEvent(int fd, uint32_t epevents);
  void ProcessKey(int key_code, int updown);

  bool IsUsbConnected();

  static void* time_key_helper(void* cookie);
  void time_key(int key_code, int count);

  bool InitScreensaver();

  // Key event input queue
  pthread_mutex_t key_queue_mutex;
  pthread_cond_t key_queue_cond;
  int key_queue[256], key_queue_len;
  char key_pressed[KEY_MAX + 1];  // under key_queue_mutex
  int key_last_down;              // under key_queue_mutex
  bool key_long_press;            // under key_queue_mutex
  int key_down_count;             // under key_queue_mutex
  bool enable_reboot;             // under key_queue_mutex
  int rel_sum;

  int consecutive_power_keys;
  int last_key;

  bool has_power_key;
  bool has_up_key;
  bool has_down_key;
  bool has_touch_screen;

  // Touch event related variables. See the comments in RecoveryUI::OnInputEvent().
  int touch_slot_;
  int touch_X_;
  int touch_Y_;
  int touch_start_X_;
  int touch_start_Y_;
  bool touch_finger_down_;
  bool touch_swiping_;
  bool is_bootreason_recovery_ui_;

  pthread_t input_thread_;

  ScreensaverState screensaver_state_;

  // The following two contain the absolute values computed from brightness_normal_ and
  // brightness_dimmed_ respectively.
  unsigned int brightness_normal_value_;
  unsigned int brightness_dimmed_value_;
};

#endif  // RECOVERY_UI_H