aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorTianjie Xu2018-02-27 17:56:11 -0600
committerTianjie Xu2018-02-28 13:19:11 -0600
commit3bbb20f557790c015e44098098375eb6cc376a42 (patch)
tree9db0b6bd746646486aa990daecf8e3302c49b4c0
parentac4818d6afe80cb71d19d34cd6c36fd9a04e7b6d (diff)
downloadplatform-bootable-recovery-3bbb20f557790c015e44098098375eb6cc376a42.tar.gz
platform-bootable-recovery-3bbb20f557790c015e44098098375eb6cc376a42.tar.xz
platform-bootable-recovery-3bbb20f557790c015e44098098375eb6cc376a42.zip
Add a singleton CacheLocation to replace the hard coded locations
This class allows us to set the following locations dynamically: cache_temp_source, last_command_file, stash_directory_base. In the updater's main function, we reset the values of these variables to their default locations in /cache; while we can set them to temp files in unit tests or host simulation. Test: unit tests pass Change-Id: I528652650caa41373617ab055d41b1f1a4ec0f87
-rw-r--r--applypatch/applypatch.cpp11
-rw-r--r--applypatch/freecache.cpp3
-rw-r--r--applypatch/include/applypatch/applypatch.h6
-rw-r--r--otautil/Android.bp1
-rw-r--r--otautil/cache_location.cpp32
-rw-r--r--otautil/include/otautil/cache_location.h72
-rw-r--r--tests/component/applypatch_test.cpp5
-rw-r--r--tests/component/updater_test.cpp21
-rw-r--r--updater/blockimg.cpp9
-rw-r--r--updater/include/updater/blockimg.h1
-rw-r--r--updater/updater.cpp5
11 files changed, 139 insertions, 27 deletions
diff --git a/applypatch/applypatch.cpp b/applypatch/applypatch.cpp
index 73701abc..7645a400 100644
--- a/applypatch/applypatch.cpp
+++ b/applypatch/applypatch.cpp
@@ -40,10 +40,9 @@
40 40
41#include "edify/expr.h" 41#include "edify/expr.h"
42#include "otafault/ota_io.h" 42#include "otafault/ota_io.h"
43#include "otautil/cache_location.h"
43#include "otautil/print_sha1.h" 44#include "otautil/print_sha1.h"
44 45
45std::string cache_temp_source = "/cache/saved.file";
46
47static int LoadPartitionContents(const std::string& filename, FileContents* file); 46static int LoadPartitionContents(const std::string& filename, FileContents* file);
48static size_t FileSink(const unsigned char* data, size_t len, int fd); 47static size_t FileSink(const unsigned char* data, size_t len, int fd);
49static int GenerateTarget(const FileContents& source_file, const std::unique_ptr<Value>& patch, 48static int GenerateTarget(const FileContents& source_file, const std::unique_ptr<Value>& patch,
@@ -404,7 +403,7 @@ int applypatch_check(const char* filename, const std::vector<std::string>& patch
404 // If the source file is missing or corrupted, it might be because we were killed in the middle 403 // If the source file is missing or corrupted, it might be because we were killed in the middle
405 // of patching it. A copy of it should have been made in cache_temp_source. If that file 404 // of patching it. A copy of it should have been made in cache_temp_source. If that file
406 // exists and matches the sha1 we're looking for, the check still passes. 405 // exists and matches the sha1 we're looking for, the check still passes.
407 if (LoadFileContents(cache_temp_source.c_str(), &file) != 0) { 406 if (LoadFileContents(CacheLocation::location().cache_temp_source().c_str(), &file) != 0) {
408 printf("failed to load cache file\n"); 407 printf("failed to load cache file\n");
409 return 1; 408 return 1;
410 } 409 }
@@ -526,7 +525,7 @@ int applypatch(const char* source_filename, const char* target_filename,
526 printf("source file is bad; trying copy\n"); 525 printf("source file is bad; trying copy\n");
527 526
528 FileContents copy_file; 527 FileContents copy_file;
529 if (LoadFileContents(cache_temp_source.c_str(), &copy_file) < 0) { 528 if (LoadFileContents(CacheLocation::location().cache_temp_source().c_str(), &copy_file) < 0) {
530 printf("failed to read copy file\n"); 529 printf("failed to read copy file\n");
531 return 1; 530 return 1;
532 } 531 }
@@ -621,7 +620,7 @@ static int GenerateTarget(const FileContents& source_file, const std::unique_ptr
621 printf("not enough free space on /cache\n"); 620 printf("not enough free space on /cache\n");
622 return 1; 621 return 1;
623 } 622 }
624 if (SaveFileContents(cache_temp_source.c_str(), &source_file) < 0) { 623 if (SaveFileContents(CacheLocation::location().cache_temp_source().c_str(), &source_file) < 0) {
625 printf("failed to back up source file\n"); 624 printf("failed to back up source file\n");
626 return 1; 625 return 1;
627 } 626 }
@@ -667,7 +666,7 @@ static int GenerateTarget(const FileContents& source_file, const std::unique_ptr
667 } 666 }
668 667
669 // Delete the backup copy of the source. 668 // Delete the backup copy of the source.
670 unlink(cache_temp_source.c_str()); 669 unlink(CacheLocation::location().cache_temp_source().c_str());
671 670
672 // Success! 671 // Success!
673 return 0; 672 return 0;
diff --git a/applypatch/freecache.cpp b/applypatch/freecache.cpp
index ec1d20ce..ea364d8e 100644
--- a/applypatch/freecache.cpp
+++ b/applypatch/freecache.cpp
@@ -33,6 +33,7 @@
33#include <android-base/stringprintf.h> 33#include <android-base/stringprintf.h>
34 34
35#include "applypatch/applypatch.h" 35#include "applypatch/applypatch.h"
36#include "otautil/cache_location.h"
36 37
37static int EliminateOpenFiles(std::set<std::string>* files) { 38static int EliminateOpenFiles(std::set<std::string>* files) {
38 std::unique_ptr<DIR, decltype(&closedir)> d(opendir("/proc"), closedir); 39 std::unique_ptr<DIR, decltype(&closedir)> d(opendir("/proc"), closedir);
@@ -92,7 +93,7 @@ static std::set<std::string> FindExpendableFiles() {
92 93
93 // We can't delete cache_temp_source; if it's there we might have restarted during 94 // We can't delete cache_temp_source; if it's there we might have restarted during
94 // installation and could be depending on it to be there. 95 // installation and could be depending on it to be there.
95 if (path == cache_temp_source) { 96 if (path == CacheLocation::location().cache_temp_source()) {
96 continue; 97 continue;
97 } 98 }
98 99
diff --git a/applypatch/include/applypatch/applypatch.h b/applypatch/include/applypatch/applypatch.h
index c8ad9150..912ead1f 100644
--- a/applypatch/include/applypatch/applypatch.h
+++ b/applypatch/include/applypatch/applypatch.h
@@ -34,12 +34,6 @@ struct FileContents {
34 std::vector<unsigned char> data; 34 std::vector<unsigned char> data;
35}; 35};
36 36
37// When there isn't enough room on the target filesystem to hold the patched version of the file,
38// we copy the original here and delete it to free up space. If the expected source file doesn't
39// exist, or is corrupted, we look to see if the cached file contains the bits we want and use it as
40// the source instead. The default location for the cached source is "/cache/saved.file".
41extern std::string cache_temp_source;
42
43using SinkFn = std::function<size_t(const unsigned char*, size_t)>; 37using SinkFn = std::function<size_t(const unsigned char*, size_t)>;
44 38
45// applypatch.cpp 39// applypatch.cpp
diff --git a/otautil/Android.bp b/otautil/Android.bp
index 5efb12d6..75cf6914 100644
--- a/otautil/Android.bp
+++ b/otautil/Android.bp
@@ -21,6 +21,7 @@ cc_library_static {
21 "SysUtil.cpp", 21 "SysUtil.cpp",
22 "DirUtil.cpp", 22 "DirUtil.cpp",
23 "ThermalUtil.cpp", 23 "ThermalUtil.cpp",
24 "cache_location.cpp",
24 "rangeset.cpp", 25 "rangeset.cpp",
25 ], 26 ],
26 27
diff --git a/otautil/cache_location.cpp b/otautil/cache_location.cpp
new file mode 100644
index 00000000..8f289487
--- /dev/null
+++ b/otautil/cache_location.cpp
@@ -0,0 +1,32 @@
1/*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#include "otautil/cache_location.h"
18
19constexpr const char kDefaultCacheTempSource[] = "/cache/saved.file";
20constexpr const char kDefaultLastCommandFile[] = "/cache/recovery/last_command";
21constexpr const char kDefaultStashDirectoryBase[] = "/cache/recovery";
22
23CacheLocation& CacheLocation::location() {
24 static CacheLocation cache_location;
25 return cache_location;
26}
27
28void CacheLocation::ResetLocations() {
29 cache_temp_source_ = kDefaultCacheTempSource;
30 last_command_file_ = kDefaultLastCommandFile;
31 stash_directory_base_ = kDefaultStashDirectoryBase;
32}
diff --git a/otautil/include/otautil/cache_location.h b/otautil/include/otautil/cache_location.h
new file mode 100644
index 00000000..85e0d485
--- /dev/null
+++ b/otautil/include/otautil/cache_location.h
@@ -0,0 +1,72 @@
1/*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#ifndef _OTAUTIL_OTAUTIL_CACHE_LOCATION_H_
18#define _OTAUTIL_OTAUTIL_CACHE_LOCATION_H_
19
20#include <string>
21
22#include "android-base/macros.h"
23
24// A singleton class to maintain the update related locations. The locations should be only set
25// once at the start of the program.
26class CacheLocation {
27 public:
28 static CacheLocation& location();
29
30 // Reset the locations to their default values.
31 void ResetLocations();
32
33 // getter and setter functions.
34 std::string cache_temp_source() const {
35 return cache_temp_source_;
36 }
37 void set_cache_temp_source(const std::string& temp_source) {
38 cache_temp_source_ = temp_source;
39 }
40
41 std::string last_command_file() const {
42 return last_command_file_;
43 }
44 void set_last_command_file(const std::string& last_command) {
45 last_command_file_ = last_command;
46 }
47
48 std::string stash_directory_base() const {
49 return stash_directory_base_;
50 }
51 void set_stash_directory_base(const std::string& base) {
52 stash_directory_base_ = base;
53 }
54
55 private:
56 CacheLocation() {}
57 DISALLOW_COPY_AND_ASSIGN(CacheLocation);
58
59 // When there isn't enough room on the target filesystem to hold the patched version of the file,
60 // we copy the original here and delete it to free up space. If the expected source file doesn't
61 // exist, or is corrupted, we look to see if the cached file contains the bits we want and use it
62 // as the source instead. The default location for the cached source is "/cache/saved.file".
63 std::string cache_temp_source_;
64
65 // Location to save the last command that stashes blocks.
66 std::string last_command_file_;
67
68 // The base directory to write stashes during update.
69 std::string stash_directory_base_;
70};
71
72#endif // _OTAUTIL_OTAUTIL_CACHE_LOCATION_H_
diff --git a/tests/component/applypatch_test.cpp b/tests/component/applypatch_test.cpp
index 21c9a52d..b6d09255 100644
--- a/tests/component/applypatch_test.cpp
+++ b/tests/component/applypatch_test.cpp
@@ -35,6 +35,7 @@
35#include "applypatch/applypatch.h" 35#include "applypatch/applypatch.h"
36#include "applypatch/applypatch_modes.h" 36#include "applypatch/applypatch_modes.h"
37#include "common/test_constants.h" 37#include "common/test_constants.h"
38#include "otautil/cache_location.h"
38#include "otautil/print_sha1.h" 39#include "otautil/print_sha1.h"
39 40
40static void sha1sum(const std::string& fname, std::string* sha1, size_t* fsize = nullptr) { 41static void sha1sum(const std::string& fname, std::string* sha1, size_t* fsize = nullptr) {
@@ -93,14 +94,14 @@ class ApplyPatchCacheTest : public ApplyPatchTest {
93 protected: 94 protected:
94 void SetUp() override { 95 void SetUp() override {
95 ApplyPatchTest::SetUp(); 96 ApplyPatchTest::SetUp();
96 cache_temp_source = old_file; 97 CacheLocation::location().set_cache_temp_source(old_file);
97 } 98 }
98}; 99};
99 100
100class ApplyPatchModesTest : public ::testing::Test { 101class ApplyPatchModesTest : public ::testing::Test {
101 protected: 102 protected:
102 void SetUp() override { 103 void SetUp() override {
103 cache_temp_source = cache_source.path; 104 CacheLocation::location().set_cache_temp_source(cache_source.path);
104 } 105 }
105 106
106 TemporaryFile cache_source; 107 TemporaryFile cache_source;
diff --git a/tests/component/updater_test.cpp b/tests/component/updater_test.cpp
index 448fe493..5bfd7cb4 100644
--- a/tests/component/updater_test.cpp
+++ b/tests/component/updater_test.cpp
@@ -41,6 +41,7 @@
41#include "common/test_constants.h" 41#include "common/test_constants.h"
42#include "edify/expr.h" 42#include "edify/expr.h"
43#include "otautil/SysUtil.h" 43#include "otautil/SysUtil.h"
44#include "otautil/cache_location.h"
44#include "otautil/error_code.h" 45#include "otautil/error_code.h"
45#include "otautil/print_sha1.h" 46#include "otautil/print_sha1.h"
46#include "updater/blockimg.h" 47#include "updater/blockimg.h"
@@ -104,7 +105,16 @@ class UpdaterTest : public ::testing::Test {
104 RegisterBuiltins(); 105 RegisterBuiltins();
105 RegisterInstallFunctions(); 106 RegisterInstallFunctions();
106 RegisterBlockImageFunctions(); 107 RegisterBlockImageFunctions();
108
109 // Mock the location of last_command_file.
110 CacheLocation::location().set_cache_temp_source(temp_saved_source_.path);
111 CacheLocation::location().set_last_command_file(temp_last_command_.path);
112 CacheLocation::location().set_stash_directory_base(temp_stash_base_.path);
107 } 113 }
114
115 TemporaryFile temp_saved_source_;
116 TemporaryFile temp_last_command_;
117 TemporaryDir temp_stash_base_;
108}; 118};
109 119
110TEST_F(UpdaterTest, getprop) { 120TEST_F(UpdaterTest, getprop) {
@@ -542,7 +552,7 @@ TEST_F(UpdaterTest, block_image_update_fail) {
542 expect("", script.c_str(), kNoCause, &updater_info); 552 expect("", script.c_str(), kNoCause, &updater_info);
543 // Updater generates the stash name based on the input file name. 553 // Updater generates the stash name based on the input file name.
544 std::string name_digest = get_sha1(update_file.path); 554 std::string name_digest = get_sha1(update_file.path);
545 std::string stash_base = "/cache/recovery/" + name_digest; 555 std::string stash_base = std::string(temp_stash_base_.path) + "/" + name_digest;
546 ASSERT_EQ(0, access(stash_base.c_str(), F_OK)); 556 ASSERT_EQ(0, access(stash_base.c_str(), F_OK));
547 ASSERT_EQ(-1, access((stash_base + src_hash).c_str(), F_OK)); 557 ASSERT_EQ(-1, access((stash_base + src_hash).c_str(), F_OK));
548 ASSERT_EQ(0, rmdir(stash_base.c_str())); 558 ASSERT_EQ(0, rmdir(stash_base.c_str()));
@@ -709,8 +719,7 @@ TEST_F(UpdaterTest, brotli_new_data) {
709} 719}
710 720
711TEST_F(UpdaterTest, last_command_update) { 721TEST_F(UpdaterTest, last_command_update) {
712 TemporaryFile temp_file; 722 std::string last_command_file = CacheLocation::location().last_command_file();
713 last_command_file = temp_file.path;
714 723
715 std::string block1 = std::string(4096, '1'); 724 std::string block1 = std::string(4096, '1');
716 std::string block2 = std::string(4096, '2'); 725 std::string block2 = std::string(4096, '2');
@@ -797,8 +806,7 @@ TEST_F(UpdaterTest, last_command_update) {
797} 806}
798 807
799TEST_F(UpdaterTest, last_command_update_unresumable) { 808TEST_F(UpdaterTest, last_command_update_unresumable) {
800 TemporaryFile temp_file; 809 std::string last_command_file = CacheLocation::location().last_command_file();
801 last_command_file = temp_file.path;
802 810
803 std::string block1 = std::string(4096, '1'); 811 std::string block1 = std::string(4096, '1');
804 std::string block2 = std::string(4096, '2'); 812 std::string block2 = std::string(4096, '2');
@@ -853,8 +861,7 @@ TEST_F(UpdaterTest, last_command_update_unresumable) {
853} 861}
854 862
855TEST_F(UpdaterTest, last_command_verify) { 863TEST_F(UpdaterTest, last_command_verify) {
856 TemporaryFile temp_file; 864 std::string last_command_file = CacheLocation::location().last_command_file();
857 last_command_file = temp_file.path;
858 865
859 std::string block1 = std::string(4096, '1'); 866 std::string block1 = std::string(4096, '1');
860 std::string block2 = std::string(4096, '2'); 867 std::string block2 = std::string(4096, '2');
diff --git a/updater/blockimg.cpp b/updater/blockimg.cpp
index 4f085b20..e93196b2 100644
--- a/updater/blockimg.cpp
+++ b/updater/blockimg.cpp
@@ -53,6 +53,7 @@
53 53
54#include "edify/expr.h" 54#include "edify/expr.h"
55#include "otafault/ota_io.h" 55#include "otafault/ota_io.h"
56#include "otautil/cache_location.h"
56#include "otautil/error_code.h" 57#include "otautil/error_code.h"
57#include "otautil/print_sha1.h" 58#include "otautil/print_sha1.h"
58#include "otautil/rangeset.h" 59#include "otautil/rangeset.h"
@@ -65,17 +66,15 @@
65#define DEBUG_ERASE 0 66#define DEBUG_ERASE 0
66 67
67static constexpr size_t BLOCKSIZE = 4096; 68static constexpr size_t BLOCKSIZE = 4096;
68static constexpr const char* STASH_DIRECTORY_BASE = "/cache/recovery";
69static constexpr mode_t STASH_DIRECTORY_MODE = 0700; 69static constexpr mode_t STASH_DIRECTORY_MODE = 0700;
70static constexpr mode_t STASH_FILE_MODE = 0600; 70static constexpr mode_t STASH_FILE_MODE = 0600;
71 71
72std::string last_command_file = "/cache/recovery/last_command";
73
74static CauseCode failure_type = kNoCause; 72static CauseCode failure_type = kNoCause;
75static bool is_retry = false; 73static bool is_retry = false;
76static std::unordered_map<std::string, RangeSet> stash_map; 74static std::unordered_map<std::string, RangeSet> stash_map;
77 75
78static void DeleteLastCommandFile() { 76static void DeleteLastCommandFile() {
77 std::string last_command_file = CacheLocation::location().last_command_file();
79 if (unlink(last_command_file.c_str()) == -1 && errno != ENOENT) { 78 if (unlink(last_command_file.c_str()) == -1 && errno != ENOENT) {
80 PLOG(ERROR) << "Failed to unlink: " << last_command_file; 79 PLOG(ERROR) << "Failed to unlink: " << last_command_file;
81 } 80 }
@@ -84,6 +83,7 @@ static void DeleteLastCommandFile() {
84// Parse the last command index of the last update and save the result to |last_command_index|. 83// Parse the last command index of the last update and save the result to |last_command_index|.
85// Return true if we successfully read the index. 84// Return true if we successfully read the index.
86static bool ParseLastCommandFile(int* last_command_index) { 85static bool ParseLastCommandFile(int* last_command_index) {
86 std::string last_command_file = CacheLocation::location().last_command_file();
87 android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(last_command_file.c_str(), O_RDONLY))); 87 android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(last_command_file.c_str(), O_RDONLY)));
88 if (fd == -1) { 88 if (fd == -1) {
89 if (errno != ENOENT) { 89 if (errno != ENOENT) {
@@ -119,6 +119,7 @@ static bool ParseLastCommandFile(int* last_command_index) {
119// Update the last command index in the last_command_file if the current command writes to the 119// Update the last command index in the last_command_file if the current command writes to the
120// stash either explicitly or implicitly. 120// stash either explicitly or implicitly.
121static bool UpdateLastCommandIndex(int command_index, const std::string& command_string) { 121static bool UpdateLastCommandIndex(int command_index, const std::string& command_string) {
122 std::string last_command_file = CacheLocation::location().last_command_file();
122 std::string last_command_tmp = last_command_file + ".tmp"; 123 std::string last_command_tmp = last_command_file + ".tmp";
123 std::string content = std::to_string(command_index) + "\n" + command_string; 124 std::string content = std::to_string(command_index) + "\n" + command_string;
124 android::base::unique_fd wfd( 125 android::base::unique_fd wfd(
@@ -676,7 +677,7 @@ static std::string GetStashFileName(const std::string& base, const std::string&
676 return ""; 677 return "";
677 } 678 }
678 679
679 std::string fn(STASH_DIRECTORY_BASE); 680 std::string fn(CacheLocation::location().stash_directory_base());
680 fn += "/" + base + "/" + id + postfix; 681 fn += "/" + base + "/" + id + postfix;
681 682
682 return fn; 683 return fn;
diff --git a/updater/include/updater/blockimg.h b/updater/include/updater/blockimg.h
index 2cc68ce9..71733b30 100644
--- a/updater/include/updater/blockimg.h
+++ b/updater/include/updater/blockimg.h
@@ -19,7 +19,6 @@
19 19
20#include <string> 20#include <string>
21 21
22extern std::string last_command_file;
23void RegisterBlockImageFunctions(); 22void RegisterBlockImageFunctions();
24 23
25#endif 24#endif
diff --git a/updater/updater.cpp b/updater/updater.cpp
index f55a0d3b..f063e5fa 100644
--- a/updater/updater.cpp
+++ b/updater/updater.cpp
@@ -34,6 +34,7 @@
34#include "otafault/config.h" 34#include "otafault/config.h"
35#include "otautil/DirUtil.h" 35#include "otautil/DirUtil.h"
36#include "otautil/SysUtil.h" 36#include "otautil/SysUtil.h"
37#include "otautil/cache_location.h"
37#include "otautil/error_code.h" 38#include "otautil/error_code.h"
38#include "updater/blockimg.h" 39#include "updater/blockimg.h"
39#include "updater/install.h" 40#include "updater/install.h"
@@ -168,6 +169,10 @@ int main(int argc, char** argv) {
168 } 169 }
169 ota_io_init(za, state.is_retry); 170 ota_io_init(za, state.is_retry);
170 171
172 // Initialize the cache_temp_source, last_command_file and stash_directory_base to their default
173 // locations.
174 CacheLocation::location().ResetLocations();
175
171 std::string result; 176 std::string result;
172 bool status = Evaluate(&state, root, &result); 177 bool status = Evaluate(&state, root, &result);
173 178