aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorDoug Zongker2012-01-09 17:16:13 -0600
committerDoug Zongker2012-01-10 12:18:17 -0600
commit9270a20a801403c9f60d6a701b39eae70d380403 (patch)
tree5bdb058af5b05a65112297a504018ee356e0ddbb /device.h
parent210f887382e0fd7e51ec6ce071972374a76f0722 (diff)
downloadplatform-bootable-recovery-9270a20a801403c9f60d6a701b39eae70d380403.tar.gz
platform-bootable-recovery-9270a20a801403c9f60d6a701b39eae70d380403.tar.xz
platform-bootable-recovery-9270a20a801403c9f60d6a701b39eae70d380403.zip
support "sideload over ADB" mode
Rather than depending on the existence of some place to store a file that is accessible to users on an an unbootable device (eg, a physical sdcard, external USB drive, etc.), add support for sideloading packages sent to the device with adb. This change adds a "minimal adbd" which supports nothing but receiving a package over adb (with the "adb sideload" command) and storing it to a fixed filename in the /tmp ramdisk, from where it can be verified and sideloaded in the usual way. This should be leave available even on locked user-build devices. The user can select "apply package from ADB" from the recovery menu, which starts minimal-adb mode (shutting down any real adbd that may be running). Once minimal-adb has received a package it exits (restarting real adbd if appropriate) and then verification and installation of the received package proceeds. Change-Id: I6fe13161ca064a98d06fa32104e1f432826582f5
Diffstat (limited to 'device.h')
-rw-r--r--device.h2
1 files changed, 1 insertions, 1 deletions
diff --git a/device.h b/device.h
index 8096a8d9..583de75e 100644
--- a/device.h
+++ b/device.h
@@ -66,7 +66,7 @@ class Device {
66 virtual int HandleMenuKey(int key, int visible) = 0; 66 virtual int HandleMenuKey(int key, int visible) = 0;
67 67
68 enum BuiltinAction { NO_ACTION, REBOOT, APPLY_EXT, APPLY_CACHE, 68 enum BuiltinAction { NO_ACTION, REBOOT, APPLY_EXT, APPLY_CACHE,
69 WIPE_DATA, WIPE_CACHE }; 69 APPLY_ADB_SIDELOAD, WIPE_DATA, WIPE_CACHE };
70 70
71 // Perform a recovery action selected from the menu. 71 // Perform a recovery action selected from the menu.
72 // 'menu_position' will be the item number of the selected menu 72 // 'menu_position' will be the item number of the selected menu