aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorDoug Zongker2012-08-22 19:26:40 -0500
committerDoug Zongker2012-08-22 19:26:40 -0500
commit02ec6b88ed4e6cf40cc257572b07c7277b7b6341 (patch)
tree2aa6f95cb875d258f62a5342ec2bb1ad0093e3bd /install.h
parenta3ccba6d314cb29b02d1dbda9a71427b11da936d (diff)
downloadplatform-bootable-recovery-02ec6b88ed4e6cf40cc257572b07c7277b7b6341.tar.gz
platform-bootable-recovery-02ec6b88ed4e6cf40cc257572b07c7277b7b6341.tar.xz
platform-bootable-recovery-02ec6b88ed4e6cf40cc257572b07c7277b7b6341.zip
add simple text to recovery UI
- recovery takes a --locale argument, which will be passed by the main system - the locale is saved in cache, in case the --locale argument is missing (eg, when recovery is started from fastboot) - we include images that have prerendered text for many locales - we split the background states into four (installing update, erasing, no command, error) so that appropriate text can be shown. Change-Id: I731b8108e83d5ccc09a4aacfc1dbf7e86b397aaf
Diffstat (limited to 'install.h')
-rw-r--r--install.h2
1 files changed, 1 insertions, 1 deletions
diff --git a/install.h b/install.h
index 1943f02d..2ada529e 100644
--- a/install.h
+++ b/install.h
@@ -23,7 +23,7 @@
23extern "C" { 23extern "C" {
24#endif 24#endif
25 25
26enum { INSTALL_SUCCESS, INSTALL_ERROR, INSTALL_CORRUPT }; 26enum { INSTALL_SUCCESS, INSTALL_ERROR, INSTALL_CORRUPT, INSTALL_NONE };
27// Install the package specified by root_path. If INSTALL_SUCCESS is 27// Install the package specified by root_path. If INSTALL_SUCCESS is
28// returned and *wipe_cache is true on exit, caller should wipe the 28// returned and *wipe_cache is true on exit, caller should wipe the
29// cache partition. 29// cache partition.