diff options
author | Tao Bao | 2017-01-03 12:15:33 -0600 |
---|---|---|
committer | Tao Bao | 2017-01-04 00:40:03 -0600 |
commit | 736d59c56754b86135d9156208645b8b1814fba1 (patch) | |
tree | b34e26851aaea9d8958f818d32c7d0e15196fa27 /ui.h | |
parent | 71633ebfb00103dd95a82cd813824dbddd9b905d (diff) | |
download | platform-bootable-recovery-736d59c56754b86135d9156208645b8b1814fba1.tar.gz platform-bootable-recovery-736d59c56754b86135d9156208645b8b1814fba1.tar.xz platform-bootable-recovery-736d59c56754b86135d9156208645b8b1814fba1.zip |
recovery: Fix the broken UI text.
UI text is broken (doesn't show any text during FDR) due to commit
d530449e54bd327e9c26209ffa0490c6508afe6c, which reordered the calls to
RecoveryUI::SetLocale() and RecoveryUI::Init().
Because Init() uses the locale info to load the localized texts (from
images), the locale must be set prior to that via SetLocale(). This CL
refactors Init() to take the locale parameter, and removes the odd
SetLocale() API.
Bug: 34029338
Test: 'Run graphics test' under recovery.
Change-Id: I620394a3d4e3705e9af5a1f6299285d143ae1b01
Diffstat (limited to 'ui.h')
-rw-r--r-- | ui.h | 21 |
1 files changed, 14 insertions, 7 deletions
@@ -21,6 +21,8 @@ | |||
21 | #include <pthread.h> | 21 | #include <pthread.h> |
22 | #include <time.h> | 22 | #include <time.h> |
23 | 23 | ||
24 | #include <string> | ||
25 | |||
24 | // Abstract class for controlling the user interface during recovery. | 26 | // Abstract class for controlling the user interface during recovery. |
25 | class RecoveryUI { | 27 | class RecoveryUI { |
26 | public: | 28 | public: |
@@ -28,14 +30,13 @@ class RecoveryUI { | |||
28 | 30 | ||
29 | virtual ~RecoveryUI() { } | 31 | virtual ~RecoveryUI() { } |
30 | 32 | ||
31 | // Initialize the object; called before anything else. Returns true on success. | 33 | // Initialize the object; called before anything else. UI texts will be |
32 | virtual bool Init(); | 34 | // initialized according to the given locale. Returns true on success. |
35 | virtual bool Init(const std::string& locale); | ||
36 | |||
33 | // Show a stage indicator. Call immediately after Init(). | 37 | // Show a stage indicator. Call immediately after Init(). |
34 | virtual void SetStage(int current, int max) = 0; | 38 | virtual void SetStage(int current, int max) = 0; |
35 | 39 | ||
36 | // After calling Init(), you can tell the UI what locale it is operating in. | ||
37 | virtual void SetLocale(const char* locale) = 0; | ||
38 | |||
39 | // Set the overall recovery state ("background image"). | 40 | // Set the overall recovery state ("background image"). |
40 | enum Icon { NONE, INSTALLING_UPDATE, ERASING, NO_COMMAND, ERROR }; | 41 | enum Icon { NONE, INSTALLING_UPDATE, ERASING, NO_COMMAND, ERROR }; |
41 | virtual void SetBackground(Icon icon) = 0; | 42 | virtual void SetBackground(Icon icon) = 0; |
@@ -122,10 +123,14 @@ class RecoveryUI { | |||
122 | // statements will be displayed. | 123 | // statements will be displayed. |
123 | virtual void EndMenu() = 0; | 124 | virtual void EndMenu() = 0; |
124 | 125 | ||
125 | protected: | 126 | protected: |
126 | void EnqueueKey(int key_code); | 127 | void EnqueueKey(int key_code); |
127 | 128 | ||
128 | private: | 129 | // The locale that's used to show the rendered texts. |
130 | std::string locale_; | ||
131 | bool rtl_locale_; | ||
132 | |||
133 | private: | ||
129 | // Key event input queue | 134 | // Key event input queue |
130 | pthread_mutex_t key_queue_mutex; | 135 | pthread_mutex_t key_queue_mutex; |
131 | pthread_cond_t key_queue_cond; | 136 | pthread_cond_t key_queue_cond; |
@@ -162,6 +167,8 @@ private: | |||
162 | 167 | ||
163 | static void* time_key_helper(void* cookie); | 168 | static void* time_key_helper(void* cookie); |
164 | void time_key(int key_code, int count); | 169 | void time_key(int key_code, int count); |
170 | |||
171 | void SetLocale(const std::string&); | ||
165 | }; | 172 | }; |
166 | 173 | ||
167 | #endif // RECOVERY_UI_H | 174 | #endif // RECOVERY_UI_H |