aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorTao Bao2017-08-02 19:11:04 -0500
committerTao Bao2017-08-10 11:31:17 -0500
commit0470ceea381775b09eee931858c3320be88cc637 (patch)
tree7beb1970589bd76180f0342c3e8ef4323c8341f6 /wear_device.cpp
parent0459799ea83d669df089c670f244771b7be211e3 (diff)
downloadplatform-bootable-recovery-0470ceea381775b09eee931858c3320be88cc637.tar.gz
platform-bootable-recovery-0470ceea381775b09eee931858c3320be88cc637.tar.xz
platform-bootable-recovery-0470ceea381775b09eee931858c3320be88cc637.zip
Allow customizing WearRecoveryUI via Makefile variables.
With the following Makefile variables, we can reduce the work of writing (copy/pasting) device-specific WearRecoveryUI classes. The list of Makefile variables (the ones useful for Wear devices): - TARGET_RECOVERY_UI_MARGIN_HEIGHT (default: 0) - TARGET_RECOVERY_UI_MARGIN_WIDTH (default: 0) Specify the margin space that we don't want to display texts. They replace the former outer_width and outer_height. - TARGET_RECOVERY_UI_TOUCH_LOW_THRESHOLD (default: 50) - TARGET_RECOVERY_UI_TOUCH_HIGH_THRESHOLD (default: 90) Specify the sensitivity of recognizing a swipe. Devices give absolute positions, so for some devices we need to adjust the thresholds. - TARGET_RECOVERY_UI_PROGRESS_BAR_BASELINE Specify the progress bar vertical position, which should be adjusted to the actual height of a device. It replaces the former progress_bar_y. - TARGET_RECOVERY_UI_ANIMATION_FPS (default: 30) Specify the animation FPS if using device-specific animation images. It replaces the former animation_fps. Devices can specify "TARGET_RECOVERY_UI_LIB := librecovery_ui_wear", with optionally defined Makefile vars above, in BoardConfig.mk to customize their WearRecoveryUI. Also remove the obsolete wear_touch.{cpp,h}, which has been merged into ui.cpp in commit 5f8dd9951d986b65d98d6a9ea38003427e9e46df. Bug: 64307776 Test: Change the device BoardConfig.mk and test recovery image. Change-Id: Id0fb2d4e3977ab5ddd31e71f9535470cab70e41b
Diffstat (limited to 'wear_device.cpp')
-rw-r--r--wear_device.cpp23
1 files changed, 23 insertions, 0 deletions
diff --git a/wear_device.cpp b/wear_device.cpp
new file mode 100644
index 00000000..3268130b
--- /dev/null
+++ b/wear_device.cpp
@@ -0,0 +1,23 @@
1/*
2 * Copyright (C) 2017 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#include "device.h"
18#include "wear_ui.h"
19
20Device* make_device() {
21 return new Device(new WearRecoveryUI);
22}
23