diff options
-rw-r--r-- | README.md | 91 |
1 files changed, 91 insertions, 0 deletions
@@ -47,3 +47,94 @@ image under recovery. | |||
47 | 1. `adb sync data` to make sure the test-dir has the images to test. | 47 | 1. `adb sync data` to make sure the test-dir has the images to test. |
48 | 2. The test will automatically pickup and verify all `_text.png` files in | 48 | 2. The test will automatically pickup and verify all `_text.png` files in |
49 | the test dir. | 49 | the test dir. |
50 | |||
51 | Using `adb` under recovery | ||
52 | -------------------------- | ||
53 | |||
54 | When running recovery image from debuggable builds (i.e. `-eng` or `-userdebug` build variants, or | ||
55 | `ro.debuggable=1` in `/prop.default`), `adbd` service is enabled and started by default, which | ||
56 | allows `adb` communication. A device should be listed under `adb devices`, either in `recovery` or | ||
57 | `sideload` state. | ||
58 | |||
59 | $ adb devices | ||
60 | List of devices attached | ||
61 | 1234567890abcdef recovery | ||
62 | |||
63 | Although `/sbin/adbd` shares the same binary between normal boot and recovery images, only a subset | ||
64 | of `adb` commands are meaningful under recovery, such as `adb root`, `adb shell`, `adb push`, `adb | ||
65 | pull` etc. `adb shell` works only after manually mounting `/system` from recovery menu (assuming a | ||
66 | valid system image on device). | ||
67 | |||
68 | ## Troubleshooting | ||
69 | |||
70 | ### `adb devices` doesn't show the device. | ||
71 | |||
72 | $ adb devices | ||
73 | List of devices attached | ||
74 | |||
75 | * Ensure `adbd` is built and running. | ||
76 | |||
77 | By default, `adbd` is always included into recovery image, as `/sbin/adbd`. `init` starts `adbd` | ||
78 | service automatically only in debuggable builds. This behavior is controlled by the recovery | ||
79 | specific `/init.rc`, whose source code is at `bootable/recovery/etc/init.rc`. | ||
80 | |||
81 | The best way to confirm a running `adbd` is by checking the serial output, which shows a service | ||
82 | start log as below. | ||
83 | |||
84 | [ 18.961986] c1 1 init: starting service 'adbd'... | ||
85 | |||
86 | * Ensure USB gadget has been enabled. | ||
87 | |||
88 | If `adbd` service has been started but device not shown under `adb devices`, use `lsusb(8)` (on | ||
89 | host) to check if the device is visible to the host. | ||
90 | |||
91 | `bootable/recovery/etc/init.rc` disables Android USB gadget (via sysfs) as part of the `fs` action | ||
92 | trigger, and will only re-enable it in debuggable builds (the `on property` rule will always run | ||
93 | _after_ `on fs`). | ||
94 | |||
95 | on fs | ||
96 | write /sys/class/android_usb/android0/enable 0 | ||
97 | |||
98 | # Always start adbd on userdebug and eng builds | ||
99 | on property:ro.debuggable=1 | ||
100 | write /sys/class/android_usb/android0/enable 1 | ||
101 | start adbd | ||
102 | |||
103 | If device is using [configfs](https://www.kernel.org/doc/Documentation/usb/gadget_configfs.txt), | ||
104 | check if configfs has been properly set up in init rc scripts. See the [example | ||
105 | configuration](https://android.googlesource.com/device/google/wahoo/+/master/init.recovery.hardware.rc) | ||
106 | for Pixel 2 devices. Note that the flag set via sysfs (i.e. the one above) is no-op when using | ||
107 | configfs. | ||
108 | |||
109 | ### `adb devices` shows the device, but in `unauthorized` state. | ||
110 | |||
111 | $ adb devices | ||
112 | List of devices attached | ||
113 | 1234567890abcdef unauthorized | ||
114 | |||
115 | recovery image doesn't honor the USB debugging toggle and the authorizations added under normal boot | ||
116 | (because such authorization data stays in /data, which recovery doesn't mount), nor does it support | ||
117 | authorizing a host device under recovery. We can use one of the following options instead. | ||
118 | |||
119 | * **Option 1 (Recommended):** Authorize a host device with adb vendor keys. | ||
120 | |||
121 | For debuggable builds, an RSA keypair can be used to authorize a host device that has the private | ||
122 | key. The public key, defined via `PRODUCT_ADB_KEYS`, will be copied to `/adb_keys`. When starting | ||
123 | the host-side `adbd`, make sure the filename (or the directory) of the matching private key has been | ||
124 | added to `$ADB_VENDOR_KEYS`. | ||
125 | |||
126 | $ export ADB_VENDOR_KEYS=/path/to/adb/private/key | ||
127 | $ adb kill-server | ||
128 | $ adb devices | ||
129 | |||
130 | `-user` builds filter out `PRODUCT_ADB_KEYS`, so no `/adb_keys` will be included there. | ||
131 | |||
132 | Note that this mechanism applies to both of normal boot and recovery modes. | ||
133 | |||
134 | * **Option 2:** Allow `adbd` to connect without authentication. | ||
135 | * `adbd` is compiled with `ALLOW_ADBD_NO_AUTH` (only on debuggable builds). | ||
136 | * `ro.adb.secure` has a value of `0`. | ||
137 | |||
138 | Both of the two conditions need to be satisfied. Although `ro.adb.secure` is a runtime property, its | ||
139 | value is set at build time (written into `/prop.default`). It defaults to `1` on `-user` builds, and | ||
140 | `0` for other build variants. The value is overridable via `PRODUCT_DEFAULT_PROPERTY_OVERRIDES`. | ||