aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* adb_install: Stop passing RecoveryUI as a parameter.Tao Bao2017-05-011-3/+1
| | | | | | | | | | | It's already a global declared in common.h which is included by adb_install.cpp. Remove '#include "minadbd/fuse_adb_provider.h"' that's not needed by adb_install.cpp (minadbd takes care of that). Test: mmma bootable/recovery Change-Id: I6d08b7abc706b4b05de2ef46a57ced2204ad297e
* Factor out option variables from int to bool typesTao Bao2015-03-251-1/+1
| | | | Change-Id: Ia897aa43e44d115bde6de91789b35723826ace22
* support "sideload over ADB" modeDoug Zongker2012-01-101-0/+24
Rather than depending on the existence of some place to store a file that is accessible to users on an an unbootable device (eg, a physical sdcard, external USB drive, etc.), add support for sideloading packages sent to the device with adb. This change adds a "minimal adbd" which supports nothing but receiving a package over adb (with the "adb sideload" command) and storing it to a fixed filename in the /tmp ramdisk, from where it can be verified and sideloaded in the usual way. This should be leave available even on locked user-build devices. The user can select "apply package from ADB" from the recovery menu, which starts minimal-adb mode (shutting down any real adbd that may be running). Once minimal-adb has received a package it exits (restarting real adbd if appropriate) and then verification and installation of the received package proceeds. Change-Id: I6fe13161ca064a98d06fa32104e1f432826582f5