aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Auto-detect whether to use the long-press UI.Elliott Hughes2015-04-101-28/+1
| | | | Change-Id: Ie77a5584e301467c6a5e164d2c62d6f036b2c0c0
* Move default implementations into Device.Elliott Hughes2015-04-091-67/+23
| | | | | | | | | | | | The current abstract class was a nice idea but has led to a lot of copy & paste in practice. Right now, no one we know of has any extra menu items, so let's make the default menu available to everyone. (If we assume that someone somewhere really does need custom device-specific menu options, a better API would let them add to our menu rather than replacing it.) Change-Id: I59f6a92f3ecd830c2ce78ce9da19eaaf472c5dfa
* Add "Apply update from sdcard" to default recovery image.Elliott Hughes2015-03-221-17/+23
| | | | | | | | | | | | | | | | | | | | | At the moment, this is the only difference in the sprout recovery image. That's silly. Let's just improve the error handling slightly and always have this option present. Also make the obscure "<3e>" less unclear. Also use "power button" as the default text rather than "enter button", because it's been years since anyone had one of those. (Longer term we should let subclassers tell us the keycode and we translate it to the correct string.) Also move the two "Reboot" options together, put "Power off" at the bottom (and use that terminology, like the real UI, rather than "Power down"), and use capitals throughout. Finally, add a README.md with some useful instructions. Change-Id: I94fb19f73d79c54fed2dda30cefb884426641b5c
* Make /cache/recovery/last_log available in recoveryNick Kralevich2014-10-221-0/+2
| | | | | | | | | | Create a new recovery UI option to allow the user to view /cache/recovery/last_log for their device. This gives enhanced debugging information which may be necessary when a failed OTA occurs. Bug: 18094012 Change-Id: Ic3228de96e9bfc2a0141c7aab4ce392a38140cf3
* add reboot-to-bootloader and power down options to recovery menuDoug Zongker2014-04-011-0/+4
| | | | | | Useful when debugging or developing for recovery. Change-Id: Ic3ab42d5e848ad3488f1c575339b55e45c8a024b
* remove DefaultDevice's UI subclassDoug Zongker2014-04-011-11/+2
| | | | | | | | | | RecoveryUI (which is the superclass of ScreenRecoveryUI), provides a basic CheckKey method that is useful for devices that have KEY_POWER, KEY_VOLUMEUP, and KEY_VOLUMEDOWN. Stop overriding it with a less featureful method; with this no recovery UI customization is needed for most handheld devices (phones, tablets, etc.). Change-Id: I7d57cfaaef79afea8af4fc3dbc570afc61aeb5bc
* support "sideload over ADB" modeDoug Zongker2012-01-101-6/+4
| | | | | | | | | | | | | | | | | | | | | Rather than depending on the existence of some place to store a file that is accessible to users on an an unbootable device (eg, a physical sdcard, external USB drive, etc.), add support for sideloading packages sent to the device with adb. This change adds a "minimal adbd" which supports nothing but receiving a package over adb (with the "adb sideload" command) and storing it to a fixed filename in the /tmp ramdisk, from where it can be verified and sideloaded in the usual way. This should be leave available even on locked user-build devices. The user can select "apply package from ADB" from the recovery menu, which starts minimal-adb mode (shutting down any real adbd that may be running). Once minimal-adb has received a package it exits (restarting real adbd if appropriate) and then verification and installation of the received package proceeds. Change-Id: I6fe13161ca064a98d06fa32104e1f432826582f5
* C++ class for device-specific codeDoug Zongker2011-10-311-0/+92
Replace the device-specific functions with a class. Move some of the key handling (for log visibility toggling and rebooting) into the UI class. Fix up the key handling so there is less crosstalk between the immediate keys and the queued keys (an increasing annoyance on button-limited devices). Change-Id: I698f6fd21c67a1e55429312a0484b6c393cad46f