aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Avoid overwrite of the error message in AbortFnTianjie Xu2018-01-291-8/+11
| | | | | | | | | | | | | The AbortFn() used to overwrite the error message, hiding the real failure reported in ErrorAbort(). And we will miss the failure in the script patterns like 'blockimageupdate() || abort()' We will ensure there's one line break at the end of ErrorAbort's error message; and append to the existing error message when calling abort(). Test: Message from ErrorAbort shows up in the log Change-Id: I3aebd06629c5129330250c7fe5e8cdead2ae85bc
* edify: Export the header and move to Soong.Tao Bao2017-10-091-1/+1
| | | | | | | | Also make matching changes to applypatch modules which include edify/expr.h. Test: mmma bootable/recovery Change-Id: Ia72be3caa010d7f56a70add2da345e631b306378
* Revert "Revert "Move error_code.h into otautil.""Tao Bao2017-10-091-1/+1
| | | | | | | | | | | | | | | | This reverts commit 26436d6d6010d5323349af7e119ff8f34f85c40c to re-land "Move error_code.h into otautil.". This way it stops requiring relative path ".." in LOCAL_C_INCLUDES (uncrypt and edify). Soong doesn't accept non-local ".." in "local_include_dirs". This CL needs to land with device-specific module changes (e.g. adding the dependency on libotautil). Test: lunch aosp_{angler,bullhead,dragon,fugu,sailfish}-userdebug; mmma bootable/recovery Change-Id: If193241801af2dae73eccd31ce57cd2b81c9fd96
* Don't include "error_code.h" in edify/expr.h.Tao Bao2017-10-051-5/+4
| | | | | | | | | | | | | Use forward declartion to avoid pull in the module that contains error_code.h (trying to move it into libotautil). Otherwise all the modules that include "edify/expr.h" need to depend on the module that exports error_code.h. .cpp sources should include "error_code.h" explicitly to use the enums. Test: lunch aosp_{angler,bullhead,dragon,fugu,sailfish}-userdebug; mmma bootable/recovery Change-Id: Ic82db2746c7deb866e8cdfb3c57e0b1ecc71c4dc
* Don't fail ReadArgs if length to parse is 0Tianjie Xu2017-03-231-1/+1
| | | | | Test: recovery component tests pass Change-Id: I0946ba498d845ec552ae7e4c79dc94618b2fdf6d
* Remove malloc in edify functionsTianjie Xu2017-03-221-44/+75
| | | | | | | | And switch them to std::vector & std::unique_ptr Bug: 32117870 Test: recovery tests passed on sailfish Change-Id: I5a45951c4bdf895be311d6d760e52e7a1b0798c3
* Cleanup ReadArgs & ReadValueArgs usageTianjie Xu2016-11-011-111/+12
| | | | | | | | ReadArgs will switch to using std::string and std::unique_ptr. Also cleanup the callers. Test: mma & component test passed. Change-Id: I4724406ae6c0c134a27bbd1cdd24ad5d343b2a3b
* Change StringValue to use std::stringTianjie Xu2016-10-141-156/+172
| | | | | | | | | | | Changing the field of 'Value' in edify to std::string from char*. Meanwhile cleaning up the users of 'Value' and switching them to cpp style. Test: compontent tests passed. Bug: 31713288 Change-Id: Iec5a7d601b1e4ca40935bf1c70d325dafecec235
* edify: Some clean-ups to libedify.Tao Bao2016-10-131-52/+13
| | | | | | | | | | | | - Remove dead declarations in expr.h: SetError(), GetError(), ClearError(). - Remove the declaration of Build() out of expr.h. - Use std::unordered_map to implement RegisterFunction() and FindFunction(); kill FinishRegistration(). - Add a testcase for calling unknown functions. Test: mmma bootable/recovery; recovery_component_test passes. Change-Id: I9af6825ae677f92b22d716a4a5682f58522af03b
* edify: Move State.script and State.errmsg to std::string.Tao Bao2016-10-041-26/+13
| | | | | | | | | | | This way we kill a few strdup() and free() calls. Test: 1. recovery_component_test still passes; 2. Applying an update with the new updater works; 3. The error code in a script with abort("E310: xyz") is recorded into last_install correctly. Change-Id: Ibda4da5937346e058a0d7cc81764d6f02920010a
* resolve merge conflicts of 50f6417 to nyc-dev-plus-aospTianjie Xu2016-05-231-10/+29
|\ | | | | | | Change-Id: I42c127f7946e678acf6596f6352f090abc0ca019
| * Allow recovery to return error codesTianjie Xu2016-05-201-10/+29
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Write error code, cause code, and retry count into last_install. So we can have more information about the reason of a failed OTA. Example of new last_install: @/cache/recovery/block.map package name 0 install result retry: 1 retry count (new) error: 30 error code (new) cause: 12 error cause (new) Details in: go/android-ota-errorcode Bug: 28471955 Change-Id: I00e7153c821e7355c1be81a86c7f228108f3dc37
* | Fix google-runtime-int warnings.Chih-Hung Hsieh2016-04-181-3/+4
|/ | | | | Bug: 28220065 Change-Id: Ida199c66692a1638be6990d583d2ed42583fb592
* edify: Switch to C++.Tao Bao2015-08-201-0/+507
Change-Id: I71aede6e29af1dc4bb858a62016c8035db5d3452