aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* refactor applypatch and friendsDoug Zongker2010-02-221-0/+2
| | | | | | | | | | | | | | | | | | | Change the applypatch function to take meaningful arguments instead of argc and argv. Move all the parsing of arguments into main.c (for the standalone binary) and into install.c (for the updater function). applypatch() takes patches as Value objects, so we can pass in blobs extracted from the package without ever writing them to temp files. The patching code is changed to read the patch from memory instead of a file. A bunch of compiler warnings (mostly about signed vs unsigned types) are fixed. Support for the IMGDIFF1 format is dropped. (We've been generating IMGDIFF2 packages for some time now.) Change-Id: I217563c500012750f27110db821928a06211323f
* fixes to edify and updater scriptDoug Zongker2009-06-121-0/+36
A few more changes to edify: - fix write_raw_image(); my last change neglected to close the write context, so the written image was corrupt. - each expression tracks the span of the source code from which it was compiled, so that assert()'s error message can include the source of the expression that failed. - the 'cookie' argument to each Function is replaced with a State object, which contains the cookie, the source script (for use with the above spans), and the current error message (replacing the global variables that were used for this purpose). - in the recovery image, a new command "ui_print" can be sent back through the command pipe to cause text to appear on the screen. Add a new ui_print() function to print things from scripts. Rename existing "print" function to "stdout".