aboutsummaryrefslogtreecommitdiffstats
path: root/tools
Commit message (Collapse)AuthorAgeFilesLines
* Set LOCAL_SDK_VERSION where possible.Anton Hansson2018-02-211-0/+1
| | | | | | | | | | | | | | | | This change sets LOCAL_SDK_VERSION for all packages where this is possible without breaking the build, and LOCAL_PRIVATE_PLATFORM_APIS := true otherwise. Setting one of these two will be made required soon, and this is a change in preparation for that. Not setting LOCAL_SDK_VERSION makes the app implicitly depend on the bootclasspath, which is often not required. This change effectively makes depending on private apis opt-in rather than opt-out. Test: make relevant packages Bug: 73535841 Change-Id: I82fee834c5d92e699e9571933faded11c6d4596e
* Import translations. DO NOT MERGEBill Yi2017-10-204-9/+9
| | | | | | | | Auto-generated-cl: translation import Exempt-From-Owner-Approval: translation import Bug: 68003463 Change-Id: Iae8fc3afc1453b6b609dae2bbff08231d00735e7
* Import translations. DO NOT MERGEBill Yi2017-02-271-1/+1
| | | | | Change-Id: I90d94072de955eca8ea38762faa5d3e5a4f295db Auto-generated-cl: translation import
* Merge "Restore the max width for recovery background texts" am: c1df344381 ↵Tianjie Xu2017-01-231-0/+3
|\ | | | | | | | | | | | | | | am: b037cff12e am: f1a371b1b0 am: 281fa9fd30 Change-Id: I109593352d526941895eafea41f87a49561f8fd7
| * Merge "Restore the max width for recovery background texts" am: c1df344381Tianjie Xu2017-01-231-0/+3
| |\ | | | | | | | | | | | | | | | am: b037cff12e Change-Id: I177c4d5edcf8e0ee9874bd1627d0ae12a43ae506
| | * Restore the max width for recovery background textsTianjie Xu2017-01-221-0/+3
| | | | | | | | | | | | | | | | | | | | | | | | Restore the max width to 900px for xxhdpi and 1200px for xxxhdpi Bug: 34541299 Test: Checked width and images passed recovery_manual_test Change-Id: If0fd51f93cfb3f965d4e9e69be5626eba89eb857
* | | Merge "Update background text images in recovery" am: f0af02fea6 am: ↵Tianjie Xu2017-01-131-2/+20
|\| | | | | | | | | | | | | | | | | | | | | | | 19e4f627d8 am: e05674f93e am: f92c313723 Change-Id: I36ab3a5d46758ef45854efd16dcf8285166d1dc4
| * | Merge "Update background text images in recovery" am: f0af02fea6Tianjie Xu2017-01-131-2/+20
| |\| | | | | | | | | | | | | | | | am: 19e4f627d8 Change-Id: Ic16111cc970780090827f3e2851e4df874a5d8cf
| | * Update background text images in recoveryTianjie Xu2017-01-061-2/+20
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Locale texts are missing in the recovery log due to an extra empty locale chunk in the png file. Fix the bug in the app and regenerate all the background texts and compress the file with pngcrush + zopflipng. Bug: 34054052 Test: Locale texts logged successfully on angler Change-Id: I89f823a53c1eb69756183e8e11113216d093304f
| | * Import translations. DO NOT MERGEBill Yi2016-11-2078-312/+390
| |/ | | | | | | | | | | | | Auto-generated-cl: translation import Bug: 32177112 Change-Id: I4d68cd0c69b40d1765cd74dfa730f56be01b5b23
* | Rename language+country resources to just languageRoozbeh Pournader2017-01-1030-0/+0
| | | | | | | | | | | | Bug: 26496609 Test: none Change-Id: I6467c8496478402614fcdb46c5399dfa28162201
* | Revert "Import translations. DO NOT MERGE"Bill Yi2016-12-0581-0/+729
| | | | | | | | | | | | This reverts commit 6ecd63e459f7e9eab062c172122e319aff8b7042. Change-Id: I66c34fc72c1e8f6a0c11e12fd7e21864f4437977
* | Import translations. DO NOT MERGEBill Yi2016-12-0381-729/+0
| | | | | | | | | | Change-Id: Ibe3698aabd36cca6e053ca099b87f09e8ad05c93 Auto-generated-cl: translation import
* | Merge "Further compress the text images with zopflipng" am: 61240f88ea am: ↵Tianjie Xu2016-08-031-0/+2
|\| | | | | | | | | | | | | | | 3e244dc301 am: 5a84cecd26 am: 8b36965175 Change-Id: I6aad408e27e8661a83c6d985d080c0ae8637eec9
| * Merge "Further compress the text images with zopflipng" am: 61240f88eaTianjie Xu2016-08-031-0/+2
| |\ | | | | | | | | | | | | | | | am: 3e244dc301 Change-Id: Id651a94190d91c508b55d3745816253160b84284
| | * Merge "Further compress the text images with zopflipng"Tianjie Xu2016-08-031-0/+2
| | |\ | | | | | | | | | | | | | | | | | | | | am: 61240f88ea Change-Id: Ib3b28e84ee331a0e9d613d3761ff4d657c23088d
| | | * Further compress the text images with zopflipngTianjie Xu2016-08-031-0/+2
| | | | | | | | | | | | | | | | | | | | | | | | Bug:30415666 Test: Graphic tests pass on angler with new image files Change-Id: I8716f53cb2f9fc6598fdc84f84e9626994faaa5e
* | | | Merge \\\\"Add docs on regeneration background text image\\\\" am: ↵Tianjie Xu2016-07-283-0/+33
|\| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | 5aa2e104c0 am: b02a58740e am: 698f75467a am: 0df6011d0f Change-Id: I9bf3d8a5357811700e7e09aec146eaf1969f6eb9
| * | | Merge \\"Add docs on regeneration background text image\\" am: 5aa2e104c0Tianjie Xu2016-07-283-0/+33
| |\| | | | | | | | | | | | | | | | | | | | | | am: b02a58740e Change-Id: Ib15f443946a97eeb6609b0aab9b91bcd3ca91d4c
| | * | Merge \"Add docs on regeneration background text image\"Tianjie Xu2016-07-283-0/+33
| | |\| | | | | | | | | | | | | | | | | | | | | am: 5aa2e104c0 Change-Id: I565fa63de18e0c806f2452c009d97c5ad4ebebc3
| | | * Add docs on regeneration background text imageTianjie Xu2016-07-283-0/+33
| | | | | | | | | | | | | | | | | | | | | | | | | | | | Also add a missing string in the recovery_l10n APP. Bug: 30415666 Change-Id: Ice2a9f7cad4ebe332b427bc0c7a9adccb6cf3af3
| | | * Add string for Installing_security_updateTianjie Xu2016-03-291-0/+4
| | | | | | | | | | | | | | | | | | | | | | | | Bug: 27837319 Change-Id: I037158697a294c3e03f186f3b4207ea700321a8a (cherry picked from commit 1ee0ff3d78c5143d4e3307bc44e3c27792e72d1e)
| | * | Import translations. DO NOT MERGEBill Yi2016-06-3078-312/+390
| |/ / | | | | | | | | | | | | | | | | | | Auto-generated-cl: translation import Bug: 29390361 Change-Id: Ie1d01357ef53bd977da8188825dd744801ae58ad
* | | Import translations. DO NOT MERGEBill Yi2016-04-263-11/+7
| | | | | | | | | | | | | | | Change-Id: Ic9a498dd7367a61fc2d380dc6eeeea0c4cafc8bf Auto-generated-cl: translation import
* | | Import translations. DO NOT MERGEBill Yi2016-04-2481-324/+328
| | | | | | | | | | | | | | | Change-Id: Ice2fc6151b69ad3a4029184a5afa6020085219f2 Auto-generated-cl: translation import
* | | Merge "Merge "Remove trailing punctuation from recovery strings." into ↵Elliott Hughes2016-04-201-4/+4
|\| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | nyc-dev am: 4eec72d am: c15177b" into nyc-mr1-dev-plus-aosp am: f39da4f * commit 'f39da4fc1b84c594d95b241d75eec1b25f7d4480': Remove trailing punctuation from recovery strings. Change-Id: I8858b1097b301b612494801cce4c2ad3274823dc
| * | Merge "Remove trailing punctuation from recovery strings." into nyc-devElliott Hughes2016-04-201-4/+4
| |\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | am: 4eec72d * commit '4eec72d2cf8c1be0068feffc804035dab756c78d': Remove trailing punctuation from recovery strings. Change-Id: I60cf10d7748227d81f60fc9d1fe18cdb01f8b2f3
| | * | Remove trailing punctuation from recovery strings.Elliott Hughes2016-04-191-4/+4
| | | | | | | | | | | | | | | | | | | | Bug: http://b/26548285 Change-Id: I235c620532e1759bfc76a4486409a4404f1c8c6a
* | | | Explicitly set the font face and color. am: 70ae70bElliott Hughes2016-04-152-7/+6
|\| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | am: 6fa5fa9 * commit '6fa5fa91bf1439e6c5070f3aee9b447f995882c1': Explicitly set the font face and color. Change-Id: I1b2079d35cb7165db738a8d9ca442fa96729979e
| * | | Explicitly set the font face and color.Elliott Hughes2016-04-152-7/+6
| |\| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | am: 70ae70b * commit '70ae70b81e452ce8a85dfbb184786c02a9072c23': Explicitly set the font face and color. Change-Id: I94011b0f4df228e6cdfe4c095542839abb689a74
| | * | Explicitly set the font face and color.Elliott Hughes2016-04-142-7/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This matches what the UI folks asked us to use. Also fix the locale parsing code. Bug: http://b/27837319 Bug: http://b/22465983 Bug: http://b/26548285 Change-Id: I316a6e1f44855313dd983950abf21b543be7ffc0
| | * | Import translations. DO NOT MERGEBill Yi2016-04-052-2/+2
| | | | | | | | | | | | | | | | | | | | Change-Id: Ic643d0e2d39e45d772ffb25001de45afdf923579 Auto-generated-cl: translation import
| | * | Import translations. DO NOT MERGEBill Yi2016-04-0481-229/+148
| | | | | | | | | | | | | | | | | | | | Change-Id: Ia0012b89f00c65ec6056d29612748e60564bab32 Auto-generated-cl: translation import
| | * | Import translations. DO NOT MERGEBill Yi2016-03-3181-312/+498
| | | | | | | | | | | | | | | | | | | | Change-Id: Id992a2cff5d431b5862f7c27f3823dbffe52f5c7 Auto-generated-cl: translation import
* | | | Import translations. DO NOT MERGEBill Yi2016-04-061-1/+1
| | | | | | | | | | | | | | | | | | | | Change-Id: Id4a5f32acb01776c95b092cc6e883036812836a9 Auto-generated-cl: translation import
* | | | Import translations. DO NOT MERGEBill Yi2016-04-051-1/+1
| | | | | | | | | | | | | | | | | | | | Change-Id: Ib4ebc02261abc4610947ab54f5e53f9958190e27 Auto-generated-cl: translation import
* | | | Import translations. DO NOT MERGEBill Yi2016-04-0481-229/+148
| | | | | | | | | | | | | | | | | | | | Change-Id: I5280c977c6c5099c681fa5069bdde9b5426d5949 Auto-generated-cl: translation import
* | | | Import translations. DO NOT MERGEBill Yi2016-03-3081-312/+498
|/ / / | | | | | | | | | | | | Change-Id: I96a3ebec0ab7b7400bcf8ffd2a899d291d8a4579 Auto-generated-cl: translation import
* | / Add string for Installing_security_updateTianjie Xu2016-03-291-0/+4
|\| | | |/ |/| | | | | | | | | | | | | am: 1ee0ff3 * commit '1ee0ff3d78c5143d4e3307bc44e3c27792e72d1e': Add string for Installing_security_update Change-Id: Ied2a3b07fbf8548688759727da527fc7a994d5a0
| * Add string for Installing_security_updateTianjie Xu2016-03-281-0/+4
| | | | | | | | | | Bug: 27837319 Change-Id: I037158697a294c3e03f186f3b4207ea700321a8a
| * Move recovery_l10n here from development/tools.Elliott Hughes2016-03-2683-0/+1038
| | | | | | | | | | | | | | | | Bug: http://b/27837319 (cherry picked from commit 3d0153a807042dd1bdb7e9fd81d16429a205d9ce) Change-Id: Iec2cd10fa77ed1881d55ac4e0ab48e45172f0cf7
* | Merge "Move recovery_l10n here from development/tools."Elliott Hughes2016-03-2683-0/+1038
|\ \
| * | Move recovery_l10n here from development/tools.Elliott Hughes2016-03-2683-0/+1038
| | | | | | | | | | | | | | | Bug: http://b/27837319 Change-Id: I116fc13ae108a59b657f5c9f7efe971de72ac743
* | | Remove dead tools.Elliott Hughes2016-03-224-398/+0
|/ / | | | | | | | | | | None of these have been touched since cupcake, except to keep them building. Change-Id: I5ed13849e6842e755c62da05f1a8a6da2583b1ee
* | Remove dumpkey build guards after completing code move.Mattias Nissler2016-02-261-10/+0
| | | | | | | | | | Bug: 27326256 Change-Id: Ia713b23e3c898c1f10af7c61ea67f34601fdcbe3
* | Move dumpkey tool to the recovery repo.Mattias Nissler2016-02-243-0/+303
|/ | | | | | | | | | The dumpkey tool is used to dump encryption keys in a custom format used by the recovery code. Nobody else uses this format AFAICT, so it's more appropriate to keep the code of the tool alongside the recovery code instead of next to mincrypt. BUG:27326256 Change-Id: I30176845617972be1d6e46e9a9218e161fbf0680
* Check all lseek calls succeed.Elliott Hughes2015-04-291-1/+1
| | | | | | | Also add missing TEMP_FAILURE_RETRYs on read, write, and lseek. Bug: http://b/20625546 Change-Id: I03b198e11c1921b35518ee2dd005a7cfcf4fd94b
* Add missing includes.Elliott Hughes2015-01-291-0/+1
| | | | Change-Id: I06ea08400efa511e627be37a4fd70fbdfadea2e6
* Recovery 64-bit compile issuesMark Salyzyn2014-03-141-2/+2
| | | | Change-Id: I92d5abd1a628feab3b0246924fab7f97ba3b9d34
* Fixed unused param warnings for check-lost+foundEdwin Vane2012-08-211-1/+1
| | | | | | | | A few simple warnings fixed to produce a clean clang build. Change-Id: I9484f860903a80e4c91e204e7e6738145535f642 Author: Edwin Vane <edwin.vane@intel.com> Reviewed-by: Ariel J Bernal <ariel.j.bernal@intel.com>