From eea3af3f911d36ac1a82a9fb95d24912cc07e3b1 Mon Sep 17 00:00:00 2001 From: Tao Bao Date: Fri, 11 Aug 2017 13:50:24 -0700 Subject: wear_ui: Expose menu_unusable_rows via Makefile var. This variable is useful on small screens (e.g. on watches) to handle long menus. We should have better way to handle this value smartly. Prior to that, expose the value to be overridable by using the generic wearable UI module (librecovery_ui_wear). Bug: 64307776 Test: Define the variable, build and boot into recovery image and check the UI menu. Change-Id: I5d7a6baa8bb4cc852bfcc2a7b3cc9686c1c8817e --- wear_ui.cpp | 7 ++++--- 1 file changed, 4 insertions(+), 3 deletions(-) (limited to 'wear_ui.cpp') diff --git a/wear_ui.cpp b/wear_ui.cpp index b8801a0b..169ef20e 100644 --- a/wear_ui.cpp +++ b/wear_ui.cpp @@ -51,8 +51,9 @@ static double now() { } WearRecoveryUI::WearRecoveryUI() - : kProgressBarBaseline(RECOVERY_UI_PROGRESS_BAR_BASELINE), menu_unusable_rows(9) { - // TODO: menu_unusable_rows should be computed based on the lines in draw_screen_locked(). + : kProgressBarBaseline(RECOVERY_UI_PROGRESS_BAR_BASELINE), + kMenuUnusableRows(RECOVERY_UI_MENU_UNUSABLE_ROWS) { + // TODO: kMenuUnusableRows should be computed based on the lines in draw_screen_locked(). // TODO: The following three variables are likely not needed. The first two are detected // automatically in ScreenRecoveryUI::LoadAnimation(), based on the actual files seen on device. @@ -268,7 +269,7 @@ void WearRecoveryUI::StartMenu(const char* const* headers, const char* const* it show_menu = true; menu_sel = initial_selection; menu_start = 0; - menu_end = visible_text_rows - 1 - menu_unusable_rows; + menu_end = visible_text_rows - 1 - kMenuUnusableRows; if (menu_items <= menu_end) menu_end = menu_items; update_screen_locked(); } -- cgit v1.2.3-54-g00ecf