/* * Copyright (C) 2012 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include #include #include #include #include #include #include #include #include #include #include "ui.h" #include "install.h" #include "common.h" #include "adb_install.h" #include "minadbd/fuse_adb_provider.h" #include "fuse_sideload.h" #include static void set_usb_driver(RecoveryUI* ui, bool enabled) { int fd = open("/sys/class/android_usb/android0/enable", O_WRONLY); if (fd < 0) { ui->Print("failed to open driver control: %s\n", strerror(errno)); return; } if (TEMP_FAILURE_RETRY(write(fd, enabled ? "1" : "0", 1)) == -1) { ui->Print("failed to set driver control: %s\n", strerror(errno)); } if (close(fd) < 0) { ui->Print("failed to close driver control: %s\n", strerror(errno)); } } static void stop_adbd(RecoveryUI* ui) { ui->Print("Stopping adbd...\n"); android::base::SetProperty("ctl.stop", "adbd"); set_usb_driver(ui, false); } static void maybe_restart_adbd(RecoveryUI* ui) { if (is_ro_debuggable()) { ui->Print("Restarting adbd...\n"); set_usb_driver(ui, true); android::base::SetProperty("ctl.start", "adbd"); } } // How long (in seconds) we wait for the host to start sending us a // package, before timing out. #define ADB_INSTALL_TIMEOUT 300 int apply_from_adb(RecoveryUI* ui, bool* wipe_cache, const char* install_file) { modified_flash = true; stop_adbd(ui); set_usb_driver(ui, true); ui->Print("\n\nNow send the package you want to apply\n" "to the device with \"adb sideload \"...\n"); pid_t child; if ((child = fork()) == 0) { execl("/sbin/recovery", "recovery", "--adbd", NULL); _exit(-1); } // FUSE_SIDELOAD_HOST_PATHNAME will start to exist once the host // connects and starts serving a package. Poll for its // appearance. (Note that inotify doesn't work with FUSE.) int result = INSTALL_ERROR; int status; bool waited = false; struct stat st; for (int i = 0; i < ADB_INSTALL_TIMEOUT; ++i) { if (waitpid(child, &status, WNOHANG) != 0) { result = INSTALL_ERROR; waited = true; break; } if (stat(FUSE_SIDELOAD_HOST_PATHNAME, &st) != 0) { if (errno == ENOENT && i < ADB_INSTALL_TIMEOUT-1) { sleep(1); continue; } else { ui->Print("\nTimed out waiting for package.\n\n"); result = INSTALL_ERROR; kill(child, SIGKILL); break; } } result = install_package(FUSE_SIDELOAD_HOST_PATHNAME, wipe_cache, install_file, false, 0); break; } if (!waited) { // Calling stat() on this magic filename signals the minadbd // subprocess to shut down. stat(FUSE_SIDELOAD_HOST_EXIT_PATHNAME, &st); // TODO(dougz): there should be a way to cancel waiting for a // package (by pushing some button combo on the device). For now // you just have to 'adb sideload' a file that's not a valid // package, like "/dev/null". waitpid(child, &status, 0); } if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) { if (WEXITSTATUS(status) == 3) { ui->Print("\nYou need adb 1.0.32 or newer to sideload\nto this device.\n\n"); } else if (!WIFSIGNALED(status)) { ui->Print("\n(adbd status %d)\n", WEXITSTATUS(status)); } } set_usb_driver(ui, false); maybe_restart_adbd(ui); return result; }