/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef RECOVERY_COMMON_H #define RECOVERY_COMMON_H #include #include #include // Not using the command-line defined macro here because this header could be included by // device-specific recovery libraries. We static assert the value consistency in recovery.cpp. static constexpr int kRecoveryApiVersion = 3; class RecoveryUI; extern RecoveryUI* ui; extern bool modified_flash; // The current stage, e.g. "1/2". extern std::string stage; // The reason argument provided in "--reason=". extern const char* reason; // fopen a file, mounting volumes and making parent dirs as necessary. FILE* fopen_path(const char *path, const char *mode); void ui_print(const char* format, ...); bool is_ro_debuggable(); bool reboot(const std::string& command); #endif // RECOVERY_COMMON_H