/* * Copyright (C) 2011 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef _RECOVERY_DEVICE_H #define _RECOVERY_DEVICE_H #include "ui.h" class Device { public: explicit Device(RecoveryUI* ui) : ui_(ui) {} virtual ~Device() {} // Called to obtain the UI object that should be used to display the recovery user interface for // this device. You should not have called Init() on the UI object already, the caller will do // that after this method returns. virtual RecoveryUI* GetUI() { return ui_; } // Called when recovery starts up (after the UI has been obtained and initialized and after the // arguments have been parsed, but before anything else). virtual void StartRecovery() {}; // Called from the main thread when recovery is at the main menu and waiting for input, and a key // is pressed. (Note that "at" the main menu does not necessarily mean the menu is visible; // recovery will be at the main menu with it invisible after an unsuccessful operation [ie OTA // package failure], or if recovery is started with no command.) // // 'key' is the code of the key just pressed. (You can call IsKeyPressed() on the RecoveryUI // object you returned from GetUI if you want to find out if other keys are held down.) // // 'visible' is true if the menu is visible. // // Returns one of the defined constants below in order to: // // - move the menu highlight (kHighlight{Up,Down}) // - invoke the highlighted item (kInvokeItem) // - do nothing (kNoAction) // - invoke a specific action (a menu position: any non-negative number) virtual int HandleMenuKey(int key, bool visible); enum BuiltinAction { NO_ACTION = 0, REBOOT = 1, APPLY_SDCARD = 2, // APPLY_CACHE was 3. APPLY_ADB_SIDELOAD = 4, WIPE_DATA = 5, WIPE_CACHE = 6, REBOOT_BOOTLOADER = 7, SHUTDOWN = 8, VIEW_RECOVERY_LOGS = 9, MOUNT_SYSTEM = 10, RUN_GRAPHICS_TEST = 11, RUN_LOCALE_TEST = 12, }; // Return the list of menu items (an array of strings, NULL-terminated). The menu_position passed // to InvokeMenuItem will correspond to the indexes into this array. virtual const char* const* GetMenuItems(); // Perform a recovery action selected from the menu. 'menu_position' will be the item number of // the selected menu item, or a non-negative number returned from HandleMenuKey(). The menu will // be hidden when this is called; implementations can call ui_print() to print information to the // screen. If the menu position is one of the builtin actions, you can just return the // corresponding enum value. If it is an action specific to your device, you actually perform it // here and return NO_ACTION. virtual BuiltinAction InvokeMenuItem(int menu_position); static const int kNoAction = -1; static const int kHighlightUp = -2; static const int kHighlightDown = -3; static const int kInvokeItem = -4; // Called before and after we do a wipe data/factory reset operation, either via a reboot from the // main system with the --wipe_data flag, or when the user boots into recovery image manually and // selects the option from the menu, to perform whatever device-specific wiping actions as needed. // Returns true on success; returning false from PreWipeData will prevent the regular wipe, and // returning false from PostWipeData will cause the wipe to be considered a failure. virtual bool PreWipeData() { return true; } virtual bool PostWipeData() { return true; } private: RecoveryUI* ui_; }; // The device-specific library must define this function (or the default one will be used, if there // is no device-specific library). It returns the Device object that recovery should use. Device* make_device(); #endif // _DEVICE_H