/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "common.h" #include "error_code.h" #include "install.h" #include "minui/minui.h" #include "otautil/SysUtil.h" #include "roots.h" #include "ui.h" #include "verifier.h" extern RecoveryUI* ui; #define ASSUMED_UPDATE_BINARY_NAME "META-INF/com/google/android/update-binary" #define PUBLIC_KEYS_FILE "/res/keys" static constexpr const char* METADATA_PATH = "META-INF/com/android/metadata"; static constexpr const char* UNCRYPT_STATUS = "/cache/recovery/uncrypt_status"; // Default allocation of progress bar segments to operations static const int VERIFICATION_PROGRESS_TIME = 60; static const float VERIFICATION_PROGRESS_FRACTION = 0.25; static const float DEFAULT_FILES_PROGRESS_FRACTION = 0.4; static const float DEFAULT_IMAGE_PROGRESS_FRACTION = 0.1; // This function parses and returns the build.version.incremental static int parse_build_number(const std::string& str) { size_t pos = str.find('='); if (pos != std::string::npos) { std::string num_string = android::base::Trim(str.substr(pos+1)); int build_number; if (android::base::ParseInt(num_string.c_str(), &build_number, 0)) { return build_number; } } LOG(ERROR) << "Failed to parse build number in " << str; return -1; } bool read_metadata_from_package(ZipArchiveHandle zip, std::string* meta_data) { ZipString metadata_path(METADATA_PATH); ZipEntry meta_entry; if (meta_data == nullptr) { LOG(ERROR) << "string* meta_data can't be nullptr"; return false; } if (FindEntry(zip, metadata_path, &meta_entry) != 0) { LOG(ERROR) << "Failed to find " << METADATA_PATH << " in update package"; return false; } meta_data->resize(meta_entry.uncompressed_length, '\0'); if (ExtractToMemory(zip, &meta_entry, reinterpret_cast(&(*meta_data)[0]), meta_entry.uncompressed_length) != 0) { LOG(ERROR) << "Failed to read metadata in update package"; return false; } return true; } // Read the build.version.incremental of src/tgt from the metadata and log it to last_install. static void read_source_target_build(ZipArchiveHandle zip, std::vector& log_buffer) { std::string meta_data; if (!read_metadata_from_package(zip, &meta_data)) { return; } // Examples of the pre-build and post-build strings in metadata: // pre-build-incremental=2943039 // post-build-incremental=2951741 std::vector lines = android::base::Split(meta_data, "\n"); for (const std::string& line : lines) { std::string str = android::base::Trim(line); if (android::base::StartsWith(str, "pre-build-incremental")){ int source_build = parse_build_number(str); if (source_build != -1) { log_buffer.push_back(android::base::StringPrintf("source_build: %d", source_build)); } } else if (android::base::StartsWith(str, "post-build-incremental")) { int target_build = parse_build_number(str); if (target_build != -1) { log_buffer.push_back(android::base::StringPrintf("target_build: %d", target_build)); } } } } // If the package contains an update binary, extract it and run it. static int try_update_binary(const char* path, ZipArchiveHandle zip, bool* wipe_cache, std::vector& log_buffer, int retry_count) { read_source_target_build(zip, log_buffer); ZipString binary_name(ASSUMED_UPDATE_BINARY_NAME); ZipEntry binary_entry; if (FindEntry(zip, binary_name, &binary_entry) != 0) { return INSTALL_CORRUPT; } const char* binary = "/tmp/update_binary"; unlink(binary); int fd = creat(binary, 0755); if (fd < 0) { PLOG(ERROR) << "Can't make " << binary; return INSTALL_ERROR; } int error = ExtractEntryToFile(zip, &binary_entry, fd); close(fd); if (error != 0) { LOG(ERROR) << "Can't copy " << ASSUMED_UPDATE_BINARY_NAME << " : " << ErrorCodeString(error); return INSTALL_ERROR; } int pipefd[2]; pipe(pipefd); // When executing the update binary contained in the package, the // arguments passed are: // // - the version number for this interface // // - an fd to which the program can write in order to update the // progress bar. The program can write single-line commands: // // progress // fill up the next part of of the progress bar // over seconds. If is zero, use // set_progress commands to manually control the // progress of this segment of the bar. // // set_progress // should be between 0.0 and 1.0; sets the // progress bar within the segment defined by the most // recent progress command. // // firmware <"hboot"|"radio"> // arrange to install the contents of in the // given partition on reboot. // // (API v2: may start with "PACKAGE:" to // indicate taking a file from the OTA package.) // // (API v3: this command no longer exists.) // // ui_print // display on the screen. // // wipe_cache // a wipe of cache will be performed following a successful // installation. // // clear_display // turn off the text display. // // enable_reboot // packages can explicitly request that they want the user // to be able to reboot during installation (useful for // debugging packages that don't exit). // // - the name of the package zip file. // // - an optional argument "retry" if this update is a retry of a failed // update attempt. // const char* args[6]; args[0] = binary; args[1] = EXPAND(RECOVERY_API_VERSION); // defined in Android.mk char temp[16]; snprintf(temp, sizeof(temp), "%d", pipefd[1]); args[2] = temp; args[3] = path; args[4] = retry_count > 0 ? "retry" : NULL; args[5] = NULL; pid_t pid = fork(); if (pid == 0) { umask(022); close(pipefd[0]); execv(binary, const_cast(args)); fprintf(stdout, "E:Can't run %s (%s)\n", binary, strerror(errno)); _exit(-1); } close(pipefd[1]); *wipe_cache = false; bool retry_update = false; char buffer[1024]; FILE* from_child = fdopen(pipefd[0], "r"); while (fgets(buffer, sizeof(buffer), from_child) != NULL) { char* command = strtok(buffer, " \n"); if (command == NULL) { continue; } else if (strcmp(command, "progress") == 0) { char* fraction_s = strtok(NULL, " \n"); char* seconds_s = strtok(NULL, " \n"); float fraction = strtof(fraction_s, NULL); int seconds = strtol(seconds_s, NULL, 10); ui->ShowProgress(fraction * (1-VERIFICATION_PROGRESS_FRACTION), seconds); } else if (strcmp(command, "set_progress") == 0) { char* fraction_s = strtok(NULL, " \n"); float fraction = strtof(fraction_s, NULL); ui->SetProgress(fraction); } else if (strcmp(command, "ui_print") == 0) { char* str = strtok(NULL, "\n"); if (str) { ui->PrintOnScreenOnly("%s", str); } else { ui->PrintOnScreenOnly("\n"); } fflush(stdout); } else if (strcmp(command, "wipe_cache") == 0) { *wipe_cache = true; } else if (strcmp(command, "clear_display") == 0) { ui->SetBackground(RecoveryUI::NONE); } else if (strcmp(command, "enable_reboot") == 0) { // packages can explicitly request that they want the user // to be able to reboot during installation (useful for // debugging packages that don't exit). ui->SetEnableReboot(true); } else if (strcmp(command, "retry_update") == 0) { retry_update = true; } else if (strcmp(command, "log") == 0) { // Save the logging request from updater and write to // last_install later. log_buffer.push_back(std::string(strtok(NULL, "\n"))); } else { LOG(ERROR) << "unknown command [" << command << "]"; } } fclose(from_child); int status; waitpid(pid, &status, 0); if (retry_update) { return INSTALL_RETRY; } if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) { LOG(ERROR) << "Error in " << path << " (Status " << WEXITSTATUS(status) << ")"; return INSTALL_ERROR; } return INSTALL_SUCCESS; } static int really_install_package(const char *path, bool* wipe_cache, bool needs_mount, std::vector& log_buffer, int retry_count) { ui->SetBackground(RecoveryUI::INSTALLING_UPDATE); ui->Print("Finding update package...\n"); // Give verification half the progress bar... ui->SetProgressType(RecoveryUI::DETERMINATE); ui->ShowProgress(VERIFICATION_PROGRESS_FRACTION, VERIFICATION_PROGRESS_TIME); LOG(INFO) << "Update location: " << path; // Map the update package into memory. ui->Print("Opening update package...\n"); if (path && needs_mount) { if (path[0] == '@') { ensure_path_mounted(path+1); } else { ensure_path_mounted(path); } } MemMapping map; if (sysMapFile(path, &map) != 0) { LOG(ERROR) << "failed to map file"; return INSTALL_CORRUPT; } // Verify package. if (!verify_package(map.addr, map.length)) { log_buffer.push_back(android::base::StringPrintf("error: %d", kZipVerificationFailure)); sysReleaseMap(&map); return INSTALL_CORRUPT; } // Try to open the package. ZipArchiveHandle zip; int err = OpenArchiveFromMemory(map.addr, map.length, path, &zip); if (err != 0) { LOG(ERROR) << "Can't open " << path << " : " << ErrorCodeString(err); log_buffer.push_back(android::base::StringPrintf("error: %d", kZipOpenFailure)); sysReleaseMap(&map); CloseArchive(zip); return INSTALL_CORRUPT; } // Verify and install the contents of the package. ui->Print("Installing update...\n"); if (retry_count > 0) { ui->Print("Retry attempt: %d\n", retry_count); } ui->SetEnableReboot(false); int result = try_update_binary(path, zip, wipe_cache, log_buffer, retry_count); ui->SetEnableReboot(true); ui->Print("\n"); sysReleaseMap(&map); CloseArchive(zip); return result; } int install_package(const char* path, bool* wipe_cache, const char* install_file, bool needs_mount, int retry_count) { modified_flash = true; auto start = std::chrono::system_clock::now(); int result; std::vector log_buffer; if (setup_install_mounts() != 0) { LOG(ERROR) << "failed to set up expected mounts for install; aborting"; result = INSTALL_ERROR; } else { result = really_install_package(path, wipe_cache, needs_mount, log_buffer, retry_count); } // Measure the time spent to apply OTA update in seconds. std::chrono::duration duration = std::chrono::system_clock::now() - start; int time_total = static_cast(duration.count()); if (ensure_path_mounted(UNCRYPT_STATUS) != 0) { LOG(WARNING) << "Can't mount " << UNCRYPT_STATUS; } else { std::string uncrypt_status; if (!android::base::ReadFileToString(UNCRYPT_STATUS, &uncrypt_status)) { PLOG(WARNING) << "failed to read uncrypt status"; } else if (!android::base::StartsWith(uncrypt_status, "uncrypt_")) { LOG(WARNING) << "corrupted uncrypt_status: " << uncrypt_status; } else { log_buffer.push_back(android::base::Trim(uncrypt_status)); } } // The first two lines need to be the package name and install result. std::vector log_header = { path, result == INSTALL_SUCCESS ? "1" : "0", "time_total: " + std::to_string(time_total), "retry: " + std::to_string(retry_count), }; std::string log_content = android::base::Join(log_header, "\n") + "\n" + android::base::Join(log_buffer, "\n"); if (!android::base::WriteStringToFile(log_content, install_file)) { PLOG(ERROR) << "failed to write " << install_file; } // Write a copy into last_log. LOG(INFO) << log_content; return result; } bool verify_package(const unsigned char* package_data, size_t package_size) { std::vector loadedKeys; if (!load_keys(PUBLIC_KEYS_FILE, loadedKeys)) { LOG(ERROR) << "Failed to load keys"; return false; } LOG(INFO) << loadedKeys.size() << " key(s) loaded from " << PUBLIC_KEYS_FILE; // Verify package. ui->Print("Verifying update package...\n"); auto t0 = std::chrono::system_clock::now(); int err = verify_file(const_cast(package_data), package_size, loadedKeys); std::chrono::duration duration = std::chrono::system_clock::now() - t0; ui->Print("Update package verification took %.1f s (result %d).\n", duration.count(), err); if (err != VERIFY_SUCCESS) { LOG(ERROR) << "Signature verification failed"; LOG(ERROR) << "error: " << kZipVerificationFailure; return false; } return true; }