/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef RECOVERY_INSTALL_H_ #define RECOVERY_INSTALL_H_ #include #include enum { INSTALL_SUCCESS, INSTALL_ERROR, INSTALL_CORRUPT, INSTALL_NONE, INSTALL_SKIPPED, INSTALL_RETRY }; // Installs the given update package. If INSTALL_SUCCESS is returned and *wipe_cache is true on // exit, caller should wipe the cache partition. int install_package(const std::string& package, bool* wipe_cache, const std::string& install_file, bool needs_mount, int retry_count); // Verify the package by ota keys. Return true if the package is verified successfully, // otherwise return false. bool verify_package(const unsigned char* package_data, size_t package_size); // Read meta data file of the package, write its content in the string pointed by meta_data. // Return true if succeed, otherwise return false. bool read_metadata_from_package(ZipArchiveHandle zip, std::string* metadata); // Verifies the compatibility info in a Treble-compatible package. Returns true directly if the // entry doesn't exist. bool verify_package_compatibility(ZipArchiveHandle package_zip); #endif // RECOVERY_INSTALL_H_