/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include /* for property_list */ #include #include /* private pmsg functions */ #include /* for AID_SYSTEM */ #include #include #include #include "adb_install.h" #include "common.h" #include "device.h" #include "error_code.h" #include "fuse_sdcard_provider.h" #include "fuse_sideload.h" #include "install.h" #include "minadbd/minadbd.h" #include "minui/minui.h" #include "otautil/DirUtil.h" #include "roots.h" #include "rotate_logs.h" #include "screen_ui.h" #include "stub_ui.h" #include "ui.h" static const struct option OPTIONS[] = { { "update_package", required_argument, NULL, 'u' }, { "retry_count", required_argument, NULL, 'n' }, { "wipe_data", no_argument, NULL, 'w' }, { "wipe_cache", no_argument, NULL, 'c' }, { "show_text", no_argument, NULL, 't' }, { "sideload", no_argument, NULL, 's' }, { "sideload_auto_reboot", no_argument, NULL, 'a' }, { "just_exit", no_argument, NULL, 'x' }, { "locale", required_argument, NULL, 'l' }, { "shutdown_after", no_argument, NULL, 'p' }, { "reason", required_argument, NULL, 'r' }, { "security", no_argument, NULL, 'e'}, { "wipe_ab", no_argument, NULL, 0 }, { "wipe_package_size", required_argument, NULL, 0 }, { "prompt_and_wipe_data", no_argument, NULL, 0 }, { NULL, 0, NULL, 0 }, }; // More bootreasons can be found in "system/core/bootstat/bootstat.cpp". static const std::vector bootreason_blacklist { "kernel_panic", "Panic", }; static const char *CACHE_LOG_DIR = "/cache/recovery"; static const char *COMMAND_FILE = "/cache/recovery/command"; static const char *LOG_FILE = "/cache/recovery/log"; static const char *LAST_INSTALL_FILE = "/cache/recovery/last_install"; static const char *LOCALE_FILE = "/cache/recovery/last_locale"; static const char *CONVERT_FBE_DIR = "/tmp/convert_fbe"; static const char *CONVERT_FBE_FILE = "/tmp/convert_fbe/convert_fbe"; static const char *CACHE_ROOT = "/cache"; static const char *DATA_ROOT = "/data"; static const char *SDCARD_ROOT = "/sdcard"; static const char *TEMPORARY_LOG_FILE = "/tmp/recovery.log"; static const char *TEMPORARY_INSTALL_FILE = "/tmp/last_install"; static const char *LAST_KMSG_FILE = "/cache/recovery/last_kmsg"; static const char *LAST_LOG_FILE = "/cache/recovery/last_log"; // We will try to apply the update package 5 times at most in case of an I/O error or // bspatch | imgpatch error. static const int RETRY_LIMIT = 4; static const int BATTERY_READ_TIMEOUT_IN_SEC = 10; // GmsCore enters recovery mode to install package when having enough battery // percentage. Normally, the threshold is 40% without charger and 20% with charger. // So we should check battery with a slightly lower limitation. static const int BATTERY_OK_PERCENTAGE = 20; static const int BATTERY_WITH_CHARGER_OK_PERCENTAGE = 15; static constexpr const char* RECOVERY_WIPE = "/etc/recovery.wipe"; static constexpr const char* DEFAULT_LOCALE = "en-US"; static std::string locale; static bool has_cache = false; RecoveryUI* ui = nullptr; bool modified_flash = false; std::string stage; const char* reason = nullptr; struct selabel_handle* sehandle; /* * The recovery tool communicates with the main system through /cache files. * /cache/recovery/command - INPUT - command line for tool, one arg per line * /cache/recovery/log - OUTPUT - combined log file from recovery run(s) * * The arguments which may be supplied in the recovery.command file: * --update_package=path - verify install an OTA package file * --wipe_data - erase user data (and cache), then reboot * --prompt_and_wipe_data - prompt the user that data is corrupt, * with their consent erase user data (and cache), then reboot * --wipe_cache - wipe cache (but not user data), then reboot * --set_encrypted_filesystem=on|off - enables / diasables encrypted fs * --just_exit - do nothing; exit and reboot * * After completing, we remove /cache/recovery/command and reboot. * Arguments may also be supplied in the bootloader control block (BCB). * These important scenarios must be safely restartable at any point: * * FACTORY RESET * 1. user selects "factory reset" * 2. main system writes "--wipe_data" to /cache/recovery/command * 3. main system reboots into recovery * 4. get_args() writes BCB with "boot-recovery" and "--wipe_data" * -- after this, rebooting will restart the erase -- * 5. erase_volume() reformats /data * 6. erase_volume() reformats /cache * 7. finish_recovery() erases BCB * -- after this, rebooting will restart the main system -- * 8. main() calls reboot() to boot main system * * OTA INSTALL * 1. main system downloads OTA package to /cache/some-filename.zip * 2. main system writes "--update_package=/cache/some-filename.zip" * 3. main system reboots into recovery * 4. get_args() writes BCB with "boot-recovery" and "--update_package=..." * -- after this, rebooting will attempt to reinstall the update -- * 5. install_package() attempts to install the update * NOTE: the package install must itself be restartable from any point * 6. finish_recovery() erases BCB * -- after this, rebooting will (try to) restart the main system -- * 7. ** if install failed ** * 7a. prompt_and_wait() shows an error icon and waits for the user * 7b. the user reboots (pulling the battery, etc) into the main system */ // Open a given path, mounting partitions as necessary. FILE* fopen_path(const char* path, const char* mode) { if (ensure_path_mounted(path) != 0) { LOG(ERROR) << "Can't mount " << path; return nullptr; } // When writing, try to create the containing directory, if necessary. Use generous permissions, // the system (init.rc) will reset them. if (strchr("wa", mode[0])) { mkdir_recursively(path, 0777, true, sehandle); } return fopen(path, mode); } // close a file, log an error if the error indicator is set static void check_and_fclose(FILE *fp, const char *name) { fflush(fp); if (fsync(fileno(fp)) == -1) { PLOG(ERROR) << "Failed to fsync " << name; } if (ferror(fp)) { PLOG(ERROR) << "Error in " << name; } fclose(fp); } bool is_ro_debuggable() { return android::base::GetBoolProperty("ro.debuggable", false); } bool reboot(const std::string& command) { std::string cmd = command; if (android::base::GetBoolProperty("ro.boot.quiescent", false)) { cmd += ",quiescent"; } return android::base::SetProperty(ANDROID_RB_PROPERTY, cmd); } static void redirect_stdio(const char* filename) { int pipefd[2]; if (pipe(pipefd) == -1) { PLOG(ERROR) << "pipe failed"; // Fall back to traditional logging mode without timestamps. // If these fail, there's not really anywhere to complain... freopen(filename, "a", stdout); setbuf(stdout, NULL); freopen(filename, "a", stderr); setbuf(stderr, NULL); return; } pid_t pid = fork(); if (pid == -1) { PLOG(ERROR) << "fork failed"; // Fall back to traditional logging mode without timestamps. // If these fail, there's not really anywhere to complain... freopen(filename, "a", stdout); setbuf(stdout, NULL); freopen(filename, "a", stderr); setbuf(stderr, NULL); return; } if (pid == 0) { /// Close the unused write end. close(pipefd[1]); auto start = std::chrono::steady_clock::now(); // Child logger to actually write to the log file. FILE* log_fp = fopen(filename, "ae"); if (log_fp == nullptr) { PLOG(ERROR) << "fopen \"" << filename << "\" failed"; close(pipefd[0]); _exit(EXIT_FAILURE); } FILE* pipe_fp = fdopen(pipefd[0], "r"); if (pipe_fp == nullptr) { PLOG(ERROR) << "fdopen failed"; check_and_fclose(log_fp, filename); close(pipefd[0]); _exit(EXIT_FAILURE); } char* line = nullptr; size_t len = 0; while (getline(&line, &len, pipe_fp) != -1) { auto now = std::chrono::steady_clock::now(); double duration = std::chrono::duration_cast>( now - start).count(); if (line[0] == '\n') { fprintf(log_fp, "[%12.6lf]\n", duration); } else { fprintf(log_fp, "[%12.6lf] %s", duration, line); } fflush(log_fp); } PLOG(ERROR) << "getline failed"; free(line); check_and_fclose(log_fp, filename); close(pipefd[0]); _exit(EXIT_FAILURE); } else { // Redirect stdout/stderr to the logger process. // Close the unused read end. close(pipefd[0]); setbuf(stdout, nullptr); setbuf(stderr, nullptr); if (dup2(pipefd[1], STDOUT_FILENO) == -1) { PLOG(ERROR) << "dup2 stdout failed"; } if (dup2(pipefd[1], STDERR_FILENO) == -1) { PLOG(ERROR) << "dup2 stderr failed"; } close(pipefd[1]); } } // command line args come from, in decreasing precedence: // - the actual command line // - the bootloader control block (one per line, after "recovery") // - the contents of COMMAND_FILE (one per line) static std::vector get_args(const int argc, char** const argv) { CHECK_GT(argc, 0); bootloader_message boot = {}; std::string err; if (!read_bootloader_message(&boot, &err)) { LOG(ERROR) << err; // If fails, leave a zeroed bootloader_message. boot = {}; } stage = std::string(boot.stage); if (boot.command[0] != 0) { std::string boot_command = std::string(boot.command, sizeof(boot.command)); LOG(INFO) << "Boot command: " << boot_command; } if (boot.status[0] != 0) { std::string boot_status = std::string(boot.status, sizeof(boot.status)); LOG(INFO) << "Boot status: " << boot_status; } std::vector args(argv, argv + argc); // --- if arguments weren't supplied, look in the bootloader control block if (args.size() == 1) { boot.recovery[sizeof(boot.recovery) - 1] = '\0'; // Ensure termination std::string boot_recovery(boot.recovery); std::vector tokens = android::base::Split(boot_recovery, "\n"); if (!tokens.empty() && tokens[0] == "recovery") { for (auto it = tokens.begin() + 1; it != tokens.end(); it++) { // Skip empty and '\0'-filled tokens. if (!it->empty() && (*it)[0] != '\0') args.push_back(std::move(*it)); } LOG(INFO) << "Got " << args.size() << " arguments from boot message"; } else if (boot.recovery[0] != 0) { LOG(ERROR) << "Bad boot message: \"" << boot_recovery << "\""; } } // --- if that doesn't work, try the command file (if we have /cache). if (args.size() == 1 && has_cache) { std::string content; if (ensure_path_mounted(COMMAND_FILE) == 0 && android::base::ReadFileToString(COMMAND_FILE, &content)) { std::vector tokens = android::base::Split(content, "\n"); // All the arguments in COMMAND_FILE are needed (unlike the BCB message, // COMMAND_FILE doesn't use filename as the first argument). for (auto it = tokens.begin(); it != tokens.end(); it++) { // Skip empty and '\0'-filled tokens. if (!it->empty() && (*it)[0] != '\0') args.push_back(std::move(*it)); } LOG(INFO) << "Got " << args.size() << " arguments from " << COMMAND_FILE; } } // Write the arguments (excluding the filename in args[0]) back into the // bootloader control block. So the device will always boot into recovery to // finish the pending work, until finish_recovery() is called. std::vector options(args.cbegin() + 1, args.cend()); if (!update_bootloader_message(options, &err)) { LOG(ERROR) << "Failed to set BCB message: " << err; } return args; } // Set the BCB to reboot back into recovery (it won't resume the install from // sdcard though). static void set_sdcard_update_bootloader_message() { std::vector options; std::string err; if (!update_bootloader_message(options, &err)) { LOG(ERROR) << "Failed to set BCB message: " << err; } } // Read from kernel log into buffer and write out to file. static void save_kernel_log(const char* destination) { int klog_buf_len = klogctl(KLOG_SIZE_BUFFER, 0, 0); if (klog_buf_len <= 0) { PLOG(ERROR) << "Error getting klog size"; return; } std::string buffer(klog_buf_len, 0); int n = klogctl(KLOG_READ_ALL, &buffer[0], klog_buf_len); if (n == -1) { PLOG(ERROR) << "Error in reading klog"; return; } buffer.resize(n); android::base::WriteStringToFile(buffer, destination); } // write content to the current pmsg session. static ssize_t __pmsg_write(const char *filename, const char *buf, size_t len) { return __android_log_pmsg_file_write(LOG_ID_SYSTEM, ANDROID_LOG_INFO, filename, buf, len); } static void copy_log_file_to_pmsg(const char* source, const char* destination) { std::string content; android::base::ReadFileToString(source, &content); __pmsg_write(destination, content.c_str(), content.length()); } // How much of the temp log we have copied to the copy in cache. static off_t tmplog_offset = 0; static void copy_log_file(const char* source, const char* destination, bool append) { FILE* dest_fp = fopen_path(destination, append ? "ae" : "we"); if (dest_fp == nullptr) { PLOG(ERROR) << "Can't open " << destination; } else { FILE* source_fp = fopen(source, "re"); if (source_fp != nullptr) { if (append) { fseeko(source_fp, tmplog_offset, SEEK_SET); // Since last write } char buf[4096]; size_t bytes; while ((bytes = fread(buf, 1, sizeof(buf), source_fp)) != 0) { fwrite(buf, 1, bytes, dest_fp); } if (append) { tmplog_offset = ftello(source_fp); } check_and_fclose(source_fp, source); } check_and_fclose(dest_fp, destination); } } static void copy_logs() { // We only rotate and record the log of the current session if there are // actual attempts to modify the flash, such as wipes, installs from BCB // or menu selections. This is to avoid unnecessary rotation (and // possible deletion) of log files, if it does not do anything loggable. if (!modified_flash) { return; } // Always write to pmsg, this allows the OTA logs to be caught in logcat -L copy_log_file_to_pmsg(TEMPORARY_LOG_FILE, LAST_LOG_FILE); copy_log_file_to_pmsg(TEMPORARY_INSTALL_FILE, LAST_INSTALL_FILE); // We can do nothing for now if there's no /cache partition. if (!has_cache) { return; } ensure_path_mounted(LAST_LOG_FILE); ensure_path_mounted(LAST_KMSG_FILE); rotate_logs(LAST_LOG_FILE, LAST_KMSG_FILE); // Copy logs to cache so the system can find out what happened. copy_log_file(TEMPORARY_LOG_FILE, LOG_FILE, true); copy_log_file(TEMPORARY_LOG_FILE, LAST_LOG_FILE, false); copy_log_file(TEMPORARY_INSTALL_FILE, LAST_INSTALL_FILE, false); save_kernel_log(LAST_KMSG_FILE); chmod(LOG_FILE, 0600); chown(LOG_FILE, AID_SYSTEM, AID_SYSTEM); chmod(LAST_KMSG_FILE, 0600); chown(LAST_KMSG_FILE, AID_SYSTEM, AID_SYSTEM); chmod(LAST_LOG_FILE, 0640); chmod(LAST_INSTALL_FILE, 0644); sync(); } // Clear the recovery command and prepare to boot a (hopefully working) system, // copy our log file to cache as well (for the system to read). This function is // idempotent: call it as many times as you like. static void finish_recovery() { // Save the locale to cache, so if recovery is next started up without a '--locale' argument // (e.g., directly from the bootloader) it will use the last-known locale. if (!locale.empty() && has_cache) { LOG(INFO) << "Saving locale \"" << locale << "\""; if (ensure_path_mounted(LOCALE_FILE) != 0) { LOG(ERROR) << "Failed to mount " << LOCALE_FILE; } else if (!android::base::WriteStringToFile(locale, LOCALE_FILE)) { PLOG(ERROR) << "Failed to save locale to " << LOCALE_FILE; } } copy_logs(); // Reset to normal system boot so recovery won't cycle indefinitely. std::string err; if (!clear_bootloader_message(&err)) { LOG(ERROR) << "Failed to clear BCB message: " << err; } // Remove the command file, so recovery won't repeat indefinitely. if (has_cache) { if (ensure_path_mounted(COMMAND_FILE) != 0 || (unlink(COMMAND_FILE) && errno != ENOENT)) { LOG(WARNING) << "Can't unlink " << COMMAND_FILE; } ensure_path_unmounted(CACHE_ROOT); } sync(); // For good measure. } struct saved_log_file { std::string name; struct stat sb; std::string data; }; static bool erase_volume(const char* volume) { bool is_cache = (strcmp(volume, CACHE_ROOT) == 0); bool is_data = (strcmp(volume, DATA_ROOT) == 0); ui->SetBackground(RecoveryUI::ERASING); ui->SetProgressType(RecoveryUI::INDETERMINATE); std::vector log_files; if (is_cache) { // If we're reformatting /cache, we load any past logs // (i.e. "/cache/recovery/last_*") and the current log // ("/cache/recovery/log") into memory, so we can restore them after // the reformat. ensure_path_mounted(volume); struct dirent* de; std::unique_ptr d(opendir(CACHE_LOG_DIR), closedir); if (d) { while ((de = readdir(d.get())) != nullptr) { if (strncmp(de->d_name, "last_", 5) == 0 || strcmp(de->d_name, "log") == 0) { std::string path = android::base::StringPrintf("%s/%s", CACHE_LOG_DIR, de->d_name); struct stat sb; if (stat(path.c_str(), &sb) == 0) { // truncate files to 512kb if (sb.st_size > (1 << 19)) { sb.st_size = 1 << 19; } std::string data(sb.st_size, '\0'); FILE* f = fopen(path.c_str(), "rbe"); fread(&data[0], 1, data.size(), f); fclose(f); log_files.emplace_back(saved_log_file{ path, sb, data }); } } } } else { if (errno != ENOENT) { PLOG(ERROR) << "Failed to opendir " << CACHE_LOG_DIR; } } } ui->Print("Formatting %s...\n", volume); ensure_path_unmounted(volume); int result; if (is_data && reason && strcmp(reason, "convert_fbe") == 0) { // Create convert_fbe breadcrumb file to signal to init // to convert to file based encryption, not full disk encryption if (mkdir(CONVERT_FBE_DIR, 0700) != 0) { ui->Print("Failed to make convert_fbe dir %s\n", strerror(errno)); return true; } FILE* f = fopen(CONVERT_FBE_FILE, "wbe"); if (!f) { ui->Print("Failed to convert to file encryption %s\n", strerror(errno)); return true; } fclose(f); result = format_volume(volume, CONVERT_FBE_DIR); remove(CONVERT_FBE_FILE); rmdir(CONVERT_FBE_DIR); } else { result = format_volume(volume); } if (is_cache) { // Re-create the log dir and write back the log entries. if (ensure_path_mounted(CACHE_LOG_DIR) == 0 && mkdir_recursively(CACHE_LOG_DIR, 0777, false, sehandle) == 0) { for (const auto& log : log_files) { if (!android::base::WriteStringToFile(log.data, log.name, log.sb.st_mode, log.sb.st_uid, log.sb.st_gid)) { PLOG(ERROR) << "Failed to write to " << log.name; } } } else { PLOG(ERROR) << "Failed to mount / create " << CACHE_LOG_DIR; } // Any part of the log we'd copied to cache is now gone. // Reset the pointer so we copy from the beginning of the temp // log. tmplog_offset = 0; copy_logs(); } return (result == 0); } // Display a menu with the specified 'headers' and 'items'. Device specific HandleMenuKey() may // return a positive number beyond the given range. Caller sets 'menu_only' to true to ensure only // a menu item gets selected. 'initial_selection' controls the initial cursor location. Returns the // (non-negative) chosen item number, or -1 if timed out waiting for input. static int get_menu_selection(const char* const* headers, const char* const* items, bool menu_only, int initial_selection, Device* device) { // Throw away keys pressed previously, so user doesn't accidentally trigger menu items. ui->FlushKeys(); ui->StartMenu(headers, items, initial_selection); int selected = initial_selection; int chosen_item = -1; while (chosen_item < 0) { int key = ui->WaitKey(); if (key == -1) { // WaitKey() timed out. if (ui->WasTextEverVisible()) { continue; } else { LOG(INFO) << "Timed out waiting for key input; rebooting."; ui->EndMenu(); return -1; } } bool visible = ui->IsTextVisible(); int action = device->HandleMenuKey(key, visible); if (action < 0) { switch (action) { case Device::kHighlightUp: selected = ui->SelectMenu(--selected); break; case Device::kHighlightDown: selected = ui->SelectMenu(++selected); break; case Device::kInvokeItem: chosen_item = selected; break; case Device::kNoAction: break; } } else if (!menu_only) { chosen_item = action; } } ui->EndMenu(); return chosen_item; } // Returns the selected filename, or an empty string. static std::string browse_directory(const std::string& path, Device* device) { ensure_path_mounted(path.c_str()); std::unique_ptr d(opendir(path.c_str()), closedir); if (!d) { PLOG(ERROR) << "error opening " << path; return ""; } std::vector dirs; std::vector zips = { "../" }; // "../" is always the first entry. dirent* de; while ((de = readdir(d.get())) != nullptr) { std::string name(de->d_name); if (de->d_type == DT_DIR) { // Skip "." and ".." entries. if (name == "." || name == "..") continue; dirs.push_back(name + "/"); } else if (de->d_type == DT_REG && android::base::EndsWithIgnoreCase(name, ".zip")) { zips.push_back(name); } } std::sort(dirs.begin(), dirs.end()); std::sort(zips.begin(), zips.end()); // Append dirs to the zips list. zips.insert(zips.end(), dirs.begin(), dirs.end()); const char* entries[zips.size() + 1]; entries[zips.size()] = nullptr; for (size_t i = 0; i < zips.size(); i++) { entries[i] = zips[i].c_str(); } const char* headers[] = { "Choose a package to install:", path.c_str(), nullptr }; int chosen_item = 0; while (true) { chosen_item = get_menu_selection(headers, entries, true, chosen_item, device); const std::string& item = zips[chosen_item]; if (chosen_item == 0) { // Go up but continue browsing (if the caller is browse_directory). return ""; } std::string new_path = path + "/" + item; if (new_path.back() == '/') { // Recurse down into a subdirectory. new_path.pop_back(); std::string result = browse_directory(new_path, device); if (!result.empty()) return result; } else { // Selected a zip file: return the path to the caller. return new_path; } } // Unreachable. } static bool yes_no(Device* device, const char* question1, const char* question2) { const char* headers[] = { question1, question2, NULL }; const char* items[] = { " No", " Yes", NULL }; int chosen_item = get_menu_selection(headers, items, true, 0, device); return (chosen_item == 1); } static bool ask_to_wipe_data(Device* device) { return yes_no(device, "Wipe all user data?", " THIS CAN NOT BE UNDONE!"); } // Return true on success. static bool wipe_data(Device* device) { modified_flash = true; ui->Print("\n-- Wiping data...\n"); bool success = device->PreWipeData() && erase_volume("/data") && (has_cache ? erase_volume("/cache") : true) && device->PostWipeData(); ui->Print("Data wipe %s.\n", success ? "complete" : "failed"); return success; } static bool prompt_and_wipe_data(Device* device) { const char* const headers[] = { "Can't load Android system. Your data may be corrupt.", "If you continue to get this message, you may need to", "perform a factory data reset and erase all user data", "stored on this device.", NULL }; const char* const items[] = { "Try again", "Factory data reset", NULL }; for (;;) { int chosen_item = get_menu_selection(headers, items, true, 0, device); if (chosen_item != 1) { return true; // Just reboot, no wipe; not a failure, user asked for it } if (ask_to_wipe_data(device)) { return wipe_data(device); } } } // Return true on success. static bool wipe_cache(bool should_confirm, Device* device) { if (!has_cache) { ui->Print("No /cache partition found.\n"); return false; } if (should_confirm && !yes_no(device, "Wipe cache?", " THIS CAN NOT BE UNDONE!")) { return false; } modified_flash = true; ui->Print("\n-- Wiping cache...\n"); bool success = erase_volume("/cache"); ui->Print("Cache wipe %s.\n", success ? "complete" : "failed"); return success; } // Secure-wipe a given partition. It uses BLKSECDISCARD, if supported. Otherwise, it goes with // BLKDISCARD (if device supports BLKDISCARDZEROES) or BLKZEROOUT. static bool secure_wipe_partition(const std::string& partition) { android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(partition.c_str(), O_WRONLY))); if (fd == -1) { PLOG(ERROR) << "Failed to open \"" << partition << "\""; return false; } uint64_t range[2] = { 0, 0 }; if (ioctl(fd, BLKGETSIZE64, &range[1]) == -1 || range[1] == 0) { PLOG(ERROR) << "Failed to get partition size"; return false; } LOG(INFO) << "Secure-wiping \"" << partition << "\" from " << range[0] << " to " << range[1]; LOG(INFO) << " Trying BLKSECDISCARD..."; if (ioctl(fd, BLKSECDISCARD, &range) == -1) { PLOG(WARNING) << " Failed"; // Use BLKDISCARD if it zeroes out blocks, otherwise use BLKZEROOUT. unsigned int zeroes; if (ioctl(fd, BLKDISCARDZEROES, &zeroes) == 0 && zeroes != 0) { LOG(INFO) << " Trying BLKDISCARD..."; if (ioctl(fd, BLKDISCARD, &range) == -1) { PLOG(ERROR) << " Failed"; return false; } } else { LOG(INFO) << " Trying BLKZEROOUT..."; if (ioctl(fd, BLKZEROOUT, &range) == -1) { PLOG(ERROR) << " Failed"; return false; } } } LOG(INFO) << " Done"; return true; } // Check if the wipe package matches expectation: // 1. verify the package. // 2. check metadata (ota-type, pre-device and serial number if having one). static bool check_wipe_package(size_t wipe_package_size) { if (wipe_package_size == 0) { LOG(ERROR) << "wipe_package_size is zero"; return false; } std::string wipe_package; std::string err_str; if (!read_wipe_package(&wipe_package, wipe_package_size, &err_str)) { PLOG(ERROR) << "Failed to read wipe package"; return false; } if (!verify_package(reinterpret_cast(wipe_package.data()), wipe_package.size())) { LOG(ERROR) << "Failed to verify package"; return false; } // Extract metadata ZipArchiveHandle zip; int err = OpenArchiveFromMemory(static_cast(&wipe_package[0]), wipe_package.size(), "wipe_package", &zip); if (err != 0) { LOG(ERROR) << "Can't open wipe package : " << ErrorCodeString(err); return false; } std::string metadata; if (!read_metadata_from_package(zip, &metadata)) { CloseArchive(zip); return false; } CloseArchive(zip); // Check metadata std::vector lines = android::base::Split(metadata, "\n"); bool ota_type_matched = false; bool device_type_matched = false; bool has_serial_number = false; bool serial_number_matched = false; for (const auto& line : lines) { if (line == "ota-type=BRICK") { ota_type_matched = true; } else if (android::base::StartsWith(line, "pre-device=")) { std::string device_type = line.substr(strlen("pre-device=")); std::string real_device_type = android::base::GetProperty("ro.build.product", ""); device_type_matched = (device_type == real_device_type); } else if (android::base::StartsWith(line, "serialno=")) { std::string serial_no = line.substr(strlen("serialno=")); std::string real_serial_no = android::base::GetProperty("ro.serialno", ""); has_serial_number = true; serial_number_matched = (serial_no == real_serial_no); } } return ota_type_matched && device_type_matched && (!has_serial_number || serial_number_matched); } // Wipe the current A/B device, with a secure wipe of all the partitions in // RECOVERY_WIPE. static bool wipe_ab_device(size_t wipe_package_size) { ui->SetBackground(RecoveryUI::ERASING); ui->SetProgressType(RecoveryUI::INDETERMINATE); if (!check_wipe_package(wipe_package_size)) { LOG(ERROR) << "Failed to verify wipe package"; return false; } std::string partition_list; if (!android::base::ReadFileToString(RECOVERY_WIPE, &partition_list)) { LOG(ERROR) << "failed to read \"" << RECOVERY_WIPE << "\""; return false; } std::vector lines = android::base::Split(partition_list, "\n"); for (const std::string& line : lines) { std::string partition = android::base::Trim(line); // Ignore '#' comment or empty lines. if (android::base::StartsWith(partition, "#") || partition.empty()) { continue; } // Proceed anyway even if it fails to wipe some partition. secure_wipe_partition(partition); } return true; } static void choose_recovery_file(Device* device) { std::vector entries; if (has_cache) { for (int i = 0; i < KEEP_LOG_COUNT; i++) { auto add_to_entries = [&](const char* filename) { std::string log_file(filename); if (i > 0) { log_file += "." + std::to_string(i); } if (ensure_path_mounted(log_file.c_str()) == 0 && access(log_file.c_str(), R_OK) == 0) { entries.push_back(std::move(log_file)); } }; // Add LAST_LOG_FILE + LAST_LOG_FILE.x add_to_entries(LAST_LOG_FILE); // Add LAST_KMSG_FILE + LAST_KMSG_FILE.x add_to_entries(LAST_KMSG_FILE); } } else { // If cache partition is not found, view /tmp/recovery.log instead. if (access(TEMPORARY_LOG_FILE, R_OK) == -1) { return; } else { entries.push_back(TEMPORARY_LOG_FILE); } } entries.push_back("Back"); std::vector menu_entries(entries.size()); std::transform(entries.cbegin(), entries.cend(), menu_entries.begin(), [](const std::string& entry) { return entry.c_str(); }); menu_entries.push_back(nullptr); const char* headers[] = { "Select file to view", nullptr }; int chosen_item = 0; while (true) { chosen_item = get_menu_selection(headers, menu_entries.data(), true, chosen_item, device); if (entries[chosen_item] == "Back") break; ui->ShowFile(entries[chosen_item].c_str()); } } static void run_graphics_test() { // Switch to graphics screen. ui->ShowText(false); ui->SetProgressType(RecoveryUI::INDETERMINATE); ui->SetBackground(RecoveryUI::INSTALLING_UPDATE); sleep(1); ui->SetBackground(RecoveryUI::ERROR); sleep(1); ui->SetBackground(RecoveryUI::NO_COMMAND); sleep(1); ui->SetBackground(RecoveryUI::ERASING); sleep(1); // Calling SetBackground() after SetStage() to trigger a redraw. ui->SetStage(1, 3); ui->SetBackground(RecoveryUI::INSTALLING_UPDATE); sleep(1); ui->SetStage(2, 3); ui->SetBackground(RecoveryUI::INSTALLING_UPDATE); sleep(1); ui->SetStage(3, 3); ui->SetBackground(RecoveryUI::INSTALLING_UPDATE); sleep(1); ui->SetStage(-1, -1); ui->SetBackground(RecoveryUI::INSTALLING_UPDATE); ui->SetProgressType(RecoveryUI::DETERMINATE); ui->ShowProgress(1.0, 10.0); float fraction = 0.0; for (size_t i = 0; i < 100; ++i) { fraction += .01; ui->SetProgress(fraction); usleep(100000); } ui->ShowText(true); } // How long (in seconds) we wait for the fuse-provided package file to // appear, before timing out. #define SDCARD_INSTALL_TIMEOUT 10 static int apply_from_sdcard(Device* device, bool* wipe_cache) { modified_flash = true; if (ensure_path_mounted(SDCARD_ROOT) != 0) { ui->Print("\n-- Couldn't mount %s.\n", SDCARD_ROOT); return INSTALL_ERROR; } std::string path = browse_directory(SDCARD_ROOT, device); if (path.empty()) { ui->Print("\n-- No package file selected.\n"); ensure_path_unmounted(SDCARD_ROOT); return INSTALL_ERROR; } ui->Print("\n-- Install %s ...\n", path.c_str()); set_sdcard_update_bootloader_message(); // We used to use fuse in a thread as opposed to a process. Since accessing // through fuse involves going from kernel to userspace to kernel, it leads // to deadlock when a page fault occurs. (Bug: 26313124) pid_t child; if ((child = fork()) == 0) { bool status = start_sdcard_fuse(path.c_str()); _exit(status ? EXIT_SUCCESS : EXIT_FAILURE); } // FUSE_SIDELOAD_HOST_PATHNAME will start to exist once the fuse in child // process is ready. int result = INSTALL_ERROR; int status; bool waited = false; for (int i = 0; i < SDCARD_INSTALL_TIMEOUT; ++i) { if (waitpid(child, &status, WNOHANG) == -1) { result = INSTALL_ERROR; waited = true; break; } struct stat sb; if (stat(FUSE_SIDELOAD_HOST_PATHNAME, &sb) == -1) { if (errno == ENOENT && i < SDCARD_INSTALL_TIMEOUT-1) { sleep(1); continue; } else { LOG(ERROR) << "Timed out waiting for the fuse-provided package."; result = INSTALL_ERROR; kill(child, SIGKILL); break; } } result = install_package(FUSE_SIDELOAD_HOST_PATHNAME, wipe_cache, TEMPORARY_INSTALL_FILE, false, 0/*retry_count*/); break; } if (!waited) { // Calling stat() on this magic filename signals the fuse // filesystem to shut down. struct stat sb; stat(FUSE_SIDELOAD_HOST_EXIT_PATHNAME, &sb); waitpid(child, &status, 0); } if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) { LOG(ERROR) << "Error exit from the fuse process: " << WEXITSTATUS(status); } ensure_path_unmounted(SDCARD_ROOT); return result; } // Returns REBOOT, SHUTDOWN, or REBOOT_BOOTLOADER. Returning NO_ACTION means to take the default, // which is to reboot or shutdown depending on if the --shutdown_after flag was passed to recovery. static Device::BuiltinAction prompt_and_wait(Device* device, int status) { for (;;) { finish_recovery(); switch (status) { case INSTALL_SUCCESS: case INSTALL_NONE: ui->SetBackground(RecoveryUI::NO_COMMAND); break; case INSTALL_ERROR: case INSTALL_CORRUPT: ui->SetBackground(RecoveryUI::ERROR); break; } ui->SetProgressType(RecoveryUI::EMPTY); int chosen_item = get_menu_selection(nullptr, device->GetMenuItems(), false, 0, device); // Device-specific code may take some action here. It may return one of the core actions // handled in the switch statement below. Device::BuiltinAction chosen_action = (chosen_item == -1) ? Device::REBOOT : device->InvokeMenuItem(chosen_item); bool should_wipe_cache = false; switch (chosen_action) { case Device::NO_ACTION: break; case Device::REBOOT: case Device::SHUTDOWN: case Device::REBOOT_BOOTLOADER: return chosen_action; case Device::WIPE_DATA: if (ui->IsTextVisible()) { if (ask_to_wipe_data(device)) { wipe_data(device); } } else { wipe_data(device); return Device::NO_ACTION; } break; case Device::WIPE_CACHE: wipe_cache(ui->IsTextVisible(), device); if (!ui->IsTextVisible()) return Device::NO_ACTION; break; case Device::APPLY_ADB_SIDELOAD: case Device::APPLY_SDCARD: { bool adb = (chosen_action == Device::APPLY_ADB_SIDELOAD); if (adb) { status = apply_from_adb(&should_wipe_cache, TEMPORARY_INSTALL_FILE); } else { status = apply_from_sdcard(device, &should_wipe_cache); } if (status == INSTALL_SUCCESS && should_wipe_cache) { if (!wipe_cache(false, device)) { status = INSTALL_ERROR; } } if (status != INSTALL_SUCCESS) { ui->SetBackground(RecoveryUI::ERROR); ui->Print("Installation aborted.\n"); copy_logs(); } else if (!ui->IsTextVisible()) { return Device::NO_ACTION; // reboot if logs aren't visible } else { ui->Print("\nInstall from %s complete.\n", adb ? "ADB" : "SD card"); } } break; case Device::VIEW_RECOVERY_LOGS: choose_recovery_file(device); break; case Device::RUN_GRAPHICS_TEST: run_graphics_test(); break; case Device::MOUNT_SYSTEM: // For a system image built with the root directory (i.e. system_root_image == "true"), we // mount it to /system_root, and symlink /system to /system_root/system to make adb shell // work (the symlink is created through the build system). (Bug: 22855115) if (android::base::GetBoolProperty("ro.build.system_root_image", false)) { if (ensure_path_mounted_at("/", "/system_root") != -1) { ui->Print("Mounted /system.\n"); } } else { if (ensure_path_mounted("/system") != -1) { ui->Print("Mounted /system.\n"); } } break; } } } static void print_property(const char *key, const char *name, void *cookie) { printf("%s=%s\n", key, name); } static std::string load_locale_from_cache() { if (ensure_path_mounted(LOCALE_FILE) != 0) { LOG(ERROR) << "Can't mount " << LOCALE_FILE; return ""; } std::string content; if (!android::base::ReadFileToString(LOCALE_FILE, &content)) { PLOG(ERROR) << "Can't read " << LOCALE_FILE; return ""; } return android::base::Trim(content); } void ui_print(const char* format, ...) { std::string buffer; va_list ap; va_start(ap, format); android::base::StringAppendV(&buffer, format, ap); va_end(ap); if (ui != nullptr) { ui->Print("%s", buffer.c_str()); } else { fputs(buffer.c_str(), stdout); } } static constexpr char log_characters[] = "VDIWEF"; void UiLogger(android::base::LogId id, android::base::LogSeverity severity, const char* tag, const char* file, unsigned int line, const char* message) { if (severity >= android::base::ERROR && ui != nullptr) { ui->Print("E:%s\n", message); } else { fprintf(stdout, "%c:%s\n", log_characters[severity], message); } } static bool is_battery_ok() { struct healthd_config healthd_config = { .batteryStatusPath = android::String8(android::String8::kEmptyString), .batteryHealthPath = android::String8(android::String8::kEmptyString), .batteryPresentPath = android::String8(android::String8::kEmptyString), .batteryCapacityPath = android::String8(android::String8::kEmptyString), .batteryVoltagePath = android::String8(android::String8::kEmptyString), .batteryTemperaturePath = android::String8(android::String8::kEmptyString), .batteryTechnologyPath = android::String8(android::String8::kEmptyString), .batteryCurrentNowPath = android::String8(android::String8::kEmptyString), .batteryCurrentAvgPath = android::String8(android::String8::kEmptyString), .batteryChargeCounterPath = android::String8(android::String8::kEmptyString), .batteryFullChargePath = android::String8(android::String8::kEmptyString), .batteryCycleCountPath = android::String8(android::String8::kEmptyString), .energyCounter = NULL, .boot_min_cap = 0, .screen_on = NULL }; healthd_board_init(&healthd_config); android::BatteryMonitor monitor; monitor.init(&healthd_config); int wait_second = 0; while (true) { int charge_status = monitor.getChargeStatus(); // Treat unknown status as charged. bool charged = (charge_status != android::BATTERY_STATUS_DISCHARGING && charge_status != android::BATTERY_STATUS_NOT_CHARGING); android::BatteryProperty capacity; android::status_t status = monitor.getProperty(android::BATTERY_PROP_CAPACITY, &capacity); ui_print("charge_status %d, charged %d, status %d, capacity %lld\n", charge_status, charged, status, capacity.valueInt64); // At startup, the battery drivers in devices like N5X/N6P take some time to load // the battery profile. Before the load finishes, it reports value 50 as a fake // capacity. BATTERY_READ_TIMEOUT_IN_SEC is set that the battery drivers are expected // to finish loading the battery profile earlier than 10 seconds after kernel startup. if (status == 0 && capacity.valueInt64 == 50) { if (wait_second < BATTERY_READ_TIMEOUT_IN_SEC) { sleep(1); wait_second++; continue; } } // If we can't read battery percentage, it may be a device without battery. In this // situation, use 100 as a fake battery percentage. if (status != 0) { capacity.valueInt64 = 100; } return (charged && capacity.valueInt64 >= BATTERY_WITH_CHARGER_OK_PERCENTAGE) || (!charged && capacity.valueInt64 >= BATTERY_OK_PERCENTAGE); } } static void set_retry_bootloader_message(int retry_count, const std::vector& args) { std::vector options; for (const auto& arg : args) { if (!android::base::StartsWith(arg, "--retry_count")) { options.push_back(arg); } } // Increment the retry counter by 1. options.push_back(android::base::StringPrintf("--retry_count=%d", retry_count + 1)); std::string err; if (!update_bootloader_message(options, &err)) { LOG(ERROR) << err; } } static bool bootreason_in_blacklist() { std::string bootreason = android::base::GetProperty("ro.boot.bootreason", ""); if (!bootreason.empty()) { for (const auto& str : bootreason_blacklist) { if (strcasecmp(str.c_str(), bootreason.c_str()) == 0) { return true; } } } return false; } static void log_failure_code(ErrorCode code, const char *update_package) { std::vector log_buffer = { update_package, "0", // install result "error: " + std::to_string(code), }; std::string log_content = android::base::Join(log_buffer, "\n"); if (!android::base::WriteStringToFile(log_content, TEMPORARY_INSTALL_FILE)) { PLOG(ERROR) << "failed to write " << TEMPORARY_INSTALL_FILE; } // Also write the info into last_log. LOG(INFO) << log_content; } int main(int argc, char **argv) { // We don't have logcat yet under recovery; so we'll print error on screen and // log to stdout (which is redirected to recovery.log) as we used to do. android::base::InitLogging(argv, &UiLogger); // Take last pmsg contents and rewrite it to the current pmsg session. static const char filter[] = "recovery/"; // Do we need to rotate? bool doRotate = false; __android_log_pmsg_file_read( LOG_ID_SYSTEM, ANDROID_LOG_INFO, filter, logbasename, &doRotate); // Take action to refresh pmsg contents __android_log_pmsg_file_read( LOG_ID_SYSTEM, ANDROID_LOG_INFO, filter, logrotate, &doRotate); // If this binary is started with the single argument "--adbd", // instead of being the normal recovery binary, it turns into kind // of a stripped-down version of adbd that only supports the // 'sideload' command. Note this must be a real argument, not // anything in the command file or bootloader control block; the // only way recovery should be run with this argument is when it // starts a copy of itself from the apply_from_adb() function. if (argc == 2 && strcmp(argv[1], "--adbd") == 0) { minadbd_main(); return 0; } time_t start = time(NULL); // redirect_stdio should be called only in non-sideload mode. Otherwise // we may have two logger instances with different timestamps. redirect_stdio(TEMPORARY_LOG_FILE); printf("Starting recovery (pid %d) on %s", getpid(), ctime(&start)); load_volume_table(); has_cache = volume_for_path(CACHE_ROOT) != nullptr; std::vector args = get_args(argc, argv); std::vector args_to_parse(args.size()); std::transform(args.cbegin(), args.cend(), args_to_parse.begin(), [](const std::string& arg) { return const_cast(arg.c_str()); }); const char *update_package = NULL; bool should_wipe_data = false; bool should_prompt_and_wipe_data = false; bool should_wipe_cache = false; bool should_wipe_ab = false; size_t wipe_package_size = 0; bool show_text = false; bool sideload = false; bool sideload_auto_reboot = false; bool just_exit = false; bool shutdown_after = false; int retry_count = 0; bool security_update = false; int arg; int option_index; while ((arg = getopt_long(args_to_parse.size(), args_to_parse.data(), "", OPTIONS, &option_index)) != -1) { switch (arg) { case 'n': android::base::ParseInt(optarg, &retry_count, 0); break; case 'u': update_package = optarg; break; case 'w': should_wipe_data = true; break; case 'c': should_wipe_cache = true; break; case 't': show_text = true; break; case 's': sideload = true; break; case 'a': sideload = true; sideload_auto_reboot = true; break; case 'x': just_exit = true; break; case 'l': locale = optarg; break; case 'p': shutdown_after = true; break; case 'r': reason = optarg; break; case 'e': security_update = true; break; case 0: { std::string option = OPTIONS[option_index].name; if (option == "wipe_ab") { should_wipe_ab = true; } else if (option == "wipe_package_size") { android::base::ParseUint(optarg, &wipe_package_size); } else if (option == "prompt_and_wipe_data") { should_prompt_and_wipe_data = true; } break; } case '?': LOG(ERROR) << "Invalid command argument"; continue; } } if (locale.empty()) { if (has_cache) { locale = load_locale_from_cache(); } if (locale.empty()) { locale = DEFAULT_LOCALE; } } printf("locale is [%s]\n", locale.c_str()); printf("stage is [%s]\n", stage.c_str()); printf("reason is [%s]\n", reason); Device* device = make_device(); if (android::base::GetBoolProperty("ro.boot.quiescent", false)) { printf("Quiescent recovery mode.\n"); ui = new StubRecoveryUI(); } else { ui = device->GetUI(); if (!ui->Init(locale)) { printf("Failed to initialize UI, use stub UI instead.\n"); ui = new StubRecoveryUI(); } } // Set background string to "installing security update" for security update, // otherwise set it to "installing system update". ui->SetSystemUpdateText(security_update); int st_cur, st_max; if (!stage.empty() && sscanf(stage.c_str(), "%d/%d", &st_cur, &st_max) == 2) { ui->SetStage(st_cur, st_max); } ui->SetBackground(RecoveryUI::NONE); if (show_text) ui->ShowText(true); struct selinux_opt seopts[] = { { SELABEL_OPT_PATH, "/file_contexts" } }; sehandle = selabel_open(SELABEL_CTX_FILE, seopts, 1); if (!sehandle) { ui->Print("Warning: No file_contexts\n"); } device->StartRecovery(); printf("Command:"); for (const auto& arg : args) { printf(" \"%s\"", arg.c_str()); } printf("\n\n"); property_list(print_property, NULL); printf("\n"); ui->Print("Supported API: %d\n", RECOVERY_API_VERSION); int status = INSTALL_SUCCESS; if (update_package != NULL) { // It's not entirely true that we will modify the flash. But we want // to log the update attempt since update_package is non-NULL. modified_flash = true; if (!is_battery_ok()) { ui->Print("battery capacity is not enough for installing package, needed is %d%%\n", BATTERY_OK_PERCENTAGE); // Log the error code to last_install when installation skips due to // low battery. log_failure_code(kLowBattery, update_package); status = INSTALL_SKIPPED; } else if (bootreason_in_blacklist()) { // Skip update-on-reboot when bootreason is kernel_panic or similar ui->Print("bootreason is in the blacklist; skip OTA installation\n"); log_failure_code(kBootreasonInBlacklist, update_package); status = INSTALL_SKIPPED; } else { status = install_package(update_package, &should_wipe_cache, TEMPORARY_INSTALL_FILE, true, retry_count); if (status == INSTALL_SUCCESS && should_wipe_cache) { wipe_cache(false, device); } if (status != INSTALL_SUCCESS) { ui->Print("Installation aborted.\n"); // When I/O error happens, reboot and retry installation RETRY_LIMIT // times before we abandon this OTA update. if (status == INSTALL_RETRY && retry_count < RETRY_LIMIT) { copy_logs(); set_retry_bootloader_message(retry_count, args); // Print retry count on screen. ui->Print("Retry attempt %d\n", retry_count); // Reboot and retry the update if (!reboot("reboot,recovery")) { ui->Print("Reboot failed\n"); } else { while (true) { pause(); } } } // If this is an eng or userdebug build, then automatically // turn the text display on if the script fails so the error // message is visible. if (is_ro_debuggable()) { ui->ShowText(true); } } } } else if (should_wipe_data) { if (!wipe_data(device)) { status = INSTALL_ERROR; } } else if (should_prompt_and_wipe_data) { ui->ShowText(true); ui->SetBackground(RecoveryUI::ERROR); if (!prompt_and_wipe_data(device)) { status = INSTALL_ERROR; } ui->ShowText(false); } else if (should_wipe_cache) { if (!wipe_cache(false, device)) { status = INSTALL_ERROR; } } else if (should_wipe_ab) { if (!wipe_ab_device(wipe_package_size)) { status = INSTALL_ERROR; } } else if (sideload) { // 'adb reboot sideload' acts the same as user presses key combinations // to enter the sideload mode. When 'sideload-auto-reboot' is used, text // display will NOT be turned on by default. And it will reboot after // sideload finishes even if there are errors. Unless one turns on the // text display during the installation. This is to enable automated // testing. if (!sideload_auto_reboot) { ui->ShowText(true); } status = apply_from_adb(&should_wipe_cache, TEMPORARY_INSTALL_FILE); if (status == INSTALL_SUCCESS && should_wipe_cache) { if (!wipe_cache(false, device)) { status = INSTALL_ERROR; } } ui->Print("\nInstall from ADB complete (status: %d).\n", status); if (sideload_auto_reboot) { ui->Print("Rebooting automatically.\n"); } } else if (!just_exit) { // If this is an eng or userdebug build, automatically turn on the text display if no command // is specified. Note that this should be called before setting the background to avoid // flickering the background image. if (is_ro_debuggable()) { ui->ShowText(true); } status = INSTALL_NONE; // No command specified ui->SetBackground(RecoveryUI::NO_COMMAND); } if (status == INSTALL_ERROR || status == INSTALL_CORRUPT) { ui->SetBackground(RecoveryUI::ERROR); if (!ui->IsTextVisible()) { sleep(5); } } Device::BuiltinAction after = shutdown_after ? Device::SHUTDOWN : Device::REBOOT; // 1. If the recovery menu is visible, prompt and wait for commands. // 2. If the state is INSTALL_NONE, wait for commands. (i.e. In user build, manually reboot into // recovery to sideload a package.) // 3. sideload_auto_reboot is an option only available in user-debug build, reboot the device // without waiting. // 4. In all other cases, reboot the device. Therefore, normal users will observe the device // reboot after it shows the "error" screen for 5s. if ((status == INSTALL_NONE && !sideload_auto_reboot) || ui->IsTextVisible()) { Device::BuiltinAction temp = prompt_and_wait(device, status); if (temp != Device::NO_ACTION) { after = temp; } } // Save logs and clean up before rebooting or shutting down. finish_recovery(); switch (after) { case Device::SHUTDOWN: ui->Print("Shutting down...\n"); android::base::SetProperty(ANDROID_RB_PROPERTY, "shutdown,"); break; case Device::REBOOT_BOOTLOADER: ui->Print("Rebooting to bootloader...\n"); android::base::SetProperty(ANDROID_RB_PROPERTY, "reboot,bootloader"); break; default: ui->Print("Rebooting...\n"); reboot("reboot,"); break; } while (true) { pause(); } // Should be unreachable. return EXIT_SUCCESS; }