/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include "roots.h" #include #include #include #include #include #include #include #include #include #include #include #include #include #include "common.h" #include "mounts.h" #include "cryptfs.h" static struct fstab *fstab = NULL; extern struct selabel_handle *sehandle; void load_volume_table() { int i; int ret; fstab = fs_mgr_read_fstab_with_dt("/etc/recovery.fstab"); if (!fstab) { LOG(ERROR) << "failed to read /etc/recovery.fstab"; return; } ret = fs_mgr_add_entry(fstab, "/tmp", "ramdisk", "ramdisk"); if (ret < 0 ) { LOG(ERROR) << "failed to add /tmp entry to fstab"; fs_mgr_free_fstab(fstab); fstab = NULL; return; } printf("recovery filesystem table\n"); printf("=========================\n"); for (i = 0; i < fstab->num_entries; ++i) { Volume* v = &fstab->recs[i]; printf(" %d %s %s %s %lld\n", i, v->mount_point, v->fs_type, v->blk_device, v->length); } printf("\n"); } Volume* volume_for_path(const char* path) { return fs_mgr_get_entry_for_mount_point(fstab, path); } // Mount the volume specified by path at the given mount_point. int ensure_path_mounted_at(const char* path, const char* mount_point) { Volume* v = volume_for_path(path); if (v == NULL) { LOG(ERROR) << "unknown volume for path [" << path << "]"; return -1; } if (strcmp(v->fs_type, "ramdisk") == 0) { // the ramdisk is always mounted. return 0; } if (!scan_mounted_volumes()) { LOG(ERROR) << "failed to scan mounted volumes"; return -1; } if (!mount_point) { mount_point = v->mount_point; } MountedVolume* mv = find_mounted_volume_by_mount_point(mount_point); if (mv) { // volume is already mounted return 0; } mkdir(mount_point, 0755); // in case it doesn't already exist if (strcmp(v->fs_type, "ext4") == 0 || strcmp(v->fs_type, "squashfs") == 0 || strcmp(v->fs_type, "vfat") == 0) { int result = mount(v->blk_device, mount_point, v->fs_type, v->flags, v->fs_options); if (result == -1 && fs_mgr_is_formattable(v)) { LOG(ERROR) << "failed to mount " << mount_point << " (" << strerror(errno) << ") , formatting....."; bool crypt_footer = fs_mgr_is_encryptable(v) && !strcmp(v->key_loc, "footer"); if (fs_mgr_do_format(v, crypt_footer) == 0) { result = mount(v->blk_device, mount_point, v->fs_type, v->flags, v->fs_options); } else { PLOG(ERROR) << "failed to format " << mount_point; return -1; } } if (result == -1) { PLOG(ERROR) << "failed to mount " << mount_point; return -1; } return 0; } LOG(ERROR) << "unknown fs_type \"" << v->fs_type << "\" for " << mount_point; return -1; } int ensure_path_mounted(const char* path) { // Mount at the default mount point. return ensure_path_mounted_at(path, nullptr); } int ensure_path_unmounted(const char* path) { Volume* v = volume_for_path(path); if (v == NULL) { LOG(ERROR) << "unknown volume for path [" << path << "]"; return -1; } if (strcmp(v->fs_type, "ramdisk") == 0) { // the ramdisk is always mounted; you can't unmount it. return -1; } if (!scan_mounted_volumes()) { LOG(ERROR) << "failed to scan mounted volumes"; return -1; } MountedVolume* mv = find_mounted_volume_by_mount_point(v->mount_point); if (mv == NULL) { // volume is already unmounted return 0; } return unmount_mounted_volume(mv); } static int exec_cmd(const char* path, char* const argv[]) { int status; pid_t child; if ((child = vfork()) == 0) { execv(path, argv); _exit(EXIT_FAILURE); } waitpid(child, &status, 0); if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) { LOG(ERROR) << path << " failed with status " << WEXITSTATUS(status); } return WEXITSTATUS(status); } int format_volume(const char* volume, const char* directory) { Volume* v = volume_for_path(volume); if (v == NULL) { LOG(ERROR) << "unknown volume \"" << volume << "\""; return -1; } if (strcmp(v->fs_type, "ramdisk") == 0) { // you can't format the ramdisk. LOG(ERROR) << "can't format_volume \"" << volume << "\""; return -1; } if (strcmp(v->mount_point, volume) != 0) { LOG(ERROR) << "can't give path \"" << volume << "\" to format_volume"; return -1; } if (ensure_path_unmounted(volume) != 0) { LOG(ERROR) << "format_volume failed to unmount \"" << v->mount_point << "\""; return -1; } if (strcmp(v->fs_type, "ext4") == 0 || strcmp(v->fs_type, "f2fs") == 0) { // if there's a key_loc that looks like a path, it should be a // block device for storing encryption metadata. wipe it too. if (v->key_loc != NULL && v->key_loc[0] == '/') { LOG(INFO) << "wiping " << v->key_loc; int fd = open(v->key_loc, O_WRONLY | O_CREAT, 0644); if (fd < 0) { LOG(ERROR) << "format_volume: failed to open " << v->key_loc; return -1; } wipe_block_device(fd, get_file_size(fd)); close(fd); } ssize_t length = 0; if (v->length != 0) { length = v->length; } else if (v->key_loc != NULL && strcmp(v->key_loc, "footer") == 0) { length = -CRYPT_FOOTER_OFFSET; } int result; if (strcmp(v->fs_type, "ext4") == 0) { if (v->erase_blk_size != 0 && v->logical_blk_size != 0) { result = make_ext4fs_directory_align(v->blk_device, length, volume, sehandle, directory, v->erase_blk_size, v->logical_blk_size); } else { result = make_ext4fs_directory(v->blk_device, length, volume, sehandle, directory); } } else { /* Has to be f2fs because we checked earlier. */ if (v->key_loc != NULL && strcmp(v->key_loc, "footer") == 0 && length < 0) { LOG(ERROR) << "format_volume: crypt footer + negative length (" << length << ") not supported on " << v->fs_type; return -1; } if (length < 0) { LOG(ERROR) << "format_volume: negative length (" << length << ") not supported on " << v->fs_type; return -1; } char *num_sectors; if (asprintf(&num_sectors, "%zd", length / 512) <= 0) { LOG(ERROR) << "format_volume: failed to create " << v->fs_type << " command for " << v->blk_device; return -1; } const char *f2fs_path = "/sbin/mkfs.f2fs"; const char* const f2fs_argv[] = {"mkfs.f2fs", "-t", "-d1", v->blk_device, num_sectors, NULL}; result = exec_cmd(f2fs_path, (char* const*)f2fs_argv); free(num_sectors); } if (result != 0) { PLOG(ERROR) << "format_volume: make " << v->fs_type << " failed on " << v->blk_device; return -1; } return 0; } LOG(ERROR) << "format_volume: fs_type \"" << v->fs_type << "\" unsupported"; return -1; } int format_volume(const char* volume) { return format_volume(volume, NULL); } int setup_install_mounts() { if (fstab == NULL) { LOG(ERROR) << "can't set up install mounts: no fstab loaded"; return -1; } for (int i = 0; i < fstab->num_entries; ++i) { Volume* v = fstab->recs + i; if (strcmp(v->mount_point, "/tmp") == 0 || strcmp(v->mount_point, "/cache") == 0) { if (ensure_path_mounted(v->mount_point) != 0) { LOG(ERROR) << "failed to mount " << v->mount_point; return -1; } } else { if (ensure_path_unmounted(v->mount_point) != 0) { LOG(ERROR) << "failed to unmount " << v->mount_point; return -1; } } } return 0; }