/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include "roots.h" #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "common.h" #include "mounts.h" static struct fstab* fstab = nullptr; extern struct selabel_handle* sehandle; void load_volume_table() { fstab = fs_mgr_read_fstab_default(); if (!fstab) { LOG(ERROR) << "Failed to read default fstab"; return; } int ret = fs_mgr_add_entry(fstab, "/tmp", "ramdisk", "ramdisk"); if (ret == -1) { LOG(ERROR) << "Failed to add /tmp entry to fstab"; fs_mgr_free_fstab(fstab); fstab = nullptr; return; } printf("recovery filesystem table\n"); printf("=========================\n"); for (int i = 0; i < fstab->num_entries; ++i) { const Volume* v = &fstab->recs[i]; printf(" %d %s %s %s %lld\n", i, v->mount_point, v->fs_type, v->blk_device, v->length); } printf("\n"); } // Finds the volume specified by the given path. fs_mgr_get_entry_for_mount_point() does exact match // only, so it attempts the prefixes recursively (e.g. "/cache/recovery/last_log", // "/cache/recovery", "/cache", "/" for a given path of "/cache/recovery/last_log") and returns the // first match or nullptr. Volume* volume_for_path(const char* path) { if (path == nullptr || path[0] == '\0') return nullptr; std::string str(path); while (true) { Volume* result = fs_mgr_get_entry_for_mount_point(fstab, str.c_str()); if (result != nullptr || str == "/") { return result; } size_t slash = str.find_last_of('/'); if (slash == std::string::npos) return nullptr; if (slash == 0) { str = "/"; } else { str = str.substr(0, slash); } } return nullptr; } // Mount the volume specified by path at the given mount_point. int ensure_path_mounted_at(const char* path, const char* mount_point) { Volume* v = volume_for_path(path); if (v == nullptr) { LOG(ERROR) << "unknown volume for path [" << path << "]"; return -1; } if (strcmp(v->fs_type, "ramdisk") == 0) { // The ramdisk is always mounted. return 0; } if (!scan_mounted_volumes()) { LOG(ERROR) << "Failed to scan mounted volumes"; return -1; } if (!mount_point) { mount_point = v->mount_point; } const MountedVolume* mv = find_mounted_volume_by_mount_point(mount_point); if (mv != nullptr) { // Volume is already mounted. return 0; } mkdir(mount_point, 0755); // in case it doesn't already exist if (strcmp(v->fs_type, "ext4") == 0 || strcmp(v->fs_type, "squashfs") == 0 || strcmp(v->fs_type, "vfat") == 0) { int result = mount(v->blk_device, mount_point, v->fs_type, v->flags, v->fs_options); if (result == -1 && fs_mgr_is_formattable(v)) { PLOG(ERROR) << "Failed to mount " << mount_point << "; formatting"; bool crypt_footer = fs_mgr_is_encryptable(v) && !strcmp(v->key_loc, "footer"); if (fs_mgr_do_format(v, crypt_footer) == 0) { result = mount(v->blk_device, mount_point, v->fs_type, v->flags, v->fs_options); } else { PLOG(ERROR) << "Failed to format " << mount_point; return -1; } } if (result == -1) { PLOG(ERROR) << "Failed to mount " << mount_point; return -1; } return 0; } LOG(ERROR) << "unknown fs_type \"" << v->fs_type << "\" for " << mount_point; return -1; } int ensure_path_mounted(const char* path) { // Mount at the default mount point. return ensure_path_mounted_at(path, nullptr); } int ensure_path_unmounted(const char* path) { const Volume* v = volume_for_path(path); if (v == nullptr) { LOG(ERROR) << "unknown volume for path [" << path << "]"; return -1; } if (strcmp(v->fs_type, "ramdisk") == 0) { // The ramdisk is always mounted; you can't unmount it. return -1; } if (!scan_mounted_volumes()) { LOG(ERROR) << "Failed to scan mounted volumes"; return -1; } MountedVolume* mv = find_mounted_volume_by_mount_point(v->mount_point); if (mv == nullptr) { // Volume is already unmounted. return 0; } return unmount_mounted_volume(mv); } static int exec_cmd(const std::vector& args) { CHECK_NE(static_cast(0), args.size()); std::vector argv(args.size()); std::transform(args.cbegin(), args.cend(), argv.begin(), [](const std::string& arg) { return const_cast(arg.c_str()); }); argv.push_back(nullptr); pid_t child; if ((child = vfork()) == 0) { execv(argv[0], argv.data()); _exit(EXIT_FAILURE); } int status; waitpid(child, &status, 0); if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) { LOG(ERROR) << args[0] << " failed with status " << WEXITSTATUS(status); } return WEXITSTATUS(status); } static int64_t get_file_size(int fd, uint64_t reserve_len) { struct stat buf; int ret = fstat(fd, &buf); if (ret) return 0; int64_t computed_size; if (S_ISREG(buf.st_mode)) { computed_size = buf.st_size - reserve_len; } else if (S_ISBLK(buf.st_mode)) { uint64_t block_device_size = get_block_device_size(fd); if (block_device_size < reserve_len || block_device_size > std::numeric_limits::max()) { computed_size = 0; } else { computed_size = block_device_size - reserve_len; } } else { computed_size = 0; } return computed_size; } int format_volume(const char* volume, const char* directory) { const Volume* v = volume_for_path(volume); if (v == nullptr) { LOG(ERROR) << "unknown volume \"" << volume << "\""; return -1; } if (strcmp(v->fs_type, "ramdisk") == 0) { LOG(ERROR) << "can't format_volume \"" << volume << "\""; return -1; } if (strcmp(v->mount_point, volume) != 0) { LOG(ERROR) << "can't give path \"" << volume << "\" to format_volume"; return -1; } if (ensure_path_unmounted(volume) != 0) { LOG(ERROR) << "format_volume: Failed to unmount \"" << v->mount_point << "\""; return -1; } if (strcmp(v->fs_type, "ext4") != 0 && strcmp(v->fs_type, "f2fs") != 0) { LOG(ERROR) << "format_volume: fs_type \"" << v->fs_type << "\" unsupported"; return -1; } // If there's a key_loc that looks like a path, it should be a block device for storing encryption // metadata. Wipe it too. if (v->key_loc != nullptr && v->key_loc[0] == '/') { LOG(INFO) << "Wiping " << v->key_loc; int fd = open(v->key_loc, O_WRONLY | O_CREAT, 0644); if (fd == -1) { PLOG(ERROR) << "format_volume: Failed to open " << v->key_loc; return -1; } wipe_block_device(fd, get_file_size(fd)); close(fd); } int64_t length = 0; if (v->length != 0) { length = v->length; } else if (v->key_loc != nullptr && strcmp(v->key_loc, "footer") == 0) { android::base::unique_fd fd(open(v->blk_device, O_RDONLY)); if (fd == -1) { PLOG(ERROR) << "format_volume: failed to open " << v->blk_device; return -1; } length = get_file_size(fd.get(), CRYPT_FOOTER_OFFSET); if (length <= 0) { LOG(ERROR) << "get_file_size: invalid size " << length << " for " << v->blk_device; return -1; } } if (strcmp(v->fs_type, "ext4") == 0) { static constexpr int kBlockSize = 4096; std::vector mke2fs_args = { "/sbin/mke2fs_static", "-F", "-t", "ext4", "-b", std::to_string(kBlockSize), }; int raid_stride = v->logical_blk_size / kBlockSize; int raid_stripe_width = v->erase_blk_size / kBlockSize; // stride should be the max of 8KB and logical block size if (v->logical_blk_size != 0 && v->logical_blk_size < 8192) { raid_stride = 8192 / kBlockSize; } if (v->erase_blk_size != 0 && v->logical_blk_size != 0) { mke2fs_args.push_back("-E"); mke2fs_args.push_back( android::base::StringPrintf("stride=%d,stripe-width=%d", raid_stride, raid_stripe_width)); } mke2fs_args.push_back(v->blk_device); if (length != 0) { mke2fs_args.push_back(std::to_string(length / kBlockSize)); } int result = exec_cmd(mke2fs_args); if (result == 0 && directory != nullptr) { std::vector e2fsdroid_args = { "/sbin/e2fsdroid_static", "-e", "-f", directory, "-a", volume, v->blk_device, }; result = exec_cmd(e2fsdroid_args); } if (result != 0) { PLOG(ERROR) << "format_volume: Failed to make ext4 on " << v->blk_device; return -1; } return 0; } // Has to be f2fs because we checked earlier. std::vector f2fs_args = { "/sbin/mkfs.f2fs", "-t", "-d1", v->blk_device }; if (length >= 512) { f2fs_args.push_back(std::to_string(length / 512)); } int result = exec_cmd(f2fs_args); if (result != 0) { PLOG(ERROR) << "format_volume: Failed to make f2fs on " << v->blk_device; return -1; } return 0; } int format_volume(const char* volume) { return format_volume(volume, nullptr); } int setup_install_mounts() { if (fstab == nullptr) { LOG(ERROR) << "can't set up install mounts: no fstab loaded"; return -1; } for (int i = 0; i < fstab->num_entries; ++i) { const Volume* v = fstab->recs + i; // We don't want to do anything with "/". if (strcmp(v->mount_point, "/") == 0) { continue; } if (strcmp(v->mount_point, "/tmp") == 0 || strcmp(v->mount_point, "/cache") == 0) { if (ensure_path_mounted(v->mount_point) != 0) { LOG(ERROR) << "Failed to mount " << v->mount_point; return -1; } } else { if (ensure_path_unmounted(v->mount_point) != 0) { LOG(ERROR) << "Failed to unmount " << v->mount_point; return -1; } } } return 0; }