/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef RECOVERY_ROOTS_H_ #define RECOVERY_ROOTS_H_ typedef struct fstab_rec Volume; // Load and parse volume data from /etc/recovery.fstab. void load_volume_table(); // Return the Volume* record for this path (or NULL). Volume* volume_for_path(const char* path); // Make sure that the volume 'path' is on is mounted. Returns 0 on // success (volume is mounted). int ensure_path_mounted(const char* path); // Similar to ensure_path_mounted, but allows one to specify the mount_point. int ensure_path_mounted_at(const char* path, const char* mount_point); // Make sure that the volume 'path' is on is unmounted. Returns 0 on // success (volume is unmounted); int ensure_path_unmounted(const char* path); // Reformat the given volume (must be the mount point only, eg // "/cache"), no paths permitted. Attempts to unmount the volume if // it is mounted. int format_volume(const char* volume); // Reformat the given volume (must be the mount point only, eg // "/cache"), no paths permitted. Attempts to unmount the volume if // it is mounted. // Copies 'directory' to root of the newly formatted volume int format_volume(const char* volume, const char* directory); // Ensure that all and only the volumes that packages expect to find // mounted (/tmp and /cache) are mounted. Returns 0 on success. int setup_install_mounts(); #endif // RECOVERY_ROOTS_H_