aboutsummaryrefslogtreecommitdiffstats
blob: 08dfcdff499497f98b72351dacaa10c50689a021 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
/*
 * Copyright (C) 2011 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _RECOVERY_DEVICE_H
#define _RECOVERY_DEVICE_H

#include "ui.h"

class Device {
  public:
    explicit Device(RecoveryUI* ui) : ui_(ui) { }
    virtual ~Device() { }

    // Called to obtain the UI object that should be used to display
    // the recovery user interface for this device.  You should not
    // have called Init() on the UI object already, the caller will do
    // that after this method returns.
    virtual RecoveryUI* GetUI() { return ui_; }

    // Called when recovery starts up (after the UI has been obtained
    // and initialized and after the arguments have been parsed, but
    // before anything else).
    virtual void StartRecovery() { };

    // Called from the main thread when recovery is at the main menu
    // and waiting for input, and a key is pressed.  (Note that "at"
    // the main menu does not necessarily mean the menu is visible;
    // recovery will be at the main menu with it invisible after an
    // unsuccessful operation [ie OTA package failure], or if recovery
    // is started with no command.)
    //
    // key is the code of the key just pressed.  (You can call
    // IsKeyPressed() on the RecoveryUI object you returned from GetUI
    // if you want to find out if other keys are held down.)
    //
    // visible is true if the menu is visible.
    //
    // Return one of the defined constants below in order to:
    //
    //   - move the menu highlight (kHighlight{Up,Down})
    //   - invoke the highlighted item (kInvokeItem)
    //   - do nothing (kNoAction)
    //   - invoke a specific action (a menu position: any non-negative number)
    virtual int HandleMenuKey(int key, int visible);

    enum BuiltinAction {
        NO_ACTION = 0,
        REBOOT = 1,
        APPLY_SDCARD = 2,
        // APPLY_CACHE was 3.
        APPLY_ADB_SIDELOAD = 4,
        WIPE_DATA = 5,
        WIPE_CACHE = 6,
        REBOOT_BOOTLOADER = 7,
        SHUTDOWN = 8,
        VIEW_RECOVERY_LOGS = 9,
        MOUNT_SYSTEM = 10,
        RUN_GRAPHICS_TEST = 11,
    };

    // Return the list of menu items (an array of strings,
    // NULL-terminated).  The menu_position passed to InvokeMenuItem
    // will correspond to the indexes into this array.
    virtual const char* const* GetMenuItems();

    // Perform a recovery action selected from the menu.
    // 'menu_position' will be the item number of the selected menu
    // item, or a non-negative number returned from
    // device_handle_key().  The menu will be hidden when this is
    // called; implementations can call ui_print() to print
    // information to the screen.  If the menu position is one of the
    // builtin actions, you can just return the corresponding enum
    // value.  If it is an action specific to your device, you
    // actually perform it here and return NO_ACTION.
    virtual BuiltinAction InvokeMenuItem(int menu_position);

    static const int kNoAction = -1;
    static const int kHighlightUp = -2;
    static const int kHighlightDown = -3;
    static const int kInvokeItem = -4;

    // Called before and after we do a wipe data/factory reset operation,
    // either via a reboot from the main system with the --wipe_data flag,
    // or when the user boots into recovery image manually and selects the
    // option from the menu, to perform whatever device-specific wiping
    // actions are needed.
    // Return true on success; returning false from PreWipeData will prevent
    // the regular wipe, and returning false from PostWipeData will cause
    // the wipe to be considered a failure.
    virtual bool PreWipeData() { return true; }
    virtual bool PostWipeData() { return true; }

  private:
    RecoveryUI* ui_;
};

// The device-specific library must define this function (or the
// default one will be used, if there is no device-specific library).
// It returns the Device object that recovery should use.
Device* make_device();

#endif  // _DEVICE_H