aboutsummaryrefslogtreecommitdiffstats
blob: 74d1a68b336069309e44e000eddbc44529c357cb (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
683
684
685
686
687
688
689
690
691
692
693
694
695
696
697
698
699
700
701
702
703
704
705
706
707
708
709
710
711
712
713
714
715
716
717
718
719
720
721
722
723
724
725
726
727
728
/*
 * Copyright (C) 2007 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "install.h"

#include <ctype.h>
#include <errno.h>
#include <fcntl.h>
#include <inttypes.h>
#include <limits.h>
#include <string.h>
#include <sys/stat.h>
#include <sys/wait.h>
#include <unistd.h>

#include <algorithm>
#include <atomic>
#include <chrono>
#include <condition_variable>
#include <functional>
#include <limits>
#include <map>
#include <mutex>
#include <string>
#include <thread>
#include <vector>

#include <android-base/file.h>
#include <android-base/logging.h>
#include <android-base/parsedouble.h>
#include <android-base/parseint.h>
#include <android-base/properties.h>
#include <android-base/stringprintf.h>
#include <android-base/strings.h>
#include <vintf/VintfObjectRecovery.h>
#include <ziparchive/zip_archive.h>

#include "common.h"
#include "error_code.h"
#include "otautil/SysUtil.h"
#include "otautil/ThermalUtil.h"
#include "private/install.h"
#include "roots.h"
#include "ui.h"
#include "verifier.h"

using namespace std::chrono_literals;

// Default allocation of progress bar segments to operations
static constexpr int VERIFICATION_PROGRESS_TIME = 60;
static constexpr float VERIFICATION_PROGRESS_FRACTION = 0.25;

static std::condition_variable finish_log_temperature;

// This function parses and returns the build.version.incremental
static std::string parse_build_number(const std::string& str) {
    size_t pos = str.find('=');
    if (pos != std::string::npos) {
        return android::base::Trim(str.substr(pos+1));
    }

    LOG(ERROR) << "Failed to parse build number in " << str;
    return "";
}

bool read_metadata_from_package(ZipArchiveHandle zip, std::string* metadata) {
  CHECK(metadata != nullptr);

  static constexpr const char* METADATA_PATH = "META-INF/com/android/metadata";
  ZipString path(METADATA_PATH);
  ZipEntry entry;
  if (FindEntry(zip, path, &entry) != 0) {
    LOG(ERROR) << "Failed to find " << METADATA_PATH;
    return false;
  }

  uint32_t length = entry.uncompressed_length;
  metadata->resize(length, '\0');
  int32_t err = ExtractToMemory(zip, &entry, reinterpret_cast<uint8_t*>(&(*metadata)[0]), length);
  if (err != 0) {
    LOG(ERROR) << "Failed to extract " << METADATA_PATH << ": " << ErrorCodeString(err);
    return false;
  }
  return true;
}

// Read the build.version.incremental of src/tgt from the metadata and log it to last_install.
static void read_source_target_build(ZipArchiveHandle zip, std::vector<std::string>* log_buffer) {
  std::string metadata;
  if (!read_metadata_from_package(zip, &metadata)) {
    return;
  }
  // Examples of the pre-build and post-build strings in metadata:
  //   pre-build-incremental=2943039
  //   post-build-incremental=2951741
  std::vector<std::string> lines = android::base::Split(metadata, "\n");
  for (const std::string& line : lines) {
    std::string str = android::base::Trim(line);
    if (android::base::StartsWith(str, "pre-build-incremental")) {
      std::string source_build = parse_build_number(str);
      if (!source_build.empty()) {
        log_buffer->push_back("source_build: " + source_build);
      }
    } else if (android::base::StartsWith(str, "post-build-incremental")) {
      std::string target_build = parse_build_number(str);
      if (!target_build.empty()) {
        log_buffer->push_back("target_build: " + target_build);
      }
    }
  }
}

#ifdef AB_OTA_UPDATER

// Parses the metadata of the OTA package in |zip| and checks whether we are
// allowed to accept this A/B package. Downgrading is not allowed unless
// explicitly enabled in the package and only for incremental packages.
static int check_newer_ab_build(ZipArchiveHandle zip) {
  std::string metadata_str;
  if (!read_metadata_from_package(zip, &metadata_str)) {
    return INSTALL_CORRUPT;
  }
  std::map<std::string, std::string> metadata;
  for (const std::string& line : android::base::Split(metadata_str, "\n")) {
    size_t eq = line.find('=');
    if (eq != std::string::npos) {
      metadata[line.substr(0, eq)] = line.substr(eq + 1);
    }
  }

  std::string value = android::base::GetProperty("ro.product.device", "");
  const std::string& pkg_device = metadata["pre-device"];
  if (pkg_device != value || pkg_device.empty()) {
    LOG(ERROR) << "Package is for product " << pkg_device << " but expected " << value;
    return INSTALL_ERROR;
  }

  // We allow the package to not have any serialno; and we also allow it to carry multiple serial
  // numbers split by "|"; e.g. serialno=serialno1|serialno2|serialno3 ... We will fail the
  // verification if the device's serialno doesn't match any of these carried numbers.
  value = android::base::GetProperty("ro.serialno", "");
  const std::string& pkg_serial_no = metadata["serialno"];
  if (!pkg_serial_no.empty()) {
    bool match = false;
    for (const std::string& number : android::base::Split(pkg_serial_no, "|")) {
      if (value == android::base::Trim(number)) {
        match = true;
        break;
      }
    }
    if (!match) {
      LOG(ERROR) << "Package is for serial " << pkg_serial_no;
      return INSTALL_ERROR;
    }
  }

  if (metadata["ota-type"] != "AB") {
    LOG(ERROR) << "Package is not A/B";
    return INSTALL_ERROR;
  }

  // Incremental updates should match the current build.
  value = android::base::GetProperty("ro.build.version.incremental", "");
  const std::string& pkg_pre_build = metadata["pre-build-incremental"];
  if (!pkg_pre_build.empty() && pkg_pre_build != value) {
    LOG(ERROR) << "Package is for source build " << pkg_pre_build << " but expected " << value;
    return INSTALL_ERROR;
  }

  value = android::base::GetProperty("ro.build.fingerprint", "");
  const std::string& pkg_pre_build_fingerprint = metadata["pre-build"];
  if (!pkg_pre_build_fingerprint.empty() && pkg_pre_build_fingerprint != value) {
    LOG(ERROR) << "Package is for source build " << pkg_pre_build_fingerprint << " but expected "
               << value;
    return INSTALL_ERROR;
  }

  // Check for downgrade version.
  int64_t build_timestamp =
      android::base::GetIntProperty("ro.build.date.utc", std::numeric_limits<int64_t>::max());
  int64_t pkg_post_timestamp = 0;
  // We allow to full update to the same version we are running, in case there
  // is a problem with the current copy of that version.
  if (metadata["post-timestamp"].empty() ||
      !android::base::ParseInt(metadata["post-timestamp"].c_str(), &pkg_post_timestamp) ||
      pkg_post_timestamp < build_timestamp) {
    if (metadata["ota-downgrade"] != "yes") {
      LOG(ERROR) << "Update package is older than the current build, expected a build "
                    "newer than timestamp "
                 << build_timestamp << " but package has timestamp " << pkg_post_timestamp
                 << " and downgrade not allowed.";
      return INSTALL_ERROR;
    }
    if (pkg_pre_build_fingerprint.empty()) {
      LOG(ERROR) << "Downgrade package must have a pre-build version set, not allowed.";
      return INSTALL_ERROR;
    }
  }

  return 0;
}

int update_binary_command(const std::string& package, ZipArchiveHandle zip,
                          const std::string& binary_path, int /* retry_count */, int status_fd,
                          std::vector<std::string>* cmd) {
  CHECK(cmd != nullptr);
  int ret = check_newer_ab_build(zip);
  if (ret != 0) {
    return ret;
  }

  // For A/B updates we extract the payload properties to a buffer and obtain the RAW payload offset
  // in the zip file.
  static constexpr const char* AB_OTA_PAYLOAD_PROPERTIES = "payload_properties.txt";
  ZipString property_name(AB_OTA_PAYLOAD_PROPERTIES);
  ZipEntry properties_entry;
  if (FindEntry(zip, property_name, &properties_entry) != 0) {
    LOG(ERROR) << "Failed to find " << AB_OTA_PAYLOAD_PROPERTIES;
    return INSTALL_CORRUPT;
  }
  uint32_t properties_entry_length = properties_entry.uncompressed_length;
  std::vector<uint8_t> payload_properties(properties_entry_length);
  int32_t err =
      ExtractToMemory(zip, &properties_entry, payload_properties.data(), properties_entry_length);
  if (err != 0) {
    LOG(ERROR) << "Failed to extract " << AB_OTA_PAYLOAD_PROPERTIES << ": " << ErrorCodeString(err);
    return INSTALL_CORRUPT;
  }

  static constexpr const char* AB_OTA_PAYLOAD = "payload.bin";
  ZipString payload_name(AB_OTA_PAYLOAD);
  ZipEntry payload_entry;
  if (FindEntry(zip, payload_name, &payload_entry) != 0) {
    LOG(ERROR) << "Failed to find " << AB_OTA_PAYLOAD;
    return INSTALL_CORRUPT;
  }
  long payload_offset = payload_entry.offset;
  *cmd = {
    binary_path,
    "--payload=file://" + package,
    android::base::StringPrintf("--offset=%ld", payload_offset),
    "--headers=" + std::string(payload_properties.begin(), payload_properties.end()),
    android::base::StringPrintf("--status_fd=%d", status_fd),
  };
  return 0;
}

#else  // !AB_OTA_UPDATER

int update_binary_command(const std::string& package, ZipArchiveHandle zip,
                          const std::string& binary_path, int retry_count, int status_fd,
                          std::vector<std::string>* cmd) {
  CHECK(cmd != nullptr);

  // On traditional updates we extract the update binary from the package.
  static constexpr const char* UPDATE_BINARY_NAME = "META-INF/com/google/android/update-binary";
  ZipString binary_name(UPDATE_BINARY_NAME);
  ZipEntry binary_entry;
  if (FindEntry(zip, binary_name, &binary_entry) != 0) {
    LOG(ERROR) << "Failed to find update binary " << UPDATE_BINARY_NAME;
    return INSTALL_CORRUPT;
  }

  unlink(binary_path.c_str());
  int fd = open(binary_path.c_str(), O_CREAT | O_WRONLY | O_TRUNC | O_CLOEXEC, 0755);
  if (fd == -1) {
    PLOG(ERROR) << "Failed to create " << binary_path;
    return INSTALL_ERROR;
  }

  int32_t error = ExtractEntryToFile(zip, &binary_entry, fd);
  close(fd);
  if (error != 0) {
    LOG(ERROR) << "Failed to extract " << UPDATE_BINARY_NAME << ": " << ErrorCodeString(error);
    return INSTALL_ERROR;
  }

  *cmd = {
    binary_path,
    std::to_string(kRecoveryApiVersion),
    std::to_string(status_fd),
    package,
  };
  if (retry_count > 0) {
    cmd->push_back("retry");
  }
  return 0;
}
#endif  // !AB_OTA_UPDATER

static void log_max_temperature(int* max_temperature, const std::atomic<bool>& logger_finished) {
  CHECK(max_temperature != nullptr);
  std::mutex mtx;
  std::unique_lock<std::mutex> lck(mtx);
  while (!logger_finished.load() &&
         finish_log_temperature.wait_for(lck, 20s) == std::cv_status::timeout) {
    *max_temperature = std::max(*max_temperature, GetMaxValueFromThermalZone());
  }
}

// If the package contains an update binary, extract it and run it.
static int try_update_binary(const std::string& package, ZipArchiveHandle zip, bool* wipe_cache,
                             std::vector<std::string>* log_buffer, int retry_count,
                             int* max_temperature) {
  read_source_target_build(zip, log_buffer);

  int pipefd[2];
  pipe(pipefd);

  std::vector<std::string> args;
#ifdef AB_OTA_UPDATER
  int ret = update_binary_command(package, zip, "/sbin/update_engine_sideload", retry_count,
                                  pipefd[1], &args);
#else
  int ret = update_binary_command(package, zip, "/tmp/update-binary", retry_count, pipefd[1],
                                  &args);
#endif
  if (ret) {
    close(pipefd[0]);
    close(pipefd[1]);
    log_buffer->push_back(android::base::StringPrintf("error: %d", kUpdateBinaryCommandFailure));
    return ret;
  }

  // When executing the update binary contained in the package, the
  // arguments passed are:
  //
  //   - the version number for this interface
  //
  //   - an FD to which the program can write in order to update the
  //     progress bar.  The program can write single-line commands:
  //
  //        progress <frac> <secs>
  //            fill up the next <frac> part of of the progress bar
  //            over <secs> seconds.  If <secs> is zero, use
  //            set_progress commands to manually control the
  //            progress of this segment of the bar.
  //
  //        set_progress <frac>
  //            <frac> should be between 0.0 and 1.0; sets the
  //            progress bar within the segment defined by the most
  //            recent progress command.
  //
  //        ui_print <string>
  //            display <string> on the screen.
  //
  //        wipe_cache
  //            a wipe of cache will be performed following a successful
  //            installation.
  //
  //        clear_display
  //            turn off the text display.
  //
  //        enable_reboot
  //            packages can explicitly request that they want the user
  //            to be able to reboot during installation (useful for
  //            debugging packages that don't exit).
  //
  //        retry_update
  //            updater encounters some issue during the update. It requests
  //            a reboot to retry the same package automatically.
  //
  //        log <string>
  //            updater requests logging the string (e.g. cause of the
  //            failure).
  //
  //   - the name of the package zip file.
  //
  //   - an optional argument "retry" if this update is a retry of a failed
  //   update attempt.
  //

  // Convert the vector to a NULL-terminated char* array suitable for execv.
  const char* chr_args[args.size() + 1];
  chr_args[args.size()] = nullptr;
  for (size_t i = 0; i < args.size(); i++) {
    chr_args[i] = args[i].c_str();
  }

  pid_t pid = fork();

  if (pid == -1) {
    close(pipefd[0]);
    close(pipefd[1]);
    PLOG(ERROR) << "Failed to fork update binary";
    log_buffer->push_back(android::base::StringPrintf("error: %d", kForkUpdateBinaryFailure));
    return INSTALL_ERROR;
  }

  if (pid == 0) {
    umask(022);
    close(pipefd[0]);
    execv(chr_args[0], const_cast<char**>(chr_args));
    // Bug: 34769056
    // We shouldn't use LOG/PLOG in the forked process, since they may cause
    // the child process to hang. This deadlock results from an improperly
    // copied mutex in the ui functions.
    fprintf(stdout, "E:Can't run %s (%s)\n", chr_args[0], strerror(errno));
    _exit(EXIT_FAILURE);
  }
  close(pipefd[1]);

  std::atomic<bool> logger_finished(false);
  std::thread temperature_logger(log_max_temperature, max_temperature, std::ref(logger_finished));

  *wipe_cache = false;
  bool retry_update = false;

  char buffer[1024];
  FILE* from_child = fdopen(pipefd[0], "r");
  while (fgets(buffer, sizeof(buffer), from_child) != nullptr) {
    std::string line(buffer);
    size_t space = line.find_first_of(" \n");
    std::string command(line.substr(0, space));
    if (command.empty()) continue;

    // Get rid of the leading and trailing space and/or newline.
    std::string args = space == std::string::npos ? "" : android::base::Trim(line.substr(space));

    if (command == "progress") {
      std::vector<std::string> tokens = android::base::Split(args, " ");
      double fraction;
      int seconds;
      if (tokens.size() == 2 && android::base::ParseDouble(tokens[0].c_str(), &fraction) &&
          android::base::ParseInt(tokens[1], &seconds)) {
        ui->ShowProgress(fraction * (1 - VERIFICATION_PROGRESS_FRACTION), seconds);
      } else {
        LOG(ERROR) << "invalid \"progress\" parameters: " << line;
      }
    } else if (command == "set_progress") {
      std::vector<std::string> tokens = android::base::Split(args, " ");
      double fraction;
      if (tokens.size() == 1 && android::base::ParseDouble(tokens[0].c_str(), &fraction)) {
        ui->SetProgress(fraction);
      } else {
        LOG(ERROR) << "invalid \"set_progress\" parameters: " << line;
      }
    } else if (command == "ui_print") {
      ui->PrintOnScreenOnly("%s\n", args.c_str());
      fflush(stdout);
    } else if (command == "wipe_cache") {
      *wipe_cache = true;
    } else if (command == "clear_display") {
      ui->SetBackground(RecoveryUI::NONE);
    } else if (command == "enable_reboot") {
      // packages can explicitly request that they want the user
      // to be able to reboot during installation (useful for
      // debugging packages that don't exit).
      ui->SetEnableReboot(true);
    } else if (command == "retry_update") {
      retry_update = true;
    } else if (command == "log") {
      if (!args.empty()) {
        // Save the logging request from updater and write to last_install later.
        log_buffer->push_back(args);
      } else {
        LOG(ERROR) << "invalid \"log\" parameters: " << line;
      }
    } else {
      LOG(ERROR) << "unknown command [" << command << "]";
    }
  }
  fclose(from_child);

  int status;
  waitpid(pid, &status, 0);

  logger_finished.store(true);
  finish_log_temperature.notify_one();
  temperature_logger.join();

  if (retry_update) {
    return INSTALL_RETRY;
  }
  if (!WIFEXITED(status) || WEXITSTATUS(status) != 0) {
    LOG(ERROR) << "Error in " << package << " (Status " << WEXITSTATUS(status) << ")";
    return INSTALL_ERROR;
  }

  return INSTALL_SUCCESS;
}

// Verifes the compatibility info in a Treble-compatible package. Returns true directly if the
// entry doesn't exist. Note that the compatibility info is packed in a zip file inside the OTA
// package.
bool verify_package_compatibility(ZipArchiveHandle package_zip) {
  LOG(INFO) << "Verifying package compatibility...";

  static constexpr const char* COMPATIBILITY_ZIP_ENTRY = "compatibility.zip";
  ZipString compatibility_entry_name(COMPATIBILITY_ZIP_ENTRY);
  ZipEntry compatibility_entry;
  if (FindEntry(package_zip, compatibility_entry_name, &compatibility_entry) != 0) {
    LOG(INFO) << "Package doesn't contain " << COMPATIBILITY_ZIP_ENTRY << " entry";
    return true;
  }

  std::string zip_content(compatibility_entry.uncompressed_length, '\0');
  int32_t ret;
  if ((ret = ExtractToMemory(package_zip, &compatibility_entry,
                             reinterpret_cast<uint8_t*>(&zip_content[0]),
                             compatibility_entry.uncompressed_length)) != 0) {
    LOG(ERROR) << "Failed to read " << COMPATIBILITY_ZIP_ENTRY << ": " << ErrorCodeString(ret);
    return false;
  }

  ZipArchiveHandle zip_handle;
  ret = OpenArchiveFromMemory(static_cast<void*>(const_cast<char*>(zip_content.data())),
                              zip_content.size(), COMPATIBILITY_ZIP_ENTRY, &zip_handle);
  if (ret != 0) {
    LOG(ERROR) << "Failed to OpenArchiveFromMemory: " << ErrorCodeString(ret);
    return false;
  }

  // Iterate all the entries inside COMPATIBILITY_ZIP_ENTRY and read the contents.
  void* cookie;
  ret = StartIteration(zip_handle, &cookie, nullptr, nullptr);
  if (ret != 0) {
    LOG(ERROR) << "Failed to start iterating zip entries: " << ErrorCodeString(ret);
    CloseArchive(zip_handle);
    return false;
  }
  std::unique_ptr<void, decltype(&EndIteration)> guard(cookie, EndIteration);

  std::vector<std::string> compatibility_info;
  ZipEntry info_entry;
  ZipString info_name;
  while (Next(cookie, &info_entry, &info_name) == 0) {
    std::string content(info_entry.uncompressed_length, '\0');
    int32_t ret = ExtractToMemory(zip_handle, &info_entry, reinterpret_cast<uint8_t*>(&content[0]),
                                  info_entry.uncompressed_length);
    if (ret != 0) {
      LOG(ERROR) << "Failed to read " << info_name.name << ": " << ErrorCodeString(ret);
      CloseArchive(zip_handle);
      return false;
    }
    compatibility_info.emplace_back(std::move(content));
  }
  CloseArchive(zip_handle);

  // VintfObjectRecovery::CheckCompatibility returns zero on success.
  std::string err;
  int result = android::vintf::VintfObjectRecovery::CheckCompatibility(compatibility_info, &err);
  if (result == 0) {
    return true;
  }

  LOG(ERROR) << "Failed to verify package compatibility (result " << result << "): " << err;
  return false;
}

static int really_install_package(const std::string& path, bool* wipe_cache, bool needs_mount,
                                  std::vector<std::string>* log_buffer, int retry_count,
                                  int* max_temperature) {
  ui->SetBackground(RecoveryUI::INSTALLING_UPDATE);
  ui->Print("Finding update package...\n");
  // Give verification half the progress bar...
  ui->SetProgressType(RecoveryUI::DETERMINATE);
  ui->ShowProgress(VERIFICATION_PROGRESS_FRACTION, VERIFICATION_PROGRESS_TIME);
  LOG(INFO) << "Update location: " << path;

  // Map the update package into memory.
  ui->Print("Opening update package...\n");

  if (needs_mount) {
    if (path[0] == '@') {
      ensure_path_mounted(path.substr(1).c_str());
    } else {
      ensure_path_mounted(path.c_str());
    }
  }

  MemMapping map;
  if (!map.MapFile(path)) {
    LOG(ERROR) << "failed to map file";
    log_buffer->push_back(android::base::StringPrintf("error: %d", kMapFileFailure));
    return INSTALL_CORRUPT;
  }

  // Verify package.
  if (!verify_package(map.addr, map.length)) {
    log_buffer->push_back(android::base::StringPrintf("error: %d", kZipVerificationFailure));
    return INSTALL_CORRUPT;
  }

  // Try to open the package.
  ZipArchiveHandle zip;
  int err = OpenArchiveFromMemory(map.addr, map.length, path.c_str(), &zip);
  if (err != 0) {
    LOG(ERROR) << "Can't open " << path << " : " << ErrorCodeString(err);
    log_buffer->push_back(android::base::StringPrintf("error: %d", kZipOpenFailure));

    CloseArchive(zip);
    return INSTALL_CORRUPT;
  }

  // Additionally verify the compatibility of the package.
  if (!verify_package_compatibility(zip)) {
    log_buffer->push_back(android::base::StringPrintf("error: %d", kPackageCompatibilityFailure));
    CloseArchive(zip);
    return INSTALL_CORRUPT;
  }

  // Verify and install the contents of the package.
  ui->Print("Installing update...\n");
  if (retry_count > 0) {
    ui->Print("Retry attempt: %d\n", retry_count);
  }
  ui->SetEnableReboot(false);
  int result = try_update_binary(path, zip, wipe_cache, log_buffer, retry_count, max_temperature);
  ui->SetEnableReboot(true);
  ui->Print("\n");

  CloseArchive(zip);
  return result;
}

int install_package(const std::string& path, bool* wipe_cache, const std::string& install_file,
                    bool needs_mount, int retry_count) {
  CHECK(!path.empty());
  CHECK(!install_file.empty());
  CHECK(wipe_cache != nullptr);

  modified_flash = true;
  auto start = std::chrono::system_clock::now();

  int start_temperature = GetMaxValueFromThermalZone();
  int max_temperature = start_temperature;

  int result;
  std::vector<std::string> log_buffer;
  if (setup_install_mounts() != 0) {
    LOG(ERROR) << "failed to set up expected mounts for install; aborting";
    result = INSTALL_ERROR;
  } else {
    result = really_install_package(path, wipe_cache, needs_mount, &log_buffer, retry_count,
                                    &max_temperature);
  }

  // Measure the time spent to apply OTA update in seconds.
  std::chrono::duration<double> duration = std::chrono::system_clock::now() - start;
  int time_total = static_cast<int>(duration.count());

  bool has_cache = volume_for_mount_point("/cache") != nullptr;
  // Skip logging the uncrypt_status on devices without /cache.
  if (has_cache) {
    static constexpr const char* UNCRYPT_STATUS = "/cache/recovery/uncrypt_status";
    if (ensure_path_mounted(UNCRYPT_STATUS) != 0) {
      LOG(WARNING) << "Can't mount " << UNCRYPT_STATUS;
    } else {
      std::string uncrypt_status;
      if (!android::base::ReadFileToString(UNCRYPT_STATUS, &uncrypt_status)) {
        PLOG(WARNING) << "failed to read uncrypt status";
      } else if (!android::base::StartsWith(uncrypt_status, "uncrypt_")) {
        LOG(WARNING) << "corrupted uncrypt_status: " << uncrypt_status;
      } else {
        log_buffer.push_back(android::base::Trim(uncrypt_status));
      }
    }
  }

  // The first two lines need to be the package name and install result.
  std::vector<std::string> log_header = {
    path,
    result == INSTALL_SUCCESS ? "1" : "0",
    "time_total: " + std::to_string(time_total),
    "retry: " + std::to_string(retry_count),
  };

  int end_temperature = GetMaxValueFromThermalZone();
  max_temperature = std::max(end_temperature, max_temperature);
  if (start_temperature > 0) {
    log_buffer.push_back("temperature_start: " + std::to_string(start_temperature));
  }
  if (end_temperature > 0) {
    log_buffer.push_back("temperature_end: " + std::to_string(end_temperature));
  }
  if (max_temperature > 0) {
    log_buffer.push_back("temperature_max: " + std::to_string(max_temperature));
  }

  std::string log_content =
      android::base::Join(log_header, "\n") + "\n" + android::base::Join(log_buffer, "\n") + "\n";
  if (!android::base::WriteStringToFile(log_content, install_file)) {
    PLOG(ERROR) << "failed to write " << install_file;
  }

  // Write a copy into last_log.
  LOG(INFO) << log_content;

  return result;
}

bool verify_package(const unsigned char* package_data, size_t package_size) {
  static constexpr const char* PUBLIC_KEYS_FILE = "/res/keys";
  std::vector<Certificate> loadedKeys;
  if (!load_keys(PUBLIC_KEYS_FILE, loadedKeys)) {
    LOG(ERROR) << "Failed to load keys";
    return false;
  }
  LOG(INFO) << loadedKeys.size() << " key(s) loaded from " << PUBLIC_KEYS_FILE;

  // Verify package.
  ui->Print("Verifying update package...\n");
  auto t0 = std::chrono::system_clock::now();
  int err = verify_file(package_data, package_size, loadedKeys,
                        std::bind(&RecoveryUI::SetProgress, ui, std::placeholders::_1));
  std::chrono::duration<double> duration = std::chrono::system_clock::now() - t0;
  ui->Print("Update package verification took %.1f s (result %d).\n", duration.count(), err);
  if (err != VERIFY_SUCCESS) {
    LOG(ERROR) << "Signature verification failed";
    LOG(ERROR) << "error: " << kZipVerificationFailure;
    return false;
  }
  return true;
}