aboutsummaryrefslogtreecommitdiffstats
blob: 78dd4cb98ccd909e52b3bedbf4484106cc483c4f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
/*
 * Copyright (C) 2007 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _MINUI_H_
#define _MINUI_H_

#include <sys/types.h>

#include <functional>
#include <string>

//
// Graphics.
//

struct GRSurface {
    int width;
    int height;
    int row_bytes;
    int pixel_bytes;
    unsigned char* data;
};

struct GRFont {
    GRSurface* texture;
    int char_width;
    int char_height;
};

int gr_init();
void gr_exit();

int gr_fb_width();
int gr_fb_height();

void gr_flip();
void gr_fb_blank(bool blank);

void gr_clear();  // clear entire surface to current color
void gr_color(unsigned char r, unsigned char g, unsigned char b, unsigned char a);
void gr_fill(int x1, int y1, int x2, int y2);

void gr_texticon(int x, int y, GRSurface* icon);

const GRFont* gr_sys_font();
int gr_init_font(const char* name, GRFont** dest);
void gr_text(const GRFont* font, int x, int y, const char *s, bool bold);
int gr_measure(const GRFont* font, const char *s);
void gr_font_size(const GRFont* font, int *x, int *y);

void gr_blit(GRSurface* source, int sx, int sy, int w, int h, int dx, int dy);
unsigned int gr_get_width(GRSurface* surface);
unsigned int gr_get_height(GRSurface* surface);

//
// Input events.
//

struct input_event;

using ev_callback = std::function<int(int fd, uint32_t epevents)>;
using ev_set_key_callback = std::function<int(int code, int value)>;

int ev_init(ev_callback input_cb);
void ev_exit();
int ev_add_fd(int fd, ev_callback cb);
void ev_iterate_available_keys(const std::function<void(int)>& f);
int ev_sync_key_state(const ev_set_key_callback& set_key_cb);

// 'timeout' has the same semantics as poll(2).
//    0 : don't block
//  < 0 : block forever
//  > 0 : block for 'timeout' milliseconds
int ev_wait(int timeout);

int ev_get_input(int fd, uint32_t epevents, input_event* ev);
void ev_dispatch();
int ev_get_epollfd();

//
// Resources
//

bool matches_locale(const std::string& prefix, const std::string& locale);

// res_create_*_surface() functions return 0 if no error, else
// negative.
//
// A "display" surface is one that is intended to be drawn to the
// screen with gr_blit().  An "alpha" surface is a grayscale image
// interpreted as an alpha mask used to render text in the current
// color (with gr_text() or gr_texticon()).
//
// All these functions load PNG images from "/res/images/${name}.png".

// Load a single display surface from a PNG image.
int res_create_display_surface(const char* name, GRSurface** pSurface);

// Load an array of display surfaces from a single PNG image.  The PNG
// should have a 'Frames' text chunk whose value is the number of
// frames this image represents.  The pixel data itself is interlaced
// by row.
int res_create_multi_display_surface(const char* name, int* frames,
                                     int* fps, GRSurface*** pSurface);

// Load a single alpha surface from a grayscale PNG image.
int res_create_alpha_surface(const char* name, GRSurface** pSurface);

// Load part of a grayscale PNG image that is the first match for the
// given locale.  The image is expected to be a composite of multiple
// translations of the same text, with special added rows that encode
// the subimages' size and intended locale in the pixel data.  See
// bootable/recovery/tools/recovery_l10n for an app that will generate
// these specialized images from Android resources.
int res_create_localized_alpha_surface(const char* name, const char* locale,
                                       GRSurface** pSurface);

// Free a surface allocated by any of the res_create_*_surface()
// functions.
void res_free_surface(GRSurface* surface);

#endif