aboutsummaryrefslogtreecommitdiffstats
path: root/ui.h
blob: 8493c6f0a25e0c61d6b8c8ac1b972a837f1436cc (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
/*
 * Copyright (C) 2011 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef RECOVERY_UI_H
#define RECOVERY_UI_H

#include <linux/input.h>
#include <pthread.h>
#include <time.h>

#include <string>

// Abstract class for controlling the user interface during recovery.
class RecoveryUI {
  public:
    RecoveryUI();

    virtual ~RecoveryUI() { }

    // Initialize the object; called before anything else. UI texts will be
    // initialized according to the given locale. Returns true on success.
    virtual bool Init(const std::string& locale);

    // Show a stage indicator.  Call immediately after Init().
    virtual void SetStage(int current, int max) = 0;

    // Set the overall recovery state ("background image").
    enum Icon { NONE, INSTALLING_UPDATE, ERASING, NO_COMMAND, ERROR };
    virtual void SetBackground(Icon icon) = 0;
    virtual void SetSystemUpdateText(bool security_update) = 0;

    // --- progress indicator ---
    enum ProgressType { EMPTY, INDETERMINATE, DETERMINATE };
    virtual void SetProgressType(ProgressType determinate) = 0;

    // Show a progress bar and define the scope of the next operation:
    //   portion - fraction of the progress bar the next operation will use
    //   seconds - expected time interval (progress bar moves at this minimum rate)
    virtual void ShowProgress(float portion, float seconds) = 0;

    // Set progress bar position (0.0 - 1.0 within the scope defined
    // by the last call to ShowProgress).
    virtual void SetProgress(float fraction) = 0;

    // --- text log ---

    virtual void ShowText(bool visible) = 0;

    virtual bool IsTextVisible() = 0;

    virtual bool WasTextEverVisible() = 0;

    // Write a message to the on-screen log (shown if the user has
    // toggled on the text display). Print() will also dump the message
    // to stdout / log file, while PrintOnScreenOnly() not.
    virtual void Print(const char* fmt, ...) __printflike(2, 3) = 0;
    virtual void PrintOnScreenOnly(const char* fmt, ...) __printflike(2, 3) = 0;

    virtual void ShowFile(const char* filename) = 0;

    // --- key handling ---

    // Wait for a key and return it.  May return -1 after timeout.
    virtual int WaitKey();

    virtual bool IsKeyPressed(int key);
    virtual bool IsLongPress();

    // Returns true if you have the volume up/down and power trio typical
    // of phones and tablets, false otherwise.
    virtual bool HasThreeButtons();

    // Erase any queued-up keys.
    virtual void FlushKeys();

    // Called on each key press, even while operations are in progress.
    // Return value indicates whether an immediate operation should be
    // triggered (toggling the display, rebooting the device), or if
    // the key should be enqueued for use by the main thread.
    enum KeyAction { ENQUEUE, TOGGLE, REBOOT, IGNORE };
    virtual KeyAction CheckKey(int key, bool is_long_press);

    // Called when a key is held down long enough to have been a
    // long-press (but before the key is released).  This means that
    // if the key is eventually registered (released without any other
    // keys being pressed in the meantime), CheckKey will be called with
    // 'is_long_press' true.
    virtual void KeyLongPress(int key);

    // Normally in recovery there's a key sequence that triggers
    // immediate reboot of the device, regardless of what recovery is
    // doing (with the default CheckKey implementation, it's pressing
    // the power button 7 times in row).  Call this to enable or
    // disable that feature.  It is enabled by default.
    virtual void SetEnableReboot(bool enabled);

    // --- menu display ---

    // Display some header text followed by a menu of items, which appears
    // at the top of the screen (in place of any scrolling ui_print()
    // output, if necessary).
    virtual void StartMenu(const char* const * headers, const char* const * items,
                           int initial_selection) = 0;

    // Set the menu highlight to the given index, wrapping if necessary.
    // Returns the actual item selected.
    virtual int SelectMenu(int sel) = 0;

    // End menu mode, resetting the text overlay so that ui_print()
    // statements will be displayed.
    virtual void EndMenu() = 0;

  protected:
    void EnqueueKey(int key_code);

    // The locale that's used to show the rendered texts.
    std::string locale_;
    bool rtl_locale_;

  private:
    // Key event input queue
    pthread_mutex_t key_queue_mutex;
    pthread_cond_t key_queue_cond;
    int key_queue[256], key_queue_len;
    char key_pressed[KEY_MAX + 1];     // under key_queue_mutex
    int key_last_down;                 // under key_queue_mutex
    bool key_long_press;               // under key_queue_mutex
    int key_down_count;                // under key_queue_mutex
    bool enable_reboot;                // under key_queue_mutex
    int rel_sum;

    int consecutive_power_keys;
    int last_key;

    bool has_power_key;
    bool has_up_key;
    bool has_down_key;

    struct key_timer_t {
        RecoveryUI* ui;
        int key_code;
        int count;
    };

    pthread_t input_thread_;

    void OnKeyDetected(int key_code);

    static int InputCallback(int fd, uint32_t epevents, void* data);
    int OnInputEvent(int fd, uint32_t epevents);
    void ProcessKey(int key_code, int updown);

    bool IsUsbConnected();

    static void* time_key_helper(void* cookie);
    void time_key(int key_code, int count);

    void SetLocale(const std::string&);
};

#endif  // RECOVERY_UI_H