aboutsummaryrefslogtreecommitdiffstats
blob: c5e154f03e3415fcfbe3d518ff9ac75d52da7eaa (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

/*
 * This program verifies the integrity of the partitions after an A/B OTA
 * update. It gets invoked by init, and will only perform the verification if
 * it's the first boot post an A/B OTA update.
 *
 * Update_verifier relies on dm-verity to capture any corruption on the partitions
 * being verified. And its behavior varies depending on the dm-verity mode.
 * Upon detection of failures:
 *   enforcing mode: dm-verity reboots the device
 *   eio mode: dm-verity fails the read and update_verifier reboots the device
 *   other mode: not supported and update_verifier reboots the device
 *
 * After a predefined number of failing boot attempts, the bootloader should
 * mark the slot as unbootable and stops trying. Other dm-verity modes (
 * for example, veritymode=EIO) are not accepted and simply lead to a
 * verification failure.
 *
 * The current slot will be marked as having booted successfully if the
 * verifier reaches the end after the verification.
 */

#include "update_verifier/update_verifier.h"

#include <dirent.h>
#include <errno.h>
#include <fcntl.h>
#include <stdio.h>
#include <string.h>
#include <unistd.h>

#include <algorithm>
#include <future>
#include <string>
#include <vector>

#include <android-base/file.h>
#include <android-base/logging.h>
#include <android-base/parseint.h>
#include <android-base/properties.h>
#include <android-base/strings.h>
#include <android-base/unique_fd.h>
#include <android/hardware/boot/1.0/IBootControl.h>
#include <cutils/android_reboot.h>

#include "otautil/rangeset.h"

using android::sp;
using android::hardware::boot::V1_0::IBootControl;
using android::hardware::boot::V1_0::BoolResult;
using android::hardware::boot::V1_0::CommandResult;

// Find directories in format of "/sys/block/dm-X".
static int dm_name_filter(const dirent* de) {
  if (android::base::StartsWith(de->d_name, "dm-")) {
    return 1;
  }
  return 0;
}

static bool read_blocks(const std::string& partition, const std::string& range_str) {
  if (partition != "system" && partition != "vendor") {
    LOG(ERROR) << "partition name must be system or vendor: " << partition;
    return false;
  }
  // Iterate the content of "/sys/block/dm-X/dm/name". If it matches "system"
  // (or "vendor"), then dm-X is a dm-wrapped system/vendor partition.
  // Afterwards, update_verifier will read every block on the care_map_file of
  // "/dev/block/dm-X" to ensure the partition's integrity.
  static constexpr auto DM_PATH_PREFIX = "/sys/block/";
  dirent** namelist;
  int n = scandir(DM_PATH_PREFIX, &namelist, dm_name_filter, alphasort);
  if (n == -1) {
    PLOG(ERROR) << "Failed to scan dir " << DM_PATH_PREFIX;
    return false;
  }
  if (n == 0) {
    LOG(ERROR) << "dm block device not found for " << partition;
    return false;
  }

  static constexpr auto DM_PATH_SUFFIX = "/dm/name";
  static constexpr auto DEV_PATH = "/dev/block/";
  std::string dm_block_device;
  while (n--) {
    std::string path = DM_PATH_PREFIX + std::string(namelist[n]->d_name) + DM_PATH_SUFFIX;
    std::string content;
    if (!android::base::ReadFileToString(path, &content)) {
      PLOG(WARNING) << "Failed to read " << path;
    } else {
      std::string dm_block_name = android::base::Trim(content);
#ifdef BOARD_AVB_ENABLE
      // AVB is using 'vroot' for the root block device but we're expecting 'system'.
      if (dm_block_name == "vroot") {
        dm_block_name = "system";
      }
#endif
      if (dm_block_name == partition) {
        dm_block_device = DEV_PATH + std::string(namelist[n]->d_name);
        while (n--) {
          free(namelist[n]);
        }
        break;
      }
    }
    free(namelist[n]);
  }
  free(namelist);

  if (dm_block_device.empty()) {
    LOG(ERROR) << "Failed to find dm block device for " << partition;
    return false;
  }

  // For block range string, first integer 'count' equals 2 * total number of valid ranges,
  // followed by 'count' number comma separated integers. Every two integers reprensent a
  // block range with the first number included in range but second number not included.
  // For example '4,64536,65343,74149,74150' represents: [64536,65343) and [74149,74150).
  RangeSet ranges = RangeSet::Parse(range_str);
  if (!ranges) {
    LOG(ERROR) << "Error parsing RangeSet string " << range_str;
    return false;
  }

  // RangeSet::Split() splits the ranges into multiple groups with same number of blocks (except for
  // the last group).
  size_t thread_num = std::thread::hardware_concurrency() ?: 4;
  std::vector<RangeSet> groups = ranges.Split(thread_num);

  std::vector<std::future<bool>> threads;
  for (const auto& group : groups) {
    auto thread_func = [&group, &dm_block_device, &partition]() {
      android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(dm_block_device.c_str(), O_RDONLY)));
      if (fd.get() == -1) {
        PLOG(ERROR) << "Error reading " << dm_block_device << " for partition " << partition;
        return false;
      }

      static constexpr size_t kBlockSize = 4096;
      std::vector<uint8_t> buf(1024 * kBlockSize);

      size_t block_count = 0;
      for (const auto& range : group) {
        size_t range_start = range.first;
        size_t range_end = range.second;
        if (lseek64(fd.get(), static_cast<off64_t>(range_start) * kBlockSize, SEEK_SET) == -1) {
          PLOG(ERROR) << "lseek to " << range_start << " failed";
          return false;
        }

        size_t remain = (range_end - range_start) * kBlockSize;
        while (remain > 0) {
          size_t to_read = std::min(remain, 1024 * kBlockSize);
          if (!android::base::ReadFully(fd.get(), buf.data(), to_read)) {
            PLOG(ERROR) << "Failed to read blocks " << range_start << " to " << range_end;
            return false;
          }
          remain -= to_read;
        }
        block_count += (range_end - range_start);
      }
      LOG(INFO) << "Finished reading " << block_count << " blocks on " << dm_block_device;
      return true;
    };

    threads.emplace_back(std::async(std::launch::async, thread_func));
  }

  bool ret = true;
  for (auto& t : threads) {
    ret = t.get() && ret;
  }
  LOG(INFO) << "Finished reading blocks on " << dm_block_device << " with " << thread_num
            << " threads.";
  return ret;
}

// Returns true to indicate a passing verification (or the error should be ignored); Otherwise
// returns false on fatal errors, where we should reject the current boot and trigger a fallback.
// Note that update_verifier should be backward compatible to not reject care_map.txt from old
// releases, which could otherwise fail to boot into the new release. For example, we've changed
// the care_map format between N and O. An O update_verifier would fail to work with N
// care_map.txt. This could be a result of sideloading an O OTA while the device having a pending N
// update.
bool verify_image(const std::string& care_map_name) {
  android::base::unique_fd care_map_fd(TEMP_FAILURE_RETRY(open(care_map_name.c_str(), O_RDONLY)));
  // If the device is flashed before the current boot, it may not have care_map.txt
  // in /data/ota_package. To allow the device to continue booting in this situation,
  // we should print a warning and skip the block verification.
  if (care_map_fd.get() == -1) {
    PLOG(WARNING) << "Failed to open " << care_map_name;
    return true;
  }
  // Care map file has four lines (two lines if vendor partition is not present):
  // First line has the block partition name (system/vendor).
  // Second line holds all ranges of blocks to verify.
  // The next two lines have the same format but for vendor partition.
  std::string file_content;
  if (!android::base::ReadFdToString(care_map_fd.get(), &file_content)) {
    LOG(ERROR) << "Error reading care map contents to string.";
    return false;
  }

  std::vector<std::string> lines;
  lines = android::base::Split(android::base::Trim(file_content), "\n");
  if (lines.size() != 2 && lines.size() != 4) {
    LOG(ERROR) << "Invalid lines in care_map: found " << lines.size()
               << " lines, expecting 2 or 4 lines.";
    return false;
  }

  for (size_t i = 0; i < lines.size(); i += 2) {
    // We're seeing an N care_map.txt. Skip the verification since it's not compatible with O
    // update_verifier (the last few metadata blocks can't be read via device mapper).
    if (android::base::StartsWith(lines[i], "/dev/block/")) {
      LOG(WARNING) << "Found legacy care_map.txt; skipped.";
      return true;
    }
    if (!read_blocks(lines[i], lines[i+1])) {
      return false;
    }
  }

  return true;
}

static int reboot_device() {
  if (android_reboot(ANDROID_RB_RESTART2, 0, nullptr) == -1) {
    LOG(ERROR) << "Failed to reboot.";
    return -1;
  }
  while (true) pause();
}

int update_verifier(int argc, char** argv) {
  for (int i = 1; i < argc; i++) {
    LOG(INFO) << "Started with arg " << i << ": " << argv[i];
  }

  sp<IBootControl> module = IBootControl::getService();
  if (module == nullptr) {
    LOG(ERROR) << "Error getting bootctrl module.";
    return reboot_device();
  }

  uint32_t current_slot = module->getCurrentSlot();
  BoolResult is_successful = module->isSlotMarkedSuccessful(current_slot);
  LOG(INFO) << "Booting slot " << current_slot << ": isSlotMarkedSuccessful="
            << static_cast<int32_t>(is_successful);

  if (is_successful == BoolResult::FALSE) {
    // The current slot has not booted successfully.

#if defined(PRODUCT_SUPPORTS_VERITY) || defined(BOARD_AVB_ENABLE)
    bool skip_verification = false;
    std::string verity_mode = android::base::GetProperty("ro.boot.veritymode", "");
    if (verity_mode.empty()) {
      // With AVB it's possible to disable verification entirely and
      // in this case ro.boot.veritymode is empty.
#if defined(BOARD_AVB_ENABLE)
      LOG(WARNING) << "verification has been disabled; marking without verification.";
      skip_verification = true;
#else
      LOG(ERROR) << "Failed to get dm-verity mode.";
      return reboot_device();
#endif
    } else if (android::base::EqualsIgnoreCase(verity_mode, "eio")) {
      // We shouldn't see verity in EIO mode if the current slot hasn't booted successfully before.
      // Continue the verification until we fail to read some blocks.
      LOG(WARNING) << "Found dm-verity in EIO mode.";
    } else if (android::base::EqualsIgnoreCase(verity_mode, "disabled")) {
      LOG(WARNING) << "dm-verity in disabled mode; marking without verification.";
      skip_verification = true;
    } else if (verity_mode != "enforcing") {
      LOG(ERROR) << "Unexpected dm-verity mode : " << verity_mode << ", expecting enforcing.";
      return reboot_device();
    }

    if (!skip_verification) {
      static constexpr auto CARE_MAP_FILE = "/data/ota_package/care_map.txt";
      if (!verify_image(CARE_MAP_FILE)) {
        LOG(ERROR) << "Failed to verify all blocks in care map file.";
        return reboot_device();
      }
    }
#else
    LOG(WARNING) << "dm-verity not enabled; marking without verification.";
#endif

    CommandResult cr;
    module->markBootSuccessful([&cr](CommandResult result) { cr = result; });
    if (!cr.success) {
      LOG(ERROR) << "Error marking booted successfully: " << cr.errMsg;
      return reboot_device();
    }
    LOG(INFO) << "Marked slot " << current_slot << " as booted successfully.";
  }

  LOG(INFO) << "Leaving update_verifier.";
  return 0;
}