aboutsummaryrefslogtreecommitdiffstats
blob: f063e5fa186a8662a035f6c5e8a537e8dc7e87ff (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
/*
 * Copyright (C) 2009 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "updater/updater.h"

#include <stdio.h>
#include <unistd.h>
#include <stdlib.h>
#include <string.h>

#include <string>

#include <android-base/logging.h>
#include <android-base/strings.h>
#include <selinux/android.h>
#include <selinux/label.h>
#include <selinux/selinux.h>
#include <ziparchive/zip_archive.h>

#include "edify/expr.h"
#include "otafault/config.h"
#include "otautil/DirUtil.h"
#include "otautil/SysUtil.h"
#include "otautil/cache_location.h"
#include "otautil/error_code.h"
#include "updater/blockimg.h"
#include "updater/install.h"

// Generated by the makefile, this function defines the
// RegisterDeviceExtensions() function, which calls all the
// registration functions for device-specific extensions.
#include "register.inc"

// Where in the package we expect to find the edify script to execute.
// (Note it's "updateR-script", not the older "update-script".)
static constexpr const char* SCRIPT_NAME = "META-INF/com/google/android/updater-script";

extern bool have_eio_error;

struct selabel_handle *sehandle;

static void UpdaterLogger(android::base::LogId /* id */, android::base::LogSeverity /* severity */,
                          const char* /* tag */, const char* /* file */, unsigned int /* line */,
                          const char* message) {
  fprintf(stdout, "%s\n", message);
}

int main(int argc, char** argv) {
  // Various things log information to stdout or stderr more or less
  // at random (though we've tried to standardize on stdout).  The
  // log file makes more sense if buffering is turned off so things
  // appear in the right order.
  setbuf(stdout, nullptr);
  setbuf(stderr, nullptr);

  // We don't have logcat yet under recovery. Update logs will always be written to stdout
  // (which is redirected to recovery.log).
  android::base::InitLogging(argv, &UpdaterLogger);

  if (argc != 4 && argc != 5) {
    LOG(ERROR) << "unexpected number of arguments: " << argc;
    return 1;
  }

  char* version = argv[1];
  if ((version[0] != '1' && version[0] != '2' && version[0] != '3') || version[1] != '\0') {
    // We support version 1, 2, or 3.
    LOG(ERROR) << "wrong updater binary API; expected 1, 2, or 3; got " << argv[1];
    return 2;
  }

  // Set up the pipe for sending commands back to the parent process.

  int fd = atoi(argv[2]);
  FILE* cmd_pipe = fdopen(fd, "wb");
  setlinebuf(cmd_pipe);

  // Extract the script from the package.

  const char* package_filename = argv[3];
  MemMapping map;
  if (!map.MapFile(package_filename)) {
    LOG(ERROR) << "failed to map package " << argv[3];
    return 3;
  }
  ZipArchiveHandle za;
  int open_err = OpenArchiveFromMemory(map.addr, map.length, argv[3], &za);
  if (open_err != 0) {
    LOG(ERROR) << "failed to open package " << argv[3] << ": " << ErrorCodeString(open_err);
    CloseArchive(za);
    return 3;
  }

  ZipString script_name(SCRIPT_NAME);
  ZipEntry script_entry;
  int find_err = FindEntry(za, script_name, &script_entry);
  if (find_err != 0) {
    LOG(ERROR) << "failed to find " << SCRIPT_NAME << " in " << package_filename << ": "
               << ErrorCodeString(find_err);
    CloseArchive(za);
    return 4;
  }

  std::string script;
  script.resize(script_entry.uncompressed_length);
  int extract_err = ExtractToMemory(za, &script_entry, reinterpret_cast<uint8_t*>(&script[0]),
                                    script_entry.uncompressed_length);
  if (extract_err != 0) {
    LOG(ERROR) << "failed to read script from package: " << ErrorCodeString(extract_err);
    CloseArchive(za);
    return 5;
  }

  // Configure edify's functions.

  RegisterBuiltins();
  RegisterInstallFunctions();
  RegisterBlockImageFunctions();
  RegisterDeviceExtensions();

  // Parse the script.

  std::unique_ptr<Expr> root;
  int error_count = 0;
  int error = parse_string(script.c_str(), &root, &error_count);
  if (error != 0 || error_count > 0) {
    LOG(ERROR) << error_count << " parse errors";
    CloseArchive(za);
    return 6;
  }

  sehandle = selinux_android_file_context_handle();
  selinux_android_set_sehandle(sehandle);

  if (!sehandle) {
    fprintf(cmd_pipe, "ui_print Warning: No file_contexts\n");
  }

  // Evaluate the parsed script.

  UpdaterInfo updater_info;
  updater_info.cmd_pipe = cmd_pipe;
  updater_info.package_zip = za;
  updater_info.version = atoi(version);
  updater_info.package_zip_addr = map.addr;
  updater_info.package_zip_len = map.length;

  State state(script, &updater_info);

  if (argc == 5) {
    if (strcmp(argv[4], "retry") == 0) {
      state.is_retry = true;
    } else {
      printf("unexpected argument: %s", argv[4]);
    }
  }
  ota_io_init(za, state.is_retry);

  // Initialize the cache_temp_source, last_command_file and stash_directory_base to their default
  // locations.
  CacheLocation::location().ResetLocations();

  std::string result;
  bool status = Evaluate(&state, root, &result);

  if (have_eio_error) {
    fprintf(cmd_pipe, "retry_update\n");
  }

  if (!status) {
    if (state.errmsg.empty()) {
      LOG(ERROR) << "script aborted (no error message)";
      fprintf(cmd_pipe, "ui_print script aborted (no error message)\n");
    } else {
      LOG(ERROR) << "script aborted: " << state.errmsg;
      const std::vector<std::string> lines = android::base::Split(state.errmsg, "\n");
      for (const std::string& line : lines) {
        // Parse the error code in abort message.
        // Example: "E30: This package is for bullhead devices."
        if (!line.empty() && line[0] == 'E') {
          if (sscanf(line.c_str(), "E%d: ", &state.error_code) != 1) {
            LOG(ERROR) << "Failed to parse error code: [" << line << "]";
          }
        }
        fprintf(cmd_pipe, "ui_print %s\n", line.c_str());
      }
    }

    // Installation has been aborted. Set the error code to kScriptExecutionFailure unless
    // a more specific code has been set in errmsg.
    if (state.error_code == kNoError) {
      state.error_code = kScriptExecutionFailure;
    }
    fprintf(cmd_pipe, "log error: %d\n", state.error_code);
    // Cause code should provide additional information about the abort.
    if (state.cause_code != kNoCause) {
      fprintf(cmd_pipe, "log cause: %d\n", state.cause_code);
      if (state.cause_code == kPatchApplicationFailure) {
        LOG(INFO) << "Patch application failed, retry update.";
        fprintf(cmd_pipe, "retry_update\n");
      }
    }

    if (updater_info.package_zip) {
      CloseArchive(updater_info.package_zip);
    }
    return 7;
  } else {
    fprintf(cmd_pipe, "ui_print script succeeded: result was [%s]\n", result.c_str());
  }

  if (updater_info.package_zip) {
    CloseArchive(updater_info.package_zip);
  }

  return 0;
}