aboutsummaryrefslogtreecommitdiffstats
blob: 1c5a41d1b1a653ec0327fcc0e0f175b4b1d1817a (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
/*
 * Copyright (C) 2008 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "common.h"
#include "verifier.h"
#include "ui.h"

#include "mincrypt/rsa.h"
#include "mincrypt/sha.h"

#include <string.h>
#include <stdio.h>
#include <errno.h>

extern RecoveryUI* ui;

// Look for an RSA signature embedded in the .ZIP file comment given
// the path to the zip.  Verify it matches one of the given public
// keys.
//
// Return VERIFY_SUCCESS, VERIFY_FAILURE (if any error is encountered
// or no key matches the signature).

int verify_file(const char* path, const RSAPublicKey *pKeys, unsigned int numKeys) {
    ui->SetProgress(0.0);

    FILE* f = fopen(path, "rb");
    if (f == NULL) {
        LOGE("failed to open %s (%s)\n", path, strerror(errno));
        return VERIFY_FAILURE;
    }

    // An archive with a whole-file signature will end in six bytes:
    //
    //   (2-byte signature start) $ff $ff (2-byte comment size)
    //
    // (As far as the ZIP format is concerned, these are part of the
    // archive comment.)  We start by reading this footer, this tells
    // us how far back from the end we have to start reading to find
    // the whole comment.

#define FOOTER_SIZE 6

    if (fseek(f, -FOOTER_SIZE, SEEK_END) != 0) {
        LOGE("failed to seek in %s (%s)\n", path, strerror(errno));
        fclose(f);
        return VERIFY_FAILURE;
    }

    unsigned char footer[FOOTER_SIZE];
    if (fread(footer, 1, FOOTER_SIZE, f) != FOOTER_SIZE) {
        LOGE("failed to read footer from %s (%s)\n", path, strerror(errno));
        fclose(f);
        return VERIFY_FAILURE;
    }

    if (footer[2] != 0xff || footer[3] != 0xff) {
        fclose(f);
        return VERIFY_FAILURE;
    }

    size_t comment_size = footer[4] + (footer[5] << 8);
    size_t signature_start = footer[0] + (footer[1] << 8);
    LOGI("comment is %d bytes; signature %d bytes from end\n",
         comment_size, signature_start);

    if (signature_start - FOOTER_SIZE < RSANUMBYTES) {
        // "signature" block isn't big enough to contain an RSA block.
        LOGE("signature is too short\n");
        fclose(f);
        return VERIFY_FAILURE;
    }

#define EOCD_HEADER_SIZE 22

    // The end-of-central-directory record is 22 bytes plus any
    // comment length.
    size_t eocd_size = comment_size + EOCD_HEADER_SIZE;

    if (fseek(f, -eocd_size, SEEK_END) != 0) {
        LOGE("failed to seek in %s (%s)\n", path, strerror(errno));
        fclose(f);
        return VERIFY_FAILURE;
    }

    // Determine how much of the file is covered by the signature.
    // This is everything except the signature data and length, which
    // includes all of the EOCD except for the comment length field (2
    // bytes) and the comment data.
    size_t signed_len = ftell(f) + EOCD_HEADER_SIZE - 2;

    unsigned char* eocd = (unsigned char*)malloc(eocd_size);
    if (eocd == NULL) {
        LOGE("malloc for EOCD record failed\n");
        fclose(f);
        return VERIFY_FAILURE;
    }
    if (fread(eocd, 1, eocd_size, f) != eocd_size) {
        LOGE("failed to read eocd from %s (%s)\n", path, strerror(errno));
        fclose(f);
        return VERIFY_FAILURE;
    }

    // If this is really is the EOCD record, it will begin with the
    // magic number $50 $4b $05 $06.
    if (eocd[0] != 0x50 || eocd[1] != 0x4b ||
        eocd[2] != 0x05 || eocd[3] != 0x06) {
        LOGE("signature length doesn't match EOCD marker\n");
        fclose(f);
        return VERIFY_FAILURE;
    }

    size_t i;
    for (i = 4; i < eocd_size-3; ++i) {
        if (eocd[i  ] == 0x50 && eocd[i+1] == 0x4b &&
            eocd[i+2] == 0x05 && eocd[i+3] == 0x06) {
            // if the sequence $50 $4b $05 $06 appears anywhere after
            // the real one, minzip will find the later (wrong) one,
            // which could be exploitable.  Fail verification if
            // this sequence occurs anywhere after the real one.
            LOGE("EOCD marker occurs after start of EOCD\n");
            fclose(f);
            return VERIFY_FAILURE;
        }
    }

#define BUFFER_SIZE 4096

    SHA_CTX ctx;
    SHA_init(&ctx);
    unsigned char* buffer = (unsigned char*)malloc(BUFFER_SIZE);
    if (buffer == NULL) {
        LOGE("failed to alloc memory for sha1 buffer\n");
        fclose(f);
        return VERIFY_FAILURE;
    }

    double frac = -1.0;
    size_t so_far = 0;
    fseek(f, 0, SEEK_SET);
    while (so_far < signed_len) {
        size_t size = BUFFER_SIZE;
        if (signed_len - so_far < size) size = signed_len - so_far;
        if (fread(buffer, 1, size, f) != size) {
            LOGE("failed to read data from %s (%s)\n", path, strerror(errno));
            fclose(f);
            return VERIFY_FAILURE;
        }
        SHA_update(&ctx, buffer, size);
        so_far += size;
        double f = so_far / (double)signed_len;
        if (f > frac + 0.02 || size == so_far) {
            ui->SetProgress(f);
            frac = f;
        }
    }
    fclose(f);
    free(buffer);

    const uint8_t* sha1 = SHA_final(&ctx);
    for (i = 0; i < numKeys; ++i) {
        // The 6 bytes is the "(signature_start) $ff $ff (comment_size)" that
        // the signing tool appends after the signature itself.
        if (RSA_verify(pKeys+i, eocd + eocd_size - 6 - RSANUMBYTES,
                       RSANUMBYTES, sha1)) {
            LOGI("whole-file signature verified against key %d\n", i);
            free(eocd);
            return VERIFY_SUCCESS;
        }
    }
    free(eocd);
    LOGE("failed to verify whole-file signature\n");
    return VERIFY_FAILURE;
}