aboutsummaryrefslogtreecommitdiffstats
blob: e2ee48804060d318fc31c4113f979448abd1ae9b (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
/*
 * Copyright (C) 2014 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "wear_ui.h"

#include <pthread.h>
#include <stdio.h>  // TODO: Remove after killing the call to sprintf().
#include <string.h>

#include <string>

#include <android-base/properties.h>
#include <android-base/strings.h>
#include <minui/minui.h>

WearRecoveryUI::WearRecoveryUI()
    : kProgressBarBaseline(RECOVERY_UI_PROGRESS_BAR_BASELINE),
      kMenuUnusableRows(RECOVERY_UI_MENU_UNUSABLE_ROWS) {
  // TODO: kMenuUnusableRows should be computed based on the lines in draw_screen_locked().

  // TODO: The following three variables are likely not needed. The first two are detected
  // automatically in ScreenRecoveryUI::LoadAnimation(), based on the actual files seen on device.
  intro_frames = 22;
  loop_frames = 60;

  touch_screen_allowed_ = true;
}

int WearRecoveryUI::GetProgressBaseline() const {
  return kProgressBarBaseline;
}

// Draw background frame on the screen.  Does not flip pages.
// Should only be called with updateMutex locked.
// TODO merge drawing routines with screen_ui
void WearRecoveryUI::draw_background_locked() {
  pagesIdentical = false;
  gr_color(0, 0, 0, 255);
  gr_fill(0, 0, gr_fb_width(), gr_fb_height());

  if (currentIcon != NONE) {
    GRSurface* frame = GetCurrentFrame();
    int frame_width = gr_get_width(frame);
    int frame_height = gr_get_height(frame);
    int frame_x = (gr_fb_width() - frame_width) / 2;
    int frame_y = (gr_fb_height() - frame_height) / 2;
    gr_blit(frame, 0, 0, frame_width, frame_height, frame_x, frame_y);
  }
}

static const char* SWIPE_HELP[] = {
  "Swipe up/down to move.",
  "Swipe left/right to select.",
  "",
  NULL
};

// TODO merge drawing routines with screen_ui
void WearRecoveryUI::draw_screen_locked() {
  char cur_selection_str[50];

  draw_background_locked();
  if (!show_text) {
    draw_foreground_locked();
  } else {
    SetColor(TEXT_FILL);
    gr_fill(0, 0, gr_fb_width(), gr_fb_height());

    int y = kMarginHeight;
    int x = kMarginWidth;
    if (show_menu) {
      std::string recovery_fingerprint =
          android::base::GetProperty("ro.bootimage.build.fingerprint", "");
      SetColor(HEADER);
      y += DrawTextLine(x + 4, y, "Android Recovery", true);
      for (auto& chunk : android::base::Split(recovery_fingerprint, ":")) {
        y += DrawTextLine(x + 4, y, chunk.c_str(), false);
      }

      // This is actually the help strings.
      y += DrawTextLines(x + 4, y, SWIPE_HELP);
      SetColor(HEADER);
      y += DrawTextLines(x + 4, y, menu_headers_);

      // Show the current menu item number in relation to total number if
      // items don't fit on the screen.
      if (menu_items > menu_end - menu_start) {
        sprintf(cur_selection_str, "Current item: %d/%d", menu_sel + 1, menu_items);
        gr_text(gr_sys_font(), x + 4, y, cur_selection_str, 1);
        y += char_height_ + 4;
      }

      // Menu begins here
      SetColor(MENU);

      for (int i = menu_start; i < menu_end; ++i) {
        if (i == menu_sel) {
          // draw the highlight bar
          SetColor(MENU_SEL_BG);
          gr_fill(x, y - 2, gr_fb_width() - x, y + char_height_ + 2);
          // white text of selected item
          SetColor(MENU_SEL_FG);
          if (menu_[i][0]) {
            gr_text(gr_sys_font(), x + 4, y, menu_[i].c_str(), 1);
          }
          SetColor(MENU);
        } else if (menu_[i][0]) {
          gr_text(gr_sys_font(), x + 4, y, menu_[i].c_str(), 0);
        }
        y += char_height_ + 4;
      }
      SetColor(MENU);
      y += 4;
      gr_fill(0, y, gr_fb_width(), y + 2);
      y += 4;
    }

    SetColor(LOG);

    // display from the bottom up, until we hit the top of the
    // screen, the bottom of the menu, or we've displayed the
    // entire text buffer.
    int row = text_row_;
    size_t count = 0;
    for (int ty = gr_fb_height() - char_height_ - kMarginHeight; ty > y + 2 && count < text_rows_;
         ty -= char_height_, ++count) {
      gr_text(gr_sys_font(), x + 4, ty, text_[row], 0);
      --row;
      if (row < 0) row = text_rows_ - 1;
    }
  }
}

// TODO merge drawing routines with screen_ui
void WearRecoveryUI::update_progress_locked() {
  draw_screen_locked();
  gr_flip();
}

void WearRecoveryUI::SetStage(int current, int max) {
}

void WearRecoveryUI::StartMenu(const char* const* headers, const char* const* items,
                               int initial_selection) {
  pthread_mutex_lock(&updateMutex);
  if (text_rows_ > 0 && text_cols_ > 0) {
    menu_headers_ = headers;
    menu_.clear();
    // "i < text_rows_" is removed from the loop termination condition,
    // which is different from the one in ScreenRecoveryUI::StartMenu().
    // Because WearRecoveryUI supports scrollable menu, it's fine to have
    // more entries than text_rows_. The menu may be truncated otherwise.
    // Bug: 23752519
    for (size_t i = 0; items[i] != nullptr; i++) {
      menu_.emplace_back(std::string(items[i], strnlen(items[i], text_cols_ - 1)));
    }
    menu_items = static_cast<int>(menu_.size());
    show_menu = true;
    menu_sel = initial_selection;
    menu_start = 0;
    menu_end = text_rows_ - 1 - kMenuUnusableRows;
    if (menu_items <= menu_end) menu_end = menu_items;
    update_screen_locked();
  }
  pthread_mutex_unlock(&updateMutex);
}

int WearRecoveryUI::SelectMenu(int sel) {
  int old_sel;
  pthread_mutex_lock(&updateMutex);
  if (show_menu) {
    old_sel = menu_sel;
    menu_sel = sel;
    if (menu_sel < 0) menu_sel = 0;
    if (menu_sel >= menu_items) menu_sel = menu_items - 1;
    if (menu_sel < menu_start) {
      menu_start--;
      menu_end--;
    } else if (menu_sel >= menu_end && menu_sel < menu_items) {
      menu_end++;
      menu_start++;
    }
    sel = menu_sel;
    if (menu_sel != old_sel) update_screen_locked();
  }
  pthread_mutex_unlock(&updateMutex);
  return sel;
}