// Copyright 2016 Google Inc. All rights reserved.
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
// http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
package android
import (
"github.com/google/blueprint"
)
// This file implements hooks that external module types can use to inject logic into existing
// module types. Each hook takes an interface as a parameter so that new methods can be added
// to the interface without breaking existing module types.
// Load hooks are run after the module's properties have been filled from the blueprint file, but
// before the module has been split into architecture variants, and before defaults modules have
// been applied.
type LoadHookContext interface {
// TODO: a new context that includes Config() but not Target(), etc.?
BaseContext
AppendProperties(...interface{})
PrependProperties(...interface{})
CreateModule(blueprint.ModuleFactory, ...interface{})
}
// Arch hooks are run after the module has been split into architecture variants, and can be used
// to add architecture-specific properties.
type ArchHookContext interface {
BaseContext
AppendProperties(...interface{})
PrependProperties(...interface{})
}
func AddLoadHook(m blueprint.Module, hook func(LoadHookContext)) {
h := &m.(Module).base().hooks
h.load = append(h.load, hook)
}
func AddArchHook(m blueprint.Module, hook func(ArchHookContext)) {
h := &m.(Module).base().hooks
h.arch = append(h.arch, hook)
}
func (x *hooks) runLoadHooks(ctx LoadHookContext, m *ModuleBase) {
if len(x.load) > 0 {
for _, x := range x.load {
x(ctx)
if ctx.Failed() {
return
}
}
}
}
func (x *hooks) runArchHooks(ctx ArchHookContext, m *ModuleBase) {
if len(x.arch) > 0 {
for _, x := range x.arch {
x(ctx)
if ctx.Failed() {
return
}
}
}
}
type InstallHookContext interface {
ModuleContext
Path() OutputPath
Symlink() bool
}
// Install hooks are run after a module creates a rule to install a file or symlink.
// The installed path is available from InstallHookContext.Path(), and
// InstallHookContext.Symlink() will be true if it was a symlink.
func AddInstallHook(m blueprint.Module, hook func(InstallHookContext)) {
h := &m.(Module).base().hooks
h.install = append(h.install, hook)
}
type installHookContext struct {
ModuleContext
path OutputPath
symlink bool
}
func (x *installHookContext) Path() OutputPath {
return x.path
}
func (x *installHookContext) Symlink() bool {
return x.symlink
}
func (x *hooks) runInstallHooks(ctx ModuleContext, path OutputPath, symlink bool) {
if len(x.install) > 0 {
mctx := &installHookContext{
ModuleContext: ctx,
path: path,
symlink: symlink,
}
for _, x := range x.install {
x(mctx)
if mctx.Failed() {
return
}
}
}
}
type hooks struct {
load []func(LoadHookContext)
arch []func(ArchHookContext)
install []func(InstallHookContext)
}
func registerLoadHookMutator(ctx RegisterMutatorsContext) {
ctx.TopDown("load_hooks", LoadHookMutator).Parallel()
}
func LoadHookMutator(ctx TopDownMutatorContext) {
if m, ok := ctx.Module().(Module); ok {
// Cast through *androidTopDownMutatorContext because AppendProperties is implemented
// on *androidTopDownMutatorContext but not exposed through TopDownMutatorContext
var loadHookCtx LoadHookContext = ctx.(*androidTopDownMutatorContext)
m.base().hooks.runLoadHooks(loadHookCtx, m.base())
}
}
func archHookMutator(ctx TopDownMutatorContext) {
if m, ok := ctx.Module().(Module); ok {
// Cast through *androidTopDownMutatorContext because AppendProperties is implemented
// on *androidTopDownMutatorContext but not exposed through TopDownMutatorContext
var archHookCtx ArchHookContext = ctx.(*androidTopDownMutatorContext)
m.base().hooks.runArchHooks(archHookCtx, m.base())
}
}