// Copyright 2016 Google Inc. All rights reserved. // // Licensed under the Apache License, Version 2.0 (the "License"); // you may not use this file except in compliance with the License. // You may obtain a copy of the License at // // http://www.apache.org/licenses/LICENSE-2.0 // // Unless required by applicable law or agreed to in writing, software // distributed under the License is distributed on an "AS IS" BASIS, // WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. // See the License for the specific language governing permissions and // limitations under the License. package android import ( "fmt" "github.com/google/blueprint" "github.com/google/blueprint/proptools" ) // This file implements common functionality for handling modules that may exist as prebuilts, // source, or both. type prebuiltDependencyTag struct { blueprint.BaseDependencyTag } var prebuiltDepTag prebuiltDependencyTag type PrebuiltProperties struct { // When prefer is set to true the prebuilt will be used instead of any source module with // a matching name. Prefer *bool `android:"arch_variant"` SourceExists bool `blueprint:"mutated"` UsePrebuilt bool `blueprint:"mutated"` } type Prebuilt struct { properties PrebuiltProperties module Module srcs *[]string src *string } func (p *Prebuilt) Name(name string) string { return "prebuilt_" + name } // The below source-related functions and the srcs, src fields are based on an assumption that // prebuilt modules have a static source property at the moment. Currently there is only one // exception, android_app_import, which chooses a source file depending on the product's DPI // preference configs. We'll want to add native support for dynamic source cases if we end up having // more modules like this. func (p *Prebuilt) SingleSourcePath(ctx ModuleContext) Path { if p.srcs != nil { if len(*p.srcs) == 0 { ctx.PropertyErrorf("srcs", "missing prebuilt source file") return nil } if len(*p.srcs) > 1 { ctx.PropertyErrorf("srcs", "multiple prebuilt source files") return nil } // Return the singleton source after expanding any filegroup in the // sources. return PathForModuleSrc(ctx, (*p.srcs)[0]) } else { if proptools.String(p.src) == "" { ctx.PropertyErrorf("src", "missing prebuilt source file") return nil } return PathForModuleSrc(ctx, *p.src) } } func (p *Prebuilt) UsePrebuilt() bool { return p.properties.UsePrebuilt } func InitPrebuiltModule(module PrebuiltInterface, srcs *[]string) { p := module.Prebuilt() module.AddProperties(&p.properties) p.srcs = srcs } func InitSingleSourcePrebuiltModule(module PrebuiltInterface, src *string) { p := module.Prebuilt() module.AddProperties(&p.properties) p.src = src } type PrebuiltInterface interface { Module Prebuilt() *Prebuilt } func RegisterPrebuiltsPreArchMutators(ctx RegisterMutatorsContext) { ctx.BottomUp("prebuilts", PrebuiltMutator).Parallel() } func RegisterPrebuiltsPostDepsMutators(ctx RegisterMutatorsContext) { ctx.TopDown("prebuilt_select", PrebuiltSelectModuleMutator).Parallel() ctx.BottomUp("prebuilt_postdeps", PrebuiltPostDepsMutator).Parallel() } // PrebuiltMutator ensures that there is always a module with an undecorated name, and marks // prebuilt modules that have both a prebuilt and a source module. func PrebuiltMutator(ctx BottomUpMutatorContext) { if m, ok := ctx.Module().(PrebuiltInterface); ok && m.Prebuilt() != nil { p := m.Prebuilt() name := m.base().BaseModuleName() if ctx.OtherModuleExists(name) { ctx.AddReverseDependency(ctx.Module(), prebuiltDepTag, name) p.properties.SourceExists = true } else { ctx.Rename(name) } } } // PrebuiltSelectModuleMutator marks prebuilts that are used, either overriding source modules or // because the source module doesn't exist. It also disables installing overridden source modules. func PrebuiltSelectModuleMutator(ctx TopDownMutatorContext) { if m, ok := ctx.Module().(PrebuiltInterface); ok && m.Prebuilt() != nil { p := m.Prebuilt() if p.srcs == nil && p.src == nil { panic(fmt.Errorf("prebuilt module did not have InitPrebuiltModule called on it")) } if !p.properties.SourceExists { p.properties.UsePrebuilt = p.usePrebuilt(ctx, nil) } } else if s, ok := ctx.Module().(Module); ok { ctx.VisitDirectDepsWithTag(prebuiltDepTag, func(m Module) { p := m.(PrebuiltInterface).Prebuilt() if p.usePrebuilt(ctx, s) { p.properties.UsePrebuilt = true s.SkipInstall() } }) } } // PrebuiltPostDepsMutator does two operations. It replace dependencies on the // source module with dependencies on the prebuilt when both modules exist and // the prebuilt should be used. When the prebuilt should not be used, disable // installing it. Secondly, it also adds a sourcegroup to any filegroups found // in the prebuilt's 'Srcs' property. func PrebuiltPostDepsMutator(ctx BottomUpMutatorContext) { if m, ok := ctx.Module().(PrebuiltInterface); ok && m.Prebuilt() != nil { p := m.Prebuilt() name := m.base().BaseModuleName() if p.properties.UsePrebuilt { if p.properties.SourceExists { ctx.ReplaceDependencies(name) } } else { m.SkipInstall() } } } // usePrebuilt returns true if a prebuilt should be used instead of the source module. The prebuilt // will be used if it is marked "prefer" or if the source module is disabled. func (p *Prebuilt) usePrebuilt(ctx TopDownMutatorContext, source Module) bool { if p.srcs != nil && len(*p.srcs) == 0 { return false } if p.src != nil && *p.src == "" { return false } // TODO: use p.Properties.Name and ctx.ModuleDir to override preference if Bool(p.properties.Prefer) { return true } return source == nil || !source.Enabled() }