// Copyright 2016 Google Inc. All rights reserved. // // Licensed under the Apache License, Version 2.0 (the "License"); // you may not use this file except in compliance with the License. // You may obtain a copy of the License at // // http://www.apache.org/licenses/LICENSE-2.0 // // Unless required by applicable law or agreed to in writing, software // distributed under the License is distributed on an "AS IS" BASIS, // WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. // See the License for the specific language governing permissions and // limitations under the License. package cc import ( "fmt" "os" "path/filepath" "strings" "github.com/google/blueprint" "android/soong/android" ) var ( versionBionicHeaders = pctx.AndroidStaticRule("versionBionicHeaders", blueprint.RuleParams{ // The `&& touch $out` isn't really necessary, but Blueprint won't // let us have only implicit outputs. Command: "$versionerCmd -o $outDir $srcDir $depsPath && touch $out", CommandDeps: []string{"$versionerCmd"}, }, "depsPath", "srcDir", "outDir") preprocessNdkHeader = pctx.AndroidStaticRule("preprocessNdkHeader", blueprint.RuleParams{ Command: "$preprocessor -o $out $in", CommandDeps: []string{"$preprocessor"}, }, "preprocessor") ) func init() { pctx.SourcePathVariable("versionerCmd", "prebuilts/clang-tools/${config.HostPrebuiltTag}/bin/versioner") } // Returns the NDK base include path for use with sdk_version current. Usable with -I. func getCurrentIncludePath(ctx android.ModuleContext) android.OutputPath { return getNdkSysrootBase(ctx).Join(ctx, "usr/include") } type headerProperties struct { // Base directory of the headers being installed. As an example: // // ndk_headers { // name: "foo", // from: "include", // to: "", // srcs: ["include/foo/bar/baz.h"], // } // // Will install $SYSROOT/usr/include/foo/bar/baz.h. If `from` were instead // "include/foo", it would have installed $SYSROOT/usr/include/bar/baz.h. From *string // Install path within the sysroot. This is relative to usr/include. To *string // List of headers to install. Glob compatible. Common case is "include/**/*.h". Srcs []string `android:"path"` // Source paths that should be excluded from the srcs glob. Exclude_srcs []string `android:"path"` // Path to the NOTICE file associated with the headers. License *string `android:"path"` // True if this API is not yet ready to be shipped in the NDK. It will be // available in the platform for testing, but will be excluded from the // sysroot provided to the NDK proper. Draft bool } type headerModule struct { android.ModuleBase properties headerProperties installPaths android.Paths licensePath android.Path } func getHeaderInstallDir(ctx android.ModuleContext, header android.Path, from string, to string) android.OutputPath { // Output path is the sysroot base + "usr/include" + to directory + directory component // of the file without the leading from directory stripped. // // Given: // sysroot base = "ndk/sysroot" // from = "include/foo" // to = "bar" // header = "include/foo/woodly/doodly.h" // output path = "ndk/sysroot/usr/include/bar/woodly/doodly.h" // full/platform/path/to/include/foo fullFromPath := android.PathForModuleSrc(ctx, from) // full/platform/path/to/include/foo/woodly headerDir := filepath.Dir(header.String()) // woodly strippedHeaderDir, err := filepath.Rel(fullFromPath.String(), headerDir) if err != nil { ctx.ModuleErrorf("filepath.Rel(%q, %q) failed: %s", headerDir, fullFromPath.String(), err) } // full/platform/path/to/sysroot/usr/include/bar/woodly installDir := getCurrentIncludePath(ctx).Join(ctx, to, strippedHeaderDir) // full/platform/path/to/sysroot/usr/include/bar/woodly/doodly.h return installDir } func (m *headerModule) GenerateAndroidBuildActions(ctx android.ModuleContext) { if String(m.properties.License) == "" { ctx.PropertyErrorf("license", "field is required") } m.licensePath = android.PathForModuleSrc(ctx, String(m.properties.License)) // When generating NDK prebuilts, skip installing MIPS headers, // but keep them when doing regular platform build. // Ndk_abis property is only set to true with build/soong/scripts/build-ndk-prebuilts.sh // TODO: Revert this once MIPS is supported in NDK again. if ctx.Config().NdkAbis() && strings.Contains(ctx.ModuleName(), "mips") { return } srcFiles := android.PathsForModuleSrcExcludes(ctx, m.properties.Srcs, m.properties.Exclude_srcs) for _, header := range srcFiles { installDir := getHeaderInstallDir(ctx, header, String(m.properties.From), String(m.properties.To)) installedPath := ctx.InstallFile(installDir, header.Base(), header) installPath := installDir.Join(ctx, header.Base()) if installPath != installedPath { panic(fmt.Sprintf( "expected header install path (%q) not equal to actual install path %q", installPath, installedPath)) } m.installPaths = append(m.installPaths, installPath) } if len(m.installPaths) == 0 { ctx.ModuleErrorf("srcs %q matched zero files", m.properties.Srcs) } } // ndk_headers installs the sets of ndk headers defined in the srcs property // to the sysroot base + "usr/include" + to directory + directory component. // ndk_headers requires the license file to be specified. Example: // // Given: // sysroot base = "ndk/sysroot" // from = "include/foo" // to = "bar" // header = "include/foo/woodly/doodly.h" // output path = "ndk/sysroot/usr/include/bar/woodly/doodly.h" func ndkHeadersFactory() android.Module { module := &headerModule{} module.AddProperties(&module.properties) android.InitAndroidModule(module) return module } type versionedHeaderProperties struct { // Base directory of the headers being installed. As an example: // // versioned_ndk_headers { // name: "foo", // from: "include", // to: "", // } // // Will install $SYSROOT/usr/include/foo/bar/baz.h. If `from` were instead // "include/foo", it would have installed $SYSROOT/usr/include/bar/baz.h. From *string // Install path within the sysroot. This is relative to usr/include. To *string // Path to the NOTICE file associated with the headers. License *string // True if this API is not yet ready to be shipped in the NDK. It will be // available in the platform for testing, but will be excluded from the // sysroot provided to the NDK proper. Draft bool } // Like ndk_headers, but preprocesses the headers with the bionic versioner: // https://android.googlesource.com/platform/bionic/+/master/tools/versioner/README.md. // // Unlike ndk_headers, we don't operate on a list of sources but rather a whole directory, the // module does not have the srcs property, and operates on a full directory (the `from` property). // // Note that this is really only built to handle bionic/libc/include. type versionedHeaderModule struct { android.ModuleBase properties versionedHeaderProperties installPaths android.Paths licensePath android.Path } func (m *versionedHeaderModule) GenerateAndroidBuildActions(ctx android.ModuleContext) { if String(m.properties.License) == "" { ctx.PropertyErrorf("license", "field is required") } m.licensePath = android.PathForModuleSrc(ctx, String(m.properties.License)) fromSrcPath := android.PathForModuleSrc(ctx, String(m.properties.From)) toOutputPath := getCurrentIncludePath(ctx).Join(ctx, String(m.properties.To)) srcFiles := ctx.GlobFiles(filepath.Join(fromSrcPath.String(), "**/*.h"), nil) var installPaths []android.WritablePath for _, header := range srcFiles { installDir := getHeaderInstallDir(ctx, header, String(m.properties.From), String(m.properties.To)) installPath := installDir.Join(ctx, header.Base()) installPaths = append(installPaths, installPath) m.installPaths = append(m.installPaths, installPath) } if len(m.installPaths) == 0 { ctx.ModuleErrorf("glob %q matched zero files", String(m.properties.From)) } processHeadersWithVersioner(ctx, fromSrcPath, toOutputPath, srcFiles, installPaths) } func processHeadersWithVersioner(ctx android.ModuleContext, srcDir, outDir android.Path, srcFiles android.Paths, installPaths []android.WritablePath) android.Path { // The versioner depends on a dependencies directory to simplify determining include paths // when parsing headers. This directory contains architecture specific directories as well // as a common directory, each of which contains symlinks to the actually directories to // be included. // // ctx.Glob doesn't follow symlinks, so we need to do this ourselves so we correctly // depend on these headers. // TODO(http://b/35673191): Update the versioner to use a --sysroot. depsPath := android.PathForSource(ctx, "bionic/libc/versioner-dependencies") depsGlob := ctx.Glob(filepath.Join(depsPath.String(), "**/*"), nil) for i, path := range depsGlob { fileInfo, err := os.Lstat(path.String()) if err != nil { ctx.ModuleErrorf("os.Lstat(%q) failed: %s", path.String, err) } if fileInfo.Mode()&os.ModeSymlink == os.ModeSymlink { dest, err := os.Readlink(path.String()) if err != nil { ctx.ModuleErrorf("os.Readlink(%q) failed: %s", path.String, err) } // Additional .. to account for the symlink itself. depsGlob[i] = android.PathForSource( ctx, filepath.Clean(filepath.Join(path.String(), "..", dest))) } } timestampFile := android.PathForModuleOut(ctx, "versioner.timestamp") ctx.Build(pctx, android.BuildParams{ Rule: versionBionicHeaders, Description: "versioner preprocess " + srcDir.Rel(), Output: timestampFile, Implicits: append(srcFiles, depsGlob...), ImplicitOutputs: installPaths, Args: map[string]string{ "depsPath": depsPath.String(), "srcDir": srcDir.String(), "outDir": outDir.String(), }, }) return timestampFile } // versioned_ndk_headers preprocesses the headers with the bionic versioner: // https://android.googlesource.com/platform/bionic/+/master/tools/versioner/README.md. // Unlike the ndk_headers soong module, versioned_ndk_headers operates on a // directory level specified in `from` property. This is only used to process // the bionic/libc/include directory. func versionedNdkHeadersFactory() android.Module { module := &versionedHeaderModule{} module.AddProperties(&module.properties) android.InitAndroidModule(module) return module } // preprocessed_ndk_header { // name: "foo", // preprocessor: "foo.sh", // srcs: [...], // to: "android", // } // // Will invoke the preprocessor as: // $preprocessor -o $SYSROOT/usr/include/android/needs_preproc.h $src // For each src in srcs. type preprocessedHeadersProperties struct { // The preprocessor to run. Must be a program inside the source directory // with no dependencies. Preprocessor *string // Source path to the files to be preprocessed. Srcs []string // Source paths that should be excluded from the srcs glob. Exclude_srcs []string // Install path within the sysroot. This is relative to usr/include. To *string // Path to the NOTICE file associated with the headers. License *string // True if this API is not yet ready to be shipped in the NDK. It will be // available in the platform for testing, but will be excluded from the // sysroot provided to the NDK proper. Draft bool } type preprocessedHeadersModule struct { android.ModuleBase properties preprocessedHeadersProperties installPaths android.Paths licensePath android.Path } func (m *preprocessedHeadersModule) GenerateAndroidBuildActions(ctx android.ModuleContext) { if String(m.properties.License) == "" { ctx.PropertyErrorf("license", "field is required") } preprocessor := android.PathForModuleSrc(ctx, String(m.properties.Preprocessor)) m.licensePath = android.PathForModuleSrc(ctx, String(m.properties.License)) srcFiles := android.PathsForModuleSrcExcludes(ctx, m.properties.Srcs, m.properties.Exclude_srcs) installDir := getCurrentIncludePath(ctx).Join(ctx, String(m.properties.To)) for _, src := range srcFiles { installPath := installDir.Join(ctx, src.Base()) m.installPaths = append(m.installPaths, installPath) ctx.Build(pctx, android.BuildParams{ Rule: preprocessNdkHeader, Description: "preprocess " + src.Rel(), Input: src, Output: installPath, Args: map[string]string{ "preprocessor": preprocessor.String(), }, }) } if len(m.installPaths) == 0 { ctx.ModuleErrorf("srcs %q matched zero files", m.properties.Srcs) } } // preprocessed_ndk_headers preprocesses all the ndk headers listed in the srcs // property by executing the command defined in the preprocessor property. func preprocessedNdkHeadersFactory() android.Module { module := &preprocessedHeadersModule{} module.AddProperties(&module.properties) android.InitAndroidModule(module) return module }