[MASTER] # Specify a configuration file. #rcfile= # Python code to execute, usually for sys.path manipulation such as # pygtk.require(). #init-hook= # Profiled execution. profile=no # Add files or directories to the blacklist. They should be base names, not # paths. ignore=CVS # Pickle collected data for later comparisons. persistent=yes # List of plugins (as comma separated values of python modules names) to load, # usually to register additional checkers. load-plugins= [MESSAGES CONTROL] # Enable the message, report, category or checker with the given id(s). You can # either give multiple identifier separated by comma (,) or put this option # multiple time. See also the "--disable" option for examples. #enable= # Disable the message, report, category or checker with the given id(s). You # can either give multiple identifiers separated by comma (,) or put this # option multiple times (only on the command line, not in the configuration # file where it should appear only once).You can also use "--disable=all" to # disable everything first and then reenable specific checks. For example, if # you want to run only the similarities checker, you can use "--disable=all # --enable=similarities". If you want to run only the classes checker, but have # no Warning level messages displayed, use"--disable=all --enable=classes # --disable=W" disable=design,fixme [REPORTS] # Set the output format. Available formats are text, parseable, colorized, msvs # (visual studio) and html. You can also give a reporter class, eg # mypackage.mymodule.MyReporterClass. output-format=text # Put messages in a separate file for each module / package specified on the # command line instead of printing them on stdout. Reports (if any) will be # written in a file name "pylint_global.[txt|html]". files-output=no # Tells whether to display a full report or only the messages reports=yes # Python expression which should return a note less than 10 (10 is the highest # note). You have access to the variables errors warning, statement which # respectively contain the number of errors / warnings messages and the total # number of statements analyzed. This is used by the global evaluation report # (RP0004). evaluation=10.0 - ((float(5 * error + warning + refactor + convention) / statement) * 10) # Add a comment according to your evaluation note. This is used by the global # evaluation report (RP0004). comment=no # Template used to display messages. This is a python new-style format string # used to format the message information. See doc for all details #msg-template= [BASIC] # Required attributes for module, separated by a comma required-attributes= # List of builtins function names that should not be used, separated by a comma bad-functions=map,filter,apply,input # Regular expression which should only match correct module names module-rgx=(([a-z_][a-z0-9_]*)|([A-Z][a-zA-Z0-9]+))$ # Regular expression which should only match correct module level names const-rgx=(([A-Z_][A-Z0-9_]*)|(__.*__))$ # Regular expression which should only match correct class names class-rgx=[A-Z_][a-zA-Z0-9]+$ # Regular expression which should only match correct function names function-rgx=[a-z_][a-z0-9_]{2,30}$ # Regular expression which should only match correct method names method-rgx=[a-z_][a-z0-9_]{2,30}$ # Regular expression which should only match correct instance attribute names attr-rgx=[a-z_][a-z0-9_]{2,30}$ # Regular expression which should only match correct argument names argument-rgx=[a-z_][a-z0-9_]{2,30}$ # Regular expression which should only match correct variable names variable-rgx=[a-z_][a-z0-9_]{2,30}$ # Regular expression which should only match correct attribute names in class # bodies class-attribute-rgx=([A-Za-z_][A-Za-z0-9_]{2,30}|(__.*__))$ # Regular expression which should only match correct list comprehension / # generator expression variable names inlinevar-rgx=[A-Za-z_][A-Za-z0-9_]*$ # Good variable names which should always be accepted, separated by a comma good-names=i,j,k,ex,Run,_ # Bad variable names which should always be refused, separated by a comma bad-names=foo,bar,baz,toto,tutu,tata # Regular expression which should only match function or class names that do # not require a docstring. no-docstring-rgx=__.*__ # Minimum line length for functions/classes that require docstrings, shorter # ones are exempt. docstring-min-length=-1 [TYPECHECK] # Tells whether missing members accessed in mixin class should be ignored. A # mixin class is detected if its name ends with "mixin" (case insensitive). ignore-mixin-members=yes # List of classes names for which member attributes should not be checked # (useful for classes with attributes dynamically set). ignored-classes=SQLObject # When zope mode is activated, add a predefined set of Zope acquired attributes # to generated-members. zope=no # List of members which are set dynamically and missed by pylint inference # system, and so shouldn't trigger E0201 when accessed. Python regular # expressions are accepted. generated-members=REQUEST,acl_users,aq_parent [MISCELLANEOUS] # List of note tags to take in consideration, separated by a comma. notes=FIXME,XXX,TODO [SIMILARITIES] # Minimum lines number of a similarity. min-similarity-lines=4 # Ignore comments when computing similarities. ignore-comments=yes # Ignore docstrings when computing similarities. ignore-docstrings=yes # Ignore imports when computing similarities. ignore-imports=no [VARIABLES] # Tells whether we should check for unused import in __init__ files. init-import=no # A regular expression matching the beginning of the name of dummy variables # (i.e. not used). dummy-variables-rgx=_|dummy # List of additional names supposed to be defined in builtins. Remember that # you should avoid to define new builtins when possible. additional-builtins= [FORMAT] # Maximum number of characters on a single line. max-line-length=80 # Regexp for a line that is allowed to be longer than the limit. ignore-long-lines=^\s*(# )??$ # Allow the body of an if to be on the same line as the test if there is no # else. single-line-if-stmt=no # List of optional constructs for which whitespace checking is disabled no-space-check=trailing-comma,dict-separator # Maximum number of lines in a module max-module-lines=1000 # String used as indentation unit. This is usually " " (4 spaces) or "\t" (1 # tab). indent-string=' ' [IMPORTS] # Deprecated modules which should not be used, separated by a comma deprecated-modules=regsub,TERMIOS,Bastion,rexec # Create a graph of every (i.e. internal and external) dependencies in the # given file (report RP0402 must not be disabled) import-graph= # Create a graph of external dependencies in the given file (report RP0402 must # not be disabled) ext-import-graph= # Create a graph of internal dependencies in the given file (report RP0402 must # not be disabled) int-import-graph= [DESIGN] # Maximum number of arguments for function / method max-args=5 # Argument names that match this expression will be ignored. Default to name # with leading underscore ignored-argument-names=_.* # Maximum number of locals for function / method body max-locals=15 # Maximum number of return / yield for function / method body max-returns=6 # Maximum number of branch for function / method body max-branches=12 # Maximum number of statements in function / method body max-statements=50 # Maximum number of parents for a class (see R0901). max-parents=7 # Maximum number of attributes for a class (see R0902). max-attributes=7 # Minimum number of public methods for a class (see R0903). min-public-methods=2 # Maximum number of public methods for a class (see R0904). max-public-methods=20 [CLASSES] # List of interface methods to ignore, separated by a comma. This is used for # instance to not check methods defines in Zope's Interface base class. ignore-iface-methods=isImplementedBy,deferred,extends,names,namesAndDescriptions,queryDescriptionFor,getBases,getDescriptionFor,getDoc,getName,getTaggedValue,getTaggedValueTags,isEqualOrExtendedBy,setTaggedValue,isImplementedByInstancesOf,adaptWith,is_implemented_by # List of method names used to declare (i.e. assign) instance attributes. defining-attr-methods=__init__,__new__,setUp # List of valid names for the first argument in a class method. valid-classmethod-first-arg=cls # List of valid names for the first argument in a metaclass class method. valid-metaclass-classmethod-first-arg=mcs [EXCEPTIONS] # Exceptions that will emit a warning when being caught. Defaults to # "Exception" overgeneral-exceptions=Exception