1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
|
# Soong
Soong is the replacement for the old Android make-based build system. It
replaces Android.mk files with Android.bp files, which are JSON-like simple
declarative descriptions of modules to build.
See [Simple Build
Configuration](https://source.android.com/compatibility/tests/development/blueprints)
on source.android.com to read how Soong is configured for testing.
## Android.bp file format
By design, Android.bp files are very simple. There are no conditionals or
control flow statements - any complexity is handled in build logic written in
Go. The syntax and semantics of Android.bp files are intentionally similar
to [Bazel BUILD files](https://www.bazel.io/versions/master/docs/be/overview.html)
when possible.
### Modules
A module in an Android.bp file starts with a module type, followed by a set of
properties in `name: value,` format:
```
cc_binary {
name: "gzip",
srcs: ["src/test/minigzip.c"],
shared_libs: ["libz"],
stl: "none",
}
```
Every module must have a `name` property, and the value must be unique across
all Android.bp files.
For a list of valid module types and their properties see
[$OUT_DIR/soong/docs/soong_build.html](https://ci.android.com/builds/latest/branches/aosp-build-tools/targets/linux/view/soong_build.html).
### Globs
Properties that take a list of files can also take glob patterns. Glob
patterns can contain the normal Unix wildcard `*`, for example "*.java". Glob
patterns can also contain a single `**` wildcard as a path element, which will
match zero or more path elements. For example, `java/**/*.java` will match
`java/Main.java` and `java/com/android/Main.java`.
### Variables
An Android.bp file may contain top-level variable assignments:
```
gzip_srcs = ["src/test/minigzip.c"],
cc_binary {
name: "gzip",
srcs: gzip_srcs,
shared_libs: ["libz"],
stl: "none",
}
```
Variables are scoped to the remainder of the file they are declared in, as well
as any child blueprint files. Variables are immutable with one exception - they
can be appended to with a += assignment, but only before they have been
referenced.
### Comments
Android.bp files can contain C-style multiline `/* */` and C++ style single-line
`//` comments.
### Types
Variables and properties are strongly typed, variables dynamically based on the
first assignment, and properties statically by the module type. The supported
types are:
* Bool (`true` or `false`)
* Integers (`int`)
* Strings (`"string"`)
* Lists of strings (`["string1", "string2"]`)
* Maps (`{key1: "value1", key2: ["value2"]}`)
Maps may values of any type, including nested maps. Lists and maps may have
trailing commas after the last value.
### Operators
Strings, lists of strings, and maps can be appended using the `+` operator.
Integers can be summed up using the `+` operator. Appending a map produces the
union of keys in both maps, appending the values of any keys that are present
in both maps.
### Defaults modules
A defaults module can be used to repeat the same properties in multiple modules.
For example:
```
cc_defaults {
name: "gzip_defaults",
shared_libs: ["libz"],
stl: "none",
}
cc_binary {
name: "gzip",
defaults: ["gzip_defaults"],
srcs: ["src/test/minigzip.c"],
}
```
### Packages
The build is organized into packages where each package is a collection of related files and a
specification of the dependencies among them in the form of modules.
A package is defined as a directory containing a file named `Android.bp`, residing beneath the
top-level directory in the build and its name is its path relative to the top-level directory. A
package includes all files in its directory, plus all subdirectories beneath it, except those which
themselves contain an `Android.bp` file.
The modules in a package's `Android.bp` and included files are part of the module.
For example, in the following directory tree (where `.../android/` is the top-level Android
directory) there are two packages, `my/app`, and the subpackage `my/app/tests`. Note that
`my/app/data` is not a package, but a directory belonging to package `my/app`.
.../android/my/app/Android.bp
.../android/my/app/app.cc
.../android/my/app/data/input.txt
.../android/my/app/tests/Android.bp
.../android/my/app/tests/test.cc
This is based on the Bazel package concept.
### Name resolution
Soong provides the ability for modules in different directories to specify
the same name, as long as each module is declared within a separate namespace.
A namespace can be declared like this:
```
soong_namespace {
imports: ["path/to/otherNamespace1", "path/to/otherNamespace2"],
}
```
Each Soong module is assigned a namespace based on its location in the tree.
Each Soong module is considered to be in the namespace defined by the
soong_namespace found in an Android.bp in the current directory or closest
ancestor directory, unless no such soong_namespace module is found, in which
case the module is considered to be in the implicit root namespace.
When Soong attempts to resolve dependency D declared my module M in namespace
N which imports namespaces I1, I2, I3..., then if D is a fully-qualified name
of the form "//namespace:module", only the specified namespace will be searched
for the specified module name. Otherwise, Soong will first look for a module
named D declared in namespace N. If that module does not exist, Soong will look
for a module named D in namespaces I1, I2, I3... Lastly, Soong will look in the
root namespace.
Until we have fully converted from Make to Soong, it will be necessary for the
Make product config to specify a value of PRODUCT_SOONG_NAMESPACES. Its value
should be a space-separated list of namespaces that Soong export to Make to be
built by the `m` command. After we have fully converted from Make to Soong, the
details of enabling namespaces could potentially change.
### Visibility
The `visibility` property on a module controls whether the module can be
used by other packages. Modules are always visible to other modules declared
in the same package. This is based on the Bazel visibility mechanism.
If specified the `visibility` property must contain at least one rule.
Each rule in the property must be in one of the following forms:
* `["//visibility:public"]`: Anyone can use this module.
* `["//visibility:private"]`: Only rules in the module's package (not its
subpackages) can use this module.
* `["//some/package:__pkg__", "//other/package:__pkg__"]`: Only modules in
`some/package` and `other/package` (defined in `some/package/*.bp` and
`other/package/*.bp`) have access to this module. Note that sub-packages do not
have access to the rule; for example, `//some/package/foo:bar` or
`//other/package/testing:bla` wouldn't have access. `__pkg__` is a special
module and must be used verbatim. It represents all of the modules in the
package.
* `["//project:__subpackages__", "//other:__subpackages__"]`: Only modules in
packages `project` or `other` or in one of their sub-packages have access to
this module. For example, `//project:rule`, `//project/library:lib` or
`//other/testing/internal:munge` are allowed to depend on this rule (but not
`//independent:evil`)
* `["//project"]`: This is shorthand for `["//project:__pkg__"]`
* `[":__subpackages__"]`: This is shorthand for `["//project:__subpackages__"]`
where `//project` is the module's package. e.g. using `[":__subpackages__"]` in
`packages/apps/Settings/Android.bp` is equivalent to
`//packages/apps/Settings:__subpackages__`.
* `["//visibility:legacy_public"]`: The default visibility, behaves as
`//visibility:public` for now. It is an error if it is used in a module.
The visibility rules of `//visibility:public` and `//visibility:private` can
not be combined with any other visibility specifications.
Packages outside `vendor/` cannot make themselves visible to specific packages
in `vendor/`, e.g. a module in `libcore` cannot declare that it is visible to
say `vendor/google`, instead it must make itself visible to all packages within
`vendor/` using `//vendor:__subpackages__`.
If a module does not specify the `visibility` property the module is
`//visibility:legacy_public`. Once the build has been completely switched over to
soong it is possible that a global refactoring will be done to change this to
`//visibility:private` at which point all modules that do not currently specify
a `visibility` property will be updated to have
`visibility = [//visibility:legacy_public]` added. It will then be the owner's
responsibility to replace that with a more appropriate visibility.
### Formatter
Soong includes a canonical formatter for blueprint files, similar to
[gofmt](https://golang.org/cmd/gofmt/). To recursively reformat all Android.bp files
in the current directory:
```
bpfmt -w .
```
The canonical format includes 4 space indents, newlines after every element of a
multi-element list, and always includes a trailing comma in lists and maps.
### Convert Android.mk files
Soong includes a tool perform a first pass at converting Android.mk files
to Android.bp files:
```
androidmk Android.mk > Android.bp
```
The tool converts variables, modules, comments, and some conditionals, but any
custom Makefile rules, complex conditionals or extra includes must be converted
by hand.
#### Differences between Android.mk and Android.bp
* Android.mk files often have multiple modules with the same name (for example
for static and shared version of a library, or for host and device versions).
Android.bp files require unique names for every module, but a single module can
be built in multiple variants, for example by adding `host_supported: true`.
The androidmk converter will produce multiple conflicting modules, which must
be resolved by hand to a single module with any differences inside
`target: { android: { }, host: { } }` blocks.
## Build logic
The build logic is written in Go using the
[blueprint](http://godoc.org/github.com/google/blueprint) framework. Build
logic receives module definitions parsed into Go structures using reflection
and produces build rules. The build rules are collected by blueprint and
written to a [ninja](http://ninja-build.org) build file.
## Other documentation
* [Best Practices](docs/best_practices.md)
* [Build Performance](docs/perf.md)
* [Generating CLion Projects](docs/clion.md)
* [Generating YouCompleteMe/VSCode compile\_commands.json file](docs/compdb.md)
* Make-specific documentation: [build/make/README.md](https://android.googlesource.com/platform/build/+/master/README.md)
## FAQ
### How do I write conditionals?
Soong deliberately does not support conditionals in Android.bp files.
Instead, complexity in build rules that would require conditionals are handled
in Go, where high level language features can be used and implicit dependencies
introduced by conditionals can be tracked. Most conditionals are converted
to a map property, where one of the values in the map will be selected and
appended to the top level properties.
For example, to support architecture specific files:
```
cc_library {
...
srcs: ["generic.cpp"],
arch: {
arm: {
srcs: ["arm.cpp"],
},
x86: {
srcs: ["x86.cpp"],
},
},
}
```
See [art/build/art.go](https://android.googlesource.com/platform/art/+/master/build/art.go)
or [external/llvm/soong/llvm.go](https://android.googlesource.com/platform/external/llvm/+/master/soong/llvm.go)
for examples of more complex conditionals on product variables or environment variables.
## Developing for Soong
To load Soong code in a Go-aware IDE, create a directory outside your android tree and then:
```bash
apt install bindfs
export GOPATH=<path to the directory you created>
build/soong/scripts/setup_go_workspace_for_soong.sh
```
This will bind mount the Soong source directories into the directory in the layout expected by
the IDE.
## Contact
Email android-building@googlegroups.com (external) for any questions, or see
[go/soong](http://go/soong) (internal).
|