1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
|
// Copyright 2019 Google Inc. All rights reserved.
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
// http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
package android
import (
"fmt"
"io"
"strings"
)
// sh_binary is for shell scripts (and batch files) that are installed as
// executable files into .../bin/
//
// Do not use them for prebuilt C/C++/etc files. Use cc_prebuilt_binary
// instead.
func init() {
RegisterModuleType("sh_binary", ShBinaryFactory)
RegisterModuleType("sh_binary_host", ShBinaryHostFactory)
RegisterModuleType("sh_test", ShTestFactory)
}
type shBinaryProperties struct {
// Source file of this prebuilt.
Src *string `android:"path,arch_variant"`
// optional subdirectory under which this file is installed into
Sub_dir *string `android:"arch_variant"`
// optional name for the installed file. If unspecified, name of the module is used as the file name
Filename *string `android:"arch_variant"`
// when set to true, and filename property is not set, the name for the installed file
// is the same as the file name of the source file.
Filename_from_src *bool `android:"arch_variant"`
// Whether this module is directly installable to one of the partitions. Default: true.
Installable *bool
}
type TestProperties struct {
// list of compatibility suites (for example "cts", "vts") that the module should be
// installed into.
Test_suites []string `android:"arch_variant"`
// the name of the test configuration (for example "AndroidTest.xml") that should be
// installed with the module.
Test_config *string `android:"arch_variant"`
}
type ShBinary struct {
ModuleBase
properties shBinaryProperties
sourceFilePath Path
outputFilePath OutputPath
}
type ShTest struct {
ShBinary
testProperties TestProperties
}
func (s *ShBinary) DepsMutator(ctx BottomUpMutatorContext) {
if s.properties.Src == nil {
ctx.PropertyErrorf("src", "missing prebuilt source file")
}
}
func (s *ShBinary) SourceFilePath(ctx ModuleContext) Path {
return PathForModuleSrc(ctx, String(s.properties.Src))
}
func (s *ShBinary) OutputFile() OutputPath {
return s.outputFilePath
}
func (s *ShBinary) SubDir() string {
return String(s.properties.Sub_dir)
}
func (s *ShBinary) Installable() bool {
return s.properties.Installable == nil || Bool(s.properties.Installable)
}
func (s *ShBinary) GenerateAndroidBuildActions(ctx ModuleContext) {
s.sourceFilePath = PathForModuleSrc(ctx, String(s.properties.Src))
filename := String(s.properties.Filename)
filename_from_src := Bool(s.properties.Filename_from_src)
if filename == "" {
if filename_from_src {
filename = s.sourceFilePath.Base()
} else {
filename = ctx.ModuleName()
}
} else if filename_from_src {
ctx.PropertyErrorf("filename_from_src", "filename is set. filename_from_src can't be true")
return
}
s.outputFilePath = PathForModuleOut(ctx, filename).OutputPath
// This ensures that outputFilePath has the correct name for others to
// use, as the source file may have a different name.
ctx.Build(pctx, BuildParams{
Rule: CpExecutable,
Output: s.outputFilePath,
Input: s.sourceFilePath,
})
}
func (s *ShBinary) AndroidMk() AndroidMkData {
return AndroidMkData{
Class: "EXECUTABLES",
OutputFile: OptionalPathForPath(s.outputFilePath),
Include: "$(BUILD_SYSTEM)/soong_cc_prebuilt.mk",
Extra: []AndroidMkExtraFunc{
func(w io.Writer, outputFile Path) {
fmt.Fprintln(w, "LOCAL_MODULE_RELATIVE_PATH :=", String(s.properties.Sub_dir))
fmt.Fprintln(w, "LOCAL_MODULE_SUFFIX :=")
fmt.Fprintln(w, "LOCAL_MODULE_STEM :=", s.outputFilePath.Rel())
},
},
}
}
func (s *ShTest) AndroidMk() AndroidMkData {
data := s.ShBinary.AndroidMk()
data.Class = "NATIVE_TESTS"
data.Extra = append(data.Extra, func(w io.Writer, outputFile Path) {
fmt.Fprintln(w, "LOCAL_COMPATIBILITY_SUITE :=",
strings.Join(s.testProperties.Test_suites, " "))
fmt.Fprintln(w, "LOCAL_TEST_CONFIG :=", String(s.testProperties.Test_config))
})
return data
}
func InitShBinaryModule(s *ShBinary) {
s.AddProperties(&s.properties)
}
// sh_binary is for a shell script or batch file to be installed as an
// executable binary to <partition>/bin.
func ShBinaryFactory() Module {
module := &ShBinary{}
InitShBinaryModule(module)
InitAndroidArchModule(module, HostAndDeviceSupported, MultilibFirst)
return module
}
// sh_binary_host is for a shell script to be installed as an executable binary
// to $(HOST_OUT)/bin.
func ShBinaryHostFactory() Module {
module := &ShBinary{}
InitShBinaryModule(module)
InitAndroidArchModule(module, HostSupported, MultilibFirst)
return module
}
func ShTestFactory() Module {
module := &ShTest{}
InitShBinaryModule(&module.ShBinary)
module.AddProperties(&module.testProperties)
InitAndroidArchModule(module, HostAndDeviceSupported, MultilibFirst)
return module
}
|