1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
|
// Copyright 2016 Google Inc. All rights reserved.
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
// http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
package cc
import (
"path/filepath"
"github.com/google/blueprint"
"android/soong/android"
)
type BinaryLinkerProperties struct {
// compile executable with -static
Static_executable *bool `android:"arch_variant"`
// set the name of the output
Stem *string `android:"arch_variant"`
// append to the name of the output
Suffix *string `android:"arch_variant"`
// if set, add an extra objcopy --prefix-symbols= step
Prefix_symbols *string
// if set, install a symlink to the preferred architecture
Symlink_preferred_arch *bool
// install symlinks to the binary. Symlink names will have the suffix and the binary
// extension (if any) appended
Symlinks []string `android:"arch_variant"`
DynamicLinker string `blueprint:"mutated"`
// Names of modules to be overridden. Listed modules can only be other binaries
// (in Make or Soong).
// This does not completely prevent installation of the overridden binaries, but if both
// binaries would be installed by default (in PRODUCT_PACKAGES) the other binary will be removed
// from PRODUCT_PACKAGES.
Overrides []string
}
func init() {
android.RegisterModuleType("cc_binary", BinaryFactory)
android.RegisterModuleType("cc_binary_host", binaryHostFactory)
}
// cc_binary produces a binary that is runnable on a device.
func BinaryFactory() android.Module {
module, _ := NewBinary(android.HostAndDeviceSupported)
return module.Init()
}
// cc_binary_host produces a binary that is runnable on a host.
func binaryHostFactory() android.Module {
module, _ := NewBinary(android.HostSupported)
return module.Init()
}
//
// Executables
//
type binaryDecorator struct {
*baseLinker
*baseInstaller
stripper
Properties BinaryLinkerProperties
toolPath android.OptionalPath
// Location of the linked, unstripped binary
unstrippedOutputFile android.Path
// Names of symlinks to be installed for use in LOCAL_MODULE_SYMLINKS
symlinks []string
// Output archive of gcno coverage information
coverageOutputFile android.OptionalPath
// Location of the file that should be copied to dist dir when requested
distFile android.OptionalPath
post_install_cmds []string
}
var _ linker = (*binaryDecorator)(nil)
func (binary *binaryDecorator) linkerProps() []interface{} {
return append(binary.baseLinker.linkerProps(),
&binary.Properties,
&binary.stripper.StripProperties)
}
func (binary *binaryDecorator) getStem(ctx BaseModuleContext) string {
stem := ctx.baseModuleName()
if String(binary.Properties.Stem) != "" {
stem = String(binary.Properties.Stem)
}
return stem + String(binary.Properties.Suffix)
}
func (binary *binaryDecorator) linkerDeps(ctx DepsContext, deps Deps) Deps {
deps = binary.baseLinker.linkerDeps(ctx, deps)
if ctx.toolchain().Bionic() {
if !Bool(binary.baseLinker.Properties.Nocrt) {
if !ctx.useSdk() {
if binary.static() {
deps.CrtBegin = "crtbegin_static"
} else {
deps.CrtBegin = "crtbegin_dynamic"
}
deps.CrtEnd = "crtend_android"
} else {
// TODO(danalbert): Add generation of crt objects.
// For `sdk_version: "current"`, we don't actually have a
// freshly generated set of CRT objects. Use the last stable
// version.
version := ctx.sdkVersion()
if version == "current" {
version = getCurrentNdkPrebuiltVersion(ctx)
}
if binary.static() {
deps.CrtBegin = "ndk_crtbegin_static." + version
} else {
if binary.static() {
deps.CrtBegin = "ndk_crtbegin_static." + version
} else {
deps.CrtBegin = "ndk_crtbegin_dynamic." + version
}
deps.CrtEnd = "ndk_crtend_android." + version
}
}
}
if binary.static() {
if ctx.selectedStl() == "libc++_static" {
deps.StaticLibs = append(deps.StaticLibs, "libm", "libc", "libdl")
}
// static libraries libcompiler_rt, libc and libc_nomalloc need to be linked with
// --start-group/--end-group along with libgcc. If they are in deps.StaticLibs,
// move them to the beginning of deps.LateStaticLibs
var groupLibs []string
deps.StaticLibs, groupLibs = filterList(deps.StaticLibs,
[]string{"libc", "libc_nomalloc", "libcompiler_rt"})
deps.LateStaticLibs = append(groupLibs, deps.LateStaticLibs...)
}
if ctx.Os() == android.LinuxBionic && !binary.static() {
deps.DynamicLinker = "linker"
deps.LinkerFlagsFile = "host_bionic_linker_flags"
}
}
if !binary.static() && inList("libc", deps.StaticLibs) {
ctx.ModuleErrorf("statically linking libc to dynamic executable, please remove libc\n" +
"from static libs or set static_executable: true")
}
return deps
}
func (binary *binaryDecorator) isDependencyRoot() bool {
return true
}
func NewBinary(hod android.HostOrDeviceSupported) (*Module, *binaryDecorator) {
module := newModule(hod, android.MultilibFirst)
binary := &binaryDecorator{
baseLinker: NewBaseLinker(module.sanitize),
baseInstaller: NewBaseInstaller("bin", "", InstallInSystem),
}
module.compiler = NewBaseCompiler()
module.linker = binary
module.installer = binary
return module, binary
}
func (binary *binaryDecorator) linkerInit(ctx BaseModuleContext) {
binary.baseLinker.linkerInit(ctx)
if !ctx.toolchain().Bionic() {
if ctx.Os() == android.Linux {
if binary.Properties.Static_executable == nil && ctx.Config().HostStaticBinaries() {
binary.Properties.Static_executable = BoolPtr(true)
}
} else if !ctx.Fuchsia() {
// Static executables are not supported on Darwin or Windows
binary.Properties.Static_executable = nil
}
}
}
func (binary *binaryDecorator) static() bool {
return Bool(binary.Properties.Static_executable)
}
func (binary *binaryDecorator) staticBinary() bool {
return binary.static()
}
func (binary *binaryDecorator) linkerFlags(ctx ModuleContext, flags Flags) Flags {
flags = binary.baseLinker.linkerFlags(ctx, flags)
if ctx.Host() && !ctx.Windows() && !binary.static() {
if !ctx.Config().IsEnvTrue("DISABLE_HOST_PIE") {
flags.LdFlags = append(flags.LdFlags, "-pie")
}
}
// MinGW spits out warnings about -fPIC even for -fpie?!) being ignored because
// all code is position independent, and then those warnings get promoted to
// errors.
if !ctx.Windows() {
flags.CFlags = append(flags.CFlags, "-fPIE")
}
if ctx.toolchain().Bionic() {
if binary.static() {
// Clang driver needs -static to create static executable.
// However, bionic/linker uses -shared to overwrite.
// Linker for x86 targets does not allow coexistance of -static and -shared,
// so we add -static only if -shared is not used.
if !inList("-shared", flags.LdFlags) {
flags.LdFlags = append(flags.LdFlags, "-static")
}
flags.LdFlags = append(flags.LdFlags,
"-nostdlib",
"-Bstatic",
"-Wl,--gc-sections",
)
} else {
if flags.DynamicLinker == "" {
if binary.Properties.DynamicLinker != "" {
flags.DynamicLinker = binary.Properties.DynamicLinker
} else {
switch ctx.Os() {
case android.Android:
if ctx.bootstrap() && !ctx.inRecovery() {
flags.DynamicLinker = "/system/bin/bootstrap/linker"
} else {
flags.DynamicLinker = "/system/bin/linker"
}
if flags.Toolchain.Is64Bit() {
flags.DynamicLinker += "64"
}
case android.LinuxBionic:
flags.DynamicLinker = ""
default:
ctx.ModuleErrorf("unknown dynamic linker")
}
}
if ctx.Os() == android.LinuxBionic {
// Use the dlwrap entry point, but keep _start around so
// that it can be used by host_bionic_inject
flags.LdFlags = append(flags.LdFlags,
"-Wl,--entry=__dlwrap__start",
"-Wl,--undefined=_start",
)
}
}
flags.LdFlags = append(flags.LdFlags,
"-pie",
"-nostdlib",
"-Bdynamic",
"-Wl,--gc-sections",
"-Wl,-z,nocopyreloc",
)
}
} else {
if binary.static() {
flags.LdFlags = append(flags.LdFlags, "-static")
}
if ctx.Darwin() {
flags.LdFlags = append(flags.LdFlags, "-Wl,-headerpad_max_install_names")
}
}
return flags
}
func (binary *binaryDecorator) link(ctx ModuleContext,
flags Flags, deps PathDeps, objs Objects) android.Path {
fileName := binary.getStem(ctx) + flags.Toolchain.ExecutableSuffix()
outputFile := android.PathForModuleOut(ctx, fileName)
ret := outputFile
var linkerDeps android.Paths
if deps.LinkerFlagsFile.Valid() {
flags.LdFlags = append(flags.LdFlags, "$$(cat "+deps.LinkerFlagsFile.String()+")")
linkerDeps = append(linkerDeps, deps.LinkerFlagsFile.Path())
}
if flags.DynamicLinker != "" {
flags.LdFlags = append(flags.LdFlags, "-Wl,-dynamic-linker,"+flags.DynamicLinker)
} else if ctx.toolchain().Bionic() && !binary.static() {
flags.LdFlags = append(flags.LdFlags, "-Wl,--no-dynamic-linker")
}
builderFlags := flagsToBuilderFlags(flags)
if binary.stripper.needsStrip(ctx) {
if ctx.Darwin() {
builderFlags.stripUseGnuStrip = true
}
strippedOutputFile := outputFile
outputFile = android.PathForModuleOut(ctx, "unstripped", fileName)
binary.stripper.strip(ctx, outputFile, strippedOutputFile, builderFlags)
}
binary.unstrippedOutputFile = outputFile
if String(binary.Properties.Prefix_symbols) != "" {
afterPrefixSymbols := outputFile
outputFile = android.PathForModuleOut(ctx, "unprefixed", fileName)
TransformBinaryPrefixSymbols(ctx, String(binary.Properties.Prefix_symbols), outputFile,
flagsToBuilderFlags(flags), afterPrefixSymbols)
}
if Bool(binary.baseLinker.Properties.Use_version_lib) {
if ctx.Host() {
versionedOutputFile := outputFile
outputFile = android.PathForModuleOut(ctx, "unversioned", fileName)
binary.injectVersionSymbol(ctx, outputFile, versionedOutputFile)
} else {
versionedOutputFile := android.PathForModuleOut(ctx, "versioned", fileName)
binary.distFile = android.OptionalPathForPath(versionedOutputFile)
if binary.stripper.needsStrip(ctx) {
out := android.PathForModuleOut(ctx, "versioned-stripped", fileName)
binary.distFile = android.OptionalPathForPath(out)
binary.stripper.strip(ctx, versionedOutputFile, out, builderFlags)
}
binary.injectVersionSymbol(ctx, outputFile, versionedOutputFile)
}
}
if ctx.Os() == android.LinuxBionic && !binary.static() {
injectedOutputFile := outputFile
outputFile = android.PathForModuleOut(ctx, "prelinker", fileName)
if !deps.DynamicLinker.Valid() {
panic("Non-static host bionic modules must have a dynamic linker")
}
binary.injectHostBionicLinkerSymbols(ctx, outputFile, deps.DynamicLinker.Path(), injectedOutputFile)
}
var sharedLibs android.Paths
// Ignore shared libs for static executables.
if !binary.static() {
sharedLibs = deps.EarlySharedLibs
sharedLibs = append(sharedLibs, deps.SharedLibs...)
sharedLibs = append(sharedLibs, deps.LateSharedLibs...)
linkerDeps = append(linkerDeps, deps.EarlySharedLibsDeps...)
linkerDeps = append(linkerDeps, deps.SharedLibsDeps...)
linkerDeps = append(linkerDeps, deps.LateSharedLibsDeps...)
}
linkerDeps = append(linkerDeps, objs.tidyFiles...)
linkerDeps = append(linkerDeps, flags.LdFlagsDeps...)
TransformObjToDynamicBinary(ctx, objs.objFiles, sharedLibs, deps.StaticLibs,
deps.LateStaticLibs, deps.WholeStaticLibs, linkerDeps, deps.CrtBegin, deps.CrtEnd, true,
builderFlags, outputFile, nil)
objs.coverageFiles = append(objs.coverageFiles, deps.StaticLibObjs.coverageFiles...)
objs.coverageFiles = append(objs.coverageFiles, deps.WholeStaticLibObjs.coverageFiles...)
binary.coverageOutputFile = TransformCoverageFilesToLib(ctx, objs, builderFlags, binary.getStem(ctx))
// Need to determine symlinks early since some targets (ie APEX) need this
// information but will not call 'install'
for _, symlink := range binary.Properties.Symlinks {
binary.symlinks = append(binary.symlinks,
symlink+String(binary.Properties.Suffix)+ctx.toolchain().ExecutableSuffix())
}
if Bool(binary.Properties.Symlink_preferred_arch) {
if String(binary.Properties.Stem) == "" && String(binary.Properties.Suffix) == "" {
ctx.PropertyErrorf("symlink_preferred_arch", "must also specify stem or suffix")
}
if ctx.TargetPrimary() {
binary.symlinks = append(binary.symlinks, ctx.baseModuleName())
}
}
return ret
}
func (binary *binaryDecorator) unstrippedOutputFilePath() android.Path {
return binary.unstrippedOutputFile
}
func (binary *binaryDecorator) symlinkList() []string {
return binary.symlinks
}
func (binary *binaryDecorator) nativeCoverage() bool {
return true
}
// /system/bin/linker -> /apex/com.android.runtime/bin/linker
func (binary *binaryDecorator) installSymlinkToRuntimeApex(ctx ModuleContext, file android.Path) {
dir := binary.baseInstaller.installDir(ctx)
dirOnDevice := android.InstallPathToOnDevicePath(ctx, dir)
target := "/" + filepath.Join("apex", "com.android.runtime", dir.Base(), file.Base())
ctx.InstallAbsoluteSymlink(dir, file.Base(), target)
binary.post_install_cmds = append(binary.post_install_cmds, makeSymlinkCmd(dirOnDevice, file.Base(), target))
for _, symlink := range binary.symlinks {
ctx.InstallAbsoluteSymlink(dir, symlink, target)
binary.post_install_cmds = append(binary.post_install_cmds, makeSymlinkCmd(dirOnDevice, symlink, target))
}
}
func (binary *binaryDecorator) install(ctx ModuleContext, file android.Path) {
// Bionic binaries (e.g. linker) is installed to the bootstrap subdirectory.
// The original path becomes a symlink to the corresponding file in the
// runtime APEX.
if isBionic(ctx.baseModuleName()) && ctx.Arch().Native && ctx.apexName() == "" && !ctx.inRecovery() {
if ctx.Device() {
binary.installSymlinkToRuntimeApex(ctx, file)
}
binary.baseInstaller.subDir = "bootstrap"
}
binary.baseInstaller.install(ctx, file)
for _, symlink := range binary.symlinks {
ctx.InstallSymlink(binary.baseInstaller.installDir(ctx), symlink, binary.baseInstaller.path)
}
if ctx.Os().Class == android.Host {
binary.toolPath = android.OptionalPathForPath(binary.baseInstaller.path)
}
}
func (binary *binaryDecorator) hostToolPath() android.OptionalPath {
return binary.toolPath
}
func init() {
pctx.HostBinToolVariable("hostBionicSymbolsInjectCmd", "host_bionic_inject")
}
var injectHostBionicSymbols = pctx.AndroidStaticRule("injectHostBionicSymbols",
blueprint.RuleParams{
Command: "$hostBionicSymbolsInjectCmd -i $in -l $linker -o $out",
CommandDeps: []string{"$hostBionicSymbolsInjectCmd"},
}, "linker")
func (binary *binaryDecorator) injectHostBionicLinkerSymbols(ctx ModuleContext, in, linker android.Path, out android.WritablePath) {
ctx.Build(pctx, android.BuildParams{
Rule: injectHostBionicSymbols,
Description: "inject host bionic symbols",
Input: in,
Implicit: linker,
Output: out,
Args: map[string]string{
"linker": linker.String(),
},
})
}
|