# dexpreopt_odex_install.mk is used to define odex creation rules for JARs and APKs
# This file depends on variables set in base_rules.mk
# Output variables: LOCAL_DEX_PREOPT, LOCAL_UNCOMPRESS_DEX, built_odex,
# dexpreopt_boot_jar_module
ifeq (true,$(LOCAL_PREFER_CODE_INTEGRITY))
LOCAL_UNCOMPRESS_DEX := true
else
LOCAL_UNCOMPRESS_DEX :=
endif
# We explicitly uncompress APKs of privileged apps, and used by
# privileged apps
ifneq (true,$(DONT_UNCOMPRESS_PRIV_APPS_DEXS))
ifeq (true,$(LOCAL_PRIVILEGED_MODULE))
LOCAL_UNCOMPRESS_DEX := true
endif
ifneq (,$(filter $(PRODUCT_LOADED_BY_PRIVILEGED_MODULES), $(LOCAL_MODULE)))
LOCAL_UNCOMPRESS_DEX := true
endif
endif # DONT_UNCOMPRESS_PRIV_APPS_DEXS
# Setting LOCAL_DEX_PREOPT based on WITH_DEXPREOPT, LOCAL_DEX_PREOPT, etc
LOCAL_DEX_PREOPT := $(strip $(LOCAL_DEX_PREOPT))
ifndef LOCAL_DEX_PREOPT # LOCAL_DEX_PREOPT undefined
LOCAL_DEX_PREOPT := $(DEX_PREOPT_DEFAULT)
endif
ifeq (false,$(LOCAL_DEX_PREOPT))
LOCAL_DEX_PREOPT :=
endif
# Only enable preopt for non tests.
ifneq (,$(filter $(LOCAL_MODULE_TAGS),tests))
LOCAL_DEX_PREOPT :=
endif
# If we have product-specific config for this module?
ifneq (,$(filter $(LOCAL_MODULE),$(DEXPREOPT_DISABLED_MODULES)))
LOCAL_DEX_PREOPT :=
endif
# Disable preopt for TARGET_BUILD_APPS
ifneq (,$(TARGET_BUILD_APPS))
LOCAL_DEX_PREOPT :=
endif
# Disable preopt if not WITH_DEXPREOPT
ifneq (true,$(WITH_DEXPREOPT))
LOCAL_DEX_PREOPT :=
endif
ifdef LOCAL_UNINSTALLABLE_MODULE
LOCAL_DEX_PREOPT :=
endif
ifeq (,$(strip $(built_dex)$(my_prebuilt_src_file)$(LOCAL_SOONG_DEX_JAR))) # contains no java code
LOCAL_DEX_PREOPT :=
endif
# if WITH_DEXPREOPT_BOOT_IMG_AND_SYSTEM_SERVER_ONLY=true and module is not in boot class path skip
# Also preopt system server jars since selinux prevents system server from loading anything from
# /data. If we don't do this they will need to be extracted which is not favorable for RAM usage
# or performance. If my_preopt_for_extracted_apk is true, we ignore the only preopt boot image
# options.
ifneq (true,$(my_preopt_for_extracted_apk))
ifeq (true,$(WITH_DEXPREOPT_BOOT_IMG_AND_SYSTEM_SERVER_ONLY))
ifeq ($(filter $(PRODUCT_SYSTEM_SERVER_JARS) $(DEXPREOPT_BOOT_JARS_MODULES),$(LOCAL_MODULE)),)
LOCAL_DEX_PREOPT :=
endif
endif
endif
my_process_profile :=
my_profile_is_text_listing :=
ifeq (false,$(WITH_DEX_PREOPT_GENERATE_PROFILE))
LOCAL_DEX_PREOPT_GENERATE_PROFILE := false
endif
ifndef LOCAL_DEX_PREOPT_GENERATE_PROFILE
# If LOCAL_DEX_PREOPT_GENERATE_PROFILE is not defined, default it based on the existence of the
# profile class listing. TODO: Use product specific directory here.
my_classes_directory := $(PRODUCT_DEX_PREOPT_PROFILE_DIR)
LOCAL_DEX_PREOPT_PROFILE := $(my_classes_directory)/$(LOCAL_MODULE).prof
ifneq (,$(wildcard $(LOCAL_DEX_PREOPT_PROFILE)))
my_process_profile := true
my_profile_is_text_listing :=
endif
else
my_process_profile := $(LOCAL_DEX_PREOPT_GENERATE_PROFILE)
my_profile_is_text_listing := true
LOCAL_DEX_PREOPT_PROFILE := $(LOCAL_DEX_PREOPT_PROFILE_CLASS_LISTING)
endif
ifeq (true,$(my_process_profile))
ifndef LOCAL_DEX_PREOPT_PROFILE
$(call pretty-error,Must have specified class listing (LOCAL_DEX_PREOPT_PROFILE))
endif
ifeq (,$(dex_preopt_profile_src_file))
$(call pretty-error, Internal error: dex_preopt_profile_src_file must be set)
endif
endif
# If LOCAL_ENFORCE_USES_LIBRARIES is not set, default to true if either of LOCAL_USES_LIBRARIES or
# LOCAL_OPTIONAL_USES_LIBRARIES are specified.
ifeq (,$(LOCAL_ENFORCE_USES_LIBRARIES))
# Will change the default to true unconditionally in the future.
ifneq (,$(LOCAL_OPTIONAL_USES_LIBRARIES))
LOCAL_ENFORCE_USES_LIBRARIES := true
endif
ifneq (,$(LOCAL_USES_LIBRARIES))
LOCAL_ENFORCE_USES_LIBRARIES := true
endif
endif
my_dexpreopt_archs :=
ifdef LOCAL_DEX_PREOPT
ifeq ($(LOCAL_MODULE_CLASS),JAVA_LIBRARIES)
my_module_multilib := $(LOCAL_MULTILIB)
# If the module is not an SDK library and it's a system server jar, only preopt the primary arch.
my_filtered_lib_name := $(patsubst %.impl,%,$(LOCAL_MODULE))
ifeq (,$(filter $(JAVA_SDK_LIBRARIES),$(my_filtered_lib_name)))
# For a Java library, by default we build odex for both 1st arch and 2nd arch.
# But it can be overridden with "LOCAL_MULTILIB := first".
ifneq (,$(filter $(PRODUCT_SYSTEM_SERVER_JARS),$(LOCAL_MODULE)))
# For system server jars, we build for only "first".
my_module_multilib := first
endif
endif
# Only preopt primary arch for translated arch since there is only an image there.
ifeq ($(TARGET_TRANSLATE_2ND_ARCH),true)
my_module_multilib := first
endif
# #################################################
# Odex for the 1st arch
my_dexpreopt_archs += $(TARGET_ARCH)
# Odex for the 2nd arch
ifdef TARGET_2ND_ARCH
ifneq ($(TARGET_TRANSLATE_2ND_ARCH),true)
ifneq (first,$(my_module_multilib))
my_dexpreopt_archs += $(TARGET_2ND_ARCH)
endif # my_module_multilib is not first.
endif # TARGET_TRANSLATE_2ND_ARCH not true
endif # TARGET_2ND_ARCH
# #################################################
else # must be APPS
# The preferred arch
# Save the module multilib since setup_one_odex modifies it.
my_2nd_arch_prefix := $(LOCAL_2ND_ARCH_VAR_PREFIX)
my_dexpreopt_archs += $(TARGET_$(my_2nd_arch_prefix)ARCH)
ifdef TARGET_2ND_ARCH
ifeq ($(my_module_multilib),both)
# The non-preferred arch
my_2nd_arch_prefix := $(if $(LOCAL_2ND_ARCH_VAR_PREFIX),,$(TARGET_2ND_ARCH_VAR_PREFIX))
my_dexpreopt_archs += $(TARGET_$(my_2nd_arch_prefix)ARCH)
endif # LOCAL_MULTILIB is both
endif # TARGET_2ND_ARCH
endif # LOCAL_MODULE_CLASS
# Record dex-preopt config.
DEXPREOPT.$(LOCAL_MODULE).DEX_PREOPT := $(LOCAL_DEX_PREOPT)
DEXPREOPT.$(LOCAL_MODULE).MULTILIB := $(LOCAL_MULTILIB)
DEXPREOPT.$(LOCAL_MODULE).DEX_PREOPT_FLAGS := $(LOCAL_DEX_PREOPT_FLAGS)
DEXPREOPT.$(LOCAL_MODULE).PRIVILEGED_MODULE := $(LOCAL_PRIVILEGED_MODULE)
DEXPREOPT.$(LOCAL_MODULE).VENDOR_MODULE := $(LOCAL_VENDOR_MODULE)
DEXPREOPT.$(LOCAL_MODULE).TARGET_ARCH := $(LOCAL_MODULE_TARGET_ARCH)
DEXPREOPT.$(LOCAL_MODULE).INSTALLED_STRIPPED := $(LOCAL_INSTALLED_MODULE)
DEXPREOPT.MODULES.$(LOCAL_MODULE_CLASS) := $(sort \
$(DEXPREOPT.MODULES.$(LOCAL_MODULE_CLASS)) $(LOCAL_MODULE))
$(call json_start)
$(call add_json_str, Name, $(LOCAL_MODULE))
$(call add_json_str, DexLocation, $(patsubst $(PRODUCT_OUT)%,%,$(LOCAL_INSTALLED_MODULE)))
$(call add_json_str, BuildPath, $(LOCAL_BUILT_MODULE))
$(call add_json_str, DexPath, $$1)
$(call add_json_str, ExtrasOutputPath, $$2)
$(call add_json_bool, PreferCodeIntegrity, $(filter true,$(LOCAL_PREFER_CODE_INTEGRITY)))
$(call add_json_bool, Privileged, $(filter true,$(LOCAL_PRIVILEGED_MODULE)))
$(call add_json_bool, UncompressedDex, $(filter true,$(LOCAL_UNCOMPRESS_DEX)))
$(call add_json_bool, HasApkLibraries, $(LOCAL_APK_LIBRARIES))
$(call add_json_list, PreoptFlags, $(LOCAL_DEX_PREOPT_FLAGS))
$(call add_json_str, ProfileClassListing, $(if $(my_process_profile),$(LOCAL_DEX_PREOPT_PROFILE)))
$(call add_json_bool, ProfileIsTextListing, $(my_profile_is_text_listing))
$(call add_json_bool, EnforceUsesLibraries, $(LOCAL_ENFORCE_USES_LIBRARIES))
$(call add_json_list, OptionalUsesLibraries, $(LOCAL_OPTIONAL_USES_LIBRARIES))
$(call add_json_list, UsesLibraries, $(LOCAL_USES_LIBRARIES))
$(call add_json_map, LibraryPaths)
$(foreach lib,$(sort $(LOCAL_USES_LIBRARIES) $(LOCAL_OPTIONAL_USES_LIBRARIES) org.apache.http.legacy.impl android.hidl.base-V1.0-java android.hidl.manager-V1.0-java),\
$(call add_json_str, $(lib), $(call intermediates-dir-for,JAVA_LIBRARIES,$(lib),,COMMON)/javalib.jar))
$(call end_json_map)
$(call add_json_list, Archs, $(my_dexpreopt_archs))
$(call add_json_str, DexPreoptImageLocation, $(LOCAL_DEX_PREOPT_IMAGE_LOCATION))
$(call add_json_bool, PreoptExtractedApk, $(my_preopt_for_extracted_apk))
$(call add_json_bool, NoCreateAppImage, $(filter false,$(LOCAL_DEX_PREOPT_APP_IMAGE)))
$(call add_json_bool, ForceCreateAppImage, $(filter true,$(LOCAL_DEX_PREOPT_APP_IMAGE)))
$(call add_json_bool, PresignedPrebuilt, $(filter PRESIGNED,$(LOCAL_CERTIFICATE)))
$(call add_json_bool, NoStripping, $(filter nostripping,$(LOCAL_DEX_PREOPT)))
$(call add_json_str, StripInputPath, $$1)
$(call add_json_str, StripOutputPath, $$2)
$(call json_end)
my_dexpreopt_config := $(intermediates)/dexpreopt.config
my_dexpreopt_script := $(intermediates)/dexpreopt.sh
my_strip_script := $(intermediates)/strip.sh
my_dexpreopt_zip := $(intermediates)/dexpreopt.zip
$(my_dexpreopt_config): PRIVATE_MODULE := $(LOCAL_MODULE)
$(my_dexpreopt_config): PRIVATE_CONTENTS := $(json_contents)
$(my_dexpreopt_config):
@echo "$(PRIVATE_MODULE) dexpreopt.config"
echo -e -n '$(subst $(newline),\n,$(subst ','\'',$(subst \,\\,$(PRIVATE_CONTENTS))))' > $@
.KATI_RESTAT: $(my_dexpreopt_script) $(my_strip_script)
$(my_dexpreopt_script): PRIVATE_MODULE := $(LOCAL_MODULE)
$(my_dexpreopt_script): PRIVATE_GLOBAL_CONFIG := $(PRODUCT_OUT)/dexpreopt.config
$(my_dexpreopt_script): PRIVATE_MODULE_CONFIG := $(my_dexpreopt_config)
$(my_dexpreopt_script): PRIVATE_STRIP_SCRIPT := $(my_strip_script)
$(my_dexpreopt_script): .KATI_IMPLICIT_OUTPUTS := $(my_strip_script)
$(my_dexpreopt_script): $(DEXPREOPT_GEN)
$(my_dexpreopt_script): $(my_dexpreopt_config) $(PRODUCT_OUT)/dexpreopt.config
@echo "$(PRIVATE_MODULE) dexpreopt gen"
$(DEXPREOPT_GEN) -global $(PRIVATE_GLOBAL_CONFIG) -module $(PRIVATE_MODULE_CONFIG) \
-dexpreopt_script $@ -strip_script $(PRIVATE_STRIP_SCRIPT)
my_dexpreopt_deps := $(my_dex_jar)
my_dexpreopt_deps += $(if $(my_process_profile),$(LOCAL_DEX_PREOPT_PROFILE))
my_dexpreopt_deps += \
$(foreach lib,$(sort $(LOCAL_USES_LIBRARIES) $(LOCAL_OPTIONAL_USES_LIBRARIES) org.apache.http.legacy.impl android.hidl.base-V1.0-java android.hidl.manager-V1.0-java),\
$(call intermediates-dir-for,JAVA_LIBRARIES,$(lib),,COMMON)/javalib.jar)
my_dexpreopt_deps += $(LOCAL_DEX_PREOPT_IMAGE_LOCATION)
# TODO: default boot images
$(my_dexpreopt_zip): PRIVATE_MODULE := $(LOCAL_MODULE)
$(my_dexpreopt_zip): $(my_dexpreopt_deps)
$(my_dexpreopt_zip): | $(DEXPREOPT_GEN_DEPS)
$(my_dexpreopt_zip): .KATI_DEPFILE := $(my_dexpreopt_zip).d
$(my_dexpreopt_zip): PRIVATE_DEX := $(my_dex_jar)
$(my_dexpreopt_zip): PRIVATE_SCRIPT := $(my_dexpreopt_script)
$(my_dexpreopt_zip): $(my_dexpreopt_script)
@echo "$(PRIVATE_MODULE) dexpreopt"
bash $(PRIVATE_SCRIPT) $(PRIVATE_DEX) $@
ifdef LOCAL_POST_INSTALL_CMD
# Add a shell command separator
LOCAL_POST_INSTALL_CMD += &&
endif
LOCAL_POST_INSTALL_CMD += \
for i in $$(zipinfo -1 $(my_dexpreopt_zip)); \
do mkdir -p $(PRODUCT_OUT)/$$(dirname $$i); \
done && \
( unzip -qo -d $(PRODUCT_OUT) $(my_dexpreopt_zip) 2>&1 | grep -v "zipfile is empty"; exit $${PIPESTATUS[0]} ) || \
( code=$$?; if [ $$code -ne 0 -a $$code -ne 1 ]; then exit $$code; fi )
$(LOCAL_INSTALLED_MODULE): PRIVATE_POST_INSTALL_CMD := $(LOCAL_POST_INSTALL_CMD)
$(LOCAL_INSTALLED_MODULE): $(my_dexpreopt_zip)
$(my_all_targets): $(my_dexpreopt_zip)
my_dexpreopt_config :=
my_dexpreopt_script :=
my_strip_script :=
my_dexpreopt_zip :=
endif # LOCAL_DEX_PREOPT