aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorDan Willemsen2017-02-13 15:41:43 -0600
committerDan Willemsen2017-02-13 16:19:47 -0600
commitb2a5c7b3693f4e44beb80575ee6cf66d89d333dd (patch)
treeb84e63c9a5501263a6633fc4a3b268454529fcfe /CleanSpec.mk
parent34fd8a168a00410f281eab1455efb797f0c7bb36 (diff)
downloadplatform-build-b2a5c7b3693f4e44beb80575ee6cf66d89d333dd.tar.gz
platform-build-b2a5c7b3693f4e44beb80575ee6cf66d89d333dd.tar.xz
platform-build-b2a5c7b3693f4e44beb80575ee6cf66d89d333dd.zip
Fix init rc installation in vendor when LOCAL_MODULE_PATH is set
The init.rc path selection uses the same partition_tag detection to select an installation partition. So make sure that we always set partition_tag even if we've been given an explicit module path. Bug: 35314904 Test: set proprietary: true to Soong module with an init rc, verify that was the only change to build-aosp_arm64.ninja Change-Id: Ic6ffd7a5177959db96a34a24896b242ee5b09e41
Diffstat (limited to 'CleanSpec.mk')
-rw-r--r--CleanSpec.mk2
1 files changed, 2 insertions, 0 deletions
diff --git a/CleanSpec.mk b/CleanSpec.mk
index b9f6e1390..9d3fc23c0 100644
--- a/CleanSpec.mk
+++ b/CleanSpec.mk
@@ -398,6 +398,8 @@ $(call add-clean-step, rm -rf $(TARGET_OUT_COMMON_INTERMEDIATES)/JAVA_LIBRARIES/
398$(call add-clean-step, rm -rf $(HOST_OUT_TESTCASES)) 398$(call add-clean-step, rm -rf $(HOST_OUT_TESTCASES))
399$(call add-clean-step, rm -rf $(TARGET_OUT_TESTCASES)) 399$(call add-clean-step, rm -rf $(TARGET_OUT_TESTCASES))
400 400
401$(call add-clean-step, rm -rf $(TARGET_OUT_ETC)/init)
402
401# ************************************************ 403# ************************************************
402# NEWER CLEAN STEPS MUST BE AT THE END OF THE LIST 404# NEWER CLEAN STEPS MUST BE AT THE END OF THE LIST
403# ************************************************ 405# ************************************************