aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorDan Willemsen2018-07-14 11:32:13 -0500
committerDan Willemsen2018-07-14 11:32:13 -0500
commit0ae41f2e79ceaa1416f73a1006c7e8e98b1105b4 (patch)
tree6ad43223d489ce6dd8d24431f2c39f4f1842cfc1 /Usage.txt
parent0e4c76743ace14e620cefb16a6095ced69adade7 (diff)
downloadplatform-build-0ae41f2e79ceaa1416f73a1006c7e8e98b1105b4.tar.gz
platform-build-0ae41f2e79ceaa1416f73a1006c7e8e98b1105b4.tar.xz
platform-build-0ae41f2e79ceaa1416f73a1006c7e8e98b1105b4.zip
Remove showcommands from docs
Test: none Change-Id: Ia0be98049710175a0f3276841ef0c0bd2ccb60b6
Diffstat (limited to 'Usage.txt')
-rw-r--r--Usage.txt17
1 files changed, 13 insertions, 4 deletions
diff --git a/Usage.txt b/Usage.txt
index 004210b47..558329bda 100644
--- a/Usage.txt
+++ b/Usage.txt
@@ -29,7 +29,7 @@ Ways to specify what to build:
29 An alternative to setting $TARGET_PRODUCT and $TARGET_BUILD_VARIANT, 29 An alternative to setting $TARGET_PRODUCT and $TARGET_BUILD_VARIANT,
30 which you may see in build servers, is to execute: 30 which you may see in build servers, is to execute:
31 31
32 make PRODUCT-<product>-<variant> 32 m PRODUCT-<product>-<variant>
33 33
34 34
35 A target may be a file path. For example, out/host/linux-x86/bin/adb . 35 A target may be a file path. For example, out/host/linux-x86/bin/adb .
@@ -46,6 +46,17 @@ Ways to specify what to build:
46 files named Android.bp 46 files named Android.bp
47 these files are defined in Blueprint syntax 47 these files are defined in Blueprint syntax
48 48
49 During a build, a few log files are generated in ${OUT} (or ${DIST_DIR}/logs
50 for dist builds):
51
52 verbose.log.gz
53 every command run, along with its outputs. This is similar to the
54 previous `m showcommands` option.
55 error.log
56 list of actions that failed during the build, and their outputs.
57 soong.log
58 verbose debug information from soong_ui
59
49 For now, the full (extremely large) compiled list of targets can be found 60 For now, the full (extremely large) compiled list of targets can be found
50 (after running the build once), split among these two files: 61 (after running the build once), split among these two files:
51 62
@@ -57,8 +68,6 @@ Ways to specify what to build:
57 tool here. 68 tool here.
58 69
59Targets that adjust an existing build: 70Targets that adjust an existing build:
60 showcommands Display the individual commands run to implement
61 the build
62 dist Copy into ${DIST_DIR} the portion of the build 71 dist Copy into ${DIST_DIR} the portion of the build
63 that must be distributed 72 that must be distributed
64 73
@@ -71,7 +80,7 @@ Variables
71 Variables can either be set in the surrounding shell environment or can be 80 Variables can either be set in the surrounding shell environment or can be
72 passed as command-line arguments. For example: 81 passed as command-line arguments. For example:
73 export I_AM_A_SHELL_VAR=1 82 export I_AM_A_SHELL_VAR=1
74 I_AM_ANOTHER_SHELL_VAR=2 make droid I_AM_A_MAKE_VAR=3 83 I_AM_ANOTHER_SHELL_VAR=2 m droid I_AM_A_MAKE_VAR=3
75 Here are some common variables and their meanings: 84 Here are some common variables and their meanings:
76 TARGET_PRODUCT The <product> to build # as described above 85 TARGET_PRODUCT The <product> to build # as described above
77 TARGET_BUILD_VARIANT The <variant> to build # as described above 86 TARGET_BUILD_VARIANT The <variant> to build # as described above