# caller might have included aux_toolchain, e.g. if custom build steps are defined ifeq ($(LOCAL_IS_AUX_MODULE),) include $(BUILD_SYSTEM)/aux_toolchain.mk endif ifeq ($(AUX_BUILD_NOT_COMPATIBLE),) ########################################################### ## Standard rules for building an executable file. ## ## Additional inputs from base_rules.make: ## None. ########################################################### ifeq ($(strip $(LOCAL_MODULE_CLASS)),) LOCAL_MODULE_CLASS := EXECUTABLES endif $(call $(aux-executable-hook)) ########################################################### ## Standard rules for building any target-side binaries ## with dynamic linkage (dynamic libraries or executables ## that link with dynamic libraries) ## ## Files including this file must define a rule to build ## the target $(linked_module). ########################################################### # The name of the target file, without any path prepended. # This duplicates logic from base_rules.mk because we need to # know its results before base_rules.mk is included. include $(BUILD_SYSTEM)/configure_module_stem.mk intermediates := $(call local-intermediates-dir) # Define the target that is the unmodified output of the linker. # The basename of this target must be the same as the final output # binary name, because it's used to set the "soname" in the binary. # The includer of this file will define a rule to build this target. linked_module := $(intermediates)/LINKED/$(my_built_module_stem) ALL_ORIGINAL_DYNAMIC_BINARIES += $(linked_module) # Because AUX_SYMBOL_FILTER_FILE depends on ALL_ORIGINAL_DYNAMIC_BINARIES, # the linked_module rules won't necessarily inherit the PRIVATE_ # variables from LOCAL_BUILT_MODULE. This tells binary.make to explicitly # define the PRIVATE_ variables for linked_module as well as for # LOCAL_BUILT_MODULE. LOCAL_INTERMEDIATE_TARGETS += $(linked_module) ################################### include $(BUILD_SYSTEM)/binary.mk ################################### aux_output := $(linked_module) ifneq ($(LOCAL_CUSTOM_BUILD_STEP_INPUT),) ifneq ($(LOCAL_CUSTOM_BUILD_STEP_OUTPUT),) # injecting custom build steps $(LOCAL_CUSTOM_BUILD_STEP_INPUT): $(aux_output) @echo "$(AUX_DISPLAY) custom copy: $(PRIVATE_MODULE) ($@)" @mkdir -p $(dir $@) $(hide) $(copy-file-to-target) aux_output := $(LOCAL_CUSTOM_BUILD_STEP_OUTPUT) endif endif $(LOCAL_BUILT_MODULE): $(aux_output) @echo "$(AUX_DISPLAY) final copy: $(PRIVATE_MODULE) ($@)" @mkdir -p $(dir $@) $(hide) $(copy-file-to-target) INSTALLED_AUX_TARGETS += $(LOCAL_INSTALLED_MODULE) $(cleantarget): PRIVATE_CLEAN_FILES += \ $(linked_module) \ # Define PRIVATE_ variables from global vars $(linked_module): PRIVATE_POST_LINK_CMD := $(LOCAL_POST_LINK_CMD) ifeq ($(LOCAL_FORCE_STATIC_EXECUTABLE),true) $(linked_module): $(all_objects) $(all_libraries) $(LOCAL_ADDITIONAL_DEPENDENCIES) $(transform-o-to-aux-static-executable) $(PRIVATE_POST_LINK_CMD) else $(linked_module): $(all_objects) $(all_libraries) $(LOCAL_ADDITIONAL_DEPENDENCIES) $(transform-o-to-aux-executable) $(PRIVATE_POST_LINK_CMD) endif endif # AUX_BUILD_NOT_COMPATIBLE