Android Build System

Status: Draft   (as of May 18, 2006)

Contents

Objective

The primary goals of reworking the build system are (1) to make dependencies work more reliably, so that when files need to rebuilt, they are, and (2) to improve performance of the build system so that unnecessary modules are not rebuilt, and so doing a top-level build when little or nothing needs to be done for a build takes as little time as possible.

Principles and Use Cases and Policy

Given the above objective, these are the overall principles and use cases that we will support. This is not an exhaustive list.

Multiple Targets

It needs to be possible to build the Android platform for multiple targets. This means:

Non-Recursive Make

To achieve the objectives, the build system will be rewritten to use make non-recursively. For more background on this, read Recursive Make Considered Harmful. For those that don't want PDF, here is the Google translated version.

Rapid Compile-Test Cycles

When developing a component, for example a C++ shared library, it must be possible to easily rebuild just that component, and not have to wait more than a couple seconds for dependency checks, and not have to wait for unneeded components to be built.

Both Environment and Config File Based Settings

To set the target, and other options, some people on the team like to have a configuration file in a directory so they do not have an environment setup script to run, and others want an environment setup script to run so they can run builds in different terminals on the same tree, or switch back and forth in one terminal. We will support both.

Object File Directory / make clean

Object files and other intermediate files will be generated into a directory that is separate from the source tree. The goal is to have make clean be "rm -rf " in the tree root directory. The primary goals of this are to simplify searching the source tree, and to make "make clean" more reliable.

SDK

The SDK will be a tarball that will allow non-OS-developers to write apps. The apps will actually be built by first building the SDK, and then building the apps against that SDK. This will hopefully (1) make writing apps easier for us, because we won't have to rebuild the OS as much, and we can use the standard java-app development tools, and (2) allow us to dog-food the SDK, to help ensure its quality. Cedric has suggested (and I agree) that apps built from the SDK should be built with ant. Stay tuned for more details as we figure out exactly how this will work.

Dependecies

Dependencies should all be automatic. Unless there is a custom tool involved (e.g. the webkit has several), the dependencies for shared and static libraries, .c, .cpp, .h, .java, java libraries, etc., should all work without intervention in the Android.mk file.

Wildcard source files

Wildcarding source file will be discouraged. It may be useful in some scenarios. The default $(wildcard *) will not work due to the current directory being set to the root of the build tree.

Multiple targets in one directory

It will be possible to generate more than one target from a given subdirectory. For example, libutils generates a shared library for the target and a static library for the host.

Makefile fragments for modules

Android.mk is the standard name for the makefile fragments that control the building of a given module. Only the top directory should have a file named "Makefile".

Use shared libraries

Currently, the simulator is not built to use shared libraries. This should be fixed, and now is a good time to do it. This implies getting shared libraries to work on Mac OS.

Nice to Have

These things would be nice to have, and this is a good place to record them, however these are not promises.

Simultaneous Builds

The hope is to be able to do two builds for different combos in the same tree at the same time, but this is a stretch goal, not a requirement. Doing two builds in the same tree, not at the same time must work. (update: it's looking like we'll get the two builds at the same time working)

Deleting headers (or other dependecies)

Problems can arise if you delete a header file that is referenced in ".d" files. The easy way to deal with this is "make clean". There should be a better way to handle it. (from fadden)

One way of solving this is introducing a dependency on the directory. The problem is that this can create extra dependecies and slow down the build. It's a tradeoff.

Multiple builds

General way to perform builds across the set of known platforms. This would make it easy to perform multiple platform builds when testing a change, and allow a wide-scale "make clean". Right now the buildspec.mk or environment variables need to be updated before each build. (from fadden)

Aftermarket Locales and Carrier

We will eventually need to add support for creating locales and carrier customizations to the SDK, but that will not be addressed right now.

Usage

You've read (or scrolled past) all of the motivations for this build system, and you want to know how to use it. This is the place.

Your first build

The Building document describes how do do builds.

build/envsetup.sh functions

If you source the file build/envsetup.sh into your bash environment, . build/envsetup.shyou'll get a few helpful shell functions:

Build flavors/types

When building for a particular product, it's often useful to have minor variations on what is ultimately the final release build. These are the currently-defined "flavors" or "types" (we need to settle on a real name for these).

eng This is the default flavor. A plain "make" is the same as "make eng". droid is an alias for eng.
  • Installs modules tagged with: eng, debug, user, and/or development.
  • Installs non-APK modules that have no tags specified.
  • Installs APKs according to the product definition files, in addition to tagged APKs.
  • ro.secure=0
  • ro.debuggable=1
  • ro.kernel.android.checkjni=1
  • adb is enabled by default.
user "make user"

This is the flavor intended to be the final release bits.

  • Installs modules tagged with user.
  • Installs non-APK modules that have no tags specified.
  • Installs APKs according to the product definition files; tags are ignored for APK modules.
  • ro.adb.secure=1
  • ro.secure=1
  • ro.debuggable=0
  • adb is disabled by default.
userdebug "make userdebug"

The same as user, except:

  • Also installs modules tagged with debug.
  • ro.debuggable=1
  • adb is enabled by default.

If you build one flavor and then want to build another, you should run "make installclean" between the two makes to guarantee that you don't pick up files installed by the previous flavor. "make clean" will also suffice, but it takes a lot longer.

More pseudotargets

Sometimes you want to just build one thing. The following pseudotargets are there for your convenience:

How to add another component to the build - Android.mk templates

You have a new library, a new app, or a new executable. For each of the common types of modules, there is a corresponding file in the templates directory. It will usually be enough to copy one of these, and fill in your own values. Some of the more esoteric values are not included in the templates, but are instead just documented here, as is the documentation on using custom tools to generate files.

Mostly, you can just look for the TODO comments in the templates and do what it says. Please remember to delete the TODO comments when you're done to keep the files clean. The templates have minimal documentation in them, because they're going to be copied, and when that gets stale, the copies just won't get updated. So read on...

Apps

Use the templates/apps file.

This template is pretty self-explanitory. See the variables below for more details.

Java Libraries

Use the templates/java_library file.

The interesting thing here is the value of LOCAL_MODULE, which becomes the name of the jar file. (Actually right now, we're not making jar files yet, just directories of .class files, but the directory is named according to what you put in LOCAL_MODULE). This name will be what goes in the LOCAL_JAVA_LIBRARIES variable in modules that depend on your java library.

C/C++ Executables

Use the templates/executable file, or the templates/executable_host file.

This template has a couple extra options that you usually don't need. Please delete the ones you don't need, and remove the TODO comments. It makes the rest of them easier to read, and you can always refer back to the templates if you need them again later.

By default, on the target these are built into /system/bin, and on the host, they're built into /host/bin. These can be overridden by setting LOCAL_MODULE_PATH or LOCAL_MODULE_RELATIVE_PATH. See Putting targets elsewhere for more.

Shared Libraries

Use the templates/shared_library file, or the templates/shared_library_host file.

Remember that on the target, we use shared libraries, and on the host, we use static libraries, since executable size isn't as big an issue, and it simplifies distribution in the SDK.

Static Libraries

Use the templates/static_library file, or the templates/static_library_host file.

Remember that on the target, we use shared libraries, and on the host, we use static libraries, since executable size isn't as big an issue, and it simplifies distribution in the SDK.

Using Custom Tools

If you have a tool that generates source files for you, it's possible to have the build system get the dependencies correct for it. Here are a couple of examples. $@ is the make built-in variable for "the current target." The red parts are the parts you'll need to change.

You need to put this after you have declared LOCAL_PATH and LOCAL_MODULE, because the $(local-generated-sources-dir) and $(local-host-generated-sources-dir) macros use these variables to determine where to put the files.

Example 1

Here, there is one generated file, called chartables.c, which doesn't depend on anything. And is built by the tool built to $(HOST_OUT_EXECUTABLES)/dftables. Note on the second to last line that a dependency is created on the tool.

intermediates:= $(local-generated-sources-dir)
GEN := $(intermediates)/chartables.c
$(GEN): PRIVATE_CUSTOM_TOOL = $(HOST_OUT_EXECUTABLES)/dftables $@
$(GEN): $(HOST_OUT_EXECUTABLES)/dftables
	$(transform-generated-source)
LOCAL_GENERATED_SOURCES += $(GEN)
Example 2

Here as a hypothetical example, we use use cat as if it were to transform a file. Pretend that it does something useful. Note how we use a target-specific variable called PRIVATE_INPUT_FILE to store the name of the input file.

intermediates:= $(local-generated-sources-dir)
GEN := $(intermediates)/file.c
$(GEN): PRIVATE_INPUT_FILE := $(LOCAL_PATH)/input.file
$(GEN): PRIVATE_CUSTOM_TOOL = cat $(PRIVATE_INPUT_FILE) > $@
$(GEN): $(LOCAL_PATH)/input.file
	$(transform-generated-source)
LOCAL_GENERATED_SOURCES += $(GEN)
Example 3

If you have several files that are all similar in name, and use the same tool, you can combine them. (here the *.lut.h files are the generated ones, and the *.cpp files are the input files)

intermediates:= $(local-generated-sources-dir)
GEN := $(addprefix $(intermediates)/kjs/, \
            array_object.lut.h \
            bool_object.lut.h \
        )
$(GEN): PRIVATE_CUSTOM_TOOL = perl libs/WebKitLib/WebKit/JavaScriptCore/kjs/create_hash_table $< -i > $@
$(GEN): $(intermediates)/%.lut.h : $(LOCAL_PATH)/%.cpp
	$(transform-generated-source)
LOCAL_GENERATED_SOURCES += $(GEN)

Platform specific conditionals

Sometimes you need to set flags specifically for different platforms. Here is a list of which values the different build-system defined variables will be set to and some examples.

HOST_OS
linux
darwin
HOST_ARCH
x86
x86_64
HOST_BUILD_TYPE
release
debug
TARGET_ARCH
arm
arm64
mips
mips64
x86
x86_64
TARGET_BUILD_TYPE
release
debug

There are also special variables to use instead of conditionals. Many of the normal variables (LOCAL_SRC_FILES, LOCAL_CFLAGS, etc) can be conditionally added to with _{arch} _{32|64}, and for the host, _{os}.

Some Examples

ifeq ($(TARGET_BUILD_TYPE),release)
LOCAL_CFLAGS += -DNDEBUG=1
endif

LOCAL_CFLAGS_arm += -DTARGET_IS_ARM

LOCAL_CFLAGS_64 += -DBIG_POINTER

# from libutils
# Use the futex based mutex and condition variable
# implementation from android-arm because it's shared mem safe
LOCAL_SRC_FILES_linux += futex_synchro.c
LOCAL_LDLIBS_linux += -lrt -ldl

Putting modules elsewhere

If you have modules that normally go somewhere, and you need to have them build somewhere else, read this.

If you have modules that need to go in a subdirectory of their normal location, for example HAL modules that need to go in /system/lib/hw or /vendor/lib/hw, set LOCAL_MODULE_RELATIVE_PATH in your Android.mk, for example:

LOCAL_MODULE_RELATIVE_PATH := hw

If you have modules that need to go in an entirely different location, for example the root filesystem instead of in /system, add these lines to your Android.mk:

LOCAL_MODULE_PATH := $(TARGET_ROOT_OUT_SBIN)
LOCAL_UNSTRIPPED_PATH := $(TARGET_ROOT_OUT_SBIN_UNSTRIPPED)

For executables and libraries, you need to specify a LOCAL_UNSTRIPPED_PATH location if you specified a LOCAL_MODULE_PATH, because on target builds, we keep the unstripped executables so GDB can find the symbols. LOCAL_UNSTRIPPED_PATH is not necessary if you only specified LOCAL_MODULE_RELATIVE_PATH.

Look in core/envsetup.mk for all of the variables defining places to build things.

FYI: If you're installing an executable to /sbin, you probably also want to set LOCAL_FORCE_STATIC_EXCUTABLE := true in your Android.mk, which will force the linker to only accept static libraries.

Android.mk variables

These are the variables that you'll commonly see in Android.mk files, listed alphabetically.

But first, a note on variable naming:

LOCAL_ANNOTATION_PROCESSORS

Set this to a list of modules built with BUILD_HOST_JAVA_LIBRARY to have their jars passed to javac with -processorpath for use as annotation processors.

LOCAL_ANNOTATION_PROCESSOR_CLASSES

Set this to a list of classes to be passed to javac as -processor arguments. This list is would be unnecessary, as javac will autodetect annotation processor classes, except that the Grok tool that is used on the Android source code does not autodetect them and requires listing them manually.

LOCAL_ASSET_FILES

In Android.mk files that include $(BUILD_PACKAGE) set this to the set of files you want built into your app. Usually:

LOCAL_ASSET_FILES += $(call find-subdir-assets)

This will probably change when we switch to ant for the apps' build system.

LOCAL_CC

If you want to use a different C compiler for this module, set LOCAL_CC to the path to the compiler. If LOCAL_CC is blank, the appropriate default compiler is used.

LOCAL_CXX

If you want to use a different C++ compiler for this module, set LOCAL_CXX to the path to the compiler. If LOCAL_CXX is blank, the appropriate default compiler is used.

LOCAL_CFLAGS

If you have additional flags to pass into the C or C++ compiler, add them here. For example:

LOCAL_CFLAGS += -DLIBUTILS_NATIVE=1

LOCAL_CPPFLAGS

If you have additional flags to pass into only the C++ compiler, add them here. For example:

LOCAL_CPPFLAGS += -ffriend-injection

LOCAL_CPPFLAGS is guaranteed to be after LOCAL_CFLAGS on the compile line, so you can use it to override flags listed in LOCAL_CFLAGS.

LOCAL_CPP_EXTENSION

If your C++ files end in something other than ".cpp", you can specify the custom extension here. For example:

LOCAL_CPP_EXTENSION := .cc

Note that all C++ files for a given module must have the same extension; it is not currently possible to mix different extensions.

LOCAL_NO_DEFAULT_COMPILER_FLAGS

Normally, the compile line for C and C++ files includes global include paths and global cflags. If LOCAL_NO_DEFAULT_COMPILER_FLAGS is non-empty, none of the default includes or flags will be used when compiling C and C++ files in this module. LOCAL_C_INCLUDES, LOCAL_CFLAGS, and LOCAL_CPPFLAGS will still be used in this case, as will any DEBUG_CFLAGS that are defined for the module.

LOCAL_COPY_HEADERS

This will be going away.

The set of files to copy to the install include tree. You must also supply LOCAL_COPY_HEADERS_TO.

This is going away because copying headers messes up the error messages, and may lead to people editing those headers instead of the correct ones. It also makes it easier to do bad layering in the system, which we want to avoid. We also aren't doing a C/C++ SDK, so there is no ultimate requirement to copy any headers.

LOCAL_COPY_HEADERS_TO

This will be going away.

The directory within "include" to copy the headers listed in LOCAL_COPY_HEADERS to.

This is going away because copying headers messes up the error messages, and may lead to people editing those headers instead of the correct ones. It also makes it easier to do bad layering in the system, which we want to avoid. We also aren't doing a C/C++ SDK, so there is no ultimate requirement to copy any headers.

LOCAL_C_INCLUDES

Additional directories to instruct the C/C++ compilers to look for header files in. These paths are rooted at the top of the tree. Use LOCAL_PATH if you have subdirectories of your own that you want in the include paths. For example:

LOCAL_C_INCLUDES += extlibs/zlib-1.2.3
LOCAL_C_INCLUDES += $(LOCAL_PATH)/src

You should not add subdirectories of include to LOCAL_C_INCLUDES, instead you should reference those files in the #include statement with their subdirectories. For example:

#include <utils/KeyedVector.h>
not #include <KeyedVector.h>

There are some components that are doing this wrong, and should be cleaned up.

LOCAL_MODULE_TAGS

Set LOCAL_MODULE_TAGS to any number of whitespace-separated tags. If the tag list is empty or contains droid, the module will get installed as part of a make droid. Otherwise, it will only get installed by running make <your-module> or with the make all pseudotarget.

LOCAL_REQUIRED_MODULES

Set LOCAL_REQUIRED_MODULES to any number of whitespace-separated module names, like "libblah" or "Email". If this module is installed, all of the modules that it requires will be installed as well. This can be used to, e.g., ensure that necessary shared libraries or providers are installed when a given app is installed.

LOCAL_FORCE_STATIC_EXECUTABLE

If your executable should be linked statically, set LOCAL_FORCE_STATIC_EXECUTABLE:=true. There is a very short list of libraries that we have in static form (currently only libc). This is really only used for executables in /sbin on the root filesystem.

LOCAL_GENERATED_SOURCES

Files that you add to LOCAL_GENERATED_SOURCES will be automatically generated and then linked in when your module is built. See the Custom Tools template makefile for an example.

LOCAL_JAVACFLAGS

If you have additional flags to pass into the javac compiler, add them here. For example:

LOCAL_JAVACFLAGS += -Xlint:deprecation

LOCAL_ERROR_PRONE_FLAGS

If you have additional flags to pass into the error prone compiler, add them here. For example:

LOCAL_ERROR_PRONE_FLAGS += -Xep:ClassCanBeStatic:ERROR

LOCAL_JAVA_LIBRARIES

When linking Java apps and libraries, LOCAL_JAVA_LIBRARIES specifies which sets of java classes to include. Currently there are two of these: core and framework. In most cases, it will look like this:

LOCAL_JAVA_LIBRARIES := core framework

Note that setting LOCAL_JAVA_LIBRARIES is not necessary (and is not allowed) when building an APK with "include $(BUILD_PACKAGE)". The appropriate libraries will be included automatically.

LOCAL_LDFLAGS

You can pass additional flags to the linker by setting LOCAL_LDFLAGS. Keep in mind that the order of parameters is very important to ld, so test whatever you do on all platforms.

LOCAL_LDLIBS

LOCAL_LDLIBS allows you to specify additional libraries that are not part of the build for your executable or library. Specify the libraries you want in -lxxx format; they're passed directly to the link line. However, keep in mind that there will be no dependency generated for these libraries. It's most useful in simulator builds where you want to use a library preinstalled on the host. The linker (ld) is a particularly fussy beast, so it's sometimes necessary to pass other flags here if you're doing something sneaky. Some examples:

LOCAL_LDLIBS += -lcurses -lpthread
LOCAL_LDLIBS += -Wl,-z,origin

LOCAL_NO_MANIFEST

If your package doesn't have a manifest (AndroidManifest.xml), then set LOCAL_NO_MANIFEST:=true. The common resources package does this.

LOCAL_PACKAGE_NAME

LOCAL_PACKAGE_NAME is the name of an app. For example, Dialer, Contacts, etc. This will probably change or go away when we switch to an ant-based build system for the apps.

LOCAL_PATCH_MODULE (experimental option)

As of January 2018, you almost certainly don't need this option, so please ask and only use it if you understand what you're doing. This feature is experimental and may go away in future.

When compiling language level 9+ .java code in packages that are part of a a system module, LOCAL_PATCH_MODULE names the module that your sources and dependencies should be patched into. The Android runtime currently (Jan 2018) doesn't implement the JEP 261 module system so this option is only supported at compile time. It should only be needed to compile tests in packages that exist in libcore and which are inconvenient to move elsewhere.

LOCAL_PATH

The directory your Android.mk file is in. You can set it by putting the following as the first line in your Android.mk:

LOCAL_PATH := $(my-dir)

The my-dir macro uses the MAKEFILE_LIST variable, so you must call it before you include any other makefiles. Also, consider that any subdirectories you inlcude might reset LOCAL_PATH, so do your own stuff before you include them. This also means that if you try to write several include lines that reference LOCAL_PATH, it won't work, because those included makefiles might reset LOCAL_PATH.

LOCAL_POST_PROCESS_COMMAND

For host executables, you can specify a command to run on the module after it's been linked. You might have to go through some contortions to get variables right because of early or late variable evaluation:

module := $(HOST_OUT_EXECUTABLES)/$(LOCAL_MODULE)
LOCAL_POST_PROCESS_COMMAND := /Developer/Tools/Rez -d __DARWIN__ -t APPL\
       -d __WXMAC__ -o $(module) Carbon.r

LOCAL_PREBUILT_EXECUTABLES

When including $(BUILD_MULTI_PREBUILT) or $(BUILD_HOST_PREBUILT), set these to executables that you want copied. They're located automatically into the right bin directory.

LOCAL_PREBUILT_LIBS

When including $(BUILD_MULTI_PREBUILT) or $(BUILD_HOST_PREBUILT), set these to libraries that you want copied. They're located automatically into the right lib directory.

LOCAL_SHARED_LIBRARIES

These are the libraries you directly link against. You don't need to pass transitively included libraries. Specify the name without the suffix:

LOCAL_SHARED_LIBRARIES := \
    libutils \
    libui \
    libaudio \
    libexpat \
    libsgl

LOCAL_SRC_FILES

The build system looks at LOCAL_SRC_FILES to know what source files to compile -- .cpp .c .y .l .java. For lex and yacc files, it knows how to correctly do the intermediate .h and .c/.cpp files automatically. If the files are in a subdirectory of the one containing the Android.mk, prefix them with the directory name:

LOCAL_SRC_FILES := \
    file1.cpp \
    dir/file2.cpp

LOCAL_STATIC_LIBRARIES

These are the static libraries that you want to include in your module. Mostly, we use shared libraries, but there are a couple of places, like executables in sbin and host executables where we use static libraries instead.

LOCAL_STATIC_LIBRARIES := \
    libutils \
    libtinyxml

LOCAL_MODULE

LOCAL_MODULE is the name of what's supposed to be generated from your Android.mk. For exmample, for libkjs, the LOCAL_MODULE is "libkjs" (the build system adds the appropriate suffix -- .so .dylib .dll). For app modules, use LOCAL_PACKAGE_NAME instead of LOCAL_MODULE. We're planning on switching to ant for the apps, so this might become moot.

LOCAL_MODULE_PATH

Instructs the build system to put the module somewhere other than what's normal for its type. If you override this, make sure you also set LOCAL_UNSTRIPPED_PATH if it's an executable or a shared library so the unstripped binary has somewhere to go. An error will occur if you forget to.

See Putting modules elsewhere for more.

LOCAL_MODULE_RELATIVE_PATH

Instructs the build system to put the module in a subdirectory under the directory that is normal for its type. If you set this you do not need to set LOCAL_UNSTRIPPED_PATH, the unstripped binaries will also use the relative path.

See Putting modules elsewhere for more.

LOCAL_MODULE_HOST_OS

This specifies which OSes are supported by this host module. It is not used for target builds. The accepted values here are combinations of linux, darwin, and windows. By default, linux and darwin(MacOS) are considered to be supported. If a module should build under windows, you must specify windows, and any others to be supported. Some examples:

LOCAL_MODULE_HOST_OS := linux
LOCAL_MODULE_HOST_OS := darwin linux windows

LOCAL_UNSTRIPPED_PATH

Instructs the build system to put the unstripped version of the module somewhere other than what's normal for its type. Usually, you override this because you overrode LOCAL_MODULE_PATH for an executable or a shared library. If you overrode LOCAL_MODULE_PATH, but not LOCAL_UNSTRIPPED_PATH, an error will occur.

See Putting modules elsewhere for more.

LOCAL_WHOLE_STATIC_LIBRARIES

These are the static libraries that you want to include in your module without allowing the linker to remove dead code from them. This is mostly useful if you want to add a static library to a shared library and have the static library's content exposed from the shared library.

LOCAL_WHOLE_STATIC_LIBRARIES := \
    libsqlite3_android

LOCAL_YACCFLAGS

Any flags to pass to invocations of yacc for your module. A known limitation here is that the flags will be the same for all invocations of YACC for your module. This can be fixed. If you ever need it to be, just ask.

LOCAL_YACCFLAGS := -p kjsyy

Implementation Details

You should never have to touch anything in the config directory unless you're adding a new platform, new tools, or adding new features to the build system. In general, please consult with the build system owner(s) (android-build-team) before you go mucking around in here. That said, here are some notes on what's going on under the hood.

Environment Setup / buildspec.mk Versioning

In order to make easier for people when the build system changes, when it is necessary to make changes to buildspec.mk or to rerun the environment setup scripts, they contain a version number in the variable BUILD_ENV_SEQUENCE_NUMBER. If this variable does not match what the build system expects, it fails printing an error message explaining what happened. If you make a change that requires an update, you need to update two places so this message will be printed.

The scripts automatically get the value from the build system, so they will trigger the warning as well.

Additional makefile variables

You probably shouldn't use these variables. Please consult android-build-team before using them. These are mostly there for workarounds for other issues, or things that aren't completely done right.

LOCAL_ADDITIONAL_DEPENDENCIES

If your module needs to depend on anything else that isn't actually built in to it, you can add those make targets to LOCAL_ADDITIONAL_DEPENDENCIES. Usually this is a workaround for some other dependency that isn't created automatically.

LOCAL_BUILT_MODULE

This should not be used, since multiple binaries are now created from a single module defintiion.

When a module is built, the module is created in an intermediate directory then copied to its final location. LOCAL_BUILT_MODULE is the full path to the intermediate file. See LOCAL_INSTALLED_MODULE for the path to the final installed location of the module.

LOCAL_IS_HOST_MODULE

Set by the host_xxx.mk includes to tell base_rules.mk and the other includes that we're building for the host.

LOCAL_INSTALLED_MODULE

This should not be used, since multiple binaries are now created from a single module defintiion.

The fully qualified path name of the final location of the module. See LOCAL_BUILT_MODULE for the location of the intermediate file that the make rules should actually be constructing.

LOCAL_MODULE_CLASS

Which kind of module this is. This variable is used to construct other variable names used to locate the modules. See base_rules.mk and envsetup.mk.

LOCAL_MODULE_SUFFIX

The suffix that will be appended to LOCAL_MODULE to form LOCAL_MODULE_NAME. For example, .so, .a, .dylib.

LOCAL_STRIP_MODULE

If set to true (the default), the binary will be stripped and a debug link will be set up so that GDB will still work. If set to no_debuglink, the binary will be stripped, but no debug link will be added. If set to keep_symbols, it will strip the debug information, but keep the symbol table. Any other value will prevent stripping.

LOCAL_SYSTEM_SHARED_LIBRARIES

Used while building the base libraries: libc, libm, libdl. Usually it should be set to "none," as it is in $(CLEAR_VARS). When building these libraries, it's set to the ones they link against. For example, libc, libstdc++ and libdl don't link against anything, and libm links against libc. Normally, when the value is none, these libraries are automatically linked in to executables and libraries, so you don't need to specify them manually.