# dexpreopt_odex_install.mk is used to define odex creation rules for JARs and APKs # This file depends on variables set in base_rules.mk # Output variables: LOCAL_DEX_PREOPT, LOCAL_UNCOMPRESS_DEX, built_odex, # dexpreopt_boot_jar_module ifeq (true,$(LOCAL_PREFER_CODE_INTEGRITY)) LOCAL_UNCOMPRESS_DEX := true else LOCAL_UNCOMPRESS_DEX := endif # We explicitly uncompress APKs of privileged apps, and used by # privileged apps ifneq (true,$(DONT_UNCOMPRESS_PRIV_APPS_DEXS)) ifeq (true,$(LOCAL_PRIVILEGED_MODULE)) LOCAL_UNCOMPRESS_DEX := true endif ifneq (,$(filter $(PRODUCT_LOADED_BY_PRIVILEGED_MODULES), $(LOCAL_MODULE))) LOCAL_UNCOMPRESS_DEX := true endif endif # DONT_UNCOMPRESS_PRIV_APPS_DEXS # Setting LOCAL_DEX_PREOPT based on WITH_DEXPREOPT, LOCAL_DEX_PREOPT, etc LOCAL_DEX_PREOPT := $(strip $(LOCAL_DEX_PREOPT)) ifndef LOCAL_DEX_PREOPT # LOCAL_DEX_PREOPT undefined LOCAL_DEX_PREOPT := $(DEX_PREOPT_DEFAULT) endif ifeq (false,$(LOCAL_DEX_PREOPT)) LOCAL_DEX_PREOPT := endif # Only enable preopt for non tests. ifneq (,$(filter $(LOCAL_MODULE_TAGS),tests)) LOCAL_DEX_PREOPT := endif # If we have product-specific config for this module? ifneq (,$(filter $(LOCAL_MODULE),$(DEXPREOPT_DISABLED_MODULES))) LOCAL_DEX_PREOPT := endif # Disable preopt for TARGET_BUILD_APPS ifneq (,$(TARGET_BUILD_APPS)) LOCAL_DEX_PREOPT := endif # Disable preopt if not WITH_DEXPREOPT ifneq (true,$(WITH_DEXPREOPT)) LOCAL_DEX_PREOPT := endif ifdef LOCAL_UNINSTALLABLE_MODULE LOCAL_DEX_PREOPT := endif ifeq (,$(strip $(built_dex)$(my_prebuilt_src_file)$(LOCAL_SOONG_DEX_JAR))) # contains no java code LOCAL_DEX_PREOPT := endif # if WITH_DEXPREOPT_BOOT_IMG_AND_SYSTEM_SERVER_ONLY=true and module is not in boot class path skip # Also preopt system server jars since selinux prevents system server from loading anything from # /data. If we don't do this they will need to be extracted which is not favorable for RAM usage # or performance. If my_preopt_for_extracted_apk is true, we ignore the only preopt boot image # options. ifneq (true,$(my_preopt_for_extracted_apk)) ifeq (true,$(WITH_DEXPREOPT_BOOT_IMG_AND_SYSTEM_SERVER_ONLY)) ifeq ($(filter $(PRODUCT_SYSTEM_SERVER_JARS) $(DEXPREOPT_BOOT_JARS_MODULES),$(LOCAL_MODULE)),) LOCAL_DEX_PREOPT := endif endif endif my_process_profile := my_profile_is_text_listing := ifeq (false,$(WITH_DEX_PREOPT_GENERATE_PROFILE)) LOCAL_DEX_PREOPT_GENERATE_PROFILE := false endif ifndef LOCAL_DEX_PREOPT_GENERATE_PROFILE # If LOCAL_DEX_PREOPT_GENERATE_PROFILE is not defined, default it based on the existence of the # profile class listing. TODO: Use product specific directory here. my_classes_directory := $(PRODUCT_DEX_PREOPT_PROFILE_DIR) LOCAL_DEX_PREOPT_PROFILE := $(my_classes_directory)/$(LOCAL_MODULE).prof ifneq (,$(wildcard $(LOCAL_DEX_PREOPT_PROFILE))) my_process_profile := true my_profile_is_text_listing := endif else my_process_profile := $(LOCAL_DEX_PREOPT_GENERATE_PROFILE) my_profile_is_text_listing := true LOCAL_DEX_PREOPT_PROFILE := $(LOCAL_DEX_PREOPT_PROFILE_CLASS_LISTING) endif ifeq (true,$(my_process_profile)) ifndef LOCAL_DEX_PREOPT_PROFILE $(call pretty-error,Must have specified class listing (LOCAL_DEX_PREOPT_PROFILE)) endif ifeq (,$(dex_preopt_profile_src_file)) $(call pretty-error, Internal error: dex_preopt_profile_src_file must be set) endif endif # If LOCAL_ENFORCE_USES_LIBRARIES is not set, default to true if either of LOCAL_USES_LIBRARIES or # LOCAL_OPTIONAL_USES_LIBRARIES are specified. ifeq (,$(LOCAL_ENFORCE_USES_LIBRARIES)) # Will change the default to true unconditionally in the future. ifneq (,$(LOCAL_OPTIONAL_USES_LIBRARIES)) LOCAL_ENFORCE_USES_LIBRARIES := true endif ifneq (,$(LOCAL_USES_LIBRARIES)) LOCAL_ENFORCE_USES_LIBRARIES := true endif endif my_dexpreopt_archs := ifdef LOCAL_DEX_PREOPT ifeq ($(LOCAL_MODULE_CLASS),JAVA_LIBRARIES) my_module_multilib := $(LOCAL_MULTILIB) # If the module is not an SDK library and it's a system server jar, only preopt the primary arch. my_filtered_lib_name := $(patsubst %.impl,%,$(LOCAL_MODULE)) ifeq (,$(filter $(JAVA_SDK_LIBRARIES),$(my_filtered_lib_name))) # For a Java library, by default we build odex for both 1st arch and 2nd arch. # But it can be overridden with "LOCAL_MULTILIB := first". ifneq (,$(filter $(PRODUCT_SYSTEM_SERVER_JARS),$(LOCAL_MODULE))) # For system server jars, we build for only "first". my_module_multilib := first endif endif # Only preopt primary arch for translated arch since there is only an image there. ifeq ($(TARGET_TRANSLATE_2ND_ARCH),true) my_module_multilib := first endif # ################################################# # Odex for the 1st arch my_dexpreopt_archs += $(TARGET_ARCH) # Odex for the 2nd arch ifdef TARGET_2ND_ARCH ifneq ($(TARGET_TRANSLATE_2ND_ARCH),true) ifneq (first,$(my_module_multilib)) my_dexpreopt_archs += $(TARGET_2ND_ARCH) endif # my_module_multilib is not first. endif # TARGET_TRANSLATE_2ND_ARCH not true endif # TARGET_2ND_ARCH # ################################################# else # must be APPS # The preferred arch # Save the module multilib since setup_one_odex modifies it. my_2nd_arch_prefix := $(LOCAL_2ND_ARCH_VAR_PREFIX) my_dexpreopt_archs += $(TARGET_$(my_2nd_arch_prefix)ARCH) ifdef TARGET_2ND_ARCH ifeq ($(my_module_multilib),both) # The non-preferred arch my_2nd_arch_prefix := $(if $(LOCAL_2ND_ARCH_VAR_PREFIX),,$(TARGET_2ND_ARCH_VAR_PREFIX)) my_dexpreopt_archs += $(TARGET_$(my_2nd_arch_prefix)ARCH) endif # LOCAL_MULTILIB is both endif # TARGET_2ND_ARCH endif # LOCAL_MODULE_CLASS # Record dex-preopt config. DEXPREOPT.$(LOCAL_MODULE).DEX_PREOPT := $(LOCAL_DEX_PREOPT) DEXPREOPT.$(LOCAL_MODULE).MULTILIB := $(LOCAL_MULTILIB) DEXPREOPT.$(LOCAL_MODULE).DEX_PREOPT_FLAGS := $(LOCAL_DEX_PREOPT_FLAGS) DEXPREOPT.$(LOCAL_MODULE).PRIVILEGED_MODULE := $(LOCAL_PRIVILEGED_MODULE) DEXPREOPT.$(LOCAL_MODULE).VENDOR_MODULE := $(LOCAL_VENDOR_MODULE) DEXPREOPT.$(LOCAL_MODULE).TARGET_ARCH := $(LOCAL_MODULE_TARGET_ARCH) DEXPREOPT.$(LOCAL_MODULE).INSTALLED_STRIPPED := $(LOCAL_INSTALLED_MODULE) DEXPREOPT.MODULES.$(LOCAL_MODULE_CLASS) := $(sort \ $(DEXPREOPT.MODULES.$(LOCAL_MODULE_CLASS)) $(LOCAL_MODULE)) $(call json_start) $(call add_json_str, Name, $(LOCAL_MODULE)) $(call add_json_str, DexLocation, $(patsubst $(PRODUCT_OUT)%,%,$(LOCAL_INSTALLED_MODULE))) $(call add_json_str, BuildPath, $(LOCAL_BUILT_MODULE)) $(call add_json_str, DexPath, $$1) $(call add_json_str, ExtrasOutputPath, $$2) $(call add_json_bool, PreferCodeIntegrity, $(filter true,$(LOCAL_PREFER_CODE_INTEGRITY))) $(call add_json_bool, Privileged, $(filter true,$(LOCAL_PRIVILEGED_MODULE))) $(call add_json_bool, UncompressedDex, $(filter true,$(LOCAL_UNCOMPRESS_DEX))) $(call add_json_bool, HasApkLibraries, $(LOCAL_APK_LIBRARIES)) $(call add_json_list, PreoptFlags, $(LOCAL_DEX_PREOPT_FLAGS)) $(call add_json_str, ProfileClassListing, $(if $(my_process_profile),$(LOCAL_DEX_PREOPT_PROFILE))) $(call add_json_bool, ProfileIsTextListing, $(my_profile_is_text_listing)) $(call add_json_bool, EnforceUsesLibraries, $(LOCAL_ENFORCE_USES_LIBRARIES)) $(call add_json_list, OptionalUsesLibraries, $(LOCAL_OPTIONAL_USES_LIBRARIES)) $(call add_json_list, UsesLibraries, $(LOCAL_USES_LIBRARIES)) $(call add_json_map, LibraryPaths) $(foreach lib,$(sort $(LOCAL_USES_LIBRARIES) $(LOCAL_OPTIONAL_USES_LIBRARIES) org.apache.http.legacy.impl android.hidl.base-V1.0-java android.hidl.manager-V1.0-java),\ $(call add_json_str, $(lib), $(call intermediates-dir-for,JAVA_LIBRARIES,$(lib),,COMMON)/javalib.jar)) $(call end_json_map) $(call add_json_list, Archs, $(my_dexpreopt_archs)) $(call add_json_str, DexPreoptImageLocation, $(LOCAL_DEX_PREOPT_IMAGE_LOCATION)) $(call add_json_bool, PreoptExtractedApk, $(my_preopt_for_extracted_apk)) $(call add_json_bool, NoCreateAppImage, $(filter false,$(LOCAL_DEX_PREOPT_APP_IMAGE))) $(call add_json_bool, ForceCreateAppImage, $(filter true,$(LOCAL_DEX_PREOPT_APP_IMAGE))) $(call add_json_bool, PresignedPrebuilt, $(filter PRESIGNED,$(LOCAL_CERTIFICATE))) $(call add_json_str, StripInputPath, $$1) $(call add_json_str, StripOutputPath, $$2) $(call json_end) my_dexpreopt_config := $(intermediates)/dexpreopt.config my_dexpreopt_script := $(intermediates)/dexpreopt.sh my_strip_script := $(intermediates)/strip.sh my_dexpreopt_zip := $(intermediates)/dexpreopt.zip $(my_dexpreopt_config): PRIVATE_MODULE := $(LOCAL_MODULE) $(my_dexpreopt_config): PRIVATE_CONTENTS := $(json_contents) $(my_dexpreopt_config): @echo "$(PRIVATE_MODULE) dexpreopt.config" echo -e -n '$(subst $(newline),\n,$(subst ','\'',$(subst \,\\,$(PRIVATE_CONTENTS))))' > $@ .KATI_RESTAT: $(my_dexpreopt_script) $(my_strip_script) $(my_dexpreopt_script): PRIVATE_MODULE := $(LOCAL_MODULE) $(my_dexpreopt_script): PRIVATE_GLOBAL_CONFIG := $(PRODUCT_OUT)/dexpreopt.config $(my_dexpreopt_script): PRIVATE_MODULE_CONFIG := $(my_dexpreopt_config) $(my_dexpreopt_script): PRIVATE_STRIP_SCRIPT := $(my_strip_script) $(my_dexpreopt_script): .KATI_IMPLICIT_OUTPUTS := $(my_strip_script) $(my_dexpreopt_script): $(DEXPREOPT_GEN) $(my_dexpreopt_script): $(my_dexpreopt_config) $(PRODUCT_OUT)/dexpreopt.config @echo "$(PRIVATE_MODULE) dexpreopt gen" $(DEXPREOPT_GEN) -global $(PRIVATE_GLOBAL_CONFIG) -module $(PRIVATE_MODULE_CONFIG) \ -dexpreopt_script $@ -strip_script $(PRIVATE_STRIP_SCRIPT) my_dexpreopt_deps := $(my_dex_jar) my_dexpreopt_deps += $(if $(my_process_profile),$(LOCAL_DEX_PREOPT_PROFILE)) my_dexpreopt_deps += \ $(foreach lib,$(sort $(LOCAL_USES_LIBRARIES) $(LOCAL_OPTIONAL_USES_LIBRARIES) org.apache.http.legacy.impl android.hidl.base-V1.0-java android.hidl.manager-V1.0-java),\ $(call intermediates-dir-for,JAVA_LIBRARIES,$(lib),,COMMON)/javalib.jar) my_dexpreopt_deps += $(LOCAL_DEX_PREOPT_IMAGE_LOCATION) # TODO: default boot images $(my_dexpreopt_zip): PRIVATE_MODULE := $(LOCAL_MODULE) $(my_dexpreopt_zip): $(my_dexpreopt_deps) $(my_dexpreopt_zip): | $(DEXPREOPT_GEN_DEPS) $(my_dexpreopt_zip): .KATI_DEPFILE := $(my_dexpreopt_zip).d $(my_dexpreopt_zip): PRIVATE_DEX := $(my_dex_jar) $(my_dexpreopt_zip): PRIVATE_SCRIPT := $(my_dexpreopt_script) $(my_dexpreopt_zip): $(my_dexpreopt_script) @echo "$(PRIVATE_MODULE) dexpreopt" bash $(PRIVATE_SCRIPT) $(PRIVATE_DEX) $@ ifdef LOCAL_POST_INSTALL_CMD # Add a shell command separator LOCAL_POST_INSTALL_CMD += && endif LOCAL_POST_INSTALL_CMD += \ for i in $$(zipinfo -1 $(my_dexpreopt_zip)); \ do mkdir -p $(PRODUCT_OUT)/$$(dirname $$i); \ done && \ ( unzip -qo -d $(PRODUCT_OUT) $(my_dexpreopt_zip) 2>&1 | grep -v "zipfile is empty"; exit $${PIPESTATUS[0]} ) || \ ( code=$$?; if [ $$code -ne 0 -a $$code -ne 1 ]; then exit $$code; fi ) $(LOCAL_INSTALLED_MODULE): PRIVATE_POST_INSTALL_CMD := $(LOCAL_POST_INSTALL_CMD) $(LOCAL_INSTALLED_MODULE): $(my_dexpreopt_zip) $(my_all_targets): $(my_dexpreopt_zip) my_dexpreopt_config := my_dexpreopt_script := my_strip_script := my_dexpreopt_zip := endif # LOCAL_DEX_PREOPT