#!/bin/sh # This is the command running inside the xterm of our # debug wrapper. It needs to take care of starting # the server command, so it can attach to the parent # process. In addition, here we run the command inside # of a gdb session to allow for debugging. # On some systems, running xterm will cause LD_LIBRARY_PATH # to be cleared, so restore it and PATH to be safe. export PATH=$PREV_PATH export LD_LIBRARY_PATH=$PREV_LD_LIBRARY_PATH # Start binderproc (or whatever sub-command is being run) # inside of gdb, giving gdb an initial command script to # automatically run the process without user intervention. gdb -q -x $2/process_wrapper_gdb.cmds --args "$@"