/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#define LOG_TAG "StreamInHAL"
//#define LOG_NDEBUG 0
#define ATRACE_TAG ATRACE_TAG_AUDIO
#include <android/log.h>
#include <hardware/audio.h>
#include <utils/Trace.h>
#include <memory>
#include "StreamIn.h"
#include "Util.h"
using ::android::hardware::audio::V2_0::MessageQueueFlagBits;
namespace android {
namespace hardware {
namespace audio {
namespace V2_0 {
namespace implementation {
using ::android::hardware::audio::common::V2_0::ThreadInfo;
namespace {
class ReadThread : public Thread {
public:
// ReadThread's lifespan never exceeds StreamIn's lifespan.
ReadThread(std::atomic<bool>* stop, audio_stream_in_t* stream,
StreamIn::CommandMQ* commandMQ, StreamIn::DataMQ* dataMQ,
StreamIn::StatusMQ* statusMQ, EventFlag* efGroup)
: Thread(false /*canCallJava*/),
mStop(stop),
mStream(stream),
mCommandMQ(commandMQ),
mDataMQ(dataMQ),
mStatusMQ(statusMQ),
mEfGroup(efGroup),
mBuffer(nullptr) {}
bool init() {
mBuffer.reset(new (std::nothrow) uint8_t[mDataMQ->getQuantumCount()]);
return mBuffer != nullptr;
}
virtual ~ReadThread() {}
private:
std::atomic<bool>* mStop;
audio_stream_in_t* mStream;
StreamIn::CommandMQ* mCommandMQ;
StreamIn::DataMQ* mDataMQ;
StreamIn::StatusMQ* mStatusMQ;
EventFlag* mEfGroup;
std::unique_ptr<uint8_t[]> mBuffer;
IStreamIn::ReadParameters mParameters;
IStreamIn::ReadStatus mStatus;
bool threadLoop() override;
void doGetCapturePosition();
void doRead();
};
void ReadThread::doRead() {
size_t availableToWrite = mDataMQ->availableToWrite();
size_t requestedToRead = mParameters.params.read;
if (requestedToRead > availableToWrite) {
ALOGW(
"truncating read data from %d to %d due to insufficient data queue "
"space",
(int32_t)requestedToRead, (int32_t)availableToWrite);
requestedToRead = availableToWrite;
}
ssize_t readResult = mStream->read(mStream, &mBuffer[0], requestedToRead);
mStatus.retval = Result::OK;
if (readResult >= 0) {
mStatus.reply.read = readResult;
if (!mDataMQ->write(&mBuffer[0], readResult)) {
ALOGW("data message queue write failed");
}
} else {
mStatus.retval = Stream::analyzeStatus("read", readResult);
}
}
void ReadThread::doGetCapturePosition() {
mStatus.retval = StreamIn::getCapturePositionImpl(
mStream, &mStatus.reply.capturePosition.frames,
&mStatus.reply.capturePosition.time);
}
bool ReadThread::threadLoop() {
// This implementation doesn't return control back to the Thread until it
// decides to stop,
// as the Thread uses mutexes, and this can lead to priority inversion.
while (!std::atomic_load_explicit(mStop, std::memory_order_acquire)) {
uint32_t efState = 0;
mEfGroup->wait(static_cast<uint32_t>(MessageQueueFlagBits::NOT_FULL),
&efState);
if (!(efState &
static_cast<uint32_t>(MessageQueueFlagBits::NOT_FULL))) {
continue; // Nothing to do.
}
if (!mCommandMQ->read(&mParameters)) {
continue; // Nothing to do.
}
mStatus.replyTo = mParameters.command;
switch (mParameters.command) {
case IStreamIn::ReadCommand::READ:
doRead();
break;
case IStreamIn::ReadCommand::GET_CAPTURE_POSITION:
doGetCapturePosition();
break;
default:
ALOGE("Unknown read thread command code %d",
mParameters.command);
mStatus.retval = Result::NOT_SUPPORTED;
break;
}
if (!mStatusMQ->write(&mStatus)) {
ALOGW("status message queue write failed");
}
mEfGroup->wake(static_cast<uint32_t>(MessageQueueFlagBits::NOT_EMPTY));
}
return false;
}
} // namespace
StreamIn::StreamIn(const sp<Device>& device, audio_stream_in_t* stream)
: mIsClosed(false),
mDevice(device),
mStream(stream),
mStreamCommon(new Stream(&stream->common)),
mStreamMmap(new StreamMmap<audio_stream_in_t>(stream)),
mEfGroup(nullptr),
mStopReadThread(false) {}
StreamIn::~StreamIn() {
ATRACE_CALL();
close();
if (mReadThread.get()) {
ATRACE_NAME("mReadThread->join");
status_t status = mReadThread->join();
ALOGE_IF(status, "read thread exit error: %s", strerror(-status));
}
if (mEfGroup) {
status_t status = EventFlag::deleteEventFlag(&mEfGroup);
ALOGE_IF(status, "read MQ event flag deletion error: %s",
strerror(-status));
}
mDevice->closeInputStream(mStream);
mStream = nullptr;
}
// Methods from ::android::hardware::audio::V2_0::IStream follow.
Return<uint64_t> StreamIn::getFrameSize() {
return audio_stream_in_frame_size(mStream);
}
Return<uint64_t> StreamIn::getFrameCount() {
return mStreamCommon->getFrameCount();
}
Return<uint64_t> StreamIn::getBufferSize() {
return mStreamCommon->getBufferSize();
}
Return<uint32_t> StreamIn::getSampleRate() {
return mStreamCommon->getSampleRate();
}
Return<void> StreamIn::getSupportedSampleRates(
getSupportedSampleRates_cb _hidl_cb) {
return mStreamCommon->getSupportedSampleRates(_hidl_cb);
}
Return<Result> StreamIn::setSampleRate(uint32_t sampleRateHz) {
return mStreamCommon->setSampleRate(sampleRateHz);
}
Return<AudioChannelMask> StreamIn::getChannelMask() {
return mStreamCommon->getChannelMask();
}
Return<void> StreamIn::getSupportedChannelMasks(
getSupportedChannelMasks_cb _hidl_cb) {
return mStreamCommon->getSupportedChannelMasks(_hidl_cb);
}
Return<Result> StreamIn::setChannelMask(AudioChannelMask mask) {
return mStreamCommon->setChannelMask(mask);
}
Return<AudioFormat> StreamIn::getFormat() {
return mStreamCommon->getFormat();
}
Return<void> StreamIn::getSupportedFormats(getSupportedFormats_cb _hidl_cb) {
return mStreamCommon->getSupportedFormats(_hidl_cb);
}
Return<Result> StreamIn::setFormat(AudioFormat format) {
return mStreamCommon->setFormat(format);
}
Return<void> StreamIn::getAudioProperties(getAudioProperties_cb _hidl_cb) {
return mStreamCommon->getAudioProperties(_hidl_cb);
}
Return<Result> StreamIn::addEffect(uint64_t effectId) {
return mStreamCommon->addEffect(effectId);
}
Return<Result> StreamIn::removeEffect(uint64_t effectId) {
return mStreamCommon->removeEffect(effectId);
}
Return<Result> StreamIn::standby() {
return mStreamCommon->standby();
}
Return<AudioDevice> StreamIn::getDevice() {
return mStreamCommon->getDevice();
}
Return<Result> StreamIn::setDevice(const DeviceAddress& address) {
return mStreamCommon->setDevice(address);
}
Return<Result> StreamIn::setConnectedState(const DeviceAddress& address,
bool connected) {
return mStreamCommon->setConnectedState(address, connected);
}
Return<Result> StreamIn::setHwAvSync(uint32_t hwAvSync) {
return mStreamCommon->setHwAvSync(hwAvSync);
}
Return<void> StreamIn::getParameters(const hidl_vec<hidl_string>& keys,
getParameters_cb _hidl_cb) {
return mStreamCommon->getParameters(keys, _hidl_cb);
}
Return<Result> StreamIn::setParameters(
const hidl_vec<ParameterValue>& parameters) {
return mStreamCommon->setParameters(parameters);
}
Return<void> StreamIn::debugDump(const hidl_handle& fd) {
return mStreamCommon->debugDump(fd);
}
Return<Result> StreamIn::start() {
return mStreamMmap->start();
}
Return<Result> StreamIn::stop() {
return mStreamMmap->stop();
}
Return<void> StreamIn::createMmapBuffer(int32_t minSizeFrames,
createMmapBuffer_cb _hidl_cb) {
return mStreamMmap->createMmapBuffer(
minSizeFrames, audio_stream_in_frame_size(mStream), _hidl_cb);
}
Return<void> StreamIn::getMmapPosition(getMmapPosition_cb _hidl_cb) {
return mStreamMmap->getMmapPosition(_hidl_cb);
}
Return<Result> StreamIn::close() {
if (mIsClosed) return Result::INVALID_STATE;
mIsClosed = true;
if (mReadThread.get()) {
mStopReadThread.store(true, std::memory_order_release);
}
if (mEfGroup) {
mEfGroup->wake(static_cast<uint32_t>(MessageQueueFlagBits::NOT_FULL));
}
return Result::OK;
}
// Methods from ::android::hardware::audio::V2_0::IStreamIn follow.
Return<void> StreamIn::getAudioSource(getAudioSource_cb _hidl_cb) {
int halSource;
Result retval =
mStreamCommon->getParam(AudioParameter::keyInputSource, &halSource);
AudioSource source(AudioSource::DEFAULT);
if (retval == Result::OK) {
source = AudioSource(halSource);
}
_hidl_cb(retval, source);
return Void();
}
Return<Result> StreamIn::setGain(float gain) {
if (!isGainNormalized(gain)) {
ALOGW("Can not set a stream input gain (%f) outside [0,1]", gain);
return Result::INVALID_ARGUMENTS;
}
return Stream::analyzeStatus("set_gain", mStream->set_gain(mStream, gain));
}
Return<void> StreamIn::prepareForReading(uint32_t frameSize,
uint32_t framesCount,
prepareForReading_cb _hidl_cb) {
status_t status;
ThreadInfo threadInfo = {0, 0};
// Wrap the _hidl_cb to return an error
auto sendError = [&threadInfo, &_hidl_cb](Result result) {
_hidl_cb(result, CommandMQ::Descriptor(), DataMQ::Descriptor(),
StatusMQ::Descriptor(), threadInfo);
};
// Create message queues.
if (mDataMQ) {
ALOGE("the client attempts to call prepareForReading twice");
sendError(Result::INVALID_STATE);
return Void();
}
std::unique_ptr<CommandMQ> tempCommandMQ(new CommandMQ(1));
// Check frameSize and framesCount
if (frameSize == 0 || framesCount == 0) {
ALOGE("Null frameSize (%u) or framesCount (%u)", frameSize,
framesCount);
sendError(Result::INVALID_ARGUMENTS);
return Void();
}
if (frameSize > Stream::MAX_BUFFER_SIZE / framesCount) {
ALOGE("Buffer too big: %u*%u bytes > MAX_BUFFER_SIZE (%u)", frameSize, framesCount,
Stream::MAX_BUFFER_SIZE);
sendError(Result::INVALID_ARGUMENTS);
return Void();
}
std::unique_ptr<DataMQ> tempDataMQ(
new DataMQ(frameSize * framesCount, true /* EventFlag */));
std::unique_ptr<StatusMQ> tempStatusMQ(new StatusMQ(1));
if (!tempCommandMQ->isValid() || !tempDataMQ->isValid() ||
!tempStatusMQ->isValid()) {
ALOGE_IF(!tempCommandMQ->isValid(), "command MQ is invalid");
ALOGE_IF(!tempDataMQ->isValid(), "data MQ is invalid");
ALOGE_IF(!tempStatusMQ->isValid(), "status MQ is invalid");
sendError(Result::INVALID_ARGUMENTS);
return Void();
}
EventFlag* tempRawEfGroup{};
status = EventFlag::createEventFlag(tempDataMQ->getEventFlagWord(),
&tempRawEfGroup);
std::unique_ptr<EventFlag, void (*)(EventFlag*)> tempElfGroup(
tempRawEfGroup, [](auto* ef) { EventFlag::deleteEventFlag(&ef); });
if (status != OK || !tempElfGroup) {
ALOGE("failed creating event flag for data MQ: %s", strerror(-status));
sendError(Result::INVALID_ARGUMENTS);
return Void();
}
// Create and launch the thread.
auto tempReadThread = std::make_unique<ReadThread>(
&mStopReadThread, mStream, tempCommandMQ.get(), tempDataMQ.get(),
tempStatusMQ.get(), tempElfGroup.get());
if (!tempReadThread->init()) {
ALOGW("failed to start reader thread: %s", strerror(-status));
sendError(Result::INVALID_ARGUMENTS);
return Void();
}
status = tempReadThread->run("reader", PRIORITY_URGENT_AUDIO);
if (status != OK) {
ALOGW("failed to start reader thread: %s", strerror(-status));
sendError(Result::INVALID_ARGUMENTS);
return Void();
}
mCommandMQ = std::move(tempCommandMQ);
mDataMQ = std::move(tempDataMQ);
mStatusMQ = std::move(tempStatusMQ);
mReadThread = tempReadThread.release();
mEfGroup = tempElfGroup.release();
threadInfo.pid = getpid();
threadInfo.tid = mReadThread->getTid();
_hidl_cb(Result::OK, *mCommandMQ->getDesc(), *mDataMQ->getDesc(),
*mStatusMQ->getDesc(), threadInfo);
return Void();
}
Return<uint32_t> StreamIn::getInputFramesLost() {
return mStream->get_input_frames_lost(mStream);
}
// static
Result StreamIn::getCapturePositionImpl(audio_stream_in_t* stream,
uint64_t* frames, uint64_t* time) {
// HAL may have a stub function, always returning ENOSYS, don't
// spam the log in this case.
static const std::vector<int> ignoredErrors{ENOSYS};
Result retval(Result::NOT_SUPPORTED);
if (stream->get_capture_position != NULL) return retval;
int64_t halFrames, halTime;
retval = Stream::analyzeStatus("get_capture_position",
stream->get_capture_position(stream, &halFrames, &halTime),
ignoredErrors);
if (retval == Result::OK) {
*frames = halFrames;
*time = halTime;
}
return retval;
};
Return<void> StreamIn::getCapturePosition(getCapturePosition_cb _hidl_cb) {
uint64_t frames = 0, time = 0;
Result retval = getCapturePositionImpl(mStream, &frames, &time);
_hidl_cb(retval, frames, time);
return Void();
}
} // namespace implementation
} // namespace V2_0
} // namespace audio
} // namespace hardware
} // namespace android