/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include <common/all-versions/IncludeGuard.h>
#include <core/all-versions/default/Conversions.h>
#include <system/audio.h>
namespace android {
namespace hardware {
namespace audio {
namespace AUDIO_HAL_VERSION {
namespace implementation {
/** Converts a status_t in Result according to the rules of AudioParameter::get*
* Note: Static method and not private method to avoid leaking status_t dependency
*/
static Result getHalStatusToResult(status_t status) {
switch (status) {
case OK:
return Result::OK;
case BAD_VALUE: // Nothing was returned, probably because the HAL does
// not handle it
return Result::NOT_SUPPORTED;
case INVALID_OPERATION: // Conversion from string to the requested type
// failed
return Result::INVALID_ARGUMENTS;
default: // Should not happen
ALOGW("Unexpected status returned by getParam: %u", status);
return Result::INVALID_ARGUMENTS;
}
}
Result ParametersUtil::getParam(const char* name, bool* value) {
String8 halValue;
Result retval = getParam(name, &halValue);
*value = false;
if (retval == Result::OK) {
if (halValue.empty()) {
return Result::NOT_SUPPORTED;
}
*value = !(halValue == AudioParameter::valueOff);
}
return retval;
}
Result ParametersUtil::getParam(const char* name, int* value) {
const String8 halName(name);
AudioParameter keys;
keys.addKey(halName);
std::unique_ptr<AudioParameter> params = getParams(keys);
return getHalStatusToResult(params->getInt(halName, *value));
}
Result ParametersUtil::getParam(const char* name, String8* value, AudioParameter context) {
const String8 halName(name);
context.addKey(halName);
std::unique_ptr<AudioParameter> params = getParams(context);
return getHalStatusToResult(params->get(halName, *value));
}
void ParametersUtil::getParametersImpl(
const hidl_vec<ParameterValue>& context, const hidl_vec<hidl_string>& keys,
std::function<void(Result retval, const hidl_vec<ParameterValue>& parameters)> cb) {
AudioParameter halKeys;
for (auto& pair : context) {
halKeys.add(String8(pair.key.c_str()), String8(pair.value.c_str()));
}
for (size_t i = 0; i < keys.size(); ++i) {
halKeys.addKey(String8(keys[i].c_str()));
}
std::unique_ptr<AudioParameter> halValues = getParams(halKeys);
Result retval =
(keys.size() == 0 || halValues->size() != 0) ? Result::OK : Result::NOT_SUPPORTED;
hidl_vec<ParameterValue> result;
result.resize(halValues->size());
String8 halKey, halValue;
for (size_t i = 0; i < halValues->size(); ++i) {
status_t status = halValues->getAt(i, halKey, halValue);
if (status != OK) {
result.resize(0);
retval = getHalStatusToResult(status);
break;
}
result[i].key = halKey.string();
result[i].value = halValue.string();
}
cb(retval, result);
}
std::unique_ptr<AudioParameter> ParametersUtil::getParams(const AudioParameter& keys) {
String8 paramsAndValues;
char* halValues = halGetParameters(keys.keysToString().string());
if (halValues != NULL) {
paramsAndValues.setTo(halValues);
free(halValues);
} else {
paramsAndValues.clear();
}
return std::unique_ptr<AudioParameter>(new AudioParameter(paramsAndValues));
}
Result ParametersUtil::setParam(const char* name, bool value) {
AudioParameter param;
param.add(String8(name), String8(value ? AudioParameter::valueOn : AudioParameter::valueOff));
return setParams(param);
}
Result ParametersUtil::setParam(const char* name, int value) {
AudioParameter param;
param.addInt(String8(name), value);
return setParams(param);
}
Result ParametersUtil::setParam(const char* name, float value) {
AudioParameter param;
param.addFloat(String8(name), value);
return setParams(param);
}
Result ParametersUtil::setParametersImpl(const hidl_vec<ParameterValue>& context,
const hidl_vec<ParameterValue>& parameters) {
AudioParameter params;
for (auto& pair : context) {
params.add(String8(pair.key.c_str()), String8(pair.value.c_str()));
}
for (size_t i = 0; i < parameters.size(); ++i) {
params.add(String8(parameters[i].key.c_str()), String8(parameters[i].value.c_str()));
}
return setParams(params);
}
Result ParametersUtil::setParam(const char* name, const DeviceAddress& address) {
AudioParameter params(String8(deviceAddressToHal(address).c_str()));
params.addInt(String8(name), int(address.device));
return setParams(params);
}
Result ParametersUtil::setParams(const AudioParameter& param) {
int halStatus = halSetParameters(param.toString().string());
switch (halStatus) {
case OK:
return Result::OK;
case -EINVAL:
return Result::INVALID_ARGUMENTS;
case -ENODATA:
return Result::INVALID_STATE;
case -ENODEV:
return Result::NOT_INITIALIZED;
// The rest of the API (*::analyseStatus) returns NOT_SUPPORTED
// when the legacy API returns -ENOSYS
// However the legacy API explicitly state that for get_paramers,
// -ENOSYS should be returned if
// "the implementation does not accept a parameter change while the
// output is active but the parameter is acceptable otherwise"
case -ENOSYS:
return Result::INVALID_STATE;
default:
return Result::INVALID_ARGUMENTS;
}
}
} // namespace implementation
} // namespace AUDIO_HAL_VERSION
} // namespace audio
} // namespace hardware
} // namespace android