/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
package android.hardware.bluetooth@1.0;
import IBluetoothHciCallbacks;
/**
* The Host Controller Interface (HCI) is the layer defined by the Bluetooth
* specification between the software that runs on the host and the Bluetooth
* controller chip. This boundary is the natural choice for a Hardware
* Abstraction Layer (HAL). Dealing only in HCI packets and events simplifies
* the stack and abstracts away power management, initialization, and other
* implementation-specific details related to the hardware.
*/
interface IBluetoothHci {
/**
* Initialize the underlying HCI interface.
*
* This method should be used to initialize any hardware interfaces
* required to communicate with the Bluetooth hardware in the
* device.
*
* The |oninitializationComplete| callback must be invoked in response
* to this function to indicate success before any other function
* (sendHciCommand, sendAclData, * sendScoData) is invoked on this
* interface.
*
* @param callback implements IBluetoothHciCallbacks which will
* receive callbacks when incoming HCI packets are received
* from the controller to be sent to the host.
*/
@entry
@callflow(next={"sendHciCommand", "sendAclData", "sendScoData", "close"})
initialize(IBluetoothHciCallbacks callback);
/**
* Send an HCI command (as specified in the Bluetooth Specification
* V4.2, Vol 2, Part 5, Section 5.4.1) to the Bluetooth controller.
* Commands must be executed in order.
*
* @param command is the HCI command to be sent
*/
@callflow(next={"sendHciCommand", "sendAclData", "sendScoData", "close"})
sendHciCommand(HciPacket command);
/**
* Send an HCI ACL data packet (as specified in the Bluetooth Specification
* V4.2, Vol 2, Part 5, Section 5.4.2) to the Bluetooth controller.
* Packets must be processed in order.
* @param data HCI data packet to be sent
*/
@callflow(next={"sendHciCommand", "sendAclData", "sendScoData", "close"})
sendAclData(HciPacket data);
/**
* Send an SCO data packet (as specified in the Bluetooth Specification
* V4.2, Vol 2, Part 5, Section 5.4.3) to the Bluetooth controller.
* Packets must be processed in order.
* @param data HCI data packet to be sent
*/
@callflow(next={"sendHciCommand", "sendAclData", "sendScoData", "close"})
sendScoData(HciPacket data);
/**
* Close the HCI interface
*/
@exit
close();
};